g_thread_create() is deprecated in GLib master, use g_thread_try_new() instead
[glsdk/gstreamer0-10.git] / libs / gst / check /
2011-12-03 Tim-Philipp Müllerg_thread_create() is deprecated in GLib master, use...
2011-06-18 Tim-Philipp MüllerBump git version after unplanned 0.10.35 release
2011-05-24 Debarshi Raycheck: add fail_unless_equals_int64
2011-04-16 Tim-Philipp Müllerlibs: gobject-introspection scanner doesn't need to...
2011-04-16 Tim-Philipp Müllerlibs: make sure gobject-introspection scanner calls...
2011-01-25 Stefan Kostchecks: add a comment to indicate that we intentionally...
2011-01-24 Tim-Philipp Müllercheck: don't leak xml file name if GST_CHECK_XML is set
2011-01-18 Tim-Philipp Müllergobject-introspection: try harder to make g-ir-scanner...
2011-01-11 Tim-Philipp Müllergobject-introspection: make g-ir-scanner try harder...
2010-12-11 Edward Herveylibs: Fix GIR build for srcdir != builddir
2010-12-07 Edward Herveylibs: Add -I$(top_srcdir)/libs to g-ir-scanner commands
2010-12-05 Edward Herveygstcheck: Don't check pad refcount too early
2010-11-21 Evan Nemersonintrospection: Include exported packages information...
2010-09-01 Tim-Philipp Müllerbuild: use new AG_GST_PKG_CONFIG_PATH m4 macro from...
2010-08-30 Edward Herveycheck: Use g_strcmp0 instead of strcmp
2010-08-05 Stefan Kostcheck: don't use c++ keywords as variable names
2010-07-16 Tim-Philipp Müllergstcheck: fix some silly list iteration code
2010-06-06 Stefan Kostcheck: use globbing for selective test invocation via...
2010-06-01 Tim-Philipp Müllercheck: log plugins available to unit tests and their...
2010-04-06 Stefan Kostbuild: fix out of sourcedir build for check
2010-04-03 Tim-Philipp Müllerlibs: point gobject-introspection scanner to .la files
2010-03-25 Tim-Philipp Müllerlibs: don't use fancy shell features when invoking...
2010-03-25 Tim-Philipp Müllerlibs: fix PKG_CONFIG_PATH used when calling gobject...
2010-03-11 Benjamin OtteFixes for -Wmissing-declarations -Wmissing-prototypes
2010-03-10 Benjamin OtteMerge branch 'work'
2010-03-10 Benjamin OtteFixes for -Wwrite-strings
2010-03-09 Sebastian Drögebuild: Make some more rules silent if requested
2010-02-18 Tim-Philipp Müllergstcheck: more debug logging for gst_check_element_push...
2010-02-15 Tim-Philipp Müllerdocs: fix gtk-doc chunk for gst_check_element_push_buff...
2010-01-10 Tim-Philipp Müllercheck: remove some cruft from header file
2010-01-05 Tim-Philipp Müllercheck: patch internal check copy some more so that...
2009-12-19 Руслан Ижбулатовcheck: patch internal check copy so it works with our...
2009-12-19 Руслан Ижбулатовcheck: update autotools and docs stuff for new check...
2009-12-17 Tim-Philipp Müllercheck: update internal libcheck to 0.9.8
2009-11-18 Priit Laescheck: fix symbol exporting when building under et_EE...
2009-10-12 Edward Herveylibs/gst/check: Make writing threadsafe. Backported...
2009-10-12 Edward Herveylibs/gst/check: Run gst-indent on libcheck.
2009-10-08 Edward Herveygst/check/consistencychecker: Check type of miniobject...
2009-09-30 Jan Schmidtlibgstcheck: Don't use character classes in sed expressions
2009-09-14 David SchleefFix out-of-tree build
2009-09-12 Sebastian Drögeintrospection: Build pkgconfig before all libraries...
2009-09-05 Sebastian Drögeintrospection: Strip Gst prefix from all types/functions
2009-09-05 Sebastian Drögeintrospection: Fix out-of-tree build
2009-09-05 Sebastian Drögeintrospection: Fix build if gir-repository is not installed
2009-09-05 Sebastian Drögecheck: Add gobject-introspection support
2009-08-10 Tim-Philipp Müllercheck: add some logging before calling gst_task_cleanup...
2009-08-08 Sebastian Drögecheck: Call gst_task_cleanup_all() in GST_END_TEST
2009-08-06 Tim-Philipp Müllercheck: add internal-check.h to BUILT_SOURCES in attempt...
2009-08-06 Tim-Philipp Müllercheck: fix symbol exporting
2009-08-06 Tim-Philipp Müllercheck: fix issues with 'make distcheck'
2009-08-06 Tim-Philipp Müllercheck: use private copy of check for libgstcheck
2009-08-06 Tim-Philipp Müllercheck: add internal copy of check-0.9.6
2009-07-28 Tim-Philipp Müllercheck: make new GstStreamConsistency structure private
2009-07-20 Edward Herveygstcheck: Add a stream consistency checking helper...
2009-04-02 Sebastian Drögegstcheck: Call gst_check_init() before creating the...
2009-03-19 Tim-Philipp Müllergstcheck: fix for check versions > 0.9.6
2009-02-04 Stefan Kostcheck: Don't assume gst_pad_get_peer returns non NULL...
2009-01-25 Thijs VermeirOnly free list of buffers once
2009-01-23 Jan SchmidtUpdate a bunch of gitignores to clean up my git status...
2008-12-10 Peter Kjellerstedtlibs/gst/check/gstcheck.h: Allow check tests to use
2008-12-09 Sebastian Drögelibs/gst/check/gstcheck.c: Revert accidentially commite...
2008-06-21 Thijs Vermeirdocs/libs/gstreamer-libs-sections.txt: Add new API...
2008-06-21 Thijs Vermeirlibs/gst/check/gstcheck.*: Also setup request pads...
2008-05-21 Wim TaymansDon't use gst_element_get_pad().
2008-04-28 Michael Smithlibs/gst/check/Makefile.am: Don't add an explicit link...
2008-04-10 Stefan Kostlibs/gst/check/gstcheck.c: Remove blank line between...
2008-03-24 Mark NauwelaertsSmall documentation fixes. Fixes #523978.
2008-03-22 Sebastian DrögeDefine G_PARAM_STATIC_STRINGS if it's undefined (GLib...
2008-02-29 Sebastian DrögeCorrect all relevant warnings found by the sparse seman...
2008-02-19 Jan Schmidtlibs/gst/check/gstcheck.*: Make the declaration in...
2008-02-01 Thijs VermeirAdd more functions for unit testing: gst_check_drop_buf...
2008-01-12 Jan Schmidtgst/gst.c: _gst_trace_on is already provided by gsttrac...
2007-12-20 Peter Kjellerstedtlibs/gst/check/gstcheck.h: Fix detection of the check...
2007-10-25 Jan SchmidtUse a custom export symbol regex for libgstcheck, as...
2007-10-16 Tim-Philipp Müllerlibs/gst/check/gstcheck.*: Allow runtime selection...
2007-08-13 Stefan KostAdd more missing docs.
2007-07-20 Stefan KostAdd libm check as we use in for plugins.
2007-06-14 Tim-Philipp Müllerlibs/gst/check/gstcheck.c: Intercept criticals and...
2007-06-14 Tim-Philipp MüllerUgly 'fix' for the controller unit test on the p5 bot...
2007-06-14 Tim-Philipp MüllerAPI: add fail_unless_equals_float() and assert_equals_f...
2007-01-16 Tim-Philipp Müllerlibs/gst/check/gstcheck.c: Actually write ABI structs...
2007-01-12 Tim-Philipp Müllerlibs/gst/check/: Add G_BEGIN_DECLS and G_END_DECLS...
2006-12-21 Stefan Kostlibs/gst/check/gstcheck.c: do not automatically (de...
2006-11-20 Sebastian Droegelibs/gst/check/gstcheck.h: Fix compilation and running...
2006-10-10 Wim Taymanslibs/gst/check/gstcheck.c: Activate/deactivate pads...
2006-09-28 Jan Schmidtconfigure.ac: Don't pull in gmodule-2.0.pc as a depende...
2006-08-17 Tim-Philipp MüllerMake gstcheck stuff show up in docs (still needs to...
2006-08-15 Tim-Philipp Müllerlibs/gst/check/gstcheck.h: Use const gchar * variables...
2006-08-15 Tim-Philipp Müllerlibs/gst/check/gstcheck.h: Fix ASSERT_CRITICAL and...
2006-07-21 Andy Wingolibs/gst/check/Makefile.am (libgstcheck_@GST_MAJORMINOR...
2006-07-02 Thomas Vander Stichelelibs/gst/check/gstcheck.c: if we get the wrong message...
2006-07-02 Thomas Vander Stichelelibs/gst/check/gstcheck.h: add some assert_ as alias...
2006-07-02 Thomas Vander Stichelemoap ignore
2006-07-01 Thomas Vander Sticheleconfigure.ac: set CFLAGS and friends to -O0 if gcov...
2006-07-01 Thomas Vander Stichelelibs/gst/check/gstcheck.*: create a macro and function...
2006-06-06 Thomas Vander Stichelecosmetics
2006-06-06 Thomas Vander Stichelelibs/gst/check/gstcheck.*: factor out the method from...
2006-06-02 Thomas Vander Stichelelibs/gst/check/gstcheck.c: make sure we unset caps
2006-06-02 Michael Smithlibs/gst/check/gstcheck.*: Add a cond/mutex to the...
2006-05-22 Thomas Vander Sticheledebugging changes
next