]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - glsdk/gstreamer0-10.git/history - plugins/elements/gstelements.c
DEBIAN: Debianization
[glsdk/gstreamer0-10.git] / plugins / elements / gstelements.c
2011-03-29 Sebastian Drögefunnel: Integrate into the build system and rename...
2010-12-31 Tim-Philipp Müllercoreelements: move input-selector and output-selector...
2010-12-31 Tim-Philipp Müllerelements: add new valve element to build
2010-02-19 Sebastian Drögecorelements: Combine redundant code
2010-02-19 Andoni Morales Ala... Fix compilation of fdsink and fdsrc with MSVC
2009-10-29 Sebastian Drögequeue2: Integrate into coreplugins
2007-05-22 Tim-Philipp Müllerplugins/: Use #ifdef for HAVE_XYZ for consistency.
2007-05-06 Stefan Kostdocs/: Correct fixxrefs options.
2006-11-28 Edward Herveylibs/gst/base/: New GstDataQueue object for threadsafe...
2006-07-26 Jan Schmidtgst/gststructure.*: Add API for setting values into...
2006-05-26 Jan Schmidtplugins/elements/: Add a use-mmap property to enable...
2006-01-30 Philippe Rouquierplugins/elements/:
2005-12-01 Thomas Vander Sticheledocument core plugins in a separate document just like...
2005-12-01 Thomas Vander Sticheleplugins/elements/: more anal cleanup
2005-11-29 Thomas Vander Stichelemove queue from core to the elements plugin ç
2005-10-16 Thomas Vander Sticheleconfigure.ac: use the gettext macro
2005-10-15 Thomas Vander Sticheleconfigure.ac: correctly make conditionals
2005-10-15 Thomas Vander Sticheleconfigure.ac: check for some headers
2005-10-13 Thomas Vander Sticheleadd correct header for WIN32
2005-10-10 Sebastien Moutteupdates for the win32 build (patch from Sebastien Moutte)
2005-10-07 Thomas Vander Stichelefdsrc does not build currently on win32 due to socketpair
2005-09-09 Jan Schmidtcheck/elements/identity.c: Make the error a little...
2005-09-03 Thomas Vander Sticheleadd a source plugin description field, to represent...
2005-07-16 Philippe KalafMoved fdsrc to gst-plugins.
2005-07-16 Philippe Kalafgst/elements/gstfdsrc.c gst/elements/gstfdsrc.h gst...
2005-07-14 Thomas Vander Stichelemore autistic cleanliness in functions/names/defines
2005-05-15 David Schleefgst/elements/gstelements.c: Don't include headers that...
2005-05-05 Wim Taymansgst/: Added object to help in making collect pad based...
2005-05-04 Andy WingoGCC 4 fixen.
2005-04-24 David Schleefgst/gstpad.c: Remove handling of filtered caps. Fix...
2005-04-12 Wim TaymansAdded typefind helper.
2005-03-21 Wim TaymansNext big merge.
2004-06-26 Wim Taymansgst/elements/: Removed multifdsink, moved it to plugins.
2004-06-24 Wim Taymansgst/elements/: Added an element that writes to multiple...
2004-04-29 David SchleefDisable parsing of a lot of files that aren't part...
2004-04-20 David Schleefcommon/as-libtool.mak: Fine-tune DLL building.
2004-04-14 David Schleefconfigure.ac: Disable various code when compiling for...
2004-03-15 Thomas Vander Sticheledon't mix tabs and spaces
2004-03-13 Thomas Vander Stichelegst-indent run on core
2004-02-11 Thomas Vander Stichelerename multidisksrc to multifilesrc
2004-01-20 Thomas Vander Stichelefix rename
2003-12-22 Benjamin Ottegst/elements/gstelements.c: Set ranks of elements to...
2003-12-04 Andy Wingoremove copyright field from plugin structs
2003-10-31 Benjamin Otteupdate plugin initialization restructuring (see email...
2003-10-28 Benjamin Ottemerge TYPEFIND branch. Major changes:
2003-06-29 Benjamin OtteGST_DEBUG reorganization containing loads of stuff:
2003-02-23 Wim Taymans- Added generic shaper element that keeps two streams...
2002-04-28 Thomas Vander Stichelerename operation
2002-04-11 Andy Wingocommit to make gstreamer follow the gtk function/macro...
2002-01-29 Benjamin Otteinclusion of GstMD5Sink
2001-12-24 Andy Wingoremoved httpsrc from core
2001-12-17 Christian Schallermore of the popular // fixes
2001-12-14 Andy Wingovestigial gstdisksrc removal
2001-10-24 David I. Lehnbasic statistics element
2001-10-21 Wim TaymansSome compiler warning removed.
2001-10-06 Steve Bakergstsinesrc is being moved into plugins/synthesis/sinesrc
2001-09-13 Joshua N. Pritikinadd assertion
2001-08-29 Erik Walthinsenoops, another gtkism, changed GtkType to GType for...
2001-08-22 Erik Walthinsenadded new gstfilesrc to replace disksrc eventually
2001-08-21 Wim TaymansLots of modifications to the plugin system.
2001-07-11 Wim TaymansAdded request pads to fakesink.
2001-07-11 Wim TaymansAdded DEBUG_FUNCPTR to most plugins.
2001-07-11 Wim TaymansSome code cleanups.
2001-06-25 Erik WalthinsenMerged from GOBJECT1 to HEAD at 200106241
2001-04-28 Steve Bakeradd factory init for sinesrc
2001-04-22 Richard BoultonMerged from BRANCH-PLUGINVER1
2001-04-20 Thomas Vander Sticheleupdate to take new gstdisksink element into account
2001-03-24 Wim TaymansModified a lot of plugins to use the caps system.
2001-03-07 Wim TaymansMerged the AUTOPLUG2 branch
2001-02-21 David I. LehnRemove alias for asyncdisksrc backwards compatability.
2001-02-04 Erik Walthinsenmoved asyncdisksrc to disksrc, no point in having a...
2001-01-19 Wim TaymansMoved queue and typefind elements to the core since...
2001-01-18 Wim TaymansAdded mthodes to request an element to create pads...
2001-01-01 Erik WalthinsenCleaned up INFO system some more, added API to select...
2000-12-30 Wim TaymansAdded some INFO in gstelements
2000-12-29 Erik WalthinsenUpdated copyright notices.
2000-12-29 Erik WalthinsenReparented everything to GstElement, removing GstSrc...
2000-12-15 Wim TaymansHeader cleanup: try to include as little as possible...
2000-11-25 Wim TaymansCode Cleanups
2000-11-25 Erik WalthinsenAdded code to force the gsttypes plugin to load before...
2000-09-09 Wim TaymansChanges to gstreamer-config to include gtk+ libs manual...
2000-08-21 Wim TaymansA first (rude) attempt at autoplug.
2000-07-17 Erik WalthinsenMegapatch, changes which states are available, how...
2000-06-25 Wim TaymansSwitched Cr and Cb in YUV2RGB fixed the avi parser...
2000-05-28 Wim TaymansRewrote the mpeg1 system stream parser.
2000-02-01 Richard BoultonTidy up of configure script.
2000-01-30 Erik Walthinseninitial checkin