]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - glsdk/gstreamer0-10.git/history - plugins/elements/gstfdsink.c
gststructure: clarify _get docs about the returned reference
[glsdk/gstreamer0-10.git] / plugins / elements / gstfdsink.c
2010-12-31 Zhang Wanminggstfdsink: fix typo
2010-10-13 Edward Herveyfdsink: cleanup get_property/set_property
2010-06-16 Wim Taymansfdsink: make sync property work correctly
2010-03-10 Benjamin OtteMerge branch 'work'
2010-03-10 Benjamin OtteFixes for -Wwrite-strings
2010-02-19 Andoni Morales Ala... Fix compilation of fdsink and fdsrc with MSVC
2009-06-19 Tim-Philipp Müllerfdsink: clean up some more error and debug messages
2009-06-18 Tim-Philipp Müllerfdsink: fix error message
2009-06-18 Benjamin Gaignardfdsink: make fdsink seekable
2009-03-20 LRNwin32: fix seeking in files >4GB
2008-12-20 Sebastian DrögeAPI: Add URI query type. This is useful to query the...
2008-06-20 Stefan Kostplugins/elements/: Remove short_description. Add basic...
2008-03-24 Wim Taymansplugins/elements/: Also retry our poll_wait when we...
2008-03-22 Sebastian DrögeDefine G_PARAM_STATIC_STRINGS if it's undefined (GLib...
2008-03-07 Ole André Vadla... Remove GstPollMode from the API, it does not make sense...
2008-02-29 Sebastian Drögeplugins/elements/: Don't reset GstPollFDs, this is...
2008-02-29 Wim Taymansgst/gstpoll.*: Added Since tags.
2008-02-29 Wim Taymansplugins/elements/: Use init macros and functions.
2008-02-28 Sebastian DrögeInitialize some uninitialized variables as spotted...
2008-02-28 Peter Kjellerstedtplugins/elements/: Port to GstPoll. See #505417.
2008-02-06 Stefan Kostgst/gstconfig.h.in: Add 'id' for example.
2008-02-05 Sebastian DrögeRevert previous changes to the behaviour of GstPadTempl...
2008-02-03 Sebastian DrögeDon't use base_init where not absolutely necessary...
2007-06-21 Stefan KostSaving relocations for GTypeInfo and GstElementDetails...
2007-03-19 Jan Schmidtlibs/gst/base/: Add ::unlock_stop to basesrc and basesi...
2006-10-09 Josep Torre Vallescommon/m4/gst-error.m4: Disable warning of statement...
2006-05-11 Stefan KostG_OBJECT_CLASS macro usage batch cleanup, fixes #337747...
2006-04-28 Stefan Kostmake GstElementDetails const
2006-04-28 Wim Taymansplugins/elements/gstfdsink.c: handle EAGAIN, EINTR...
2006-03-11 Tim-Philipp Müllerplugins/elements/: Emit RESOURCE_NO_SPACE_LEFT error...
2006-01-30 Philippe Rouquierplugins/elements/:
2006-01-04 Wim TaymansSmall updates to various docs.
2005-12-01 Thomas Vander Stichelefix typo
2005-12-01 Thomas Vander Sticheleplugins/elements/: more anal cleanup
2005-10-15 Thomas Vander Stichelewhitespace fixes
2005-09-28 Tim-Philipp Müllergst/elements/: Make element details static.
2005-07-05 Andy Wingogst/elements, testsuite: Null if we got it...
2005-03-08 Wim TaymansRemove threadsafe properties. Fix elements because...
2004-08-17 Benjamin Ottegst/: s/gst_pad_new/&_from_template/ register pad templ...
2004-05-07 David SchleefChanges to handle compilers that don't have variadic...
2004-03-15 Thomas Vander Sticheledon't mix tabs and spaces
2004-03-13 Thomas Vander Stichelegst-indent run on core
2004-01-08 Benjamin Ottegst/gstutils.h: GST_PARENT_CALL and
2003-10-31 Benjamin Otteupdate plugin initialization restructuring (see email...
2003-10-08 Andy Wingos/GstBuffer/GstData/ in the API where you can pass...
2003-06-29 Benjamin OtteGST_DEBUG reorganization containing loads of stuff:
2002-11-21 Wim TaymansSmall cleanups, more descriptive properties
2002-09-29 Andy Wingoadding ::license field to core plugins
2002-04-20 Andy Wingoa hack to work around intltool's brokenness a current...
2002-03-24 Andy Wingofilter newlines out of GST_DEBUG statements to reflect...
2002-03-18 Andy Wingos/gst_element_install_std_props/gst_element_class_insta...
2001-12-17 Christian Schallermore of the popular // fixes
2001-12-13 Wim TaymansMore Michael fixage
2001-07-11 Wim TaymansSome code cleanups.
2001-06-25 Erik WalthinsenMerged from GOBJECT1 to HEAD at 200106241
2001-01-29 Wim TaymansThis is a megapatch with the following changes:
2001-01-01 Erik WalthinsenMega update of INFO, DEBUG, and ERROR subsystems, renam...
2000-12-29 Erik WalthinsenUpdated copyright notices.
2000-12-29 Erik WalthinsenReparented everything to GstElement, removing GstSrc...
2000-12-12 Erik WalthinsenAdded LAME encoder. Wow.
2000-11-25 Wim TaymansCode Cleanups
2000-03-27 Wim TaymansDocumentation updates. All standard library objects...
2000-02-27 Wim TaymansThis is a rather large patch. Switched on -Wall compile...
2000-01-30 Erik Walthinseninitial checkin