]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - glsdk/gstreamer0-10.git/history - plugins/elements/gstfilesink.c
ignore more
[glsdk/gstreamer0-10.git] / plugins / elements / gstfilesink.c
2005-05-09 Wim TaymansRemove old query functions. Ported old code.
2005-05-06 Andy Wingogst/gstquery.h
2005-05-05 Wim Taymansgst/: Added object to help in making collect pad based...
2005-03-08 Wim TaymansRemove threadsafe properties. Fix elements because...
2005-01-24 Tim-Philipp MüllerDon't unref seek event twice in case where fflush(...
2004-11-06 Ronald S. Bultjedocs/pwg/: Typo fixes.
2004-08-17 Benjamin Ottegst/: s/gst_pad_new/&_from_template/ register pad templ...
2004-07-12 Steve LhommeHandle binary files under Windows
2004-05-07 David SchleefChanges to handle compilers that don't have variadic...
2004-04-29 Sebastien Cotegst/elements/gstfilesink.c: Patch from Sebastien Cote...
2004-03-18 Thomas Vander Sticheleupdated translation return silently when filesink not...
2004-03-15 Thomas Vander Sticheledon't mix tabs and spaces
2004-03-13 Thomas Vander Stichelegst-indent run on core
2004-02-22 Thomas Vander Stichelefix errors
2004-02-07 Ramon Garcia FernandezTrying to fix the mess that I made with the two previou...
2004-02-07 Ramon Garcia FernandezReverted changes made to fix unsigned-signed warnings...
2004-02-04 David Schleefdocs/random/ds/0.9-suggested-changes: random notes
2004-01-31 Thomas Vander Stichelesuffix errors with period.
2004-01-29 Thomas Vander SticheleGST_ELEMENT_ERROR
2004-01-19 Thomas Vander Sticheleremoving ending punctuation dots
2004-01-18 Thomas Vander Stichelechanging error signal add error codes and domains
2004-01-08 Benjamin Ottegst/gstutils.h: GST_PARENT_CALL and
2004-01-07 Ronald S. Bultjegst/elements/gstfilesink.c: Fix for if we pass NULL...
2003-11-24 Benjamin Otteimplement URI schemes
2003-10-31 Benjamin Otteupdate plugin initialization restructuring (see email...
2003-10-20 Ronald S. BultjeProperly give an error if no file was given
2003-10-08 Andy Wingos/GstBuffer/GstData/ in the API where you can pass...
2003-09-30 Andy Wingomake filesink handle events only in the chainfunction
2003-09-16 Thomas Vander Stichelereverting error patches before making a branch.
2003-09-14 Benjamin Otteimplement translatable error messages using gerror.
2003-09-13 Ronald S. BultjeImplement seekability-only-if-available
2003-07-22 Ronald S. BultjeAdd support for not incrementing bytecounter while...
2003-06-29 Benjamin OtteGST_DEBUG reorganization containing loads of stuff:
2003-06-07 Ronald S. BultjeActually, size should be a guint (because GST_BUFFER_SI...
2003-06-07 Ronald S. BultjeMake filesink fail with some grace, see #114614
2003-06-06 Ronald S. BultjeSome adjustments to allow for setting a new filename...
2003-06-01 Ronald S. BultjeI don't know how I ever got to introducing this madness...
2002-12-30 Wim Taymans- major API breakage (one of the last, I promise...)
2002-11-21 Wim TaymansSmall cleanups, more descriptive properties
2002-10-25 David SchleefConvert from sys_errlist[] to g_strerror()
2002-09-29 Andy Wingoadding ::license field to core plugins
2002-09-01 Wim TaymansDon't doe EOS in a state change function
2002-07-30 Wim TaymansUse fancy macros
2002-07-24 Wim Taymans- Implemented seekmasks, query types and formats in...
2002-07-08 Wim Taymans- Removed bufferpool code and move that to gstbuffer.c
2002-06-08 Wim TaymansA discont event is the right way to handle seeking...
2002-05-26 Wim Taymans- The clock_wait now returns the difference between...
2002-04-28 Thomas Vander Stichelerename operation