identity: unlock clock wait when appropriate
[glsdk/gstreamer0-10.git] / plugins / elements / gstidentity.c
2011-12-02 Mark Nauwelaertsidentity: unlock clock wait when appropriate
2011-09-07 Piotr Fusikdocs, gst: typo fixes
2011-01-28 Tim-Philipp Mülleridentity: print unset buffer timestamps or durations...
2010-10-07 Tim-Philipp Müllerelements: minor performance improvement when doing...
2010-10-07 Tim-Philipp Mülleridentity: use g_object_notify_by_pspec() and remove...
2010-09-09 Sebastian Drögeidentity: identity is GAP flag aware, no need to let...
2009-10-28 Tim-Philipp MüllerRemove GST_DEBUG_FUNCPTR where they're pointless
2009-10-06 Tim-Philipp Müllerdataqueue, elements: avoid unnecessary runtime type...
2009-05-31 Tim-Philipp Mülleridentity: hack around g_object_notify() bug by protecti...
2009-04-03 Edward HerveyRemove unused variables detected by LLVM's Clang static...
2009-03-06 Alessandro Decinaidentity: ignore the return value of gst_pad_event_defa...
2009-02-05 Stefan Kostcleanup: remove unused variables in _class_init() and...
2008-11-21 Stefan Kostplugins/elements/gstidentity.c: Don't warning on offset...
2008-10-31 Stefan Kostplugins/elements/gstidentity.c: Doc typo. Use return...
2008-06-20 Stefan Kostplugins/elements/: Remove short_description. Add basic...
2008-04-09 Sebastian Drögeplugins/elements/gstidentity.c: Fix imperfect timestamp...
2008-03-24 Mark Nauwelaertsplugins/elements/gstidentity.c: Identity is not always...
2008-03-22 Sebastian DrögeDefine G_PARAM_STATIC_STRINGS if it's undefined (GLib...
2008-02-05 Sebastian DrögeRevert previous changes to the behaviour of GstPadTempl...
2008-02-03 Sebastian DrögeDon't use base_init where not absolutely necessary...
2007-11-21 Laurent Glayalplugins/elements/gstidentity.*: Add property to disable...
2007-06-21 Stefan KostSaving relocations for GTypeInfo and GstElementDetails...
2007-06-08 Wim Taymansplugins/elements/gstidentity.c: Don't overflow in retim...
2007-05-06 Stefan Kostdocs/: Correct fixxrefs options.
2007-03-20 Zaheer Abbas Meraliplugins/elements/gstidentity.c (gst_identity_check_impe...
2007-03-09 Thomas Vander Sticheleplugins/elements/gstidentity.*: Separate out check...
2007-03-08 Zaheer Abbas Meraliplugins/elements/gstidentity.c: Fix check for perfect...
2007-03-08 Wim Taymanslibs/gst/base/gstbasetransform.*: Add support for dropp...
2007-03-07 Zaheer Abbas Meraliplugins/elements/gstidentity.c: Only post bus message...
2007-03-07 Zaheer Abbas Meraliplugins/elements/gstidentity.c: Rename non-perfect...
2007-03-07 Zaheer Abbas Meraliplugins/elements/gstidentity.*: Emit bus message if...
2006-12-16 Tim-Philipp Müllerplugins/elements/gstidentity.c: Print additional debug...
2006-09-29 Wim Taymanslibs/gst/net/: Stop reading commands when EOF as well.
2006-08-28 Michael Smithplugins/elements/gstidentity.c: Revert previous change...
2006-08-28 Michael Smithplugins/elements/gstidentity.c: Unset DISCONT on buffer...
2006-08-28 Wim Taymanslibs/gst/base/gstbasesrc.c: Small comment update.
2006-05-11 Stefan KostG_OBJECT_CLASS macro usage batch cleanup, fixes #337747...
2006-05-04 James AndrewarthaMake sure gstprivate.h and/or config.h are always inclu...
2006-04-28 Stefan Kostmake GstElementDetails const
2006-01-10 Edward Herveyplugins/elements/gstidentity.c: Set the buffer offset...
2006-01-04 Wim TaymansSmall updates to various docs.
2005-12-06 Thomas Vander Sticheleexpand tabs
2005-11-30 Thomas Vander Sticheleplugins/elements/gstidentity.c: make initialization...
2005-11-29 Thomas Vander Sticheledo CVS surgery and related build fixery to move element...
2005-11-29 Edward Herveygst/base/gstbasesink.c: Properly handle non GST_FORMAT_...
2005-11-29 Edward Herveygst/base/gstbasetransform.c: The event virtual method...
2005-11-21 Wim TaymansMore segment updates, replace code in plugins with...
2005-11-21 Andy Wingo*.*: Ran scripts/update-macros. Oh yes. gst/gstobject...
2005-11-15 Wim Taymansgst/base/gstbasesink.c: 0 segment values are 0 in any...
2005-10-15 Thomas Vander Stichelewhitespace fixes
2005-10-12 Wim Taymansgst/base/gstbasesink.c: No need to prerol after receivi...
2005-10-04 Wim Taymansgst/elements/: Protect last_message with lock.
2005-09-28 Tim-Philipp Müllergst/elements/: Make element details static.
2005-08-28 Andy Wingogst/gstutils.h (GST_BOILERPLATE_FULL): Prototype instan...
2005-07-22 Wim Taymansdocs/design/part-events.txt: Small update.
2005-07-16 Wim Taymansgst/base/gstbasesink.*: Store and use discont values...
2005-07-15 Andy Wingogst/elements/gstidentity.c (marshal_VOID__MINIOBJECT...
2005-07-15 Wim Taymansgst/base/gstbasetransform.*: Make passthrough work...
2005-07-01 Andy Wingotests/network-clock.scm: Commentary update.
2005-05-30 Wim Taymansgst/elements/gstidentity.c: Protect last_message proper...
2005-05-18 Ronald S. Bultjegst/elements/gstidentity.c: Workaround until signals...
2005-05-16 David Schleefcheck/Makefile.am: remove GstData checks
2005-03-31 Wim Taymansgst/: Added start/stop methods to transform base class...
2005-03-29 Wim Taymansgst/: Simplify pad activation.
2005-03-21 Wim TaymansNext big merge.
2005-03-08 Wim TaymansRemove threadsafe properties. Fix elements because...
2005-03-07 Wim TaymansFirst THREADED backport attempt, focusing on adding...
2004-11-08 Christophe Fergeaugst/elements/: Subtract size of internally stored data...
2004-11-03 Christophe Fergeaugst/elements/gstidentity.c: GstBuffer is a boxed type...
2004-10-05 Thomas Vander Sticheleconfigure.ac
2004-09-03 Wim Taymansgst/elements/: Added datarate properties to limit the...
2004-08-17 Benjamin Ottegst/: s/gst_pad_new/&_from_template/ register pad templ...
2004-06-26 Thomas Vander Stichelecheck stream
2004-06-25 Thomas Vander Sticheleprint offset_end
2004-06-18 Thomas Vander Sticheleadd sync to identity
2004-06-09 Wim Taymansgst/elements/: Print more buffer info in fakesink.
2004-05-13 Thomas Vander Stichelegst/elements/gstidentity.c: add duration debug
2004-04-20 Thomas Vander Stichelemaking _set_property warn on unknown properties use...
2004-03-21 Benjamin Ottegst/: clean up used memory in this elements correctly...
2004-03-15 Thomas Vander Sticheledon't mix tabs and spaces
2004-03-13 Thomas Vander Stichelegst-indent run on core
2004-02-03 Benjamin Ottegst/: get rid of gstmarshal.h dependency. It's not...
2004-01-31 Thomas Vander Stichelesuffix errors with period.
2004-01-30 Benjamin Otteparts of the patch submitted in bug #113913
2004-01-29 Thomas Vander SticheleGST_ELEMENT_ERROR
2004-01-18 Thomas Vander Stichelechanging error signal add error codes and domains
2004-01-08 Benjamin Ottegst/gstutils.h: GST_PARENT_CALL and
2004-01-01 David SchleefNegotiation fixes
2003-12-22 David SchleefMerge CAPS branch
2003-11-13 David SchleefChange G_TYPE_POINTER to the appropriate type in g_sign...
2003-10-31 Benjamin Otteupdate plugin initialization restructuring (see email...
2003-10-08 Andy Wingos/GstBuffer/GstData/ in the API where you can pass...
2003-09-16 Thomas Vander Stichelereverting error patches before making a branch.
2003-09-14 Benjamin Otteimplement translatable error messages using gerror.
2003-06-29 Benjamin OtteGST_DEBUG reorganization containing loads of stuff:
2003-04-17 Wim Taymans- Added a property to perform caps negotiation in the...
2003-02-01 David SchleefConvert %lld and %llu in printf formats to G_G[U]INT64_...
2003-01-09 David I. Lehnmore connect -> link updates
2003-01-09 Thomas Vander Stichelecode cleanups and further deprecation fixes
2003-01-09 Thomas Vander Stichelefirst pass of connect->link gst-plugins and other stuff...
next