]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - glsdk/gstreamer0-10.git/history - plugins/elements/gsttee.c
DEBIAN: Debianization
[glsdk/gstreamer0-10.git] / plugins / elements / gsttee.c
2011-12-04 Tim-Philipp MüllerWork around deprecated thread API in glib master
2011-09-07 Piotr Fusikdocs, gst: typo fixes
2011-04-13 Ole André Vadla... elements: Fix pad callbacks so they handle when parent...
2010-10-07 Tim-Philipp Müllerelements: minor performance improvement when doing...
2010-10-07 Tim-Philipp Müllertee: use g_object_notify_by_pspec() if possible
2010-08-16 Stefan Kostplugins: add example launch lines and more explanation...
2010-01-11 Håvard Grafftee: make release_pad threadsafe
2009-12-22 Wim Taymanstee: small cleanups, use some G_LIKELY
2009-12-22 Olivier Crêtetee: Don't crash if there is no source pad
2009-12-09 Havard Grafftee: release pads in dispose
2009-12-07 Edward Herveytee: avoid expensive typechecks, and avoid getting...
2009-12-03 Stefan Kosttee: add special case for only one pad conected
2009-12-03 Stefan Kosttee: only message once per received buffer
2009-12-03 Stefan Kosttee: remove unused offset member
2009-12-03 Stefan Kosttee: only notify alloc-pad property if changed.
2009-10-28 Tim-Philipp MüllerRemove GST_DEBUG_FUNCPTR where they're pointless
2009-10-21 Wim Taymanstee: implement custom acceptcaps function
2009-06-19 Wim Taymanstee: add buffer-list support
2009-04-09 Olivier Cretetee: add property to control the alloc pad
2008-12-08 Wim Taymansplugins/elements/gsttee.c: Check for changed pads-list...
2008-10-14 Sebastian Drögeplugins/elements/gsttee.c: Fix flow aggregation of...
2008-08-15 Ole André Vadla... plugins/elements/gsttee.*: Protect pad_alloc with a...
2008-08-07 Stefan Kostplugins/elements/gsttee.c: Unlock, instead of locking...
2008-07-29 Stefan Kostplugins/elements/gsttee.*: Reverting as not everything...
2008-07-29 Stefan Kostplugins/elements/gsttee.*: Relay tag events in tee...
2008-06-20 Stefan Kostplugins/elements/: Remove short_description. Add basic...
2008-03-22 Sebastian DrögeDefine G_PARAM_STATIC_STRINGS if it's undefined (GLib...
2008-02-29 Sebastian DrögeCorrect all relevant warnings found by the sparse seman...
2008-02-05 Sebastian DrögeRevert previous changes to the behaviour of GstPadTempl...
2008-02-03 Sebastian DrögeDon't use base_init where not absolutely necessary...
2007-07-03 Wim Taymansplugins/elements/gsttee.c: Be a lot smarter when decidi...
2007-06-21 Stefan KostSaving relocations for GTypeInfo and GstElementDetails...
2007-02-09 Andy Wingotests/check/pipelines/simple-launch-lines.c (test_tee...
2006-10-11 Wim Taymansdocs/plugins/: Update element args.
2006-05-11 Stefan KostG_OBJECT_CLASS macro usage batch cleanup, fixes #337747...
2006-04-28 Stefan Kostmake GstElementDetails const
2006-01-27 Jan Schmidtplugins/elements/gsttee.c: Always prefer an actual...
2006-01-26 Julien Moutteplugins/elements/gsttee.c: Apply patch from #328715...
2006-01-04 Wim TaymansSmall updates to various docs.
2005-11-21 Andy Wingo*.*: Ran scripts/update-macros. Oh yes. gst/gstobject...
2005-11-16 Thomas Vander Stichelegst/gstpad.*: add gst_pad_new_from_static_template...
2005-11-16 Thomas Vander Stichelefix pad tempalte leak in tee
2005-10-15 Thomas Vander Stichelewhitespace fixes
2005-10-04 Wim Taymansgst/elements/: Protect last_message with lock.
2005-09-30 Edward Herveygst/elements/gsttee.c: Let's not iterate pads we're...
2005-09-28 Tim-Philipp Müllergst/elements/: Make element details static.
2005-09-27 Wim Taymansgst/: Leak fixes, the fold functions need to unref...
2005-08-28 Andy Wingogst/gstutils.h (GST_BOILERPLATE_FULL): Prototype instan...
2005-06-28 Wim Taymansgst/: The deprecated pad loop function is removed now.
2005-06-27 Andy Wingogst/base/gsttypefindhelper.c (gst_type_find_helper...
2005-06-25 Wim Taymansgst/elements/gsttee.c: Core takes STREAM_LOCK for us...
2005-05-25 Wim Taymansgst/: Implement gst_pad_pause/start/stop_task(), take...
2005-05-05 Andy Wingocruft removal
2005-05-04 Andy WingoGCC 4 fixen.
2005-03-21 Wim TaymansNext big merge.
2005-03-08 Wim TaymansRemove threadsafe properties. Fix elements because...
2005-03-07 Wim TaymansFirst THREADED backport attempt, focusing on adding...
2005-01-17 Ronald S. Bultjegst/elements/gsttee.c: I think this is actually moer...
2005-01-14 Ronald S. Bultjegst/elements/gsttee.c: Fix negotiation.
2004-08-17 Benjamin Ottegst/: s/gst_pad_new/&_from_template/ register pad templ...
2004-05-28 Stéphane Loeuillet- removing some trailing commas in enums to please...
2004-03-21 Benjamin Ottegst/: clean up used memory in this elements correctly...
2004-03-15 Thomas Vander Sticheledon't mix tabs and spaces
2004-03-13 Thomas Vander Stichelegst-indent run on core
2004-01-25 Benjamin Ottegst/elements/gstbufferstore.c: fix bug where buffer...
2004-01-11 Benjamin Ottegst/elements/gstbufferstore.c: initialize debugging...
2004-01-08 Benjamin Ottegst/gstutils.h: GST_PARENT_CALL and
2004-01-04 David Schleefgst/elements/gsttee.c: Remove usage of gst_pad_proxy_fi...
2003-12-31 David SchleefNegotiation fixes
2003-12-23 David Schleefgst/elements/: Use gst_pad_proxy_getcaps().
2003-12-22 David SchleefMerge CAPS branch
2003-12-13 Benjamin Otteremoved GST_*_CAST. Disabling of type checking is done...
2003-11-03 David SchleefAdd G_DISABLE_DEPRECATED and fix deprecated code
2003-10-31 Benjamin Otteupdate plugin initialization restructuring (see email...
2003-10-08 Andy Wingos/GstBuffer/GstData/ in the API where you can pass...
2003-08-19 David Schleefconvert pad templates to GST_CAPS_ANY
2003-06-29 Benjamin OtteGST_DEBUG reorganization containing loads of stuff:
2003-05-30 Wim Taymans- the result from the getcaps function should be sunken...
2003-05-19 David SchleefFix caps negotiation problems.
2003-03-02 Wim TaymansBetter capsnego
2003-02-01 David SchleefConvert %lld and %llu in printf formats to G_G[U]INT64_...
2003-01-09 David I. Lehnmore connect -> link updates
2003-01-09 Thomas Vander Stichelecode cleanups and further deprecation fixes
2003-01-09 Thomas Vander Stichelefirst pass of connect->link gst-plugins and other stuff...
2002-09-29 Andy Wingoadding ::license field to core plugins
2002-09-12 Wim Taymans- Make the return GList of gst_element_get_pad_list...
2002-09-10 Ronald S. BultjeThis changes an important part of the plugin API, gst_p...
2002-07-24 Wim Taymans- Implemented seekmasks, query types and formats in...
2002-05-31 Wim TaymansRemove crappy event code from tee
2002-04-20 Andy Wingoa hack to work around intltool's brokenness a current...
2002-04-11 Andy Wingocommit to make gstreamer follow the gtk function/macro...
2002-03-30 Wim Taymans- Remove the propsprivate header file
2002-02-24 Benjamin Ottefixes:
2002-02-12 Thomas Vander Sticheleupdating tee to use properties
2002-02-05 Thomas Vander Stichelethis fix makes sure that we actually request a pad...
2002-02-04 Thomas Vander Stichelesmall compile fix
2002-02-02 Wim TaymansFix a serious leak in tee
2002-01-13 Wim TaymansLanded the new improved capsnegotiation system.
2001-12-25 Wim TaymansTee Fixes. added cothread_stop (not used) improved...
2001-12-19 Zaheer Abbas MeraliAdded capsnego to the Tee Element
next