]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - glsdk/gstreamer0-10.git/history - plugins/elements/gsttypefindelement.c
gststructure: clarify _get docs about the returned reference
[glsdk/gstreamer0-10.git] / plugins / elements / gsttypefindelement.c
2011-08-26 Josep Torratypefinder: use GST_TYPE_FIND_NONE instead of 0
2011-01-28 Stefan Kosttypefind: don't take object lock for reading the found...
2011-01-25 Tim-Philipp Müllerdocs: flesh out typefindelement docs some more
2011-01-25 Stefan Kosttypefind: code and comment cleanups
2011-01-25 Stefan Kosttypefind: canonicalize signal name
2011-01-25 Stefan Kostdocs: mention have-type signal in the docs.
2010-08-02 Stefan Kosttypefind: add comment and more logging
2010-06-18 Tim-Philipp Müllertypefind: make sure buffers' metadata is writable befor...
2010-03-17 Edward Herveytypefind: deactivate pad if we can't get length or...
2010-02-13 Edward Herveytypefind: Reset the working mode when going to READY...
2010-02-12 Thiago Santostypefind: Avoid messing pads activation
2010-02-12 Sebastian Drögetypefindelement: Protect internal fields from concurren...
2010-01-22 Tim-Philipp Müllertypefind: don't leak uri string
2010-01-20 Tim-Philipp Müllergst_private.h: make sure gst_private.h is included...
2010-01-12 Wim Taymanstypefindelement: use new typefind function
2009-10-28 Tim-Philipp MüllerRemove GST_DEBUG_FUNCPTR where they're pointless
2009-07-02 Tim-Philipp Müllertypefindelement: log probability in debug message
2009-05-12 Arnout Vandecappelletypefind: don't leak the force-caps property
2009-01-22 Wim TaymansMerge branch 'master' of ssh://git.freedesktop.org...
2009-01-22 Wim TaymansMerge branch 'master' of ssh://git.freedesktop.org...
2009-01-21 Wim TaymansIf no type was found using the typefind functions,...
2008-10-31 Stefan Kostplugins/elements/gstidentity.c: Doc typo. Use return...
2008-06-20 Stefan Kostplugins/elements/: Remove short_description. Add basic...
2008-05-27 Wim Taymansplugins/elements/gsttypefindelement.c: Use faster and...
2008-05-13 Sebastian Drögeplugins/elements/gsttypefindelement.c: Clean up on...
2008-05-13 Sebastian Drögeplugins/elements/gsttypefindelement.c: Forward FLUSH_ST...
2008-04-02 Wim Taymansplugins/elements/gsttypefindelement.*: Cleanup properties.
2008-03-22 Sebastian DrögeDefine G_PARAM_STATIC_STRINGS if it's undefined (GLib...
2008-02-29 Sebastian DrögeCorrect all relevant warnings found by the sparse seman...
2008-02-05 Sebastian DrögeRevert previous changes to the behaviour of GstPadTempl...
2008-02-03 Sebastian DrögeDon't use base_init where not absolutely necessary...
2007-10-29 Tim-Philipp Müllerplugins/elements/gsttypefindelement.c: Post special...
2007-10-08 Wim Taymansplugins/elements/gsttypefindelement.c: Move detecting...
2007-06-21 Stefan KostSaving relocations for GTypeInfo and GstElementDetails...
2007-01-30 Tim-Philipp Müllerplugins/elements/gsttypefindelement.c: Don't leak found...
2006-04-28 Stefan Kostplugins/elements/gsttypefindelement.c: reverted wrong...
2006-04-28 Stefan Kostmake GstElementDetails const
2006-04-28 Michael Smithplugins/elements/gsttypefindelement.c: If we get EOS...
2006-04-06 Tim-Philipp Müllergst/gstinfo.c: Add some newlines.
2006-04-04 Tim-Philipp Müllerplugins/elements/gsttypefindelement.c: More debug info...
2006-03-31 Michael Smithplugins/elements/gsttypefindelement.c: Do not typefind...
2006-03-29 Tim-Philipp Müllerplugins/elements/gsttypefindelement.*: When typefinding...
2006-03-14 Tim-Philipp Müllergst/gstpipeline.c: Add 'Since: 0.10.5' to gtk-doc blurb...
2006-03-03 Tim-Philipp Müllerplugins/elements/gsttypefindelement.*: Use gst_type_fin...
2006-03-03 Tim-Philipp Müllerplugins/elements/gsttypefindelement.c: Deprecate "maxim...
2006-03-03 Tim-Philipp Müllerplugins/elements/gsttypefindelement.c: Use gst_type_fin...
2006-02-27 Tim-Philipp Müllerplugins/elements/gsttypefindelement.c: When we get...
2006-02-26 Tim-Philipp Müllerplugins/elements/gsttypefindelement.c: This should...
2006-02-26 Tim-Philipp Müllerplugins/elements/gsttypefindelement.c: Use gst_pad_chec...
2006-02-15 Tim-Philipp Müllerplugins/elements/gsttypefindelement.c: We can do peeks...
2006-02-14 Tim-Philipp Müllerplugins/elements/gsttypefindelement.c: When typefinding...
2006-02-03 Tim-Philipp Müllerplugins/elements/gsttypefindelement.c: Post TYPE_NOT_FO...
2006-01-18 Tim-Philipp Müllerplugins/elements/gsttypefindelement.c: 'have-type'...
2006-01-04 Wim TaymansSmall updates to various docs.
2005-12-14 Jan Schmidtgst/gstpad.c: Don't allow activation of a srcpad in...
2005-12-12 Michael Smithgst/gsttypefindfactory.c: Don't unref factories after...
2005-12-12 Tim-Philipp Müllerplugins/elements/gsttypefindelement.c: Catch the specia...
2005-12-12 Michael Smithplugins/elements/gsttypefindelement.c: Now that we...
2005-12-09 Michael Smithplugins/elements/gsttypefindelement.c: Fix leaking...
2005-12-06 Thomas Vander Sticheleexpand tabs
2005-11-16 Wim Taymanscheck/Makefile.am: Enable valgrind check that should...
2005-11-15 Thomas Vander SticheleRevert all these unrefs, they don't even pass make...
2005-11-15 Johan DahlinAnd gst_object_unref here too
2005-11-15 Johan Dahlingst/: Free pad templates, fixes a couple of leaks.
2005-11-09 Tim-Philipp Müllergst/: Use GST_DEBUG_FUNCPTR() more extensively.
2005-11-03 Tim-Philipp Müllerdocs/manual/advanced-position.xml: Update seek example...
2005-11-02 Johan Dahlingst/elements/gsttypefindelement.c (gst_type_find_elemen...
2005-10-19 Wim Taymansgst/: API change fix.
2005-10-15 Thomas Vander Stichelewhitespace fixes
2005-10-13 Thomas Vander Stichelegst/elements/: fix some signedness
2005-10-12 Wim TaymansUse GstClockTime in _get_state() instead of GTimeVal.
2005-09-28 Tim-Philipp Müllergst/elements/: Make element details static.
2005-09-16 David Schleefcheck/gst/gstplugin.c: More testing
2005-09-07 Stefan Kostgst/: splitted gsttypefind into gsttypefind, gsttypefin...
2005-09-02 Andy Wingogst/gstelement.h (GstState): Renamed from GstElementSta...
2005-08-28 Andy Wingogst/gstutils.h (GST_BOILERPLATE_FULL): Prototype instan...
2005-08-01 Tim-Philipp Müllergst/elements/gsttypefindelement.*: Set caps on all...
2005-08-01 Tim-Philipp Müllergst/elements/gsttypefindelement.*: Set caps on first...
2005-06-28 Andy Wingo*.c: Don't cast to GST_OBJECT when reffing or unreffing...
2005-06-27 Andy Wingogst/base/gsttypefindhelper.c (gst_type_find_helper...
2005-06-23 Jan Schmidtgst/elements/gsttypefindelement.c: Don't restart typefi...
2005-06-02 Andy Wingogst/elements/gsttypefindelement.c (do_pull_typefind...
2005-05-25 Ronald S. Bultjegst/base/gstbasesrc.c: Don't go in pull mode for non...
2005-05-16 David Schleefcheck/Makefile.am: remove GstData checks
2005-05-09 Ronald S. Bultjegst/: Handle negative offsets better. Fixes decodebin.
2005-05-09 Wim TaymansRemove old query functions. Ported old code.
2005-05-05 Andy Wingocruft removal
2005-05-04 Andy WingoGCC 4 fixen.
2005-04-20 Wim Taymansgst/: Make gst_caps_replace() work like other _replace...
2005-04-12 Wim TaymansAdded typefind helper.
2005-03-07 Wim TaymansFirst THREADED backport attempt, focusing on adding...
2005-01-28 Ronald S. Bultjegst/elements/gsttypefindelement.c: Fix buffer pushing...
2004-11-08 Christophe Fergeaugst/elements/: Subtract size of internally stored data...
2004-10-08 Wim Taymansgst/elements/gsttypefindelement.c: Handle EOS events...
2004-10-06 Wim Taymansgst/elements/gsttypefindelement.c: Push the buffer...
2004-09-26 Thomas Vander Stichelefix typefind discont handling, #153657
2004-08-12 Benjamin Ottegst/elements/gstfilesrc.c: work with non-regular files...
2004-07-25 Benjamin Ottegst/autoplug/gstspideridentity.c: don't delay links...
2004-05-28 Stéphane Loeuillet- removing some trailing commas in enums to please...
2004-05-11 Benjamin Ottegst/elements/gstfilesrc.c: compute mapsize correctly
next