2003-09-11 |
Thomas Vander Stichele | ignore these test code |
tree | commitdiff |
2003-08-07 |
Andy Wingo | cache return values of _gst_debug_nameof_funcptr |
tree | commitdiff |
2003-08-02 |
David Schleef | Add another test |
tree | commitdiff |
2003-07-05 |
Christian Schaller | SPEC and build fixes, should be possible to make tarbal... |
tree | commitdiff |
2003-06-29 |
Benjamin Otte | GST_DEBUG reorganization containing loads of stuff: |
tree | commitdiff |
2003-06-13 |
Wim Taymans | - some more checks |
tree | commitdiff |
2003-06-13 |
Wim Taymans | - Added testcase for fixed flag on caps/props |
tree | commitdiff |
2003-05-19 |
Benjamin Otte | spaling eroah |
tree | commitdiff |
2003-05-19 |
Benjamin Otte | check if required elements are installed |
tree | commitdiff |
2003-05-18 |
Thomas Vander Stichele | applying http://bugzilla.gnome.org/show_bug.cgi?id... |
tree | commitdiff |
2003-05-17 |
Benjamin Otte | added tests for gst_caps_{to,from}_string |
tree | commitdiff |
2003-05-09 |
Benjamin Otte | make test fail when it fails (d'oh) |
tree | commitdiff |
2003-04-18 |
David Schleef | Add caps list test that shows incorrect behavior |
tree | commitdiff |
2003-04-17 |
Benjamin Otte | one more test |
tree | commitdiff |
2003-04-16 |
Benjamin Otte | bugfixing in pipeline parsing. Fixed the 2 pipelines... |
tree | commitdiff |
2003-04-16 |
Benjamin Otte | add a breaking testcase |
tree | commitdiff |
2003-04-15 |
Benjamin Otte | destroyed gst_*_destroy in the examples - use gst_objec... |
tree | commitdiff |
2003-04-10 |
Benjamin Otte | added tests for parsing stuff |
tree | commitdiff |
2003-03-25 |
Wim Taymans | - Added dir to hold state change related testsuites |
tree | commitdiff |
2003-03-10 |
Wim Taymans | Added scheduler refcount test |
tree | commitdiff |
2003-02-25 |
Wim Taymans | more .cvsignore |
tree | commitdiff |
2003-02-25 |
Wim Taymans | I'm too lazy to comment this |
tree | commitdiff |
2003-02-25 |
Wim Taymans | Yes, I'm annoyed |
tree | commitdiff |
2003-01-25 |
Wim Taymans | Fixed tee test |
tree | commitdiff |
2003-01-21 |
Thomas Vander Stichele | fix |
tree | commitdiff |
2003-01-21 |
Thomas Vander Stichele | various test fixes :) |
tree | commitdiff |
2003-01-21 |
Thomas Vander Stichele | don't make failing tests |
tree | commitdiff |
2003-01-12 |
Wim Taymans | Add vishnu's index dumping app |
tree | commitdiff |
2003-01-10 |
David I. Lehn | connect -> link |
tree | commitdiff |
2003-01-09 |
Thomas Vander Stichele | code cleanups and further deprecation fixes |
tree | commitdiff |
2003-01-09 |
Thomas Vander Stichele | first pass of connect->link gst-plugins and other stuff... |
tree | commitdiff |
2003-01-05 |
Thomas Vander Stichele | set up thread test environment |
tree | commitdiff |
2003-01-05 |
Wim Taymans | Applied patch 13357 |
tree | commitdiff |
2003-01-03 |
David I. Lehn | use AM_CFLAGS |
tree | commitdiff |
2002-12-31 |
David I. Lehn | format properly |
tree | commitdiff |
2002-12-31 |
David I. Lehn | ignore some more cruft |
tree | commitdiff |
2002-12-31 |
Christian Schaller | fix disting |
tree | commitdiff |
2002-12-19 |
Wim Taymans | Removed old cache testsuite |
tree | commitdiff |
2002-12-13 |
Wim Taymans | Added indexers testsuite |
tree | commitdiff |
2002-12-07 |
Thomas Vander Stichele | variety is spicy |
tree | commitdiff |
2002-12-05 |
Leif Johnson | + fixing compile warnings about uninitialized variable |
tree | commitdiff |
2002-12-03 |
Wim Taymans | Check state changes before going into enless loops |
tree | commitdiff |
2002-12-03 |
David I. Lehn | use AM_CFLAGS dummy NULL init for vars to deal with... |
tree | commitdiff |
2002-12-03 |
Wim Taymans | Do some error checking to make this test succeed |
tree | commitdiff |
2002-12-03 |
Wim Taymans | Make sure the thread goes back to NULL before leaving... |
tree | commitdiff |
2002-12-02 |
Wim Taymans | Add small cache testsuite |
tree | commitdiff |
2002-11-29 |
Thomas Vander Stichele | random cleanups and paranoia checks |
tree | commitdiff |
2002-11-19 |
Wim Taymans | I suppose this is where done=FALSE should be done.. |
tree | commitdiff |
2002-11-18 |
Thomas Vander Stichele | adding tests |
tree | commitdiff |
2002-11-18 |
Thomas Vander Stichele | some more thread tests |
tree | commitdiff |
2002-11-14 |
Thomas Vander Stichele | threadc still fails |
tree | commitdiff |
2002-11-14 |
Thomas Vander Stichele | another thread test, this still fails |
tree | commitdiff |
2002-11-14 |
Thomas Vander Stichele | adding back threads tests |
tree | commitdiff |
2002-11-13 |
Thomas Vander Stichele | cleanups in code fix tests to run and complete if they... |
tree | commitdiff |
2002-11-02 |
Wim Taymans | Added clock test program |
tree | commitdiff |
2002-11-02 |
David I. Lehn | use AM_CFLAGS instead of CFLAGS |
tree | commitdiff |
2002-10-29 |
Thomas Vander Stichele | mainloop test and some caps fixes that had to go in |
tree | commitdiff |
2002-09-12 |
Thomas Vander Stichele | new thread test, not yet active |
tree | commitdiff |
2002-09-12 |
Thomas Vander Stichele | converting this to separate binaries so they can be... |
tree | commitdiff |
2002-09-10 |
Ronald S. Bultje | This changes an important part of the plugin API, gst_p... |
tree | commitdiff |
2002-08-28 |
Thomas Vander Stichele | adding a property test |
tree | commitdiff |
2002-07-01 |
Thomas Vander Stichele | for better or worse, make distcheck now passes again |
tree | commitdiff |
2002-07-01 |
Thomas Vander Stichele | fake fails on a make distcheck |
tree | commitdiff |
2002-07-01 |
Thomas Vander Stichele | dist fixes |
tree | commitdiff |
2002-07-01 |
Thomas Vander Stichele | fixing tests |
tree | commitdiff |
2002-07-01 |
Thomas Vander Stichele | identify failing tests |
tree | commitdiff |
2002-05-30 |
Thomas Vander Stichele | big mistake |
tree | commitdiff |
2002-05-25 |
Andy Wingo | re-enable thread test, although it does not work but... |
tree | commitdiff |
2002-05-11 |
Andy Wingo | make gst-inspect-gui call the proper gst-inspect |
tree | commitdiff |
2002-05-11 |
Andy Wingo | Return TESTS_ENVIRONMENT, necessary to make the registr... |
tree | commitdiff |
2002-05-11 |
Andy Wingo | fix refcounting tests so that they compile and run... |
tree | commitdiff |
2002-05-10 |
Wim Taymans | Fix the plugin testsuite, only registry.c doesn't work yet |
tree | commitdiff |
2002-05-10 |
Andy Wingo | added a get_perms_func to gstxmlregistry that will... |
tree | commitdiff |
2002-05-10 |
Andy Wingo | Fix automake badness |
tree | commitdiff |
2002-05-10 |
Andy Wingo | GST_PLUGIN_PATH gets split into the user registry some... |
tree | commitdiff |
2002-05-09 |
Thomas Vander Stichele | various more tests enabling |
tree | commitdiff |
2002-05-09 |
Thomas Vander Stichele | fixing up tests |
tree | commitdiff |
2002-05-09 |
Thomas Vander Stichele | refcounting tests sure would be nice to have |
tree | commitdiff |
2002-05-09 |
Thomas Vander Stichele | tried fixing, failed spectacularly |
tree | commitdiff |
2002-05-09 |
Thomas Vander Stichele | why does this test fail ? |
tree | commitdiff |
2002-05-09 |
Thomas Vander Stichele | allowing failing tests to be built |
tree | commitdiff |
2002-05-08 |
Wim Taymans | Totally rewritten registry handling. |
tree | commitdiff |
2002-05-07 |
Andy Wingo | hopefully fix distcheck issues |
tree | commitdiff |
2002-05-05 |
Andy Wingo | Fix the tests so that builds that are not --enable... |
tree | commitdiff |
2002-04-23 |
Thomas Vander Stichele | adding clock example |
tree | commitdiff |
2002-04-21 |
Thomas Vander Stichele | added name test |
tree | commitdiff |
2002-04-14 |
Steve Baker | update for changed dparams api |
tree | commitdiff |
2002-04-12 |
Thomas Vander Stichele | check fix |
tree | commitdiff |
2002-04-11 |
Andy Wingo | commit to make gstreamer follow the gtk function/macro... |
tree | commitdiff |
2002-04-11 |
Thomas Vander Stichele | more werror fixes |
tree | commitdiff |
2002-04-11 |
Thomas Vander Stichele | removing unused vars |
tree | commitdiff |
2002-03-19 |
Andy Wingo | removal of //-style comments don't link plugins to... |
tree | commitdiff |
2002-03-04 |
Steve Baker | reflect new dparams api |
tree | commitdiff |
2002-02-22 |
Thomas Vander Stichele | uncomment it in the DIRS to avoid errors |
tree | commitdiff |
2002-02-22 |
Thomas Vander Stichele | test program doesn't leave iterate atm, commenting it |
tree | commitdiff |
2002-02-22 |
Thomas Vander Stichele | right include |
tree | commitdiff |
2002-02-22 |
Thomas Vander Stichele | add to DIST_SUBDIRS |
tree | commitdiff |
2002-02-21 |
Steve Baker | generate the makefile for dparams testing |
tree | commitdiff |
2002-02-12 |
Thomas Vander Stichele | use properties |
tree | commitdiff |
2002-02-12 |
Thomas Vander Stichele | fixing up tests to work with property callbacks |
tree | commitdiff |
next |