]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - glsdk/gstreamer0-10.git/history - tests
test commit
[glsdk/gstreamer0-10.git] / tests /
2007-08-24 Jan Schmidttests/check/gst/gstbin.c: Fix leaks in the new unit...
2007-08-16 Wim Taymansgst/gstbin.c: Improve debugging.
2007-08-16 Wim Taymansgst/gstbin.c: Fix annoying bug in the sorted iterator...
2007-08-14 Wim Taymansgst/gstbin.c: Always change the state of a NO_PREROLL...
2007-08-03 Sebastian Drögelibs/gst/controller/: API: Add GstLFOControlSource...
2007-07-16 Jan Schmidttests/check/elements/.cvsignore: Add file to cvsignore...
2007-07-16 Jan Schmidttests/check/elements/multiqueue.c: Use a GStaticMutex...
2007-07-16 Jan Schmidttests/check/pipelines/stress.c: Make sure we set the...
2007-07-16 Jan Schmidttests/check/elements/tee.c: Make the tee stress-test...
2007-07-08 Tim-Philipp Müllergst/gststructure.c: When deserialising foo=bar without...
2007-07-06 Sebastian Drögelibs/gst/controller/: API: Refactor GstController into...
2007-07-03 Wim Taymansplugins/elements/gsttee.c: Be a lot smarter when decidi...
2007-06-26 Jan Schmidtplugins/elements/gstmultiqueue.*: Take the multiqueue...
2007-06-19 Andy Wingotests/check/pipelines/simple-launch-lines.c
2007-06-19 Andy Wingotests/check/pipelines/simple-launch-lines.c
2007-06-18 Wim Taymansgst/gstbin.*: Immediatly commit the toplevel bin state...
2007-06-15 Wim TaymansImprove debugging.
2007-06-14 Tim-Philipp MüllerAPI: add fail_unless_equals_float() and assert_equals_f...
2007-06-09 Sebastian Drögelibs/gst/controller/: Protect against values larger...
2007-06-07 Stefan Kosttests/examples/controller/audio-example.c: Improve...
2007-06-06 Tim-Philipp MüllerFix multiqueue leaking buffers and events when downstre...
2007-06-06 Sebastian Drögelibs/gst/controller/: Factor out the 'set' logic into...
2007-06-06 Tim-Philipp MüllerAPI: add GstParamSpecFraction, so elements can have...
2007-05-24 Wim Taymanstests/check/gst/gstbin.c: Allow refcount of 3 and 4...
2007-05-23 Wim Taymanstests/check/gst/gstsystemclock.c: Improve test_async_or...
2007-05-22 Tim-Philipp Müllerplugins/: Use #ifdef for HAVE_XYZ for consistency.
2007-05-21 Sebastian Drögelibs/gst/controller/gstcontroller.*: Clarify the docs...
2007-05-21 Jan Schmidttests/check/gst/gstbuffer.c: Disable part of the gst_bu...
2007-05-21 Sebastian Drögetests/check/gst/gstpad.c: Add unit test for the improve...
2007-05-17 Sebastian Drögelibs/gst/controller/: Add a new private GstControlPoint...
2007-05-12 Wim Taymansplugins/elements/gstqueue.*: Refactor an cleanup queue...
2007-05-11 Tim-Philipp Müllergst/gsturi.c: Don't leak plugin feature.
2007-05-09 Peter Kjellerstedtgst/: Maintain API and ABI when --disable-parse is...
2007-05-09 Tim-Philipp Müllertests/benchmarks/: Set a good example and don't leak...
2007-05-04 Tim-Philipp Müllerlibs/gst/controller/: Don't crash if someone tries...
2007-04-26 Tim-Philipp MüllerAPI: add gst_buffer_try_new_and_alloc() plus unit test...
2007-04-19 Stefan Kosttests/benchmarks/: Total licensification.
2007-04-19 Stefan Kosttests/benchmarks/: Change licence to LGPL as granted...
2007-04-13 Jan Schmidtgst/gstelement.c: Don't output the same debug statement...
2007-04-05 Wim Taymanslibs/gst/base/gstbasesink.c: Fix leak caused when refus...
2007-04-05 Wim Taymanslibs/gst/base/gstbasesink.c: Don't accept anything...
2007-03-28 Tim-Philipp Müllerplugins/elements/gstmultiqueue.c: Don't leak GCond.
2007-03-22 Wim Taymanstests/check/gst/gstsystemclock.c: Unref some more to...
2007-03-22 Wim Taymansgst/gstsystemclock.c: Fix anoying regression that survi...
2007-03-19 Wim Taymansdocs/gst/gstreamer-sections.txt: Add new element field...
2007-02-28 Wim Taymanslibs/gst/base/gstbasesink.c: Improve latency query...
2007-02-28 Thomas Vander Sticheleplug test leak
2007-02-28 Thomas Vander Sticheleactually use the env var for tests
2007-02-28 Thomas Vander Sticheletests/check/generic/states.c: Copy the current generic...
2007-02-27 Wim TaymansAPI: gst_bus_timed_pop()
2007-02-15 Wim Taymanstests/check/gst/gstevent.c: Improve debugging.
2007-02-13 Wim Taymanstests/check/gst/gstsegment.c: Fix check
2007-02-12 Wim Taymansdocs/design/draft-latency.txt: Small update.
2007-02-09 Andy Wingotests/check/pipelines/simple-launch-lines.c
2007-02-09 Andy Wingotests/check/: Add ABI checks for PPC32.
2007-02-09 Andy Wingotests/check/pipelines/simple-launch-lines.c (test_tee...
2007-02-05 Sebastian Drögetests/check/elements/filesrc.c: Add unit test for the...
2007-01-17 Tim-Philipp Müllertests/check/: Add ABI structs for HPPA (see #393796).
2007-01-15 Stefan Kosttests/check/gst/gsttask.c: Fix header comment.
2007-01-12 Tim-Philipp Müllertests/check/: Add minimal unit test for beforementioned...
2007-01-11 Tim-Philipp Müllertests/check/gst/gstpad.c: Fix 'make check' too.
2007-01-09 Tim-Philipp Müllertests/check/.cvsignore: Ignore test-registry.xml as...
2007-01-08 Tim-Philipp MüllerAPI: add gst_update_registry() (#391296).
2007-01-08 Tim-Philipp Müllergst/gstregistry.c: Plugin extension on HP-UX is .sl...
2007-01-04 Stefan Kosttests/check/Makefile.am: disable test again, as there...
2007-01-04 Stefan Kosttests/check/: enable queue test again, add tests for...
2007-01-02 Tim-Philipp MüllerCompile adapter test/example only if the required heade...
2006-12-21 Stefan Kosttests/check/: sync .cvsignome and CLEANFILES
2006-12-21 Stefan Kosttests/check/Makefile.am: fix distcheck
2006-12-21 Stefan Kostdocs/design/part-states.txt: two tiny additional comments
2006-12-21 Stefan Kosttests/check/elements/queue.c: fix race in underrun...
2006-12-21 Stefan Kosttests/check/elements/.cvsignore: ignore more
2006-12-21 Stefan Kostlibs/gst/check/gstcheck.c: do not automatically (de...
2006-12-19 Edward Herveygst/gstsegment.c: Fine tune the cases where the segment...
2006-12-09 Jan Schmidttests/check/gst/gstbin.c: It is acceptable to have...
2006-12-07 René Stadlergst/gstclock.c: Make period ids add the interval to...
2006-11-20 Wim Taymansgst/gstsegment.c: Fix boundary checking in to_running_t...
2006-11-09 Jan Schmidttests/examples/adapter/.cvsignore: Ignore build file...
2006-11-09 Jan Schmidttests/examples/adapter/: Add new files from the previou...
2006-11-09 Jan SchmidtDo some optimisation work in GstAdapter to avoid copies...
2006-11-08 Tim-Philipp Müllertests/examples/typefind/typefind.c: Make typefind eleme...
2006-11-06 Stefan Kosttests/check/gst/gsttag.c: relicence (okay with author...
2006-10-26 Tim-Philipp Müllergst/gststructure.c: If someone tries to set a non-UTF8...
2006-10-11 Tim-Philipp Müllerlibs/gst/controller/gstcontroller.c: Fix refcounting...
2006-10-09 Wim Taymansgst/gstevent.c: Rename some more @cur to @start to...
2006-10-09 Wim Taymansdocs/design/part-qos.txt: Fix typo.
2006-10-09 Tim-Philipp MüllerAPI: add gst_tag_list_is_empty() (#360467).
2006-10-07 Tim-Philipp Müllergst/gsttaglist.*: Minor fixes to GST_IS_TAG_LIST and...
2006-10-02 Wim Taymanstests/check/gst/gstghostpad.c: Fix leak in check.
2006-10-02 Alessandro Decinagst/gstevent.c: Fix gst_mini_object_make_writable(...
2006-09-29 Tim-Philipp Müllertests/check/libs/controller.c: Add test for the previou...
2006-09-28 Jan Schmidttests/examples/manual/.cvsignore: OK, so it's actually...
2006-09-28 Jan Schmidttests/examples/manual/Makefile.am: Gah, declare vars...
2006-09-28 Jan Schmidtgst/: Re-commit the registry changes, along with an...
2006-09-27 Tim-Philipp Müllertests/check/gst/gstcaps.c: Add some tests for gst_caps_...
2006-09-17 Tim-Philipp Müllergst/gstformat.c: Fix locking order (must take lock...
2006-09-16 Thomas Vander SticheleExtract the manual examples again like we used to do.
2006-09-15 Wim Taymansgst/: Small cleanups in docs and code.
2006-08-31 Wim Taymansdocs/design/part-gstghostpad.txt: Update ascii art...
2006-08-31 Edward HerveyRefactored *_new() functions.
next