]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - glsdk/gstreamer0-10.git/history - testsuite/refcounting
ignore these test code
[glsdk/gstreamer0-10.git] / testsuite / refcounting /
2003-09-11 Thomas Vander Sticheleignore these test code
2003-05-19 Benjamin Ottespaling eroah
2003-05-19 Benjamin Ottecheck if required elements are installed
2003-05-18 Thomas Vander Sticheleapplying http://bugzilla.gnome.org/show_bug.cgi?id...
2003-04-15 Benjamin Ottedestroyed gst_*_destroy in the examples - use gst_objec...
2003-03-10 Wim TaymansAdded scheduler refcount test
2003-02-25 Wim TaymansI'm too lazy to comment this
2003-01-21 Thomas Vander Stichelefix
2003-01-21 Thomas Vander Stichelevarious test fixes :)
2003-01-10 David I. Lehnconnect -> link
2002-11-02 David I. Lehnuse AM_CFLAGS instead of CFLAGS
2002-10-29 Thomas Vander Stichelemainloop test and some caps fixes that had to go in
2002-05-11 Andy Wingofix refcounting tests so that they compile and run...
2002-05-10 Andy Wingoadded a get_perms_func to gstxmlregistry that will...
2002-05-09 Thomas Vander Stichelerefcounting tests sure would be nice to have
2002-04-11 Andy Wingocommit to make gstreamer follow the gtk function/macro...
2001-12-04 wrobell- some fixes to int2float making automake 1.5 happy...
2001-11-27 Thomas Vander Sticheleremoved bin from tests
2001-11-27 Andy Wingofix stupid commit
2001-11-27 Andy Wingofor the love of god, let this be the last distcheck...
2001-11-26 Andy Wingotry some more to fix make distcheck
2001-11-24 Andy WingoGstObject is no longer instantiatable in glib2
2001-05-31 Wim TaymansRemoved the thread test so make distcheck works.
2001-05-31 Wim TaymansAdded the mem.h file in noinst_HEADERS.
2001-05-27 Wim TaymansMakfeile updates.
2001-05-25 Erik WalthinsenMerged from INCSCHED on 200505251!!!