]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - glsdk/gstreamer0-10.git/history - tools/gst-launch.c
g_thread_init() is deprecated in glib master
[glsdk/gstreamer0-10.git] / tools / gst-launch.c
2011-12-03 Tim-Philipp Müllerg_thread_init() is deprecated in glib master
2011-06-18 Tim-Philipp MüllerBump git version after unplanned 0.10.35 release
2011-05-27 Tim-Philipp Müllertools: catch and print missing-plugin messages in gst...
2011-04-16 Tim-Philipp Müllergst-launch: remove newline from translatable string
2011-02-24 Stefan Kostgst-launch: add index support
2011-02-13 Tim-Philipp Müllergst-launch: pretty-print datetime tags
2010-09-17 Sebastian Drögegst-launch: Use g_file_test() instead of access() which...
2010-09-09 Stefan Kostgst-launch: add a sync bus handler and move state-chang...
2010-07-16 Sebastian DrögeRevert "-launch: disable CLOCK_LOST message handling"
2010-07-08 Tim-Philipp Müllertools: remove -p shorthand for --no-sigusr-handler
2010-06-25 Sebastian Drögegstxml: Deprecate GstXml and related functions
2010-06-24 Tim-Philipp Müllertools: deprecate gst-xmllaunch and print fat warning...
2010-06-24 Tim-Philipp Müllergst-launch: rename new --no-play command line option...
2010-06-15 Tim-Philipp Müllergst-launch: print more errors to stderr and suppress...
2010-04-30 Stefan Kostgst-launch: add -p option to disable play handler.
2010-04-09 Wim Taymanslaunch: make -q be more quiet
2010-02-16 Tim-Philipp Müllertools: call g_set_prgname() before doing the option...
2010-02-16 Tim-Philipp MüllerRevert "tools: Move gst_tools_print_version call to...
2010-02-12 Tim-Philipp Müllergst-launch: don't leak timeout GSource
2010-01-20 Benjamin Ottetools: Run g_thread_init() unconditionally
2009-12-23 Wim Taymanslaunch: also print leaked objects
2009-12-09 Ole André Vadla... tools: Move gst_tools_print_version call to avoid warni...
2009-12-02 David Schleeftools: Fix check for Windows
2009-11-07 Tim-Philipp Müllergst-launch: wake up less often to check if we've been...
2009-10-07 Stefan Kostbuild: sprintf, sscanf need stdio.h
2009-10-07 Edward Herveygst-launch: Don't activate tracing if not requested.
2009-07-08 Philip Jägenstedttools: Fix compilation if option parsing is disabled
2009-06-03 Tim-Philipp Müllergst-launch: refer to element, pad, or object in some...
2009-06-02 David Schleeftools: Set pipeline to PAUSED before waiting for main...
2009-05-21 Tim-Philipp Müllergst-launch: don't use G_GUINT32_FORMAT in translatable...
2009-05-14 Sebastian Drögegst-launch: Print the path string for message sources
2009-05-11 Wim Taymans-launch: connect to deep-notify with right name
2009-04-16 Wim Taymans-launch: disable CLOCK_LOST message handling
2009-04-10 Wim Taymans-launch: handle clock-lost messages
2009-03-31 Thiago Santosgst-launch: Fixes error when DISABLE_FAULT_HANDLER...
2009-03-27 Thiago SantosAdds flag for eos on shutdown in gst-launch. Fixes...
2009-02-19 Tim-Philipp Müllertools: print normal output to stdout, and only errors...
2009-02-19 Tim-Philipp Müllertools: use g_print*() instead of *printf() in gst-launch
2009-02-18 Wim TaymansAdd message to request a state change
2009-02-15 Stefan Kostgst-launch: add -q/--quiet option to supress any non...
2008-11-21 Wim Taymanstools/gst-launch.c: Make gst-launch handle LATENCY...
2008-11-04 Wim Taymanstools/gst-launch.c: Print the message seqnums.
2008-10-12 Jan Schmidttools/gst-launch.c: Change the printing of the 'bufferi...
2008-02-05 Stefan Kosttools/gst-launch.c: Dump one graph per pipeline state...
2007-12-11 Stefan KostChange GST_GET_TIMESTAMP into gst_util_get_timestamp...
2007-11-28 Stefan Kostgst/: Fix wrong order of args in GST_CLOCK_DIFF() usage.
2007-10-29 Stefan KostImprove bin graph dumping, by using the envvar to speci...
2007-10-17 Stefan KostAllow dumping pipelines as dot graphs. Fixes #456573.
2007-09-23 Tim-Philipp Müllerplugins/elements/gstfakesink.c: Add some debug text...
2007-08-17 Wim Taymanstools/gst-launch.c: Don´t try to do any state managemen...
2007-08-16 Wim Taymansgst/gstmessage.h: Add some more docs for the messages.
2007-07-03 Wim Taymanstools/gst-launch.c: When we got an error, there is...
2007-06-15 Stefan Kosttools/gst-launch.c: Remove crufy code. GOption does...
2007-05-24 Wim Taymanstools/gst-launch.c: When buffering goes from a two...
2007-05-12 Wim Taymanstools/gst-launch.c: Give more interesting info when...
2007-03-08 Wim Taymanstools/gst-launch.c: Print INFO messages.
2007-02-23 Wim Taymansgst/gstpipeline.c: Don't ref a NULL clock in _provide_c...
2007-02-21 Thomas Vander Sticheletools/gst-launch.c: Make sure that we actually show...
2007-01-05 Tim-Philipp Müllertools/: Call g_thread_init() really really early, befor...
2006-09-27 Tim-Philipp Müllertests/check/gst/gstcaps.c: Add some tests for gst_caps_...
2006-09-18 Wim Taymansgst/gstelement.c: Use _DEBUG_OBJECT some more.
2006-09-15 Wim Taymanstools/gst-launch.c: Added some comments here and there.
2006-08-21 Tim-Philipp Müllergst/gstxml.c: Chain up to parent class in dispose funct...
2006-08-15 Tim-Philipp Müllertools/gst-launch.c: More space on the left for the...
2006-07-26 Jan Schmidttools/gst-launch.c: If the top-level of the parse is...
2006-07-08 Andy Wingotools/gst-launch.c (main): Handle err == NULL. gst...
2006-05-13 Tim-Philipp Müllertools/gst-launch.c: Fix use of uninitialized variable...
2006-05-12 Tim-Philipp Müllertools/gst-launch.c: Print something more intelligible...
2006-05-09 Tim-Philipp Müllertools/: Fix up includes: need to include stdlib.h in...
2006-05-05 Tim-Philipp Müllertools/: Use the string passed to g_option_context_new...
2006-05-05 Tim-Philipp Müllertools/: Add back --version command line option (#340460).
2006-02-14 Wim Taymanstools/gst-launch.c: NO_PREROLL is not an ERROR so don...
2006-02-04 Tim-Philipp Müllertools/gst-launch.c: Catch errors during preroll (#320084).
2005-11-28 Edward Herveytools/gst-launch.c: Clarify the output strings, makes...
2005-10-27 Wim Taymansgst/base/gstbasesink.c: Some more debug.
2005-10-18 Wim TaymansSeriously, this is better than a previous commit as...
2005-10-18 Wim TaymansMake messages future proof. state-change gets a flag...
2005-10-13 Thomas Vander Stichelegst/base/: fix up debugging
2005-10-13 Stefan Kostfix GOption context leaks doc fixes
2005-10-12 Wim TaymansSome doc updates.
2005-10-12 Wim TaymansUse GstClockTime in _get_state() instead of GTimeVal.
2005-10-11 Thomas Vander Stichelemore str null protection
2005-10-11 Thomas Vander Stichelegst/gst-i18n-lib.h: check for ENABLE_NLS, not GETTEXT_P...
2005-10-10 Wim Taymanscheck/: Check fixes, use API as stated in design docs...
2005-10-10 RonaldMerged in popt removal + GOption addition patch from...
2005-10-08 Wim Taymansgst/gstmessage.*: Clean up.
2005-10-08 Wim Taymanstools/gst-launch.c: Better message printout.
2005-10-08 Wim TaymansAdded extra field to STATE_CHANGE message with the...
2005-10-07 Thomas Vander Sticheledon't use if not declared
2005-10-04 Tim-Philipp Müllertools/gst-launch.c: Don't try to run erroneous pipelines.
2005-09-20 Wim TaymansThe timeout handler should have lower priority than...
2005-09-19 Wim TaymansGstBusHandler -> GstBusFunc, return value has the same...
2005-09-02 Andy Wingogst/gstelement.h (GstState): Renamed from GstElementSta...
2005-08-25 Jan SchmidtRevert unpopular change for GST_MESSAGE_SRC to GObject.
2005-08-24 Jan SchmidtChange GST_MESSAGE_SRC to be a GObject rather than...
2005-08-15 Thomas Vander Sticheledon't convert NULL structures to strings
2005-07-19 Wim Taymanstools/gst-launch.c: Don't block forever for the state...
2005-07-15 Wim TaymansTotally dump messages in -launch with the -m option.
2005-07-12 Wim Taymansgst/base/gstbasetransform.c: Added more debug info...
2005-07-11 Thomas Vander Stichelevalgrind unit tests as check-local; add gst_deinit
next