]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - glsdk/gstreamer0-10.git/history - tools/gst-xmlinspect.c
g_thread_init() is deprecated in glib master
[glsdk/gstreamer0-10.git] / tools / gst-xmlinspect.c
2011-12-03 Tim-Philipp Müllerg_thread_init() is deprecated in glib master
2011-11-27 Stefan Sauerwarnings: avoid set-but-unused warnings with load-save...
2010-02-16 Tim-Philipp Müllertools: call g_set_prgname() before doing the option...
2010-01-20 Benjamin Ottetools: Run g_thread_init() unconditionally
2009-12-09 Sebastian Drögetools: Move gst_tools_print_version() for the remaining...
2009-08-18 Sebastian Drögetools: Use iterate_internal_links instead of deprecated...
2008-07-31 Sebastian DrögeRemove GST_DISABLE_(ENUMTYPES|INDEX|URI) everywhere.
2008-04-12 Tim-Philipp Müllertools/gst-xmlinspect.c: De-cruft a bit. If no argument...
2007-10-15 Stefan Kosttools/gst-inspect.c: Save approx. 400 1 byte allocs...
2007-01-05 Tim-Philipp Müllertools/: Call g_thread_init() really really early, befor...
2006-06-07 Wim TaymansFix leak spotted by coverity checker. Fixes #343827
2006-05-09 Tim-Philipp Müllertools/: Fix up includes: need to include stdlib.h in...
2006-05-05 Tim-Philipp Müllertools/: Use the string passed to g_option_context_new...
2006-05-05 Tim-Philipp Müllertools/: Add back --version command line option (#340460).
2006-01-20 Jan Schmidttools/: URL_HANDLER is not a plugin feature we can...
2005-12-06 Thomas Vander Sticheleexpand tabs
2005-11-30 Thomas Vander Stichelevarious fixes to make
2005-10-13 Stefan Kostfix GOption context leaks doc fixes
2005-10-10 RonaldMerged in popt removal + GOption addition patch from...
2005-09-18 David Schleefcheck/Makefile.am: Fix environment variables.
2005-09-15 David Schleefremove
2005-08-24 Stefan KostFixed long standing mem-leak
2005-08-01 Stefan Kostdeactivate and remove dparams (libgstcontrol)
2005-07-18 Wim TaymansRemoved plugable schedulers.
2005-06-08 Andy Wingogst/gstutils.c: RPAD fixes all around.
2005-05-09 Wim TaymansRemove old query functions. Ported old code.
2005-05-04 Andy WingoGCC 4 fixen.
2005-04-12 Ronald S. BultjeUse libxml2 for registry parsing, use staticpadtemplate...
2005-03-21 Wim TaymansNext big merge.
2005-03-07 Wim TaymansFirst THREADED backport attempt, focusing on adding...
2004-05-14 Stéphane Loeuillettypos : unkown => unknown
2004-05-07 David SchleefChanges to handle compilers that don't have variadic...
2004-03-15 Thomas Vander Sticheledon't mix tabs and spaces
2004-03-13 Thomas Vander Stichelegst-indent run on core
2004-02-16 Johan DahlinSpelling fix
2004-02-16 Johan DahlinSpelling fix
2003-12-22 David SchleefMerge CAPS branch
2003-12-04 Andy Wingoremove copyright field from plugin structs
2003-11-29 David SchleefRemove old autoplug code
2003-11-24 Benjamin Otteimplement URI schemes
2003-10-31 Benjamin Otteupdate plugin initialization restructuring (see email...
2003-10-28 Iain HolmesInitialise some variables to get the thing to compile
2003-10-28 Benjamin Ottemerge TYPEFIND branch. Major changes:
2003-08-19 David Schleeffurther i18n: call setlocale()
2003-06-29 Benjamin OtteGST_DEBUG reorganization containing loads of stuff:
2003-04-04 Wim TaymansFix #109350, aplied patch from Peter N. Lundblad.
2003-03-16 Christian MeyerFixed bug #108514.
2003-03-11 Brian CameronNow support ISO-style variable-argument macros, which...
2003-02-21 Wim Taymans- indentation fixes
2003-02-20 Wim Taymansgst-xmlinspect dumps the plugin info to an xml file...