]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - glsdk/gstreamer0-10.git/history - tools
ignore more
[glsdk/gstreamer0-10.git] / tools /
2004-05-14 Stéphane Loeuillettypos : unkown => unknown
2004-05-10 David Schleefgst/gstinfo.h: Add missing inline function.
2004-05-07 David SchleefChanges to handle compilers that don't have variadic...
2004-05-04 Thomas Vander Stichelereorganize C/LIB flags add gst_info to gstcompat.h
2004-05-02 Stéphane Loeuillethum, vorbisfile => oggdemux ! vorbisdec ! audioconvert
2004-05-02 Stéphane Loeuilletfirst try at hunting old elements that where renamed...
2004-04-29 Benjamin Ottegst/: remove useless _gst_progname stuff
2004-04-14 Thomas Vander Sticheleprint rank numerically as well
2004-04-13 Thomas Vander Stichelebuild fix
2004-03-15 Thomas Vander Sticheledon't mix tabs and spaces
2004-03-15 Thomas Vander Sticheleuncommit
2004-03-15 Johan Dahlintools/Makefile.am (EXTRA_DIST): Add gst-indent
2004-03-15 Thomas Vander Sticheledistcheck fixes
2004-03-14 Thomas Vander Sticheleg_error fix, m/m version fix
2004-03-14 Thomas Vander Sticheleupdate
2004-03-14 Thomas Vander Sticheledon't spill paths from registry until we fix the generi...
2004-03-13 Thomas Vander Stichelegst-indent run on core
2004-03-13 Thomas Vander Sticheleadding gst-indent as a noinst tool
2004-03-10 David Schleeftools/gst-run.c: Fix crash when no relevant tools were...
2004-03-09 Thomas Vander Stichelereleasing 0.7.6
2004-03-06 David SchleefREQUIREMENTS: Add bison and flex.
2004-03-02 Christophe Fergeautools/: add calls to bind_textdomain_codeset
2004-03-02 Thomas Vander Sticheletrim fat from nonversioned binaries
2004-03-01 Thomas Vander Sticheleconfigure.ac: remove whitespace
2004-02-19 Thomas Vander Stichelesome fixes from jdahlin
2004-02-19 David Schleeflibs/gst/control/: Additional fixes to get double dpara...
2004-02-16 Johan DahlinSpelling fix
2004-02-16 Johan DahlinSpelling fix
2004-02-12 Thomas Vander Stichelefixes for --disable-loadsave --disable-registry
2004-02-12 Thomas Vander Stichelespec update tools install fixes
2004-02-12 Thomas Vander Sticheleignore more files
2004-02-11 Thomas Vander Sticheleupdates
2004-02-11 Thomas Vander Sticheleremove unversioned feedback script
2004-02-11 Thomas Vander Sticheleversion gst-feedback
2004-02-04 Thomas Vander Stichelemore ignores
2004-02-04 Thomas Vander Sticheleadding more ignores
2004-02-04 Thomas Vander Sticheledistcheck fix
2004-02-04 Thomas Vander Stichelereturn after printing versions
2004-02-04 Thomas Vander Sticheleinstall docs versioned
2004-02-04 Thomas Vander Sticheleadd gst-run wrapper code build original tools as versio...
2004-02-03 Thomas Vander Stichelemore simplifying
2004-02-03 Thomas Vander Sticheleuse AM_CFLAGS
2004-02-03 Thomas Vander Sticheleadd error symbol start translating gst-inspect
2004-01-20 Thomas Vander Stichelefix output of typefind add GPL headers fix doc snippet
2004-01-13 Thomas Vander Sticheletranslating parsing error messages
2004-01-13 Thomas Vander Sticheleupdate nl transition add gst-launch to be translated
2004-01-12 Benjamin Otteupdate - this is huge, because it includes *.bb, *...
2004-01-11 Benjamin Ottetools/gst-inspect.c: improve output of caps a bit
2003-12-22 David SchleefMerge CAPS branch
2003-12-05 Thomas Vander Stichelemore trademark fixing
2003-12-04 Andy Wingoremove copyright field from plugin structs
2003-11-29 David SchleefRemove old autoplug code
2003-11-24 Benjamin Ottedon't use strdup_value_contents for strings
2003-11-24 Benjamin Otteimplement URI schemes
2003-11-24 Benjamin Ottemerge in tagging
2003-11-14 Thomas Vander Sticheleput GST_CACHE_DIR in config.h
2003-11-14 Thomas Vander Sticheleremoving GST_CONFIG_DIR
2003-11-04 David Schleefcosmetic change. GObjects contain properties, not...
2003-10-31 Benjamin Otteupdate plugin initialization restructuring (see email...
2003-10-29 Iain HolmesNULL terminate the g_build_filename args.
2003-10-28 Iain HolmesInitialise some variables to get the thing to compile
2003-10-28 Benjamin Ottemerge TYPEFIND branch. Major changes:
2003-09-29 Iain HolmesUpdate the documentation here too to include more detai...
2003-09-27 David Schleefchange scripts directory to register-scripts
2003-09-14 David SchleefUse gst_caps_to_string to print caps. Add max_iterations.
2003-09-11 Thomas Vander Stichelecheck for md5sink in pipeline
2003-08-21 David Schleefshow the rank of a plugin feature. (actually, only...
2003-08-19 David Schleefignore more files
2003-08-19 David SchleefRemove the superfluous use of { }
2003-08-19 David Schleeffurther i18n: call setlocale()
2003-08-19 David SchleefAdd code to spawn each file in ${plugindirectory}/scrip...
2003-08-19 Ronald S. BultjeAdd SIGUSR1/SIGUSR2 as play/stop signals. Also add...
2003-08-18 David SchleefShow signals/actions of parent classes
2003-08-15 David SchleefMove man pages from %.1 to %.1.in, and add a rule to...
2003-07-27 David SchleefChange printing of float props to %g
2003-07-25 Brian CameronProperly handle null string value, preventing core...
2003-07-14 David SchleefAdd number-of-iterations option.
2003-07-12 David SchleefUpdate for new debugging system
2003-07-01 David SchleefAdd SIGINT handling. ctrl-C is more graceful now
2003-06-29 Benjamin OtteGST_DEBUG reorganization containing loads of stuff:
2003-06-25 Brian CameronFixed gst-inspect so it doesn't core dump on Solaris.
2003-05-18 David SchleefAdd new man page. Fix a few typos in other man pages.
2003-05-18 Benjamin Otteadded filtered caps to man page
2003-05-17 Thomas Vander Sticheleadding typefind binary
2003-05-06 Benjamin Ottesimple fix: these are signed ints, not unsigned
2003-04-28 Benjamin Otteparsing returns elements, not bins - so put it into...
2003-04-25 Benjamin Otteupdate man page to new pipeline parsing and make it...
2003-04-23 Thomas Vander Stichelemake the user registry location major-minor versioned...
2003-04-13 David SchleefFall back on sa_handler if sa_sigaction doesn't work
2003-04-10 Benjamin Ottepatch to gst-launch - a pipeline parsing can result...
2003-04-04 Benjamin Ottework around popt bug
2003-04-04 Wim TaymansFix #109350, aplied patch from Peter N. Lundblad.
2003-03-16 Christian MeyerFixed bug #108514.
2003-03-11 Brian CameronNow support ISO-style variable-argument macros, which...
2003-02-25 Wim TaymansI'm too lazy to comment this
2003-02-21 Wim TaymansAdd xmlinspect to README
2003-02-21 Wim Taymans- indentation fixes
2003-02-21 Wim Taymans- added indexing, dynamic params, signals, actions...
2003-02-20 Wim TaymansAdded pad implementation + element properties
2003-02-20 Wim Taymansgst-xmlinspect dumps the plugin info to an xml file...
next