glsdk/gstreamer0-10.git
9 years agoqueue2: fix refactoring of draining-on-eos, munge flow return to FLOW_OK
Tim-Philipp Müller [Mon, 28 Nov 2011 01:10:20 +0000 (01:10 +0000)]
queue2: fix refactoring of draining-on-eos, munge flow return to FLOW_OK

9 years agoqueue2: add bufferlist support
Tim-Philipp Müller [Thu, 3 Nov 2011 10:34:49 +0000 (10:34 +0000)]
queue2: add bufferlist support

We want to maintain buffer lists if possible.

9 years agoqueue2: split out draining of queue on FLOW_UNEXPECTED into separate function
Tim-Philipp Müller [Thu, 3 Nov 2011 13:02:36 +0000 (13:02 +0000)]
queue2: split out draining of queue on FLOW_UNEXPECTED into separate function

9 years agoqueue2: pass item type enum to _enqueue instead of simple isbuffer boolean
Tim-Philipp Müller [Thu, 3 Nov 2011 08:55:20 +0000 (08:55 +0000)]
queue2: pass item type enum to _enqueue instead of simple isbuffer boolean

Avoids some unnecessary GST_IS_EVENT()

9 years agowarnings: avoid set-but-unused warnings with load-save disabled
Stefan Sauer [Sun, 27 Nov 2011 19:36:31 +0000 (20:36 +0100)]
warnings: avoid set-but-unused warnings with load-save disabled

9 years agouri: fix wrong G_GNUC_MALLOC
Tim-Philipp Müller [Sat, 26 Nov 2011 19:45:48 +0000 (19:45 +0000)]
uri: fix wrong G_GNUC_MALLOC

_get_protocols() points to const memory in 0.10
despite the non-const return value.

9 years agolibs: sprinkle some G_GNUC_MALLOC
Tim-Philipp Müller [Sat, 26 Nov 2011 18:58:38 +0000 (18:58 +0000)]
libs: sprinkle some G_GNUC_MALLOC

Maybe gcc can do something clever with that, or at least
warn us if we don't save the return value somewhere.

9 years agogst: sprinkle some G_GNUC_MALLOC
Tim-Philipp Müller [Sat, 26 Nov 2011 18:57:44 +0000 (18:57 +0000)]
gst: sprinkle some G_GNUC_MALLOC

Maybe gcc can do something clever with that, or at least
warn us if we don't save the return value somewhere.

9 years agobuffer: add gst_buffer_{set,get}_qdata()
Tim-Philipp Müller [Wed, 16 Nov 2011 01:04:45 +0000 (01:04 +0000)]
buffer: add gst_buffer_{set,get}_qdata()

Allows people/us to attach arbitrary metadata to buffers.

https://bugzilla.gnome.org/show_bug.cgi?id=664720

API: gst_buffer_set_qdata()
API: get_buffer_get_qdata()

9 years agopad: Remove g_warning() if pad accepted caps that are not a subset of the pad caps
Sebastian Dröge [Thu, 24 Nov 2011 10:15:29 +0000 (11:15 +0100)]
pad: Remove g_warning() if pad accepted caps that are not a subset of the pad caps

This check is correct but unfortunately it's impossible to implement
in a threadsafe way because the caps could have changed in the meantime.

Fixes bug #659606.

9 years agomultiqueue: check filled state of queues even if another one is empty
Vincent Penquerc'h [Mon, 3 Oct 2011 11:34:20 +0000 (12:34 +0100)]
multiqueue: check filled state of queues even if another one is empty

This will avoid a case where overrun is never signalled if some
stream never produces any data, causing playbin2 to not end preroll.

https://bugzilla.gnome.org/show_bug.cgi?id=660778

9 years agobaseparse: Return template caps instead of other side's peer caps if get_sink_caps...
Sebastian Dröge [Wed, 23 Nov 2011 12:42:56 +0000 (13:42 +0100)]
baseparse: Return template caps instead of other side's peer caps if get_sink_caps vfunc is not implemented

Using gst_pad_proxy_get_caps() breaks backwards compatibility with old
parsers because it will propagate the other side's fields like "parsed"
and "framed" and also breaks parser/converters.

Fixes bug #664221.

9 years agogst-inspect: print current value as default value
Tim-Philipp Müller [Sat, 12 Nov 2011 16:42:14 +0000 (16:42 +0000)]
gst-inspect: print current value as default value

Instead of printing separate 'Current' and 'Default' values
(the former obtained via g_object_get() and the latter from
the property GParamSpec), simply print the Current value as
the Default value. This is the right thing to do for almost
all elements and avoids confusion if a subclass of a base
class chooses a different default than the base class.

9 years agogst, controller: replace g_list_prepend + reverse with GQueue
Tim-Philipp Müller [Sat, 12 Nov 2011 14:55:07 +0000 (14:55 +0000)]
gst, controller: replace g_list_prepend + reverse with GQueue

9 years agoAndroid: build audio controller example
Stefan Sauer [Wed, 9 Nov 2011 10:05:59 +0000 (11:05 +0100)]
Android: build audio controller example

Add buildsystem hooks for building the audiocontroller example
with the NDK.

Signed-off-by: Reynaldo H. Verdejo Pinochet <reynaldo@collabora.com>
9 years agogstvalue: consider lists and ranges equal if they hold the same set
Vincent Penquerc'h [Tue, 8 Nov 2011 18:09:28 +0000 (18:09 +0000)]
gstvalue: consider lists and ranges equal if they hold the same set

This fixes caps operations when different elements advertise some
of their caps' properties differently (eg, for audio channels, either
a range from 1 to 2, or a list of 1 and 2).

https://bugzilla.gnome.org/show_bug.cgi?id=663643

9 years agotests: add a subset test for structure
Stefan Sauer [Wed, 9 Nov 2011 10:24:26 +0000 (11:24 +0100)]
tests: add a subset test for structure

9 years agodocs: also fix wrong call order for controller in manual
Stefan Sauer [Fri, 28 Oct 2011 11:39:58 +0000 (13:39 +0200)]
docs: also fix wrong call order for controller in manual

9 years agotests: pad: add test to verify flushing behaviour
René Stadler [Tue, 8 Nov 2011 11:22:21 +0000 (12:22 +0100)]
tests: pad: add test to verify flushing behaviour

Seems like a trivial case, but this was actually broken in 0.11 recently.

9 years agodocs: fix Since: markers for API added after 0.10.35
Tim-Philipp Müller [Tue, 8 Nov 2011 00:32:36 +0000 (00:32 +0000)]
docs: fix Since: markers for API added after 0.10.35

9 years agowin32: update .def file for new API
Tim-Philipp Müller [Tue, 8 Nov 2011 00:15:49 +0000 (00:15 +0000)]
win32: update .def file for new API

API: gst_caps_is_strictly_equal()

9 years agogstcaps: remove unneeded use of gint64
Vincent Penquerc'h [Thu, 27 Oct 2011 11:59:57 +0000 (12:59 +0100)]
gstcaps: remove unneeded use of gint64

https://bugzilla.gnome.org/show_bug.cgi?id=662777

9 years agogstvalue: quicker version of intersection when we do not need the result
Vincent Penquerc'h [Thu, 27 Oct 2011 11:24:13 +0000 (12:24 +0100)]
gstvalue: quicker version of intersection when we do not need the result

https://bugzilla.gnome.org/show_bug.cgi?id=662777

9 years agogststructure: simplify return statement in gst_structure_can_intersect
Vincent Penquerc'h [Thu, 27 Oct 2011 11:02:43 +0000 (12:02 +0100)]
gststructure: simplify return statement in gst_structure_can_intersect

https://bugzilla.gnome.org/show_bug.cgi?id=662777

9 years agogststructure: early out when we know a value cannot be a subset
Vincent Penquerc'h [Thu, 27 Oct 2011 10:41:30 +0000 (11:41 +0100)]
gststructure: early out when we know a value cannot be a subset

If two values can be ordered, but are unequal, they are
necessarily distinct, thus one cannot be a subset of the other.

https://bugzilla.gnome.org/show_bug.cgi?id=662777

9 years agogstvalue: quicker test for substraction emptiness
Vincent Penquerc'h [Thu, 27 Oct 2011 09:35:53 +0000 (10:35 +0100)]
gstvalue: quicker test for substraction emptiness

When we do not care about the actual resulting set,
but only whether it is empty of not, we can skip a fair bit
of GValue juggling.

Add a function that does so, since we cannot just pass NULL
to the existing API as it may be part of the API contract.

https://bugzilla.gnome.org/show_bug.cgi?id=662777

9 years agogststructure: rejig test ordering for speed
Vincent Penquerc'h [Thu, 27 Oct 2011 08:45:41 +0000 (09:45 +0100)]
gststructure: rejig test ordering for speed

https://bugzilla.gnome.org/show_bug.cgi?id=662777

9 years agobasetransform: Only use the cached transform on strictly equal caps
Sjoerd Simons [Thu, 3 Nov 2011 15:36:59 +0000 (15:36 +0000)]
basetransform: Only use the cached transform on strictly equal caps

https://bugzilla.gnome.org/show_bug.cgi?id=663333

9 years agocaps: Add gst_caps_is_strictly_equal
Sjoerd Simons [Thu, 3 Nov 2011 15:35:32 +0000 (15:35 +0000)]
caps: Add gst_caps_is_strictly_equal

9 years agointrospection: add Value annotations for GST_SECOND, GST_MSECOND, GST_USECOND, GST_NS...
Peteris Krisjanis [Sat, 15 Oct 2011 19:52:25 +0000 (22:52 +0300)]
introspection: add Value annotations for GST_SECOND, GST_MSECOND, GST_USECOND, GST_NSECOND constants

gobject-introspection won't parse them properly otherwise.

Still need to force the right type though (either GstClockTime or
guint64), but Type: xyz has no effect for me here, so someone with
a newer g-i needs to test this.

Some other defines are also missing, e.g. GST_CLOCK_TIME_NONE.

9 years agoconfigure: suppress unused variable warnings if gst debugging is disabled
Tim-Philipp Müller [Fri, 4 Nov 2011 00:03:05 +0000 (00:03 +0000)]
configure: suppress unused variable warnings if gst debugging is disabled

https://bugzilla.gnome.org/show_bug.cgi?id=662952

9 years agoconfigure: fix typo around GLIB_EXTRA_CFLAGS in GST_ALL_CXXFLAGS
Tim-Philipp Müller [Fri, 4 Nov 2011 00:02:07 +0000 (00:02 +0000)]
configure: fix typo around GLIB_EXTRA_CFLAGS in GST_ALL_CXXFLAGS

9 years agoqueue: use statically allocated GQueue
Tim-Philipp Müller [Thu, 3 Nov 2011 23:08:52 +0000 (23:08 +0000)]
queue: use statically allocated GQueue

9 years agobin: use statically allocated GQueue
Tim-Philipp Müller [Thu, 3 Nov 2011 22:58:50 +0000 (22:58 +0000)]
bin: use statically allocated GQueue

Because we can.

9 years agocollectpads2: use flags enum instead of guint in structure
Tim-Philipp Müller [Thu, 3 Nov 2011 22:51:57 +0000 (22:51 +0000)]
collectpads2: use flags enum instead of guint in structure

9 years agoqueue2: use statically allocated GQueue
Tim-Philipp Müller [Thu, 3 Nov 2011 08:47:20 +0000 (08:47 +0000)]
queue2: use statically allocated GQueue

9 years agoghostpad: Don't cache internal proxy pad target
Nicolas Dufresne [Tue, 25 Oct 2011 21:26:50 +0000 (17:26 -0400)]
ghostpad: Don't cache internal proxy pad target

The internal proxy pad target is simply a cache of the internal proxy pad
peer. This patch uses the well implement GstPad peer handling to obtain the
target. This fixes issues with target not being set in both direction when
two ghostpads are linked together (empty bin).

https://bugzilla.gnome.org/show_bug.cgi?id=658517

9 years agoadapter: simplify gst_adapter_take_list()
Tim-Philipp Müller [Tue, 1 Nov 2011 14:17:21 +0000 (14:17 +0000)]
adapter: simplify gst_adapter_take_list()

Use a stack-allocated GQueue to assemble our GList.

9 years agoconfigure: make GLIB_EXTRA_CFLAGS overwritable
Tim-Philipp Müller [Mon, 31 Oct 2011 17:45:44 +0000 (17:45 +0000)]
configure: make GLIB_EXTRA_CFLAGS overwritable

Make 'make GLIB_EXTRA_CFLAGS=...' work.

9 years agofilter: deprecate gst_filter_run()
Tim-Philipp Müller [Sun, 30 Oct 2011 21:54:36 +0000 (21:54 +0000)]
filter: deprecate gst_filter_run()

It's not really used outside of core at all, and has
serious namespace issues. If anyone feels the need to
revive this one, please use a less generic name space.

API: deprecate gst_filter_run()
API: deprecate GstFilterFunc

9 years agoregistry: don't use soon-to-be-deprecated gst_filter_run()
Tim-Philipp Müller [Sun, 30 Oct 2011 21:39:36 +0000 (21:39 +0000)]
registry: don't use soon-to-be-deprecated gst_filter_run()

Lines-of-code savings are negligible anyway.

9 years agopluginfeature: deprecate gst_plugin_feature_type_name_filter()
Tim-Philipp Müller [Sun, 30 Oct 2011 21:21:59 +0000 (21:21 +0000)]
pluginfeature: deprecate gst_plugin_feature_type_name_filter()

It's only used internally anyway and the helper struct
has namespace issues.

API: deprecated gst_plugin_feature_type_name_filter()
API: deprecated GstTypeNameData

9 years agotaglist: add to_string and new_from_string functions
Tim-Philipp Müller [Sun, 30 Oct 2011 09:58:16 +0000 (09:58 +0000)]
taglist: add to_string and new_from_string functions

We want to make GstTagList opaque and not have people use
GstStructure API on it.

API: gst_tag_list_to_string()
API: gst_tag_list_new_from_string()

9 years agotaglist: avoid pointless tag name -> quark lookups
Tim-Philipp Müller [Sun, 30 Oct 2011 00:46:22 +0000 (01:46 +0100)]
taglist: avoid pointless tag name -> quark lookups

We never get a tag name quark from a caller, it's always a
string, from which we'll try to look up our tag info in the
hash table, so change the hash table key from quark to string.
Avoids a bunch of pointless string => quark lookup in the
global quark table. We need to do an extra string => quark
conversion now when we copy a taglist, but in that case we're
in a slow path anyway.

9 years agotaglist: add gst_tag_list_is_equal()
Tim-Philipp Müller [Sat, 29 Oct 2011 23:44:44 +0000 (00:44 +0100)]
taglist: add gst_tag_list_is_equal()

API: gst_tag_list_is_equal()

9 years agostructure: identical structures are definitely equal
Tim-Philipp Müller [Sat, 29 Oct 2011 22:52:22 +0000 (23:52 +0100)]
structure: identical structures are definitely equal

9 years agobasetransform: Also fush the cache when changing the upstream caps suggestion
Sjoerd Simons [Fri, 28 Oct 2011 09:53:32 +0000 (11:53 +0200)]
basetransform: Also fush the cache when changing the upstream caps suggestion

9 years agobasetransform: Add debug output when returning a cached transform
Sjoerd Simons [Fri, 28 Oct 2011 09:50:23 +0000 (11:50 +0200)]
basetransform: Add debug output when returning a cached transform

9 years agocollectpads2: Fix refcount handling if a buffer was dropped due to clipping
Sebastian Dröge [Fri, 28 Oct 2011 08:54:19 +0000 (10:54 +0200)]
collectpads2: Fix refcount handling if a buffer was dropped due to clipping

9 years agocollectpads2: Merge the clip and prepare_buffer function into one
Sebastian Dröge [Fri, 28 Oct 2011 08:37:21 +0000 (10:37 +0200)]
collectpads2: Merge the clip and prepare_buffer function into one

9 years agocollectpads2: Merge clipping API from old collectpads
Sebastian Dröge [Fri, 28 Oct 2011 08:17:06 +0000 (10:17 +0200)]
collectpads2: Merge clipping API from old collectpads

9 years agobasesink: make default query function name show up in gst-inspect
Tim-Philipp Müller [Fri, 28 Oct 2011 08:19:29 +0000 (09:19 +0100)]
basesink: make default query function name show up in gst-inspect

9 years agocollectpads2: avoid hanging in case of sparse newsegment events
Mark Nauwelaerts [Tue, 27 Sep 2011 13:48:52 +0000 (15:48 +0200)]
collectpads2: avoid hanging in case of sparse newsegment events

... in the extent that a non-waiting pad (so indicated by newsegment)
turns out to provide the best buffer, which is then forced to waiting
for book-keeping purposes, but that should only be temporary.

See bug #415754.

9 years agocollectpads2: Use G_DEFINE_TYPE instead of GST_BOILERPLATE
Sebastian Dröge [Fri, 28 Oct 2011 07:38:35 +0000 (09:38 +0200)]
collectpads2: Use G_DEFINE_TYPE instead of GST_BOILERPLATE

9 years agocollectpads2: Add to the documentation
Sebastian Dröge [Fri, 28 Oct 2011 07:35:50 +0000 (09:35 +0200)]
collectpads2: Add to the documentation

9 years agowin32: Add new collectpads2 API
Sebastian Dröge [Fri, 28 Oct 2011 07:26:11 +0000 (09:26 +0200)]
win32: Add new collectpads2 API

9 years agobase: Add collectpads2
Sebastian Dröge [Fri, 28 Oct 2011 07:18:55 +0000 (09:18 +0200)]
base: Add collectpads2

This handles muxing of sparse/subtitle streams and has
lots of cleanup. Still missing is special support for
live streams but this can be added later without breaking
API/ABI.

Based on the version from the videomixer plugin.
https://bugzilla.gnome.org/show_bug.cgi?id=415754

9 years agobasetransform: Fix refcount leak
Jan Schmidt [Thu, 27 Oct 2011 12:08:14 +0000 (23:08 +1100)]
basetransform: Fix refcount leak

Don't leak peercaps and a ref to the basetransform when returning
the cached caps.

9 years agocontroller: fix wrong order of calls in the docs.
Stefan Sauer [Thu, 27 Oct 2011 08:38:10 +0000 (10:38 +0200)]
controller: fix wrong order of calls in the docs.

9 years agoevent: clarify docs for step event
Stefan Sauer [Wed, 26 Oct 2011 10:23:07 +0000 (12:23 +0200)]
event: clarify docs for step event

9 years agoregistry: add support for GST_REGISTRY_REUSE_PLUGIN_SCANNER=no
Tim-Philipp Müller [Tue, 18 Oct 2011 22:19:47 +0000 (23:19 +0100)]
registry: add support for GST_REGISTRY_REUSE_PLUGIN_SCANNER=no

This will make sure we spawn a new plugin scanner helper for each plugin
to be introspected, which helps with making sure we don't load too many
shared objects (libs, plugins) at the same time on systems where there
is a hard limit like on Android.

A better version might re-use the scanner for up to N times, though
it's not clear whether that would actually improve things dramatically.

https://bugzilla.gnome.org/show_bug.cgi?id=662091

9 years agocaps: No need to require writable caps for _append/_merge second caps
Thiago Santos [Fri, 21 Oct 2011 13:23:04 +0000 (10:23 -0300)]
caps: No need to require writable caps for _append/_merge second caps

The second caps ownership is transfered, no need to require it to
be writable from the caller function. Instead, _append and _merge
make it writable on their own.

Discovered because of an assertion on encoding-profile.c in
_get_input_caps using _merge but not passing writable caps.

9 years agobaseparse: Fix documentation, it's pre_push_frame and not pre_push_buffer
Sebastian Dröge [Thu, 20 Oct 2011 14:59:01 +0000 (16:59 +0200)]
baseparse: Fix documentation, it's pre_push_frame and not pre_push_buffer

9 years agobasetransform: cache transformed caps where appropriate
Vincent Penquerc'h [Thu, 20 Oct 2011 13:02:44 +0000 (14:02 +0100)]
basetransform: cache transformed caps where appropriate

Speeds up negotiation a fair bit on a contrived pipeline
with a dozen colorspace conversions.

Hopefully clears out the cache every time it ought to.

https://bugzilla.gnome.org/show_bug.cgi?id=662291

9 years agoFix broken android building due to name change in 01d87250a845e55d6
Reynaldo H. Verdejo Pinochet [Thu, 20 Oct 2011 13:45:30 +0000 (10:45 -0300)]
Fix broken android building due to name change in 01d87250a845e55d6

9 years agobasebarse: Add detect vfunc to allow subclasses to do format detection before anythin...
Sebastian Dröge [Thu, 20 Oct 2011 06:31:18 +0000 (08:31 +0200)]
basebarse: Add detect vfunc to allow subclasses to do format detection before anything else

API: GstBaseParseClass::detect()

This is called with the first buffers until the subclass has finished detection
and only afterwards the original buffers are handled as before. The vfunc allows
detection of the stream format without breaking the upstream framing.

9 years agopad: not only describe conditions in the docs, also check them in the code
Stefan Sauer [Thu, 20 Oct 2011 06:57:57 +0000 (08:57 +0200)]
pad: not only describe conditions in the docs, also check them in the code

When blocking pads, check if the pad is in the rigt direction. Log some info
for the developer and return FALSE, instead of just locking up.

9 years agomessage: protect against null message sources
Thiago Santos [Tue, 18 Oct 2011 22:21:58 +0000 (19:21 -0300)]
message: protect against null message sources

Message sources can be null, check if it is before trying to
access its name.

9 years agobaseparse: add since doc to new getcaps function
Thiago Santos [Tue, 18 Oct 2011 11:48:37 +0000 (08:48 -0300)]
baseparse: add since doc to new getcaps function

9 years agologging: more logging and prefer human readable details over memory locations
Stefan Sauer [Tue, 18 Oct 2011 12:08:19 +0000 (14:08 +0200)]
logging: more logging and prefer human readable details over memory locations

9 years agodebugutils: improve display of ghost- and proxypads
Stefan Sauer [Tue, 18 Oct 2011 12:05:37 +0000 (14:05 +0200)]
debugutils: improve display of ghost- and proxypads

Handle virtual links between ghost and proxypads when iterating pads instead of
when linking. Besides using less code this provides a more accurate picture.

9 years agobaseparse: add getcaps function
Thiago Santos [Mon, 17 Oct 2011 17:42:08 +0000 (14:42 -0300)]
baseparse: add getcaps function

Adds a getcaps function to the sink pad to make parsers propagate
downstream caps restrictions to upstream.

The pipeline "audiotestsrc num-buffers=100 ! faac ! aacparse !
"audio/mpeg, version=(int)4, stream-format=(string)adts" ! filesink"
wouldn't work because aacparse wouldn't propagate the adts restriction
upstream to faac.

This patch adds a default getcaps to the sink pad to simply proxy
downstream caps and also adds a 'get_sink_caps' function pointer
to GstBaseParseClass for subclasses that need more refined getcaps.

https://bugzilla.gnome.org/show_bug.cgi?id=661874

9 years agobasesrc: also update the stream time
Wim Taymans [Tue, 18 Oct 2011 10:39:03 +0000 (12:39 +0200)]
basesrc: also update the stream time

9 years agobaseparse: Fix handling of queued frames
Sebastian Dröge [Tue, 18 Oct 2011 08:58:14 +0000 (10:58 +0200)]
baseparse: Fix handling of queued frames

gst_base_parse_push_frame() already frees the frame, no need to
do it another time again.

9 years agobus: give watch source a name
Tim-Philipp Müller [Sun, 16 Oct 2011 20:12:07 +0000 (21:12 +0100)]
bus: give watch source a name

Give our GSource a meaningful name. Source names can be
used for debugging and profiling, for example with
systemtap or gdb.

9 years agogstbuffer: Add transfer annotations for gst_buffer_join()
Edward Hervey [Fri, 14 Oct 2011 07:35:09 +0000 (09:35 +0200)]
gstbuffer: Add transfer annotations for gst_buffer_join()

9 years agobus: fix typo in the docs
Stefan Sauer [Thu, 13 Oct 2011 15:33:06 +0000 (17:33 +0200)]
bus: fix typo in the docs

9 years agodebugutils: show if an element is state-locked
Stefan Sauer [Thu, 13 Oct 2011 14:48:02 +0000 (16:48 +0200)]
debugutils: show if an element is state-locked

9 years agologging: use _OBJECT variants more
Stefan Sauer [Thu, 13 Oct 2011 14:42:10 +0000 (16:42 +0200)]
logging: use _OBJECT variants more

9 years agobuffer: Use an inline function instead of a macro for gst_buffer_replace()
Sebastian Dröge [Thu, 13 Oct 2011 08:19:34 +0000 (10:19 +0200)]
buffer: Use an inline function instead of a macro for gst_buffer_replace()

This gives us type checks by the compiler and more useful compiler errors.

9 years agoevent: Use an inline function instead of a macro for gst_event_replace()
Sebastian Dröge [Thu, 13 Oct 2011 08:18:51 +0000 (10:18 +0200)]
event: Use an inline function instead of a macro for gst_event_replace()

This gives us type checks by the compiler and more useful compiler errors.

9 years agobasesrc: properly adjust start time
Wim Taymans [Wed, 12 Oct 2011 15:17:09 +0000 (17:17 +0200)]
basesrc: properly adjust start time

When we do a non-flushing seek and closed the current segment,
make sure that we open the next segment from where we closed.

9 years agoutils: catch invalid instance sizes in gst_type_register_static_full()
Tim-Philipp Müller [Mon, 10 Oct 2011 18:41:33 +0000 (19:41 +0100)]
utils: catch invalid instance sizes in gst_type_register_static_full()

Add guards to catch overly large instance sizes.

https://bugzilla.gnome.org/show_bug.cgi?id=660955

9 years agogstparse: prefix generated parser functions so they don't get exported
Tim-Philipp Müller [Sat, 8 Oct 2011 13:17:25 +0000 (14:17 +0100)]
gstparse: prefix generated parser functions so they don't get exported

Don't export those 35-something random _gst_parse_yy* symbols. These were
never in any header files and also blacklisted from our .def files, in
case anyone wonders.

9 years agopipeline: Use pipeline category for one more log message
Thiago Santos [Fri, 7 Oct 2011 12:45:20 +0000 (09:45 -0300)]
pipeline: Use pipeline category for one more log message

Makes debugging easier.

9 years agoGST_PTR_FORMAT: Add GstBuffer ptr format and use in GST_SCHEDULING
Robert Swain [Fri, 7 Oct 2011 14:36:10 +0000 (16:36 +0200)]
GST_PTR_FORMAT: Add GstBuffer ptr format and use in GST_SCHEDULING

GstBuffer pointers can now be printed using GST_PTR_FORMAT. This is used
in the very useful GST_SCHEDULING debug logs in gstpad.c and allows for
easier and more information tracking of buffer progress through a
pipeline with just debug logging.

9 years agobaseparse: send duration message when updating internal duration
Mark Nauwelaerts [Thu, 6 Oct 2011 12:34:09 +0000 (14:34 +0200)]
baseparse: send duration message when updating internal duration

9 years agobaseparse: Return success if optional start/stop method is not provided
Stas Sergeev [Mon, 26 Sep 2011 10:36:46 +0000 (14:36 +0400)]
baseparse: Return success if optional start/stop method is not provided

This allows to not implement the optional start/stop methods.

9 years agogstquery: Make debugging message more informative
Edward Hervey [Mon, 3 Oct 2011 07:29:10 +0000 (09:29 +0200)]
gstquery: Make debugging message more informative

For all the newcomers out there who still don't know the values of
GstQueryType enum by heart...
... and old-timers who've got better things to do :)

9 years agobaseparse: make estimating the position in query handler actually work
Tim-Philipp Müller [Fri, 30 Sep 2011 14:25:20 +0000 (15:25 +0100)]
baseparse: make estimating the position in query handler actually work

No point estimating if we don't set the result afterwards.

9 years agobaseparse: answer position query in stream time and try upstream first
Vincent Penquerc'h [Mon, 26 Sep 2011 12:14:42 +0000 (13:14 +0100)]
baseparse: answer position query in stream time and try upstream first

Let the demuxer have first say as well.

https://bugzilla.gnome.org/show_bug.cgi?id=659485

9 years agogst.h: include header for atomic queue
Tim-Philipp Müller [Fri, 30 Sep 2011 13:52:01 +0000 (14:52 +0100)]
gst.h: include header for atomic queue

9 years agotests: add minimal test for GstAtomicQueue
Tim-Philipp Müller [Fri, 30 Sep 2011 13:50:51 +0000 (14:50 +0100)]
tests: add minimal test for GstAtomicQueue

Just new + free.

9 years agobasetransform: send delayed events earlier
Vincent Penquerc'h [Mon, 26 Sep 2011 18:52:13 +0000 (19:52 +0100)]
basetransform: send delayed events earlier

Some elements (such as videorate) might push buffers early,
for instance in in transform_ip. We want events (and in particular
any NEWSEGMENT event) to be pushed before that.

This fixes transmageddon wedging on converting a file starting
with a non zero offset to Ogg.

https://bugzilla.gnome.org/show_bug.cgi?id=660165

9 years agogst: Fix compiler warnings on 64 bit mingw-w64
Raimo Järvi [Sun, 25 Sep 2011 21:30:47 +0000 (00:30 +0300)]
gst: Fix compiler warnings on 64 bit mingw-w64

Fixes bug #660083.

9 years agoexamples: fix bogus g_object_unref in helloworld example
Tim-Philipp Müller [Sun, 25 Sep 2011 15:10:53 +0000 (16:10 +0100)]
examples: fix bogus g_object_unref in helloworld example

GMainLoop is not a GObject.

https://bugzilla.gnome.org/show_bug.cgi?id=424143

9 years agobasetransform: delay serialized events when src caps are not set yet
Vincent Penquerc'h [Tue, 20 Sep 2011 12:04:06 +0000 (13:04 +0100)]
basetransform: delay serialized events when src caps are not set yet

https://bugzilla.gnome.org/show_bug.cgi?id=659571

9 years agopad: Set caps on pad before checking if the pad is linked
Stas Sergeev [Tue, 13 Sep 2011 13:04:31 +0000 (17:04 +0400)]
pad: Set caps on pad before checking if the pad is linked

This allows the setcaps handler and notify::caps to link
the pad downstream and doesn't require hacks to always
provide a peer to the pad, like in decodebin2.

9 years agocaps: use g_value_take_string() and gst_value_get_caps() instead of accessing interna...
Fabrizio (Misto) Milo [Thu, 15 Sep 2011 18:49:43 +0000 (11:49 -0700)]
caps: use g_value_take_string() and gst_value_get_caps() instead of accessing internal fields

9 years agopad: add more debug logging for other chain function code path as well
Tim-Philipp Müller [Fri, 16 Sep 2011 12:38:41 +0000 (13:38 +0100)]
pad: add more debug logging for other chain function code path as well