glsdk/gstreamer0-10.git
9 years agoMultiarch backward comaptibility.
Nikhil Devshatwar [Wed, 15 May 2013 12:22:36 +0000 (17:52 +0530)]
Multiarch backward comaptibility.

9 years agobaseparse: do not wait for more data when draining, it will never come
Vincent Penquerc'h [Wed, 20 Jun 2012 11:44:33 +0000 (11:44 +0000)]
baseparse: do not wait for more data when draining, it will never come

9 years agobaseparse: print unsigned values as unsigned values
Vincent Penquerc'h [Tue, 19 Jun 2012 09:35:49 +0000 (09:35 +0000)]
baseparse: print unsigned values as unsigned values

Avoids G_MAXUINT confusingly being printed as -1, among others.

9 years agoutils: add quark and mini-object boilerplate macros
Rob Clark [Wed, 13 Jun 2012 23:54:51 +0000 (18:54 -0500)]
utils: add quark and mini-object boilerplate macros

9 years agohack: disable buffer writability check
Rob Clark [Wed, 13 Jun 2012 23:53:29 +0000 (18:53 -0500)]
hack: disable buffer writability check

For private buffer metadata (ie. elements that attach their own private
bookkeeping data to a buffer), we don't care about preserving immutability
semantics of a buffer..

9 years agobasetransform: don't do unnecessary pad_alloc()
Rob Clark [Wed, 26 May 2010 19:42:40 +0000 (14:42 -0500)]
basetransform: don't do unnecessary pad_alloc()

Don't allocate a buffer in passthrough mode.

9 years agoRefresh gstreamer-sections.txt
Alessandro Decina [Fri, 6 May 2011 07:29:46 +0000 (09:29 +0200)]
Refresh gstreamer-sections.txt

9 years agoAdd GST_EVENT_LIVE_FLUSH.
Alessandro Decina [Fri, 6 May 2011 06:40:26 +0000 (08:40 +0200)]
Add GST_EVENT_LIVE_FLUSH.

This is needed by live sources to unblock buffer_alloc going from PLAYING to
PAUSED.

Currently basesrc assumes that ::create can always be unblocked. When going from
PLAYING to PAUSED it can happen that a live source is blocked in a buffer_alloc
call and so we need a way to unblock it.

9 years agoAdd GstEventCrop event
Rob Clark [Mon, 24 May 2010 21:49:20 +0000 (16:49 -0500)]
Add GstEventCrop event

This event can be used to set cropping / region-of-interest to take effect
on the following buffer.

9 years agoadd GstQueryBuffers query
Rob Clark [Wed, 19 May 2010 20:48:09 +0000 (15:48 -0500)]
add GstQueryBuffers query

This query is used by buffer allocator, for example a video sink element,
to find out any minimum buffer requirements of upstream elements that uses
pad_alloc() to allocate buffers.  For example, some cameras may have need
for additional padding/boarder around the frame (for vstab), or some video
decoders may have requirements for a certain minimum number of buffers (so
they can hold refs to reference-frames)

9 years agoChanges to make it possible to LD_PRELOAD libttif
Rob Clark [Sun, 4 Apr 2010 14:14:34 +0000 (09:14 -0500)]
Changes to make it possible to LD_PRELOAD libttif

1) if GST_USING_PRINTF_EXTENSION, then prepend the fmt string with "<%P> " and
pass object as a normal arg.  When using TTIF, you want the whole fmt string,
including the object name prefix, to be constant.  This way, only the fmt
string pointer needs to be logged.
2) GstDebugTraceLocation: small optimization to stash __FILE__, __LINE__, and
GST_FUNCTION together and pass as a single ptr.. the optimization is probably
lost in the noise with the default printf() based traces, but makes more of a
difference with faster trace systems

Incorporate modifications by Ricardo Salveti de Araujo in order to work out
some errors from recent versions of GStreamer.

9 years agogst-launch: add --loop argument
Rob Clark [Sat, 13 Feb 2010 21:29:13 +0000 (15:29 -0600)]
gst-launch: add --loop argument

if --loop is specified, automatically seek to beginning of clip when EOS is received

10 years agoRelease 0.10.36 freedesktop-RELEASE-0.10.36
Tim-Philipp Müller [Mon, 20 Feb 2012 23:11:03 +0000 (23:11 +0000)]
Release 0.10.36

10 years agopo: update translations
Tim-Philipp Müller [Mon, 20 Feb 2012 21:33:22 +0000 (21:33 +0000)]
po: update translations

10 years agobaseparse: fix reverse playback
Mark Nauwelaerts [Mon, 13 Feb 2012 17:09:51 +0000 (18:09 +0100)]
baseparse: fix reverse playback

... especially for all-keyframe (audio) cases.

10 years agobaseparse: bitrate mechanics should not deal with duration update
Mark Nauwelaerts [Tue, 7 Feb 2012 10:28:41 +0000 (11:28 +0100)]
baseparse: bitrate mechanics should not deal with duration update

... since that is already handled by _update_duration, or should not be done
altogether if the duration is determined by non-estimated means.

Fixes #669502.

10 years ago0.10.35.3 pre-release
Tim-Philipp Müller [Sun, 5 Feb 2012 13:31:36 +0000 (13:31 +0000)]
0.10.35.3 pre-release

10 years agoregistry: fix compilation with --disable-registry
Havard Graff [Wed, 4 Jan 2012 16:10:15 +0000 (17:10 +0100)]
registry: fix compilation with --disable-registry

__registry_reuse_plugin_scanner is only defined when
GST_DISABLE_REGISTRY is not defined.

gstregistry.c: In function 'gst_registry_scan_plugin_file':
gstregistry.c:1131:8: error: '__registry_reuse_plugin_scanner' undeclared (first use in this function)

https://bugzilla.gnome.org/show_bug.cgi?id=667284

10 years agobin: reset the EOS detection machinery after sending an EOS message
Vincent Penquerc'h [Thu, 2 Feb 2012 17:18:22 +0000 (17:18 +0000)]
bin: reset the EOS detection machinery after sending an EOS message

This will allow detecting further EOS, for instance after looping
a stream without changing states.

https://bugzilla.gnome.org/show_bug.cgi?id=668289

10 years agoFixes the lack of an include directive in gst/gstpreset.h
João Paulo Pizani Flor [Mon, 30 Jan 2012 16:48:44 +0000 (14:48 -0200)]
Fixes the lack of an include directive in gst/gstpreset.h

It blocked the build of external libraries depending on gstreamer-core (namely, gstreamermm).
Complete bug report at https://bugzilla.gnome.org/show_bug.cgi?id=669036

10 years agocollectpads2: Move private fields from the public structs to private structs
Sebastian Dröge [Fri, 27 Jan 2012 14:02:52 +0000 (15:02 +0100)]
collectpads2: Move private fields from the public structs to private structs

Fixes bug #668764.

10 years agobaseparse: clear adapter in reset so baseparse is reusable
Antoine Tremblay [Thu, 12 Jan 2012 19:53:11 +0000 (19:53 +0000)]
baseparse: clear adapter in reset so baseparse is reusable

GstBaseParse was not clearing its adapter on reset causing
problems when a pipeline went for example from PLAYING to NULL
state and then back to PLAYING again. The data from the last
stream would be used in the parser.

https://bugzilla.gnome.org/show_bug.cgi?id=667444

10 years agogststructure: clarify _get docs about the returned reference
Vincent Penquerc'h [Wed, 11 Jan 2012 12:19:20 +0000 (12:19 +0000)]
gststructure: clarify _get docs about the returned reference

https://bugzilla.gnome.org/show_bug.cgi?id=667689

10 years agobasesink: don't compensate for render-delay twice
Havard Graff [Tue, 29 Nov 2011 13:22:44 +0000 (14:22 +0100)]
basesink: don't compensate for render-delay twice

https://bugzilla.gnome.org/show_bug.cgi?id=667298

10 years agogst: include locale.h before any other i18n headers
Tim-Philipp Müller [Thu, 5 Jan 2012 00:30:30 +0000 (00:30 +0000)]
gst: include locale.h before any other i18n headers

This is also how we do it in -base.

https://bugzilla.gnome.org/show_bug.cgi?id=667290

10 years agoplugins: explicitly cast initialization values to the correct type
Idar Tollefsen [Sun, 1 Jan 2012 15:47:14 +0000 (16:47 +0100)]
plugins: explicitly cast initialization values to the correct type

https://bugzilla.gnome.org/show_bug.cgi?id=667288

10 years agopoll: include correct poll.h based on autoconf test
Idar Tollefsen [Sun, 1 Jan 2012 19:17:41 +0000 (20:17 +0100)]
poll: include correct poll.h based on autoconf test

https://bugzilla.gnome.org/show_bug.cgi?id=667286

10 years agoconfigure: check for sys/poll.h
Tim-Philipp Müller [Wed, 4 Jan 2012 23:46:19 +0000 (23:46 +0000)]
configure: check for sys/poll.h

https://bugzilla.gnome.org/show_bug.cgi?id=667286

10 years agoAutomatic update of common submodule
Tim-Philipp Müller [Wed, 4 Jan 2012 19:38:30 +0000 (19:38 +0000)]
Automatic update of common submodule

From 59a7a68 to cb5da59

10 years agoAutomatic update of common submodule
Tim-Philipp Müller [Wed, 4 Jan 2012 19:25:50 +0000 (19:25 +0000)]
Automatic update of common submodule

From e4a9407 to 59a7a68

10 years agoconvert Makefile spaces to tabs
David Schleef [Sun, 1 Jan 2012 01:37:20 +0000 (17:37 -0800)]
convert Makefile spaces to tabs

10 years agofilesrc: return any remaining data on EOS before returning FLOW_UNEXPECTED
Tim-Philipp Müller [Sun, 25 Dec 2011 12:39:49 +0000 (12:39 +0000)]
filesrc: return any remaining data on EOS before returning FLOW_UNEXPECTED

10 years agofilesrc: minor cosmetic changes
Tim-Philipp Müller [Sun, 25 Dec 2011 12:29:46 +0000 (12:29 +0000)]
filesrc: minor cosmetic changes

Rename woffset variable, maintain separate bytes_read in addition
to length variable.

10 years agobasetransform: suggestion compatible with upstream is not much of a suggestion
Mark Nauwelaerts [Mon, 19 Dec 2011 11:33:18 +0000 (12:33 +0100)]
basetransform: suggestion compatible with upstream is not much of a suggestion

... in that upstream is already complying with that suggestion.

Fixes #666174.

10 years agocollectpads2: delay collecting buffer if a pad newly set waiting
Mark Nauwelaerts [Thu, 15 Dec 2011 13:31:05 +0000 (14:31 +0100)]
collectpads2: delay collecting buffer if a pad newly set waiting

... as commented; make code correspond to it (again).

10 years agofilesrc: do not mistake short reads for EOS
Vincent Penquerc'h [Mon, 12 Dec 2011 13:05:36 +0000 (13:05 +0000)]
filesrc: do not mistake short reads for EOS

While local filesystems will usually not cause short reads,
this may happen on seekable files on some remote filesystems.
Instead, loop till we get the requested amount of data, or
an actual EOS (ie, 0 bytes).

https://bugzilla.gnome.org/show_bug.cgi?id=665921

10 years agoglib-compat: Add license boilerplate for LGPL
Sebastian Dröge [Mon, 12 Dec 2011 10:54:56 +0000 (11:54 +0100)]
glib-compat: Add license boilerplate for LGPL

10 years ago0.10.35.2 pre-release
Tim-Philipp Müller [Sat, 10 Dec 2011 01:04:10 +0000 (01:04 +0000)]
0.10.35.2 pre-release

10 years agopo: update translations
Tim-Philipp Müller [Sat, 10 Dec 2011 01:16:05 +0000 (01:16 +0000)]
po: update translations

10 years agopreset: allow applications to specify an extra preset dir
Stefan Sauer [Wed, 7 Dec 2011 15:01:07 +0000 (16:01 +0100)]
preset: allow applications to specify an extra preset dir

An extra application preset dir help to organize presets created for special
purposes. Fixes #660760
API: gst_preset_set_app_dir(), gst_preset_get_app_dir()

10 years agobasetransform: Fix code path to come up with possible caps if incompatible caps are...
Sebastian Dröge [Thu, 8 Dec 2011 17:00:00 +0000 (18:00 +0100)]
basetransform: Fix code path to come up with possible caps if incompatible caps are provided to buffer_alloc()

Previous code could almost never work and this should be slightly
better.

10 years agobasetransform: Fall back to upstream provided caps if suggested caps are not supporte...
Sebastian Dröge [Thu, 8 Dec 2011 16:21:30 +0000 (17:21 +0100)]
basetransform: Fall back to upstream provided caps if suggested caps are not supported by the sinkpad

10 years agobasetransform: Fall back to upstream provided caps if fixation of suggested caps...
Sebastian Dröge [Thu, 8 Dec 2011 16:07:05 +0000 (17:07 +0100)]
basetransform: Fall back to upstream provided caps if fixation of suggested caps failed

10 years agobasetransform: Refactor gst_base_transform_buffer_alloc() code
Sebastian Dröge [Thu, 8 Dec 2011 16:02:28 +0000 (17:02 +0100)]
basetransform: Refactor gst_base_transform_buffer_alloc() code

Don't check if upstream provided caps are compatible with upstream
and don't try to fixate these caps. They must be fixated in any case.

10 years agobaseparse: do not use a byte value instead of a time value when bisecting
Vincent Penquerc'h [Wed, 7 Dec 2011 17:57:49 +0000 (17:57 +0000)]
baseparse: do not use a byte value instead of a time value when bisecting

This fixes FLAC seeking on some FLAC files.

10 years agoselector: Push newsegment events before any buffers are pushed in the unit test
Sebastian Dröge [Wed, 7 Dec 2011 10:04:42 +0000 (11:04 +0100)]
selector: Push newsegment events before any buffers are pushed in the unit test

10 years agoinputselector: Don't send a NEWSEGMENT event if a buffer arrived before the segment...
Sebastian Dröge [Wed, 7 Dec 2011 10:01:49 +0000 (11:01 +0100)]
inputselector: Don't send a NEWSEGMENT event if a buffer arrived before the segment was configured

10 years agooutputselector: Don't send last segment/buffer when no segment was configured yet
Sebastian Dröge [Wed, 7 Dec 2011 10:01:31 +0000 (11:01 +0100)]
outputselector: Don't send last segment/buffer when no segment was configured yet

10 years agobasetransform: If suggested caps are not compatible with upstream try to come up...
Sebastian Dröge [Wed, 7 Dec 2011 08:50:40 +0000 (09:50 +0100)]
basetransform: If suggested caps are not compatible with upstream try to come up with compatible caps

Fixes bug #662199.

10 years agoindexfactory: fix memory leak
Tim-Philipp Müller [Tue, 6 Dec 2011 23:52:53 +0000 (23:52 +0000)]
indexfactory: fix memory leak

Introduced by commit bd302bb6 pluginfeature: avoid duplicating feature->name

https://bugzilla.gnome.org/show_bug.cgi?id=459466
https://bugzilla.gnome.org/show_bug.cgi?id=665703

10 years agofakesink: Make event/buffer verbose output consistent with identity
Sebastian Dröge [Tue, 6 Dec 2011 13:55:15 +0000 (14:55 +0100)]
fakesink: Make event/buffer verbose output consistent with identity

10 years agoidentity: Print buffer flags in the verbose output
Sebastian Dröge [Tue, 6 Dec 2011 13:55:11 +0000 (14:55 +0100)]
identity: Print buffer flags in the verbose output

10 years agofakesrc: Make event/buffer verbose output consistent with identity and print buffer...
Sebastian Dröge [Tue, 6 Dec 2011 13:53:47 +0000 (14:53 +0100)]
fakesrc: Make event/buffer verbose output consistent with identity and print buffer flags

10 years agocheck: allow non-joinable threads in private g_thread_create() copy
Tim-Philipp Müller [Sun, 4 Dec 2011 21:19:04 +0000 (21:19 +0000)]
check: allow non-joinable threads in private g_thread_create() copy

Looks like some tests use non-joinable threads after all.

10 years agoSuppress deprecation warnings in selected files, for g_static_rec_mutex_* mostly
Tim-Philipp Müller [Sun, 4 Dec 2011 14:38:26 +0000 (14:38 +0000)]
Suppress deprecation warnings in selected files, for g_static_rec_mutex_* mostly

GStaticRecMutex is part of our API/ABI, not much we can do here in 0.10.

10 years agoWork around deprecated thread API in glib master
Tim-Philipp Müller [Sun, 4 Dec 2011 13:35:38 +0000 (13:35 +0000)]
Work around deprecated thread API in glib master

Add private replacements for deprecated functions such as
g_mutex_new(), g_mutex_free(), g_cond_new() etc., mostly
to avoid the deprecation warnings. We can't change most of
these in 0.10 because they're part of our API and ABI.

10 years agobenchmarks: g_thread_create() is deprecated in GLib master, use g_thread_try_new...
Tim-Philipp Müller [Sun, 4 Dec 2011 13:09:53 +0000 (13:09 +0000)]
benchmarks: g_thread_create() is deprecated in GLib master, use g_thread_try_new() instead

10 years agonet: initialise GError variables to NULL
Tim-Philipp Müller [Sun, 4 Dec 2011 13:04:35 +0000 (13:04 +0000)]
net: initialise GError variables to NULL

10 years agog_thread_init() is deprecated in glib master
Tim-Philipp Müller [Sat, 3 Dec 2011 17:40:53 +0000 (17:40 +0000)]
g_thread_init() is deprecated in glib master

It's not needed any longer.

10 years agotagsetter: update for thread API deprecations in glib master
Tim-Philipp Müller [Sat, 3 Dec 2011 16:02:36 +0000 (16:02 +0000)]
tagsetter: update for thread API deprecations in glib master

10 years agotaglist: update for thread API deprecations in glib master
Tim-Philipp Müller [Sat, 3 Dec 2011 15:36:58 +0000 (15:36 +0000)]
taglist: update for thread API deprecations in glib master

10 years agog_thread_create() is deprecated in GLib master, use g_thread_try_new() instead
Tim-Philipp Müller [Sat, 3 Dec 2011 13:58:51 +0000 (13:58 +0000)]
g_thread_create() is deprecated in GLib master, use g_thread_try_new() instead

10 years agoidentity: unlock clock wait when appropriate
Mark Nauwelaerts [Fri, 2 Dec 2011 12:19:38 +0000 (13:19 +0100)]
identity: unlock clock wait when appropriate

... notably FLUSH and state change to READY.

10 years agobus: use GST_MESSAGE_SOURCE_NAME() which also takes care of src=NULL.
Stefan Sauer [Thu, 1 Dec 2011 15:25:07 +0000 (16:25 +0100)]
bus: use GST_MESSAGE_SOURCE_NAME() which also takes care of src=NULL.

10 years agobasetransform: Always intersect the suggested sink caps with the peer caps
Sebastian Dröge [Wed, 30 Nov 2011 12:59:46 +0000 (13:59 +0100)]
basetransform: Always intersect the suggested sink caps with the peer caps

This makes sure that we get correct and complete caps. The suggested caps
could be incomplete, e.g. video/x-raw-rgb without any fields, and by
intersecting with the peer caps we get something usable.

Fixes bug #662199.

10 years agoevent: warn and fail instead of creating newsegment events in GST_FORMAT_UNDEFINED
Tim-Philipp Müller [Wed, 30 Nov 2011 00:24:32 +0000 (00:24 +0000)]
event: warn and fail instead of creating newsegment events in GST_FORMAT_UNDEFINED

10 years agogstelement: add gst_element_class_add_pad_template_from_static
Vincent Penquerc'h [Mon, 28 Nov 2011 12:30:15 +0000 (12:30 +0000)]
gstelement: add gst_element_class_add_pad_template_from_static

This function helps ensure the pad template is unreffed
without having to complicate the calling code.

https://bugzilla.gnome.org/show_bug.cgi?id=662664

10 years agoqueue2: fix refactoring of draining-on-eos, munge flow return to FLOW_OK
Tim-Philipp Müller [Mon, 28 Nov 2011 01:10:20 +0000 (01:10 +0000)]
queue2: fix refactoring of draining-on-eos, munge flow return to FLOW_OK

10 years agoqueue2: add bufferlist support
Tim-Philipp Müller [Thu, 3 Nov 2011 10:34:49 +0000 (10:34 +0000)]
queue2: add bufferlist support

We want to maintain buffer lists if possible.

10 years agoqueue2: split out draining of queue on FLOW_UNEXPECTED into separate function
Tim-Philipp Müller [Thu, 3 Nov 2011 13:02:36 +0000 (13:02 +0000)]
queue2: split out draining of queue on FLOW_UNEXPECTED into separate function

10 years agoqueue2: pass item type enum to _enqueue instead of simple isbuffer boolean
Tim-Philipp Müller [Thu, 3 Nov 2011 08:55:20 +0000 (08:55 +0000)]
queue2: pass item type enum to _enqueue instead of simple isbuffer boolean

Avoids some unnecessary GST_IS_EVENT()

10 years agowarnings: avoid set-but-unused warnings with load-save disabled
Stefan Sauer [Sun, 27 Nov 2011 19:36:31 +0000 (20:36 +0100)]
warnings: avoid set-but-unused warnings with load-save disabled

10 years agouri: fix wrong G_GNUC_MALLOC
Tim-Philipp Müller [Sat, 26 Nov 2011 19:45:48 +0000 (19:45 +0000)]
uri: fix wrong G_GNUC_MALLOC

_get_protocols() points to const memory in 0.10
despite the non-const return value.

10 years agolibs: sprinkle some G_GNUC_MALLOC
Tim-Philipp Müller [Sat, 26 Nov 2011 18:58:38 +0000 (18:58 +0000)]
libs: sprinkle some G_GNUC_MALLOC

Maybe gcc can do something clever with that, or at least
warn us if we don't save the return value somewhere.

10 years agogst: sprinkle some G_GNUC_MALLOC
Tim-Philipp Müller [Sat, 26 Nov 2011 18:57:44 +0000 (18:57 +0000)]
gst: sprinkle some G_GNUC_MALLOC

Maybe gcc can do something clever with that, or at least
warn us if we don't save the return value somewhere.

10 years agobuffer: add gst_buffer_{set,get}_qdata()
Tim-Philipp Müller [Wed, 16 Nov 2011 01:04:45 +0000 (01:04 +0000)]
buffer: add gst_buffer_{set,get}_qdata()

Allows people/us to attach arbitrary metadata to buffers.

https://bugzilla.gnome.org/show_bug.cgi?id=664720

API: gst_buffer_set_qdata()
API: get_buffer_get_qdata()

10 years agopad: Remove g_warning() if pad accepted caps that are not a subset of the pad caps
Sebastian Dröge [Thu, 24 Nov 2011 10:15:29 +0000 (11:15 +0100)]
pad: Remove g_warning() if pad accepted caps that are not a subset of the pad caps

This check is correct but unfortunately it's impossible to implement
in a threadsafe way because the caps could have changed in the meantime.

Fixes bug #659606.

10 years agomultiqueue: check filled state of queues even if another one is empty
Vincent Penquerc'h [Mon, 3 Oct 2011 11:34:20 +0000 (12:34 +0100)]
multiqueue: check filled state of queues even if another one is empty

This will avoid a case where overrun is never signalled if some
stream never produces any data, causing playbin2 to not end preroll.

https://bugzilla.gnome.org/show_bug.cgi?id=660778

10 years agobaseparse: Return template caps instead of other side's peer caps if get_sink_caps...
Sebastian Dröge [Wed, 23 Nov 2011 12:42:56 +0000 (13:42 +0100)]
baseparse: Return template caps instead of other side's peer caps if get_sink_caps vfunc is not implemented

Using gst_pad_proxy_get_caps() breaks backwards compatibility with old
parsers because it will propagate the other side's fields like "parsed"
and "framed" and also breaks parser/converters.

Fixes bug #664221.

10 years agogst-inspect: print current value as default value
Tim-Philipp Müller [Sat, 12 Nov 2011 16:42:14 +0000 (16:42 +0000)]
gst-inspect: print current value as default value

Instead of printing separate 'Current' and 'Default' values
(the former obtained via g_object_get() and the latter from
the property GParamSpec), simply print the Current value as
the Default value. This is the right thing to do for almost
all elements and avoids confusion if a subclass of a base
class chooses a different default than the base class.

10 years agogst, controller: replace g_list_prepend + reverse with GQueue
Tim-Philipp Müller [Sat, 12 Nov 2011 14:55:07 +0000 (14:55 +0000)]
gst, controller: replace g_list_prepend + reverse with GQueue

10 years agoAndroid: build audio controller example
Stefan Sauer [Wed, 9 Nov 2011 10:05:59 +0000 (11:05 +0100)]
Android: build audio controller example

Add buildsystem hooks for building the audiocontroller example
with the NDK.

Signed-off-by: Reynaldo H. Verdejo Pinochet <reynaldo@collabora.com>
10 years agogstvalue: consider lists and ranges equal if they hold the same set
Vincent Penquerc'h [Tue, 8 Nov 2011 18:09:28 +0000 (18:09 +0000)]
gstvalue: consider lists and ranges equal if they hold the same set

This fixes caps operations when different elements advertise some
of their caps' properties differently (eg, for audio channels, either
a range from 1 to 2, or a list of 1 and 2).

https://bugzilla.gnome.org/show_bug.cgi?id=663643

10 years agotests: add a subset test for structure
Stefan Sauer [Wed, 9 Nov 2011 10:24:26 +0000 (11:24 +0100)]
tests: add a subset test for structure

10 years agodocs: also fix wrong call order for controller in manual
Stefan Sauer [Fri, 28 Oct 2011 11:39:58 +0000 (13:39 +0200)]
docs: also fix wrong call order for controller in manual

10 years agotests: pad: add test to verify flushing behaviour
René Stadler [Tue, 8 Nov 2011 11:22:21 +0000 (12:22 +0100)]
tests: pad: add test to verify flushing behaviour

Seems like a trivial case, but this was actually broken in 0.11 recently.

10 years agodocs: fix Since: markers for API added after 0.10.35
Tim-Philipp Müller [Tue, 8 Nov 2011 00:32:36 +0000 (00:32 +0000)]
docs: fix Since: markers for API added after 0.10.35

10 years agowin32: update .def file for new API
Tim-Philipp Müller [Tue, 8 Nov 2011 00:15:49 +0000 (00:15 +0000)]
win32: update .def file for new API

API: gst_caps_is_strictly_equal()

10 years agogstcaps: remove unneeded use of gint64
Vincent Penquerc'h [Thu, 27 Oct 2011 11:59:57 +0000 (12:59 +0100)]
gstcaps: remove unneeded use of gint64

https://bugzilla.gnome.org/show_bug.cgi?id=662777

10 years agogstvalue: quicker version of intersection when we do not need the result
Vincent Penquerc'h [Thu, 27 Oct 2011 11:24:13 +0000 (12:24 +0100)]
gstvalue: quicker version of intersection when we do not need the result

https://bugzilla.gnome.org/show_bug.cgi?id=662777

10 years agogststructure: simplify return statement in gst_structure_can_intersect
Vincent Penquerc'h [Thu, 27 Oct 2011 11:02:43 +0000 (12:02 +0100)]
gststructure: simplify return statement in gst_structure_can_intersect

https://bugzilla.gnome.org/show_bug.cgi?id=662777

10 years agogststructure: early out when we know a value cannot be a subset
Vincent Penquerc'h [Thu, 27 Oct 2011 10:41:30 +0000 (11:41 +0100)]
gststructure: early out when we know a value cannot be a subset

If two values can be ordered, but are unequal, they are
necessarily distinct, thus one cannot be a subset of the other.

https://bugzilla.gnome.org/show_bug.cgi?id=662777

10 years agogstvalue: quicker test for substraction emptiness
Vincent Penquerc'h [Thu, 27 Oct 2011 09:35:53 +0000 (10:35 +0100)]
gstvalue: quicker test for substraction emptiness

When we do not care about the actual resulting set,
but only whether it is empty of not, we can skip a fair bit
of GValue juggling.

Add a function that does so, since we cannot just pass NULL
to the existing API as it may be part of the API contract.

https://bugzilla.gnome.org/show_bug.cgi?id=662777

10 years agogststructure: rejig test ordering for speed
Vincent Penquerc'h [Thu, 27 Oct 2011 08:45:41 +0000 (09:45 +0100)]
gststructure: rejig test ordering for speed

https://bugzilla.gnome.org/show_bug.cgi?id=662777

10 years agobasetransform: Only use the cached transform on strictly equal caps
Sjoerd Simons [Thu, 3 Nov 2011 15:36:59 +0000 (15:36 +0000)]
basetransform: Only use the cached transform on strictly equal caps

https://bugzilla.gnome.org/show_bug.cgi?id=663333

10 years agocaps: Add gst_caps_is_strictly_equal
Sjoerd Simons [Thu, 3 Nov 2011 15:35:32 +0000 (15:35 +0000)]
caps: Add gst_caps_is_strictly_equal

10 years agointrospection: add Value annotations for GST_SECOND, GST_MSECOND, GST_USECOND, GST_NS...
Peteris Krisjanis [Sat, 15 Oct 2011 19:52:25 +0000 (22:52 +0300)]
introspection: add Value annotations for GST_SECOND, GST_MSECOND, GST_USECOND, GST_NSECOND constants

gobject-introspection won't parse them properly otherwise.

Still need to force the right type though (either GstClockTime or
guint64), but Type: xyz has no effect for me here, so someone with
a newer g-i needs to test this.

Some other defines are also missing, e.g. GST_CLOCK_TIME_NONE.

10 years agoconfigure: suppress unused variable warnings if gst debugging is disabled
Tim-Philipp Müller [Fri, 4 Nov 2011 00:03:05 +0000 (00:03 +0000)]
configure: suppress unused variable warnings if gst debugging is disabled

https://bugzilla.gnome.org/show_bug.cgi?id=662952

10 years agoconfigure: fix typo around GLIB_EXTRA_CFLAGS in GST_ALL_CXXFLAGS
Tim-Philipp Müller [Fri, 4 Nov 2011 00:02:07 +0000 (00:02 +0000)]
configure: fix typo around GLIB_EXTRA_CFLAGS in GST_ALL_CXXFLAGS

10 years agoqueue: use statically allocated GQueue
Tim-Philipp Müller [Thu, 3 Nov 2011 23:08:52 +0000 (23:08 +0000)]
queue: use statically allocated GQueue