From 039b9656692478d6fcd7a65c227b59eb12b75e83 Mon Sep 17 00:00:00 2001 From: Rob Clark Date: Wed, 19 May 2010 15:48:09 -0500 Subject: [PATCH] add GstQueryBuffers query This query is used by buffer allocator, for example a video sink element, to find out any minimum buffer requirements of upstream elements that uses pad_alloc() to allocate buffers. For example, some cameras may have need for additional padding/boarder around the frame (for vstab), or some video decoders may have requirements for a certain minimum number of buffers (so they can hold refs to reference-frames) --- gst/gstquark.c | 3 +- gst/gstquark.h | 7 ++- gst/gstquery.c | 141 +++++++++++++++++++++++++++++++++++++++++++++++++ gst/gstquery.h | 16 +++++- 4 files changed, 164 insertions(+), 3 deletions(-) diff --git a/gst/gstquark.c b/gst/gstquark.c index 91a201271..0459b4e2c 100644 --- a/gst/gstquark.c +++ b/gst/gstquark.c @@ -50,7 +50,8 @@ static const gchar *_quark_strings[] = { "intermediate", "GstMessageStepStart", "active", "eos", "sink-message", "message", "GstMessageQOS", "running-time", "stream-time", "jitter", "quality", "processed", "dropped", "buffering-ranges", "GstMessageProgress", - "code", "text", "percent", "timeout" + "code", "text", "percent", "timeout", + "GstQueryBuffers", "caps", "count", "width", "height" }; GQuark _priv_gst_quark_table[GST_QUARK_MAX]; diff --git a/gst/gstquark.h b/gst/gstquark.h index 6e16ee5d7..350f9fc68 100644 --- a/gst/gstquark.h +++ b/gst/gstquark.h @@ -132,8 +132,13 @@ typedef enum _GstQuarkId GST_QUARK_TEXT = 103, GST_QUARK_PERCENT = 104, GST_QUARK_TIMEOUT = 105, + GST_QUARK_QUERY_BUFFERS = 106, + GST_QUARK_CAPS = 107, + GST_QUARK_COUNT = 108, + GST_QUARK_WIDTH = 109, + GST_QUARK_HEIGHT = 110, - GST_QUARK_MAX = 106 + GST_QUARK_MAX = 111 } GstQuarkId; extern GQuark _priv_gst_quark_table[GST_QUARK_MAX]; diff --git a/gst/gstquery.c b/gst/gstquery.c index 2b1c38229..1d7f5f99b 100644 --- a/gst/gstquery.c +++ b/gst/gstquery.c @@ -96,6 +96,7 @@ static GstQueryTypeDefinition standard_definitions[] = { {GST_QUERY_BUFFERING, "buffering", "Buffering status", 0}, {GST_QUERY_CUSTOM, "custom", "Custom query", 0}, {GST_QUERY_URI, "uri", "URI of the source or sink", 0}, + {GST_QUERY_BUFFERS, "buffers", "Minimum buffer requirements", 0}, {GST_QUERY_NONE, NULL, NULL, 0} }; @@ -1490,3 +1491,143 @@ gst_query_parse_uri (GstQuery * query, gchar ** uri) *uri = g_value_dup_string (gst_structure_id_get_value (query->structure, GST_QUARK (URI))); } + +/** + * gst_query_new_buffers: + * @caps: the #GstCaps for the buffers that are going to be allocated + * + * Constructs a new buffer requirements query object to query buffer + * requirements for a particular caps. Use gst_query_unref() when done + * with it. + * + * Returns: A #GstQuery + */ +GstQuery * +gst_query_new_buffers (GstCaps * caps) +{ + GstQuery *query; + GstStructure *structure; + + /* XXX could add size here, for linear (non YUV/RGB) buffers? But I'm not + * entirely sure what is the use-case for that.. it should be easy enough + * to add more optional reply fields later + */ + structure = gst_structure_id_new (GST_QUARK (QUERY_BUFFERS), + GST_QUARK (CAPS), GST_TYPE_CAPS, caps, + GST_QUARK (COUNT), G_TYPE_INT, -1, + GST_QUARK (WIDTH), G_TYPE_INT, -1, + GST_QUARK (HEIGHT), G_TYPE_INT, -1, NULL); + + query = gst_query_new (GST_QUERY_BUFFERS, structure); + + return query; +} + +/** + * gst_query_set_buffers_count: + * @count: minimum number of buffers required + * + * Answer a buffers query by setting the minimum number of buffers required. + * If there is no minimum buffer count requirement, don't set this field in + * the query. + */ +void +gst_query_set_buffers_count (GstQuery * query, gint count) +{ + GstStructure *structure; + + g_return_if_fail (GST_QUERY_TYPE (query) == GST_QUERY_BUFFERS); + + structure = gst_query_get_structure (query); + gst_structure_id_set (structure, GST_QUARK (COUNT), G_TYPE_INT, count, NULL); +} + +/** + * gst_query_set_buffers_dimensions: + * @width: minimum buffer width + * @height: minimum buffer height + * + * Answer a buffers query by setting the minimum buffer dimensions required. + * If there is no minimum buffer dimensions (beyond the width/height specified + * in the #GstCaps), don't set this field in the query. + */ +void +gst_query_set_buffers_dimensions (GstQuery * query, gint width, gint height) +{ + GstStructure *structure; + + g_return_if_fail (GST_QUERY_TYPE (query) == GST_QUERY_BUFFERS); + + structure = gst_query_get_structure (query); + gst_structure_id_set (structure, + GST_QUARK (WIDTH), G_TYPE_INT, width, + GST_QUARK (HEIGHT), G_TYPE_INT, height, NULL); +} + +/** + * gst_query_parse_buffers_caps: + * @query: a #GstQuery + * @caps: the storage for the #GstCaps pointer, or NULL + * + * Parse a buffers query. + */ +void +gst_query_parse_buffers_caps (GstQuery * query, const GstCaps ** caps) +{ + GstStructure *structure; + + g_return_if_fail (GST_QUERY_TYPE (query) == GST_QUERY_BUFFERS); + + structure = gst_query_get_structure (query); + if (caps) + *caps = gst_value_get_caps (gst_structure_id_get_value (structure, + GST_QUARK (CAPS))); +} + +/** + * gst_query_parse_buffers_count: + * @query: a #GstQuery + * @count: the storage for minimum number of buffers, or NULL + * + * Parse a buffers query answer to see the minimum number of buffers + * required. A returned value of -1 means there is no minimum requirement + */ +void +gst_query_parse_buffers_count (GstQuery * query, gint * count) +{ + GstStructure *structure; + + g_return_if_fail (GST_QUERY_TYPE (query) == GST_QUERY_BUFFERS); + + structure = gst_query_get_structure (query); + if (count) + *count = g_value_get_int (gst_structure_id_get_value (structure, + GST_QUARK (COUNT))); +} + +/** + * gst_query_parse_buffers_dimensions: + * @query: a #GstQuery + * @width: the storage for minimum width, or NULL + * @height: the storage for minimum height, or NULL + * + * Parse a buffers query answer to see the minimum buffer dimensions required. + * A returned value of -1 for either dimension means there is no minimum + * requirement in that axis + */ +void +gst_query_parse_buffers_dimensions (GstQuery * query, gint * width, + gint * height) +{ + GstStructure *structure; + + g_return_if_fail (GST_QUERY_TYPE (query) == GST_QUERY_BUFFERS); + + structure = gst_query_get_structure (query); + if (width) + *width = g_value_get_int (gst_structure_id_get_value (structure, + GST_QUARK (WIDTH))); + if (height) + *height = g_value_get_int (gst_structure_id_get_value (structure, + GST_QUARK (HEIGHT))); +} diff --git a/gst/gstquery.h b/gst/gstquery.h index 2166537ef..8dd710abd 100644 --- a/gst/gstquery.h +++ b/gst/gstquery.h @@ -31,6 +31,7 @@ #include #include #include +#include G_BEGIN_DECLS @@ -51,6 +52,9 @@ G_BEGIN_DECLS * @GST_QUERY_CUSTOM: a custom application or element defined query. Since * 0.10.22. * @GST_QUERY_URI: query the URI of the source or sink. Since 0.10.22. + * @GST_QUERY_BUFFERS: query the upstream users of pad_alloc()'d buffers to + * find any particular requirements about buffer size (padding) or numbers of + * buffers. Since ?.?.?. * * Standard predefined Query types */ @@ -69,7 +73,8 @@ typedef enum { GST_QUERY_FORMATS, GST_QUERY_BUFFERING, GST_QUERY_CUSTOM, - GST_QUERY_URI + GST_QUERY_URI, + GST_QUERY_BUFFERS } GstQueryType; /** @@ -336,6 +341,15 @@ GstQuery * gst_query_new_uri (void) G_GNUC_MALLOC; void gst_query_parse_uri (GstQuery *query, gchar **uri); void gst_query_set_uri (GstQuery *query, const gchar *uri); +/* buffer requirements query */ +GstQuery * gst_query_new_buffers (GstCaps * caps); +void gst_query_set_buffers_count (GstQuery * query, gint count); +void gst_query_set_buffers_dimensions (GstQuery * query, gint width, gint height); +void gst_query_parse_buffers_caps (GstQuery * query, const GstCaps ** caps); +void gst_query_parse_buffers_count (GstQuery * query, gint * count); +void gst_query_parse_buffers_dimensions (GstQuery * query, gint * width, gint * height); + + G_END_DECLS #endif /* __GST_QUERY_H__ */ -- 2.26.2