]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - glsdk/gstreamer0-10.git/shortlog
glsdk/gstreamer0-10.git
2009-11-18 Tim-Philipp... plugin-scanner: rename plugin-scanner helper binary...
2009-11-18 Tim-Philipp... Revert "structure: don't check type twice"
2009-11-18 Stefan Koststructure: don't check type twice
2009-11-18 Sebastian Drögeevent: Add step event quark
2009-11-17 Tim-Philipp... gst-uninstalled: add paths for gst-qa-system
2009-11-17 Tim-Philipp... docs: set GST_PLUGIN_SCANNER when calling gtkdoc-scangobj
2009-11-17 Stefan Koststructure: remove some blank lines (previous gst-indent...
2009-11-17 Stefan Koststructure: use local variable earlier
2009-11-17 Stefan Koststructure: don't check enum types twice.
2009-11-16 Jan Schmidtcheck: Add a debug status to the systemclock test
2009-11-16 Wim TaymansTODO: remove stepping from TODO
2009-11-16 Wim Taymansbasesink: fix position reporting
2009-11-16 Sebastian Drögeutils: API: Add multiplication and addition functions...
2009-11-16 Sebastian Drögegstutils: API: Add fraction helper functions
2009-11-13 Stefan Kostdebug: add more debug logging to help tracking parsing...
2009-11-13 Ole André Vadla... miniobject: avoid race when recycling buffers
2009-11-12 Stefan Kostwhitespace: remove blanks in doc-comment
2009-11-12 Руслан Ижбулатовregistry: Import _priv_gst_dll_handle into gstregistry.c
2009-11-12 Руслан Ижбулатовtests: Do not list libgstcheck as a requirement for...
2009-11-11 Jan Schmidtbasesink: Fix treating base_time as unsigned in positio...
2009-11-10 Sebastian Drögeregistry: API: Add gst_{default,}_registry_get_feature_...
2009-11-10 Thiago Santosqueue2: fix printf format
2009-11-10 Thiago Santosqueue2: avoid crashing due to negative percent
2009-11-10 Thiago Santosqueue2: Fix small doc typo
2009-11-10 Tim-Philipp... registrychunks: fix compilation with debugging disabled
2009-11-09 Stefan Kostplanning: add thoughts about foreign registry cache...
2009-11-09 Stefan Kostinspect: allow to get plugin-install-info for all insta...
2009-11-09 Wim Taymansdocs: don't forget to unref the pad
2009-11-07 Tim-Philipp... gst-launch: wake up less often to check if we've been...
2009-11-05 Tim-Philipp... gstconfig.h: add define to force printf format checking...
2009-11-05 Edward Herveytests: Make sure we use the local libgstbase and not...
2009-11-05 Tim-Philipp... docs: fix typo
2009-11-05 Tim-Philipp... taglist: avoid looking up GstTagInfo twice in a row
2009-11-05 Edward Herveygstregistrychunks: We're certain plugin_name is an...
2009-11-05 Bastien Noceraimplement buffering-left argument to buffer messages
2009-11-05 Wim Taymansquery: whitespace fixes
2009-11-05 Wim Taymansghostpad: fix locking
2009-11-05 Stefan Kostghostpad: don't release mutex twice
2009-11-05 Stefan Kostghostpad: skip type check in internal api
2009-11-05 Wim Taymanspad: indentation fix
2009-11-05 Stefan Kostpad: rename new api from _refed to _reffed.
2009-11-04 Stefan Kostelement: access padtemplate list directly to avoid...
2009-11-04 Sebastian Drögeevent: Add a FIXME 0.11 for having flush events that...
2009-11-04 Jan Schmidtregistrychunks: Fix a printf compile warning on 64...
2009-11-04 Sebastian Drögeghostpad: Make sure that nobody sets the proxypad or...
2009-11-04 Jan Schmidtplugin loader: Don't fail after a short read/write
2009-11-04 Jan Schmidtplugin loader: Don't crash on bogus plugin details
2009-11-04 Jan Schmidtgst-indent: Use the same logic to find gnuindent as...
2009-11-03 Stefan Kostbuild: include stdio.h for FILE
2009-11-03 Tim-Philipp... docs: add another example to the gst-launch man page
2009-11-02 Tim-Philipp... gsttypefind: avoid one more run-time type check
2009-11-02 Sebastian Drögestructure: API: Add gst_structure_id_has_field{,_typed}
2009-11-02 Edward Herveygsttypefind: Use _CAST variants when the type has alred...
2009-11-01 Sebastian Drögeghostpad: Implement iterate internal links
2009-10-31 Sebastian Drögeparser: Make sure that signal user data is freed by...
2009-10-31 Sebastian Drögeparser: Use GSlice for allocating the structs
2009-10-31 Sebastian Drögeparser: Always get DelayedLink information from the...
2009-10-31 Edward Herveypo: queue2 has moved to core
2009-10-29 Sebastian Drögequeue2: Add to the docs
2009-10-29 Sebastian Drögequeue2: Use "Queue 2" as long name
2009-10-29 Sebastian Drögequeue2: Use GST_BOILERPLATE_FULL() and add pad template...
2009-10-29 Sebastian Drögequeue2: Use gst_element_class_set_details_simple()
2009-10-29 Sebastian Drögequeue2: Integrate into coreplugins
2009-10-29 Sebastian Drögequeue2: Move struct declarations to a separate header
2009-10-29 Sebastian Drögequeue2: Move queue2 to gstreamer coreplugins
2009-10-29 Tim-Philipp... Remove GST_DEBUG_FUNCPTR where they're pointless
2009-10-29 Wim Taymansqueue2: add custom acceptcaps function
2009-10-29 Mark Nauwelaertsqueue2: post error message when pausing task if so...
2009-10-29 Wim Taymansqueue2: fix leak and improve buffering
2009-10-29 Wim Taymansqueue2: flush differently, avoiding deadlocks
2009-10-29 Wim Taymansqueue2: add temp-template property
2009-10-29 LRNwin32: fix seeking in large files
2009-10-29 Frederic CrozatMake sure gettext returns translations in UTF-8 encodin...
2009-10-29 Stefan KostCleanup Plugin docs. Link to signals and properties...
2009-10-29 Stefan Kostgst/playback/gstqueue2.c: Do not double notify. Remove...
2009-10-29 Wim Taymansdocs/design/draft-keyframe-force.txt: Fix typo.
2009-10-29 Wim Taymansgst/playback/gstqueue2.c: Include extra buffering stats...
2009-10-29 Wim Taymansgst/playback/gstqueue2.c: Update the estimated input...
2009-10-29 Wim Taymansgst/playback/gstqueue2.c: The queue is never filled...
2009-10-29 Sebastian DrögeUse G_PARAM_STATIC_STRINGS everywhere for GParamSpecs...
2009-10-29 Wim Taymansgst/playback/gstqueue2.c: Use separate timers for input...
2009-10-29 Wim Taymansgst/playback/gstqueue2.c: Pause the timer to measure...
2009-10-29 Wim Taymansgst/playback/: Refactor some common code to filter...
2009-10-29 Wim Taymansgst/playback/: Add playbin2.
2009-10-29 Wim Taymansgst/playback/gstqueue2.c: Fix queue negotiation. See...
2009-10-29 Wim Taymansgst/playback/gstqueue2.c: Fix compilation wrt printf...
2009-10-29 Jan SchmidtFix a bunch of compile warnings shown with Forte.
2009-10-29 Wim Taymansgst/playback/gstqueue2.c: Also fix #476514 for queue2.
2009-10-29 Tim-Philipp... gst/: Printf format fixes (#465028).
2009-10-29 Wim Taymansgst/playback/gstqueue2.c: Use other metrics as well...
2009-10-29 Wim Taymansgst/playback/gstplaybasebin.c: Small debug improvement.
2009-10-29 David Schleefgst/playback/gstqueue2.c: Fix compile error from ignore...
2009-10-29 Edward Herveygst/playback/gstqueue2.c: Fix build on MacOSX.
2009-10-29 Wim Taymansgst/playback/gstqueue2.c: Fix a division by zero when...
2009-10-29 Thiago Sousa... gst/playback/gstqueue2.c: Wait for preroll before attem...
2009-10-29 Wim Taymansgst/playback/gstqueue2.c: Fix compilation.
2009-10-29 Thiago Sousa... gst/playback/gstqueue2.c: Add pull based scheduling...
2009-10-29 Wim TaymansSome more fseeko checks.
2009-10-29 Wim Taymansgst/playback/gstqueue2.c: Include stdio to define fseeko.
2009-10-29 Thiago Sousa... gst/playback/gstqueue2.c: Add support for filebased...
next