glsdk/gstreamer0-10.git
2011-01-21 Tim-Philipp... Release 0.10.32
2011-01-20 Tim-Philipp... Revert "configure: require gobject-introspection >...
2011-01-18 Tim-Philipp... docs: fix spelling of 'threshold' in app dev manual
2011-01-18 Tim-Philipp... 0.10.31.4 pre-release
2011-01-18 Tim-Philipp... gobject-introspection: try harder to make g-ir-scanner...
2011-01-14 Tim-Philipp... docs: fix garbled UTF-8 characters when generating...
2011-01-13 Tim-Philipp... gobject-introspection: another attempt to make g-i...
2011-01-12 Tim-Philipp... configure: require gobject-introspection >= 0.9.12
2011-01-12 Tim-Philipp... controller: update g-i include paths as well for header...
2011-01-11 Tim-Philipp... 0.10.31.3 pre-release
2011-01-11 Tim-Philipp... po: update translations
2011-01-11 Benjamin Ottecontroller: Fix headers to use < > in #include statements
2011-01-11 Benjamin Ottegstnet: Fix --c-include for gir generation
2011-01-11 Tim-Philipp... gobject-introspection: make g-ir-scanner try harder...
2011-01-11 Tim-Philipp... pkgconfig: also add libdir to -uninstalled .pc files
2011-01-11 Stefan KostAutomatic update of common submodule
2011-01-11 Stefan Kostvalve: fixe the property link and the sice docs
2011-01-11 Raimo Järvigstpoll: fix compiler warning with MingW
2011-01-10 Thiago Santostest: outputselector: Add another negotiation test
2011-01-10 Thiago Santosoutputselector: Improve get and set caps functions
2011-01-10 Tim-Philipp... Automatic update of common submodule
2011-01-10 Tim-Philipp... Automatic update of common submodule
2011-01-10 Thiago Santostests: selector: unref peer pad
2011-01-10 Wim Taymansbasesrc: make sure we wait and release the live lock
2011-01-10 Edward Herveyregistry: Don't replace valid existing plugins by black...
2011-01-08 Tim-Philipp... configure, gst-uninstalled: remove a few bashism
2011-01-07 Tim-Philipp... 0.10.31.2 pre-release
2011-01-07 Tim-Philipp... indexers: fix two small leaks
2011-01-07 Tim-Philipp... tests: never disable g_assert() and cast checks for...
2011-01-06 Tim-Philipp... registry: ignore old libgstvalve.so and libgstselector...
2011-01-06 Tim-Philipp... Revert "padtemplate: allow disablinbg the template...
2011-01-06 Thiago Santosoutput-selector: Add pad-negotiation-mode property
2011-01-06 Tim-Philipp... docs: mention extra input-selector pad properties
2011-01-06 Tim-Philipp... po: update translations
2011-01-06 Tim-Philipp... info: avoid unnecessary malloc/free for each log functi...
2011-01-06 christian schallerUpdate spec file with latest changes and enable GIR
2011-01-05 David Schleefobject: Fix creation of default name
2011-01-05 Edward HerveyGstElement: Add a more flexible way to get request...
2011-01-05 Tim-Philipp... inputselector: remove "select-all" property
2011-01-05 Tim-Philipp... gst: remove safety check for GLib < 2.8
2011-01-05 Edward Herveygstdatetime: Disable usage of GDateTime on MacOSX
2011-01-05 Wim Taymansdesign: more updates for the progress messages
2011-01-04 Edward Herveypwg: Fix link to GObject documentation
2011-01-04 Edward Herveypluginloader: Always mark reception as complete after...
2011-01-04 Tim-Philipp... gstinfo: don't use printf extensions if GLib isn't...
2011-01-03 Edward Herveygstpoll: Fix for (p)select backend
2011-01-03 Tim-Philipp... gstvalue: make new gst_value_list_merge() work properly
2011-01-02 Stefan Kosttags: don't produce duplicated entries when merging...
2011-01-02 Tim-Philipp... basesrc, basesink: add some FIXMEs for the type of...
2010-12-31 Tim-Philipp... inputselector: make pad's get_type function thread...
2010-12-31 Tim-Philipp... coreelements: remove unused files
2010-12-31 Sebastian Drögeinputselector: Protected g_object_notify() calls for...
2010-12-31 Zhang Wanmingtests: fix typo
2010-12-31 Zhang Wanminggstfdsink: fix typo
2010-12-31 Zhang Wanmingdocs: fix typo
2010-12-31 Tim-Philipp... tests: remove output-selector test which needs elements...
2010-12-31 Tim-Philipp... checks: enable input-selector and output-selector unit...
2010-12-31 Tim-Philipp... docs: add input-selector and output-selector to docs
2010-12-31 Tim-Philipp... coreelements: GST_BOILERPLATE already sets parent_class
2010-12-31 Tim-Philipp... input-selector, output-selector: minor clean-ups
2010-12-31 Tim-Philipp... coreelements: move input-selector and output-selector...
2010-12-31 Stefan Kostoutput-selector-test: don't hardcode videosinks and...
2010-12-31 Thiago Santosoutputselector: Avoid losing the last_buffer when switching
2010-12-31 Thiago Santosoutputselector: Recheck pending switch after pushing...
2010-12-31 Stefan Kostinputselector: log times in human readable form
2010-12-31 Stefan Kostinputselector: move reoccuring logs to LOG and remove...
2010-12-31 Stefan Kostvarious (gst): add missing G_PARAM_STATIC_STRINGS flags
2010-12-31 Stefan Kostinputselector: sync with copy in -base
2010-12-31 Stefan Kostoutputselector: move the debug init to the boilerplate...
2010-12-31 Stefan Kostinputselector: use GST_BOILERPLATE macro
2010-12-31 Benjamin OtteAdd -Wwrite-strings
2010-12-31 Benjamin OtteAdd -Wmissing-declarations -Wmissing-prototypes to...
2010-12-31 Benjamin Ottegst_element_class_set_details => gst_element_class_set_...
2010-12-31 Sebastian DrögeRevert "inputselector: Protect g_object_notify() with...
2010-12-31 Kipp Cannoninputselector: Protect g_object_notify() with the objec...
2010-12-31 Sebastian Drögeinputselector: Remove useless variables and fix a unini...
2010-12-31 Sebastian Drögeinputselector: Make sure that running_time->timestamp...
2010-12-31 Sebastian Drögeinputselector: Use the start time (i.e. timestamp)...
2010-12-31 Sebastian Drögeinputselector: Improve debugging
2010-12-31 Wim TaymansRevert "inputselector: use get_caps_reffed()"
2010-12-31 Wim Taymansinputselector: use get_caps_reffed()
2010-12-31 Stefan Kostinputselector: also add inline to the proto to fix...
2010-12-31 Edward Herveygst: Remove dead assignments and resulting unused variables
2010-12-31 Sebastian Drögeinputselector: Use the same iterate internal links...
2010-12-31 Tim-Philipp... input-selector: Remove GST_DEBUG_FUNCPTR where they...
2010-12-31 David Schleefinput-selector: Remove Ronald Bultje from Authors field
2010-12-31 Wim Taymansinputselector: set output caps before pushing
2010-12-31 Wim Taymansinputselector: install an acceptcaps function
2010-12-31 Michael SmithRemove executable bits from non-executable files.
2010-12-31 Sebastian Drögeinputselector: Use new single iterator for the internal...
2010-12-31 Havard Graffoutputselector: make GST_FORMAT_TIME the default segmen...
2010-12-31 Sebastian Drögeinputselector: Use iterate internal links instead of...
2010-12-31 Tommi Myöhänenoutputselector: check for pending srcpad in _get_property()
2010-12-31 Stefan Kostoutputselector: do the pad_alloc for the pad that is...
2010-12-31 Lasse Laukkanenoutput-selector: serialize setting and actual changing...
2010-12-31 Lasse Laukkanenoutput-selector: unref latest buffer also when resendin...
2010-12-31 Lasse Laukkanenoutput-selector: keep ref to buffer for resending only...
2010-12-31 Wim Taymansinputselector: don't leak pads in iterator
2010-12-31 Sebastian Drögeinputselector: Notify when the tags property of the...
2010-12-31 Stefan Kostselector: remove not needed instance var (previous...
next