glsdk/gstreamer0-10.git
2011-06-15 Tim-Philipp... Release 0.10.35
2011-06-14 Javier JardónUse "const" instead G_CONST_RETURN
2011-06-14 David SchleefWork around changes in g_atomic API
2011-06-14 Руслан Ижбулатовsystemclock: Placate gcc by defining EWOULDBLOCK to...
2011-06-14 Руслан Ижбулатовpoll: Fix WAKE_EVENT() to behave posixly on Windows
2011-05-14 Tim-Philipp... Release 0.10.34
2011-05-12 Vincent Penquerc'hbasesrc: do not set first buffer timestamp to 0 for...
2011-05-10 Mark Nauwelaertsmultiqueue: ensure thread safety when adding a pad
2011-05-10 Tim-Philipp... Release 0.10.33
2011-05-06 Tim-Philipp... baseparse: don't post loads of empty taglists
2011-05-06 Stefan Kostinfo: avoid redefinition of symbols when debugging...
2011-05-04 Tim-Philipp... tests: fix compiler warning in new miniobject test
2011-05-03 Thiago Santosminiobject: Fix dup_mini_object function to handle...
2011-05-03 Stefan Kostdocs: it its %TRUE (constant)
2011-05-03 Stefan Kostdocs: fix copy'n'paste doc header mistake
2011-05-03 Stefan Kostdocs: add two trivial doc blobs
2011-05-03 Stefan Kostdocs: add missing parameter docs
2011-05-03 Stefan Kostdocs: add docs for GstDPPacketizer
2011-05-03 Stefan Kostdocs: improve the syntax for the capsintersectmode...
2011-05-03 Stefan Kostdocs: fixup broken xref
2011-05-03 Stefan Kostdocs: add new api to -section.txt
2011-05-03 Stefan Kostdocs: fix gtk-doc syntax
2011-05-03 Stefan Kostdocs: don't duplicate info that we take from element...
2011-05-03 Stefan Kostdocs: remove non existing symbol
2011-05-03 Stefan Kostdocs: we don't need to document private members in...
2011-04-30 Tim-Philipp... 0.10.32.4 pre-release
2011-04-29 Tim-Philipp... pluginfeature: include plugin.h in header where we...
2011-04-27 Tim-Philipp... 0.10.32.3 pre-release
2011-04-26 Tim-Philipp... Revert lockfree GstBus for the release
2011-04-25 David Schleefminor inline documentation fix
2011-04-24 Tim-Philipp... Automatic update of common submodule
2011-04-24 Tim-Philipp... tests: clean up properly in the bin test_link_structure...
2011-04-24 Tim-Philipp... registry: when removing a cached-but-no-longer-existing...
2011-04-24 Tim-Philipp... pluginfeature: store pointer to plugin in addition...
2011-04-24 Tim-Philipp... registry: use TRACE log level to log files that don...
2011-04-21 Thiago Santosbasetransform: fix negotiation regression
2011-04-21 Tim-Philipp... tests: add simple pipeline-in-pipeline unit test
2011-04-21 Mark Nauwelaertsbus: also allow popping a message without timeout if...
2011-04-19 Havard Graffpad: unlock before freeing the cache to avoid deadlock
2011-04-19 Havard Graffbasetransform: don't unref trans until the function...
2011-04-19 Tim-Philipp... docs: add note/warning to gst_index_get_writer_id(...
2011-04-19 Tim-Philipp... baseparse: don't deadlock when setting external index
2011-04-19 Tim-Philipp... baseparse: make fmtlist constant
2011-04-19 Tim-Philipp... query: const-ify formats arguments to gst_query_set_for...
2011-04-16 Tim-Philipp... docs: remove reference to baseparse API that didn't...
2011-04-16 Tim-Philipp... 0.10.32.2 pre-release
2011-04-16 Tim-Philipp... po: update translations
2011-04-16 Tim-Philipp... gst-launch: remove newline from translatable string
2011-04-16 Tim-Philipp... gst: gobject-introspection scanner doesn't need to...
2011-04-16 Sebastian Drögegst: make sure gobject-introspection scanner calls...
2011-04-16 Tim-Philipp... libs: gobject-introspection scanner doesn't need to...
2011-04-16 Tim-Philipp... libs: make sure gobject-introspection scanner calls...
2011-04-16 Tim-Philipp... win32: add new baseparse API to libgstbase.def
2011-04-16 Sebastian Drögewin32: Add exports for the GstParseContext and GstBuffe...
2011-04-15 Tim-Philipp... pluginloader: only run gst-plugin-scanner with /usr...
2011-04-15 Tim-Philipp... baseparse: expose gst_base_parse_frame_free() for compl...
2011-04-15 Tim-Philipp... baseparse: init frames on the stack with gst_base_parse...
2011-04-15 Tim-Philipp... baseparse: more debug logging, minor clean-up
2011-04-15 Tim-Philipp... baseparse: change gst_base_parse_frame_init() to not...
2011-04-15 Tim-Philipp... baseparse: make GstBaseParseFrame handling more binding...
2011-04-15 Tim-Philipp... baseparse: register boxed type for GstBaseFrameParse
2011-04-15 Sebastian Drögequeue2: Add missing ) to the ring-buffer-max-size prope...
2011-04-15 Robert Swainbaseparse: Remove unused but set variable
2011-04-14 Sebastian Drögebufferlist: Add boxed type for GstBufferListIterator...
2011-04-14 Sebastian Drögeparse: Add boxed type for GstParseContext for gobject...
2011-04-14 Sebastian Drögegst: Add some more gobject-introspection annotations
2011-04-14 Sebastian Drögemultiqueue: Don't leak the sinkpad name
2011-04-14 Sebastian Drögemultiqueue: Don't leak pads in the named pads unit...
2011-04-14 Sebastian Drögeutils: Fix caps leaks in gst_element_factory_can_accept...
2011-04-13 David Schleefparser: Allow element names to begin with digits
2011-04-13 David Schleeftests: Add test for greatest common divisor
2011-04-13 Ole André Vadla... elements: Fix pad callbacks so they handle when parent...
2011-04-13 Ole André Vadla... base: Fix pad callbacks so they handle when parent...
2011-04-13 Ole André Vadla... ghostpad: Fix pad callbacks so they handle when parent...
2011-04-13 Janne Grunauqueue2: prevent calculation with GST_CLOCK_TIME_NONE...
2011-04-11 Tim-Philipp... tests: fix unusued-but-assigned-variable warnings with...
2011-04-11 Tim-Philipp... tests: disable test_many_bins unit test for now
2011-04-11 Tim-Philipp... pluginloader: fix compiler warnings
2011-04-11 Tim-Philipp... tests: allow more time for the test_many_bins pipeline...
2011-04-11 Jan Schmidtpluginloader: make sure gst-plugin-scanner is called...
2011-04-11 Robert Swainpad: Allow tracking of buffers in GST_SCHEDULING debug...
2011-04-10 Alessandro... android: make it ready for androgenizer
2011-04-09 Tim-Philipp... trace: don't put code with side effects into g_return_i...
2011-04-09 Tim-Philipp... docs: minor fixes for baseparse docs
2011-04-09 Tim-Philipp... element: unref event in default_send_event in case...
2011-04-08 Tim-Philipp... baseparse: minor variable name clean-up
2011-04-08 Tim-Philipp... baseparse: rename _set_frame_props() to _set_frame_rate()
2011-04-08 Tim-Philipp... baseparse: replace format flags with gst_base_parse_set...
2011-04-08 Tim-Philipp... baseparse: make DRAIN and SYNC flags on baseparse,...
2011-04-08 Tim-Philipp... baseparse: add some padding to GstBaseParseFrame
2011-04-08 Tim-Philipp... baseparse: fix typo in docs for GST_BASE_PARSE_FORMAT_F...
2011-04-08 Tim-Philipp... baseparse: use GQueue instead of GList for queued frames
2011-04-08 Zaheer Abbas... baseparse: add GST_BASE_PARSE_FLOW_QUEUED to queue...
2011-04-08 Tim-Philipp... baseparse: add to docs and fix up gtk-doc markup a...
2011-04-08 Tim-Philipp... baseparse: replace set_seek() with _set_average_bitrate...
2011-04-08 Tim-Philipp... baseparse: rename GstBaseFormat to GstBaseFormatFlags...
2011-04-08 Tim-Philipp... baseparse: don't expose GstAdapter in public header
2011-04-08 Tim-Philipp... baseparse: move various segment-related members into...
2011-04-08 Tim-Philipp... baseparse: remove unused GST_BASE_PARSE_{SINK,SRC}_NAME
2011-04-08 Tim-Philipp... baseparse: re-indent header
next