]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - glsdk/gstreamer0-10.git/shortlog
glsdk/gstreamer0-10.git
2007-06-21 Jan SchmidtBeef up and include the docs for gst_type_register_stat...
2007-06-21 Wim Taymansplugins/elements/gstmultiqueue.c: Fix setting max-...
2007-06-21 Stefan KostSaving relocations for GTypeInfo and GstElementDetails...
2007-06-21 Tim-Philipp... docs/pwg/advanced-types.xml: Fix typo in iana.org URI.
2007-06-19 Andy Wingotests/check/pipelines/simple-launch-lines.c
2007-06-19 Andy Wingotests/check/pipelines/simple-launch-lines.c
2007-06-19 Wim Taymansplugins/elements/gstmultiqueue.c: Fix event leak.
2007-06-19 Wim Taymansgst/gstbin.c: Move the common code for posting state...
2007-06-19 Jan Schmidtdocs/random/release: Add a note about updating the...
2007-06-18 Wim Taymansplugins/elements/gstmultiqueue.c: Make sure we don...
2007-06-18 Wim Taymansplugins/elements/gstmultiqueue.c: Update queue state...
2007-06-18 Wim Taymansgst/gstbin.*: Immediatly commit the toplevel bin state...
2007-06-17 Thomas Vander... po/: Update translations.
2007-06-15 Jan Schmidtgst/gstpad.c: Fix typo in the docs.
2007-06-15 Wim Taymansdocs/libs/gstreamer-libs-sections.txt: Add docs for...
2007-06-15 Wim Taymansplugins/elements/gstmultiqueue.c: Don't use GSlice...
2007-06-15 Wim Taymansplugins/elements/gstmultiqueue.c: Remove debug printf.
2007-06-15 Wim Taymanslibs/gst/base/gstdataqueue.*: Various cleanups.
2007-06-15 Wim Taymanslibs/gst/base/gstbasetransform.c: Work around the broke...
2007-06-15 Wim TaymansImprove debugging.
2007-06-15 Stefan Kostdocs/pwg/advanced-types.xml: Added more formats to...
2007-06-15 Stefan Kosttools/gst-launch.c: Remove crufy code. GOption does...
2007-06-14 Stefan Kostlibs/gst/controller/gstcontroller.c: Fix wrong getter...
2007-06-14 Tim-Philipp... libs/gst/check/gstcheck.c: Intercept criticals and...
2007-06-14 Edward Herveygst/gstparamspecs.c: Since this file doesn't include...
2007-06-14 Tim-Philipp... Ugly 'fix' for the controller unit test on the p5 bot...
2007-06-14 Stefan Kostlibs/gst/base/gstbasesink.c: Add two breaks thats where...
2007-06-14 Tim-Philipp... API: add fail_unless_equals_float() and assert_equals_f...
2007-06-14 Stefan Kostgst/gstpad.c: Show the caps change in the log to help...
2007-06-14 Tim-Philipp... docs/pwg/building-boiler.xml: Fix typos, spotted by...
2007-06-13 Jan Schmidtdocs/plugins/tmpl/.cvsignore: Ignore file to keep the...
2007-06-13 Jan Schmidtdocs/plugins/: Pull fdsink into the docs too.
2007-06-11 Sebastian Drögelibs/gst/controller/gstinterpolation.c: Actually use...
2007-06-10 Sebastian Drögelibs/gst/controller/gstcontroller.c: Unset the minimum...
2007-06-09 Sebastian Drögelibs/gst/controller/: Protect against values larger...
2007-06-08 Sebastian Drögedocs/random/slomo/controller.txt: Add some thoughts...
2007-06-08 Wim Taymansplugins/elements/gstidentity.c: Don't overflow in retim...
2007-06-07 Sébastien Mouttelibs/gst/controller/gstinterpolation.c: Use gst_util_gu...
2007-06-07 Tim-Philipp... gst/gstutils.c: Small docs addition.
2007-06-07 Stefan KostREADME: Remove that test line again.
2007-06-07 Stefan KostREADME: Test commit mail sending.
2007-06-07 Stefan Kostconfigure.ac: Fix typo and test commit mail sending.
2007-06-07 Stefan Kosttests/examples/controller/audio-example.c: Improve...
2007-06-07 Wim Taymansgst/gstbin.c: Add helper function to find messages.
2007-06-06 Tim-Philipp... Fix multiqueue leaking buffers and events when downstre...
2007-06-06 Sebastian Drögelibs/gst/controller/gstcontroller.c: Clarify docs:...
2007-06-06 Sebastian Drögelibs/gst/controller/: Factor out the 'set' logic into...
2007-06-06 Tim-Philipp... gst/gstparamspecs.c: Don't use GLib-2.10 functions...
2007-06-06 Tim-Philipp... API: add GstParamSpecFraction, so elements can have...
2007-06-05 Wim Taymansgst/gstobject.c: Fix signal signature.
2007-06-05 Jan SchmidtAUTHORS: I should probably be listed as an author by...
2007-06-05 Tim-Philipp... gst/gstvalue.c: Make docs for gst_value_compare() menti...
2007-06-05 Jan Schmidtconfigure.ac: Back to CVS
2007-06-05 Jan SchmidtRelease 0.10.13 "With or without you"
2007-06-05 Jan SchmidtUpdate .po files
2007-05-29 Thomas Vander... trigger a mail
2007-05-29 Thomas Vander... trigger a mail
2007-05-29 Thomas Vander... trigger a mail
2007-05-29 Thomas Vander... send a mail
2007-05-29 Thomas Vander... test commit
2007-05-29 Thomas Vander... test commit
2007-05-29 Thomas Vander... test commit
2007-05-29 Thomas Vander... test commit
2007-05-29 Thomas Vander... test commit
2007-05-29 Thomas Vander... test commit
2007-05-29 Thomas Vander... test commit
2007-05-25 Wim Taymansgst/gstbin.c: Make sure that the child bin stops after...
2007-05-25 Wim Taymanslibs/gst/base/gstcollectpads.c: Use additional refcount...
2007-05-24 Wim Taymanstools/gst-launch.c: When buffering goes from a two...
2007-05-24 Tim-Philipp... libs/gst/base/gstdataqueue.c: Eliminate tabs and traili...
2007-05-24 Wim Taymanstests/check/gst/gstbin.c: Allow refcount of 3 and 4...
2007-05-24 Tim-Philipp... plugins/elements/: These are not installed headers...
2007-05-24 Wim Taymansgst/gstbin.c: Enable latency for next release.
2007-05-23 Wim Taymanstests/check/gst/gstsystemclock.c: Improve test_async_or...
2007-05-22 Tim-Philipp... gst/gstbin.*: 'private' is a c++ keyword, let's not...
2007-05-22 Tim-Philipp... plugins/: Use #ifdef for HAVE_XYZ for consistency.
2007-05-22 Mark Nauwelaertsplugins/elements/gstfilesink.*: Fix position reporting...
2007-05-22 Edward HerveyAdd a property for bins that handle the state change...
2007-05-22 Thomas Vander... add quote
2007-05-22 Sebastian Drögelibs/gst/controller/gstinterpolation.c: Use an array...
2007-05-22 Stefan Kostgst/gstelement.c (gst_element_requires_clock, gst_eleme...
2007-05-21 Sebastian Drögelibs/gst/controller/gstinterpolation.c: Add support...
2007-05-21 Sebastian Drögelibs/gst/controller/gstcontroller.*: Clarify the docs...
2007-05-21 Jan Schmidttests/check/gst/gstbuffer.c: Disable part of the gst_bu...
2007-05-21 Sebastian Drögetests/check/gst/gstpad.c: Add unit test for the improve...
2007-05-21 Wim Taymansdocs/design/part-synchronisation.txt: Small addition.
2007-05-21 Wim Taymansgst/gstpad.c: Added simple version of improved caps...
2007-05-21 Wim Taymanslibs/gst/base/gstbasetransform.h: Fix macro for locking...
2007-05-19 Tim-Philipp... docs/plugins/tmpl/.cvsignore: Ignore more.
2007-05-18 Edward Herveyplugins/elements/gstqueue.c: Hello, I am Mr Taymans...
2007-05-18 Edward Herveyplugins/elements/gstqueue.c: Release the queue lock !
2007-05-17 Sebastian Drögedocs/libs/gstreamer-libs-sections.txt: Add the two...
2007-05-17 Sebastian Drögelibs/gst/controller/: API: gst_controller_suggest_next_...
2007-05-17 Sebastian Drögelibs/gst/controller/: Save last synced value from the...
2007-05-17 Sebastian Drögelibs/gst/controller/: Add a new private GstControlPoint...
2007-05-17 Edward Herveygst/gstsegment.c: Small doc fix.
2007-05-16 Tim-Philipp... gst/gstplugin.c: If we fail to load a plugin because...
2007-05-13 David Schleefdocs/Makefile.am: the gtk-doc makefile snippet correctl...
2007-05-13 David Schleefgst/gstutils.h: Reword some documentation.
2007-05-13 David Schleefgst/gstplugin.c: gst_plugin_register_func() doesn't...
next