]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - glsdk/gstreamer0-10.git/shortlog
glsdk/gstreamer0-10.git
2007-11-06 Jan Schmidttests/check/gst/gstobject.c: Disable silly racy test...
2007-11-04 Tim-Philipp... ChangeLog surgery: mention bug number
2007-11-04 Murray Cumminggst/gstobject.c: Corrected the registration of the...
2007-11-02 Tim-Philipp... gst/: Move declaration of private _gst_foo_initialize...
2007-11-02 Tim-Philipp... gtk-doc fixes; trailing-comma-in-enum fix.
2007-11-02 Tim-Philipp... gst/gst.c: Clean up on deinit (not the external ones...
2007-11-01 Tim-Philipp... gst/gstinfo.h: Remove __declspec(dllimport) for MSVC...
2007-11-01 Tim-Philipp... g_type_class_ref() other types as well, see #349410...
2007-11-01 Tim-Philipp... gst/gstformat.c: g_type_class_ref() our GstFormat type...
2007-11-01 Tim-Philipp... tests/check/elements/tee.c: Simplify, simplify, simplif...
2007-10-31 Ole André Vadla... Fix a couple of missing includes for MSVC2005 and a...
2007-10-31 Tim-Philipp... tests/examples/metadata/read-metadata.c: Use _KEEP...
2007-10-31 Stefan Kostlibs/gst/base/gstbasesrc.c: Its "Since:" and not "...
2007-10-30 Wim TaymansAdd a new last-buffer property that contains the last...
2007-10-29 Stefan KostImprove bin graph dumping, by using the envvar to speci...
2007-10-29 Tim-Philipp... plugins/elements/gsttypefindelement.c: Post special...
2007-10-29 Stefan KostDocument new env-var. Add one log-line after dumpng...
2007-10-26 Tim-Philipp... configure.ac: Ugly hack to put the (recently removed...
2007-10-25 Wim Taymanslibs/gst/base/gstbasesink.c: Reset last seen position...
2007-10-25 Alessandro... gst/: Patch from Alessandro Decina adding get_type_full...
2007-10-25 Jan Schmidtplugins/elements/gstmultiqueue.c: Make it so that pads...
2007-10-25 Jan SchmidtUse a custom export symbol regex for libgstcheck, as...
2007-10-25 Tim-Philipp... tests/check/gst/gststructure.c: Disable test that check...
2007-10-24 Tim-Philipp... API: add GST_TAG_ARTIST_SORTNAME
2007-10-24 Tim-Philipp... gst/gststructure.c: Also allow white space for names...
2007-10-22 Wim Taymansdocs/design/: Small updates.
2007-10-22 Edgard Limadocs/gst/gstreamer-sections.txt: Fixed documentation...
2007-10-22 Stefan Kostgst/gstdebugutils.c: Reflow code to fix uninitialized...
2007-10-22 Edgard LimaAdded GstStructure to gst_value_table and its related...
2007-10-19 Tim-Philipp... gst/gstbus.c: When no GSource callback has been set...
2007-10-17 Stefan KostAllow dumping pipelines as dot graphs. Fixes #456573.
2007-10-16 Tim-Philipp... gst/gststructure.c: Allow '+' as well, it can be part...
2007-10-16 Tim-Philipp... API: add gst_bus_pop_filtered
2007-10-16 Tim-Philipp... docs/libs/gstreamer-libs-sections.txt: Make gtk-doc...
2007-10-16 Tim-Philipp... libs/gst/check/gstcheck.*: Allow runtime selection...
2007-10-16 Stefan KostRevert serialisation change and constrain structure...
2007-10-16 Stefan Kostgst/gststructure.c: Improve serialization and fix tests.
2007-10-15 Wim Taymanstools/gst-inspect.c: Don't crash when inspecting an...
2007-10-15 Tim-Philipp... tests/check/gst/gststructure.c: Add unit test for escap...
2007-10-15 Wim Taymansplugins/elements/: Fix queue negotiation. If acceptcaps...
2007-10-15 Stefan Kostgst/: Add some more comments and debug output. Quote...
2007-10-15 Stefan Kostgst/gstbuffer.h: Define GST_BUFFER_FLAG_GAP more strict...
2007-10-15 Stefan Kosttools/gst-inspect.c: Save approx. 400 1 byte allocs...
2007-10-15 Stefan Kostgst/gstinfo.c: Fix some spelling errors.
2007-10-14 Wim Taymansgst/gstbin.c: Correctly set the next state if all of...
2007-10-13 Tim-Philipp... gst/gstbin.c: Don't shadow local variable.
2007-10-13 Tim-Philipp... gst/: Use already-interned string for the private GstPl...
2007-10-10 Tim-Philipp... docs/libs/gstreamer-libs-sections.txt: Add new API...
2007-10-10 Wim Taymanslibs/gst/base/gstbasesink.*: Add function to wait for...
2007-10-10 Tim-Philipp... gst/gstplugin.h: Cast description string constants...
2007-10-09 Tim-Philipp... gst/gstinfo.h: Use __FUNCTION__ instead of __PRETTY_FUN...
2007-10-09 Wim Taymansgst/gstbin.c: Work around a problem with pipelines...
2007-10-09 Tim-Philipp... gst/: Put more strings into the GLib quark table. No...
2007-10-09 Tim-Philipp... docs/manual/advanced-dataaccess.xml: Don't imply that...
2007-10-08 Tim-Philipp... win32/common/: Update generated files.
2007-10-08 Tim-Philipp... docs/manual/advanced-autoplugging.xml: Prefix section...
2007-10-08 Tim-Philipp... docs/manual/: Call g_thread_init() before g_option_cont...
2007-10-08 Wim Taymanslibs/gst/base/gstbasesink.c: When we received EOS and...
2007-10-08 Wim Taymansplugins/elements/gsttypefindelement.c: Move detecting...
2007-10-08 Wim Taymanslibs/gst/base/gstbasesink.c: Don't try to preroll non...
2007-10-05 Wim Taymansgst/: Small comment and documentation update.
2007-10-05 Wim Taymanslibs/gst/base/gstbasesrc.c: Rework the locking of bases...
2007-10-05 Wim Taymanstests/check/pipelines/simple-launch-lines.c: Fix compil...
2007-10-03 Stefan Kostgst/gstelement.c: Use meaningful categories for the...
2007-10-03 Stefan Kosttests/check/pipelines/cleanup.c: Print message name...
2007-10-03 Stefan Kostdocs/design/draft-tagreading.txt: Add some more thoughts.
2007-10-03 Stefan Kosttests/check/pipelines/simple-launch-lines.c: Print...
2007-10-03 Stefan Kostlibs/gst/base/gsttypefindhelper.c: Speedup typefinding...
2007-10-03 Stefan Kostgst/gstplugin.c: Fix docs that mention 'plugin_desc...
2007-10-03 Tim-Philipp... gst/gstclock.h: Fix up broken GST_CLOCK_FLAGS macro...
2007-10-02 Wim Taymanslibs/gst/base/gstbasesrc.c: Call unlock for live source...
2007-10-02 Edward Herveyplugins/elements/gstqueue.c: Comment the segment-relate...
2007-10-01 Wim Taymanslibs/gst/base/gstbasesrc.c: Also initialize the counter...
2007-10-01 Edward Herveyplugins/elements/gstqueue.c: Disable code that's breaki...
2007-09-30 Sebastian Drögedocs/gst/gstreamer-sections.txt: Add M_PI and IMPORT_SY...
2007-09-29 Sébastien Mouttegst/gstinfo.h: Add an explicit variable importation...
2007-09-28 Felipe Contrerasplugins/elements/gstqueue.c: Improve debugging. Fixes...
2007-09-28 Felipe Contrerasplugins/elements/gstqueue.c: First patch of code cleanu...
2007-09-26 Wim Taymansgst/gstbus.c: Improve debugging when dealing with _poll().
2007-09-26 Tim-Philipp... gst/gstregistryxml.c: Fix memory leak I introduced...
2007-09-26 Michael Smithgst/gstbuffer.c: Make it once again possible to free...
2007-09-25 Tim-Philipp... API: add GST_TAG_COMPOSER, fixes #459809.
2007-09-24 Sebastian Drögegst/gstplugin.*: Add the 3-clause BSD license and the...
2007-09-24 Tim-Philipp... docs/faq/getting.xml: Add Q+A about different GStreamer...
2007-09-24 Wim Taymanslibs/gst/base/gstbasesink.c: Return correct gboolean...
2007-09-24 Wim Taymanslibs/gst/base/gstbasesink.c: Simplify latency query.
2007-09-24 Wim Taymansgst/: Fix small typos in the docs.
2007-09-24 Wim Taymansdocs/design/: Documentation updates and typo fixes.
2007-09-23 Tim-Philipp... plugins/elements/gstfakesink.c: Add some debug text...
2007-09-22 Thomas Vander... updated translations
2007-09-22 Thomas Vander... po/: Added Spanish translation.
2007-09-21 Wim Taymansplugins/elements/gstqueue.c: Fix printf arguments.
2007-09-20 Stefan Kosttests/check/generic/states.c: Improved state change...
2007-09-20 Stefan Kostgst/gstbin.h: Move priv to the right place.
2007-09-19 Wim Taymanslibs/gst/base/gstbasesrc.c: Don't unref the event after...
2007-09-19 Stefan KostIgnore registries in any format.
2007-09-19 Tim-Philipp... gst/glib-compat-private.h: Add compatibility macro...
2007-09-19 Stefan Kostgst/gstelementfactory.c: Release static caps. Fixes...
2007-09-18 Tim-Philipp... gst/gstinfo.*: Make some internal API take const gchar...
2007-09-17 Wim Taymansgst/gstbin.c: A latency query fails when one of the...
next