glsdk/gstreamer0-10.git
2011-12-03 Tim-Philipp... g_thread_create() is deprecated in GLib master, use...
2011-12-02 Mark Nauwelaertsidentity: unlock clock wait when appropriate
2011-12-01 Stefan Sauerbus: use GST_MESSAGE_SOURCE_NAME() which also takes...
2011-11-30 Sebastian Drögebasetransform: Always intersect the suggested sink...
2011-11-30 Tim-Philipp... event: warn and fail instead of creating newsegment...
2011-11-28 Vincent Penquerc'hgstelement: add gst_element_class_add_pad_template_from...
2011-11-28 Tim-Philipp... queue2: fix refactoring of draining-on-eos, munge flow...
2011-11-28 Tim-Philipp... queue2: add bufferlist support
2011-11-28 Tim-Philipp... queue2: split out draining of queue on FLOW_UNEXPECTED...
2011-11-28 Tim-Philipp... queue2: pass item type enum to _enqueue instead of...
2011-11-27 Stefan Sauerwarnings: avoid set-but-unused warnings with load-save...
2011-11-26 Tim-Philipp... uri: fix wrong G_GNUC_MALLOC
2011-11-26 Tim-Philipp... libs: sprinkle some G_GNUC_MALLOC
2011-11-26 Tim-Philipp... gst: sprinkle some G_GNUC_MALLOC
2011-11-25 Tim-Philipp... buffer: add gst_buffer_{set,get}_qdata()
2011-11-24 Sebastian Drögepad: Remove g_warning() if pad accepted caps that are...
2011-11-24 Vincent Penquerc'hmultiqueue: check filled state of queues even if anothe...
2011-11-23 Sebastian Drögebaseparse: Return template caps instead of other side...
2011-11-12 Tim-Philipp... gst-inspect: print current value as default value
2011-11-12 Tim-Philipp... gst, controller: replace g_list_prepend + reverse with...
2011-11-09 Stefan SauerAndroid: build audio controller example
2011-11-09 Vincent Penquerc'hgstvalue: consider lists and ranges equal if they hold...
2011-11-09 Stefan Sauertests: add a subset test for structure
2011-11-08 Stefan Sauerdocs: also fix wrong call order for controller in manual
2011-11-08 René Stadlertests: pad: add test to verify flushing behaviour
2011-11-08 Tim-Philipp... docs: fix Since: markers for API added after 0.10.35
2011-11-08 Tim-Philipp... win32: update .def file for new API
2011-11-07 Vincent Penquerc'hgstcaps: remove unneeded use of gint64
2011-11-07 Vincent Penquerc'hgstvalue: quicker version of intersection when we do...
2011-11-07 Vincent Penquerc'hgststructure: simplify return statement in gst_structur...
2011-11-07 Vincent Penquerc'hgststructure: early out when we know a value cannot...
2011-11-07 Vincent Penquerc'hgstvalue: quicker test for substraction emptiness
2011-11-07 Vincent Penquerc'hgststructure: rejig test ordering for speed
2011-11-04 Sjoerd Simonsbasetransform: Only use the cached transform on strictl...
2011-11-04 Sjoerd Simonscaps: Add gst_caps_is_strictly_equal
2011-11-04 Peteris Krisjanisintrospection: add Value annotations for GST_SECOND...
2011-11-04 Tim-Philipp... configure: suppress unused variable warnings if gst...
2011-11-04 Tim-Philipp... configure: fix typo around GLIB_EXTRA_CFLAGS in GST_ALL...
2011-11-03 Tim-Philipp... queue: use statically allocated GQueue
2011-11-03 Tim-Philipp... bin: use statically allocated GQueue
2011-11-03 Tim-Philipp... collectpads2: use flags enum instead of guint in structure
2011-11-03 Tim-Philipp... queue2: use statically allocated GQueue
2011-11-03 Nicolas Dufresneghostpad: Don't cache internal proxy pad target
2011-11-01 Tim-Philipp... adapter: simplify gst_adapter_take_list()
2011-10-31 Tim-Philipp... configure: make GLIB_EXTRA_CFLAGS overwritable
2011-10-30 Tim-Philipp... filter: deprecate gst_filter_run()
2011-10-30 Tim-Philipp... registry: don't use soon-to-be-deprecated gst_filter_run()
2011-10-30 Tim-Philipp... pluginfeature: deprecate gst_plugin_feature_type_name_f...
2011-10-30 Tim-Philipp... taglist: add to_string and new_from_string functions
2011-10-30 Tim-Philipp... taglist: avoid pointless tag name -> quark lookups
2011-10-30 Tim-Philipp... taglist: add gst_tag_list_is_equal()
2011-10-29 Tim-Philipp... structure: identical structures are definitely equal
2011-10-28 Sjoerd Simonsbasetransform: Also fush the cache when changing the...
2011-10-28 Sjoerd Simonsbasetransform: Add debug output when returning a cached...
2011-10-28 Sebastian Drögecollectpads2: Fix refcount handling if a buffer was...
2011-10-28 Sebastian Drögecollectpads2: Merge the clip and prepare_buffer functio...
2011-10-28 Sebastian Drögecollectpads2: Merge clipping API from old collectpads
2011-10-28 Tim-Philipp... basesink: make default query function name show up...
2011-10-28 Mark Nauwelaertscollectpads2: avoid hanging in case of sparse newsegmen...
2011-10-28 Sebastian Drögecollectpads2: Use G_DEFINE_TYPE instead of GST_BOILERPLATE
2011-10-28 Sebastian Drögecollectpads2: Add to the documentation
2011-10-28 Sebastian Drögewin32: Add new collectpads2 API
2011-10-28 Sebastian Drögebase: Add collectpads2
2011-10-27 Jan Schmidtbasetransform: Fix refcount leak
2011-10-27 Stefan Sauercontroller: fix wrong order of calls in the docs.
2011-10-26 Stefan Sauerevent: clarify docs for step event
2011-10-26 Tim-Philipp... registry: add support for GST_REGISTRY_REUSE_PLUGIN_SCA...
2011-10-21 Thiago Santoscaps: No need to require writable caps for _append...
2011-10-20 Sebastian Drögebaseparse: Fix documentation, it's pre_push_frame and...
2011-10-20 Vincent Penquerc'hbasetransform: cache transformed caps where appropriate
2011-10-20 Reynaldo H... Fix broken android building due to name change in 01d87...
2011-10-20 Sebastian Drögebasebarse: Add detect vfunc to allow subclasses to...
2011-10-20 Stefan Sauerpad: not only describe conditions in the docs, also...
2011-10-18 Thiago Santosmessage: protect against null message sources
2011-10-18 Thiago Santosbaseparse: add since doc to new getcaps function
2011-10-18 Stefan Sauerlogging: more logging and prefer human readable details...
2011-10-18 Stefan Sauerdebugutils: improve display of ghost- and proxypads
2011-10-18 Thiago Santosbaseparse: add getcaps function
2011-10-18 Wim Taymansbasesrc: also update the stream time
2011-10-18 Sebastian Drögebaseparse: Fix handling of queued frames
2011-10-16 Tim-Philipp... bus: give watch source a name
2011-10-16 Edward Herveygstbuffer: Add transfer annotations for gst_buffer_join()
2011-10-13 Stefan Sauerbus: fix typo in the docs
2011-10-13 Stefan Sauerdebugutils: show if an element is state-locked
2011-10-13 Stefan Sauerlogging: use _OBJECT variants more
2011-10-13 Sebastian Drögebuffer: Use an inline function instead of a macro for...
2011-10-13 Sebastian Drögeevent: Use an inline function instead of a macro for...
2011-10-12 Wim Taymansbasesrc: properly adjust start time
2011-10-10 Tim-Philipp... utils: catch invalid instance sizes in gst_type_registe...
2011-10-08 Tim-Philipp... gstparse: prefix generated parser functions so they...
2011-10-07 Thiago Santospipeline: Use pipeline category for one more log message
2011-10-07 Robert SwainGST_PTR_FORMAT: Add GstBuffer ptr format and use in...
2011-10-06 Mark Nauwelaertsbaseparse: send duration message when updating internal...
2011-10-03 Stas Sergeevbaseparse: Return success if optional start/stop method...
2011-10-03 Edward Herveygstquery: Make debugging message more informative
2011-09-30 Tim-Philipp... baseparse: make estimating the position in query handle...
2011-09-30 Vincent Penquerc'hbaseparse: answer position query in stream time and...
2011-09-30 Tim-Philipp... gst.h: include header for atomic queue
2011-09-30 Tim-Philipp... tests: add minimal test for GstAtomicQueue
2011-09-27 Vincent Penquerc'hbasetransform: send delayed events earlier
next