/* config.h.in. Generated from configure.ac by autoheader. */ /* Define if building universal (internal helper macro) */ #undef AC_APPLE_UNIVERSAL_BUILD /* Default audio sink */ #undef DEFAULT_AUDIOSINK /* Default audio source */ #undef DEFAULT_AUDIOSRC /* Default video sink */ #undef DEFAULT_VIDEOSINK /* Default video source */ #undef DEFAULT_VIDEOSRC /* Default visualizer */ #undef DEFAULT_VISUALIZER /* Disable Orc */ #undef DISABLE_ORC /* Define if an old libdts is used */ #undef DTS_OLD /* Define to 1 if translation of program messages to the user's native language is requested. */ #undef ENABLE_NLS /* The x in 2.x */ #undef FAAD2_MINOR_VERSION /* Define if AAC is using new api prefix */ #undef FAAD_IS_NEAAC /* gettext package name */ #undef GETTEXT_PACKAGE /* The GIO library directory. */ #undef GIO_LIBDIR /* The GIO modules directory. */ #undef GIO_MODULE_DIR /* The GIO install prefix. */ #undef GIO_PREFIX /* Define if GSM header in gsm/ subdir */ #undef GSM_HEADER_IN_SUBDIR /* GStreamer API Version */ #undef GST_API_VERSION /* Extra platform specific plugin suffix */ #undef GST_EXTRA_MODULE_SUFFIX /* Defined if gcov is enabled to force a rebuild due to config.h changing */ #undef GST_GCOV_ENABLED /* EGL module name */ #undef GST_GL_LIBEGL_MODULE_NAME /* GLES2 module name */ #undef GST_GL_LIBGLESV2_MODULE_NAME /* OpenGL module name */ #undef GST_GL_LIBGL_MODULE_NAME /* Defined when registry scanning through fork is unsafe */ #undef GST_HAVE_UNSAFE_FORK /* Default errorlevel to use */ #undef GST_LEVEL_DEFAULT /* GStreamer license */ #undef GST_LICENSE /* mjpegtools API evolution */ #undef GST_MJPEGTOOLS_API /* package name in plugins */ #undef GST_PACKAGE_NAME /* package origin */ #undef GST_PACKAGE_ORIGIN /* GStreamer package release date/time for plugins as YYYY-MM-DD */ #undef GST_PACKAGE_RELEASE_DATETIME /* Define if static plugins should be built */ #undef GST_PLUGIN_BUILD_STATIC /* Define to enable Windows ACM library (used by acm). */ #undef HAVE_ACM /* Define to enable Android Media (used by androidmedia). */ #undef HAVE_ANDROID_MEDIA /* Define to enable AirPort Express Wireless sink (used by apexsink). */ #undef HAVE_APEXSINK /* Define to enable Apple video (used by applemedia). */ #undef HAVE_APPLE_MEDIA /* Define to enable ASS/SSA renderer (used by assrender). */ #undef HAVE_ASSRENDER /* Define to enable AVC Video Services (used by avcsrc). */ #undef HAVE_AVC /* Define if building with AVFoundation */ #undef HAVE_AVFOUNDATION /* Define to enable Bluez (used by bluez). */ #undef HAVE_BLUEZ /* Bluez5 detected */ #undef HAVE_BLUEZ5 /* Define to enable bs2b (used by bs2b). */ #undef HAVE_BS2B /* Define to enable bz2 library (used by bz2). */ #undef HAVE_BZ2 /* Define to 1 if you have the MacOS X function CFLocaleCopyCurrent in the CoreFoundation framework. */ #undef HAVE_CFLOCALECOPYCURRENT /* Define to 1 if you have the MacOS X function CFPreferencesCopyAppValue in the CoreFoundation framework. */ #undef HAVE_CFPREFERENCESCOPYAPPVALUE /* Define to enable chromaprint (used by chromaprint). */ #undef HAVE_CHROMAPRINT /* Define if the target CPU is AARCH64 */ #undef HAVE_CPU_AARCH64 /* Define if the target CPU is an Alpha */ #undef HAVE_CPU_ALPHA /* Define if the target CPU is an ARC */ #undef HAVE_CPU_ARC /* Define if the target CPU is an ARM */ #undef HAVE_CPU_ARM /* Define if the target CPU is a CRIS */ #undef HAVE_CPU_CRIS /* Define if the target CPU is a CRISv32 */ #undef HAVE_CPU_CRISV32 /* Define if the target CPU is a HPPA */ #undef HAVE_CPU_HPPA /* Define if the target CPU is an x86 */ #undef HAVE_CPU_I386 /* Define if the target CPU is a IA64 */ #undef HAVE_CPU_IA64 /* Define if the target CPU is a M68K */ #undef HAVE_CPU_M68K /* Define if the target CPU is a MIPS */ #undef HAVE_CPU_MIPS /* Define if the target CPU is a PowerPC */ #undef HAVE_CPU_PPC /* Define if the target CPU is a 64 bit PowerPC */ #undef HAVE_CPU_PPC64 /* Define if the target CPU is a S390 */ #undef HAVE_CPU_S390 /* Define if the target CPU is a SPARC */ #undef HAVE_CPU_SPARC /* Define if the target CPU is a x86_64 */ #undef HAVE_CPU_X86_64 /* Define to enable Curl plugin (used by curl). */ #undef HAVE_CURL /* Define to enable daala (used by daala). */ #undef HAVE_DAALA /* Define to enable DASH plug-in (used by dash). */ #undef HAVE_DASH /* Define to enable libdc1394 (used by dc1394). */ #undef HAVE_DC1394 /* Define if the GNU dcgettext() function is already present or preinstalled. */ #undef HAVE_DCGETTEXT /* Define to enable decklink (used by decklink). */ #undef HAVE_DECKLINK /* Define to enable Direct3D plug-in (used by direct3dsink). */ #undef HAVE_DIRECT3D /* Define to enable directfb (used by dfbvideosink ). */ #undef HAVE_DIRECTFB /* Define to enable DirectSound (used by directsoundsrc). */ #undef HAVE_DIRECTSOUND /* Define to 1 if you have the header file. */ #undef HAVE_DLFCN_H /* define for working do while(0) macros */ #undef HAVE_DOWHILE_MACROS /* Define to enable DTLS plugin (used by dtls). */ #undef HAVE_DTLS /* Define to enable dts library (used by dtsdec). */ #undef HAVE_DTS /* Define to enable DVB Source (used by dvb). */ #undef HAVE_DVB /* Define to enable building of experimental plug-ins. */ #undef HAVE_EXPERIMENTAL /* Define to enable building of plug-ins with external deps. */ #undef HAVE_EXTERNAL /* Define to enable AAC encoder plug-in (used by faac). */ #undef HAVE_FAAC /* Define to enable AAC decoder plug-in (used by faad). */ #undef HAVE_FAAD /* Define to enable linux framebuffer (used by fbdevsink). */ #undef HAVE_FBDEV /* Define to 1 if you have the header file. */ #undef HAVE_FCNTL_H /* FIONREAD ioctl found in sys/filio.h */ #undef HAVE_FIONREAD_IN_SYS_FILIO /* FIONREAD ioctl found in sys/ioclt.h */ #undef HAVE_FIONREAD_IN_SYS_IOCTL /* Define to enable Flite plugin (used by flite). */ #undef HAVE_FLITE /* Define to enable fluidsynth (used by fluidsynth). */ #undef HAVE_FLUIDSYNTH /* Define to 1 if you have the `getpagesize' function. */ #undef HAVE_GETPAGESIZE /* Define if the GNU gettext() function is already present or preinstalled. */ #undef HAVE_GETTEXT /* Define to enable gl elements (used by gl). */ #undef HAVE_GL /* Define to 1 if the system has the type `GLchar'. */ #undef HAVE_GLCHAR /* Define to 1 if the system has the type `GLeglImageOES'. */ #undef HAVE_GLEGLIMAGEOES /* Define to 1 if the system has the type `GLintptr'. */ #undef HAVE_GLINTPTR /* Define to 1 if the system has the type `GLsizeiptr'. */ #undef HAVE_GLSIZEIPTR /* Define to 1 if the system has the type `GLsync'. */ #undef HAVE_GLSYNC /* Define to 1 if the system has the type `GLuint64'. */ #undef HAVE_GLUINT64 /* Define to enable gme decoder (used by gme). */ #undef HAVE_GME /* Define to 1 if you have the `gmtime_r' function. */ #undef HAVE_GMTIME_R /* Use graphene */ #undef HAVE_GRAPHENE /* Define to enable GSettings plugin (used by gsettings). */ #undef HAVE_GSETTINGS /* Define to enable GSM library (used by gsmenc gsmdec). */ #undef HAVE_GSM /* Define to enable Gtk+ elements (used by gtk). */ #undef HAVE_GTK3 /* Define if Gtk+ 3.0 GL is installed */ #undef HAVE_GTK3_GL /* Define if gudev is installed */ #undef HAVE_GUDEV /* Define to enable http live streaming plugin (used by hls). */ #undef HAVE_HLS /* Define if you have the iconv() function and it works. */ #undef HAVE_ICONV /* Define to 1 if you have the header file. */ #undef HAVE_INTTYPES_H /* Define if building for Apple iOS */ #undef HAVE_IOS /* Use libjpeg */ #undef HAVE_JPEG /* Define to enable Kate (used by kate). */ #undef HAVE_KATE /* Define to enable ladspa (used by ladspa). */ #undef HAVE_LADSPA /* Define to enable libde265 HEVC/H.265 decoder (used by libde265). */ #undef HAVE_LIBDE265 /* Define if libgcrypt is available */ #undef HAVE_LIBGCRYPT /* Define if gme 0.5.6 or newer is available */ #undef HAVE_LIBGME_ACCURACY /* Define to enable mms protocol library (used by libmms). */ #undef HAVE_LIBMMS /* Define to 1 if you have the `nsl' library (-lnsl). */ #undef HAVE_LIBNSL /* Define to 1 if you have the `socket' library (-lsocket). */ #undef HAVE_LIBSOCKET /* Define if libusb 1.x is installed */ #undef HAVE_LIBUSB /* Define to enable libvisual visualization library (used by libvisual). */ #undef HAVE_LIBVISUAL /* Define to enable Linear Systems SDI plugin (used by linsys). */ #undef HAVE_LINSYS /* Define if we have liblrdf */ #undef HAVE_LRDF /* Define to enable lv2 (used by lv2). */ #undef HAVE_LV2 /* Define to 1 if you have the header file. */ #undef HAVE_MEMORY_H /* Define to enable libmimic library (used by mimic). */ #undef HAVE_MIMIC /* Define to 1 if you have a working `mmap' system call. */ #undef HAVE_MMAP /* Define to enable modplug (used by modplug). */ #undef HAVE_MODPLUG /* Define to enable mpeg2enc (used by mpeg2enc). */ #undef HAVE_MPEG2ENC /* Define to enable mpg123 audio decoder (used by mpg123). */ #undef HAVE_MPG123 /* Define to enable mplex (used by mplex). */ #undef HAVE_MPLEX /* Define to 1 if you have the header file. */ #undef HAVE_MSACM_H /* Define to enable musepackdec (used by musepack). */ #undef HAVE_MUSEPACK /* Define to enable nas plug-in (used by nassink). */ #undef HAVE_NAS /* Define to enable neon http client plugins (used by neonhttpsrc). */ #undef HAVE_NEON /* Define to 1 if you have the header file. */ #undef HAVE_NETINET_IN_H /* Define to 1 if you have the header file. */ #undef HAVE_NETINET_IP_H /* Define to 1 if you have the header file. */ #undef HAVE_NETINET_TCP_H /* Define if nettle is available */ #undef HAVE_NETTLE /* Define to enable ofa plugins (used by ofa). */ #undef HAVE_OFA /* Define to enable OpenAL plugin (used by openal). */ #undef HAVE_OPENAL /* Define to enable opencv plugins (used by opencv). */ #undef HAVE_OPENCV /* Define to 1 if you have the header file. */ #undef HAVE_OPENCV2_CONTRIB_CONTRIB_HPP /* Define to 1 if you have the header file. */ #undef HAVE_OPENCV2_CORE_CORE_C_H /* Define to 1 if you have the header file. */ #undef HAVE_OPENCV2_CORE_TYPES_C_H /* Define to 1 if you have the header file. */ #undef HAVE_OPENCV2_CORE_VERSION_HPP /* Define to 1 if you have the header file. */ #undef HAVE_OPENCV2_HIGHGUI_HIGHGUI_C_H /* Define to 1 if you have the header file. */ #undef HAVE_OPENCV2_IMGPROC_IMGPROC_C_H /* Define to 1 if you have the header file. */ #undef HAVE_OPENCV2_IMGPROC_IMGPROC_HPP /* Define to 1 if you have the header file. */ #undef HAVE_OPENCV2_LEGACY_COMPAT_HPP /* Define to 1 if you have the header file. */ #undef HAVE_OPENCV2_LEGACY_LEGACY_HPP /* Define to 1 if you have the header file. */ #undef HAVE_OPENCV2_OBJDETECT_OBJDETECT_HPP /* Define to 1 if you have the header file. */ #undef HAVE_OPENCV2_VIDEO_BACKGROUND_SEGM_HPP /* Define to enable openexr library (used by openexr). */ #undef HAVE_OPENEXR /* Define to enable openh264 library (used by openh264). */ #undef HAVE_OPENH264 /* Define to enable openjpeg library (used by openjpeg). */ #undef HAVE_OPENJPEG /* Define if OpenJPEG 1 is used */ #undef HAVE_OPENJPEG_1 /* Define to enable openni2 library (used by openni2). */ #undef HAVE_OPENNI2 /* Define to enable OpenSL ES (used by opensl). */ #undef HAVE_OPENSLES /* Define if openssl is available */ #undef HAVE_OPENSSL /* Define to enable opus (used by opus). */ #undef HAVE_OPUS /* Use Orc */ #undef HAVE_ORC /* Apple Mac OS X operating system detected */ #undef HAVE_OSX /* Use libpng */ #undef HAVE_PNG /* Define if you have POSIX threads libraries and header files. */ #undef HAVE_PTHREAD /* Define to 1 if you have the header file. */ #undef HAVE_PTHREAD_H /* Have PTHREAD_PRIO_INHERIT. */ #undef HAVE_PTHREAD_PRIO_INHERIT /* Define to enable pvrvideosink (used by pvr). */ #undef HAVE_PVR /* Define to enable Qt elements (used by qt). */ #undef HAVE_QT /* Define if Qt Wayland integration is installed */ #undef HAVE_QT_WAYLAND /* Define if Qt X11 integration is installed */ #undef HAVE_QT_X11 /* Define if RDTSC is available */ #undef HAVE_RDTSC /* Define to enable resindvd plugin (used by resindvd). */ #undef HAVE_RESINDVD /* Define to enable rsvg decoder (used by rsvg). */ #undef HAVE_RSVG /* Have RSVG 2.36.2 or newer */ #undef HAVE_RSVG_2_36_2 /* Define to enable rtmp library (used by rtmp). */ #undef HAVE_RTMP /* Define to enable SBC bluetooth audio codec (used by sbc). */ #undef HAVE_SBC /* Define to enable Schroedinger video codec (used by schro). */ #undef HAVE_SCHRO /* Define to enable SDL plug-in (used by sdlvideosink sdlaudiosink). */ #undef HAVE_SDL /* Define to enable POSIX shared memory source and sink (used by shm). */ #undef HAVE_SHM /* Define to enable Smooth Streaming plug-in (used by smoothstreaming). */ #undef HAVE_SMOOTHSTREAMING /* Define to enable sndfile plug-in (used by sfdec sfenc). */ #undef HAVE_SNDFILE /* Define to enable sndio audio (used by sndio). */ #undef HAVE_SNDIO /* Define to enable soundtouch plug-in (used by soundtouch). */ #undef HAVE_SOUNDTOUCH /* Defined if the available libSoundTouch is >= 1.4 */ #undef HAVE_SOUNDTOUCH_1_4 /* Define to enable Spandsp (used by spandsp). */ #undef HAVE_SPANDSP /* Define to enable spc decoder (used by spc). */ #undef HAVE_SPC /* Define to enable srtp library (used by srtp). */ #undef HAVE_SRTP /* Define if libssh2 is available */ #undef HAVE_SSH2 /* Define to 1 if you have the header file. */ #undef HAVE_STDINT_H /* Define to 1 if you have the header file. */ #undef HAVE_STDLIB_H /* Define to 1 if you have the header file. */ #undef HAVE_STRINGS_H /* Define to 1 if you have the header file. */ #undef HAVE_STRING_H /* Define to 1 if you have the header file. */ #undef HAVE_SYS_PARAM_H /* Define to 1 if you have the header file. */ #undef HAVE_SYS_SOCKET_H /* Define to 1 if you have the header file. */ #undef HAVE_SYS_STAT_H /* Define to 1 if you have the header file. */ #undef HAVE_SYS_TIME_H /* Define to 1 if you have the header file. */ #undef HAVE_SYS_TYPES_H /* Define to 1 if you have the header file. */ #undef HAVE_SYS_UTSNAME_H /* Define to enable Teletext decoder (used by teletextdec). */ #undef HAVE_TELETEXTDEC /* Define if libtiger is available */ #undef HAVE_TIGER /* Define to enable timidity midi soft synth plugin (used by timidity). */ #undef HAVE_TIMIDITY /* Define to 1 if you have the header file. */ #undef HAVE_UNISTD_H /* Define to enable UVC H264 (used by uvch264). */ #undef HAVE_UVCH264 /* Define if valgrind should be used */ #undef HAVE_VALGRIND /* Define to enable Video CD (used by vcdsrc). */ #undef HAVE_VCD /* Define to enable VDPAU (used by vdpau). */ #undef HAVE_VDPAU /* Define if building with VideoToolbox */ #undef HAVE_VIDEOTOOLBOX /* Define if building with VideoToolbox >= 10.9.6 */ #undef HAVE_VIDEOTOOLBOX_10_9_6 /* Define to enable vo-aacenc library (used by vo-aacenc). */ #undef HAVE_VOAACENC /* Define to enable vo-amrwbenc library (used by vo-amrwbenc). */ #undef HAVE_VOAMRWBENC /* Define to enable WASAPI plug-in (used by wasapi). */ #undef HAVE_WASAPI /* Define to enable wayland sink (used by wayland ). */ #undef HAVE_WAYLAND /* Define to enable WebP (used by webp ). */ #undef HAVE_WEBP /* Define to enable wildmidi midi soft synth plugin (used by wildmidi). */ #undef HAVE_WILDMIDI /* Have WildMidi 0.2.2 or earlier library */ #undef HAVE_WILDMIDI_0_2_2 /* Defined if compiling for Windows */ #undef HAVE_WIN32 /* Define to 1 if you have the header file. */ #undef HAVE_WINDOWS_H /* Define to enable Windows internet library (used by wininet). */ #undef HAVE_WININET /* Define to 1 if you have the header file. */ #undef HAVE_WININET_H /* Define to enable Winks plug-in (used by winks). */ #undef HAVE_WINKS /* Define to enable winscreencap plug-in (used by winscreencap). */ #undef HAVE_WINSCREENCAP /* Define to 1 if you have the header file. */ #undef HAVE_WINSOCK2_H /* Define to 1 if you have the header file. */ #undef HAVE_WS2TCPIP_H /* Define if you have X11 library */ #undef HAVE_X11 /* Define to enable x265 plug-in (used by x265). */ #undef HAVE_X265 /* Define to enable xvid plugins (used by xvid). */ #undef HAVE_XVID /* Define to enable ZBar barcode detector (used by zbar). */ #undef HAVE_ZBAR /* the host CPU */ #undef HOST_CPU /* library dir */ #undef LIBDIR /* directory in which the detected libvisual's plugins are located */ #undef LIBVISUAL_PLUGINSBASEDIR /* gettext locale dir */ #undef LOCALEDIR /* Define to the sub-directory in which libtool stores uninstalled libraries. */ #undef LT_OBJDIR /* Define if the old MusePack API is used */ #undef MPC_IS_OLD_API /* OpenCV path name */ #undef OPENCV_PATH_NAME /* opencv install prefix */ #undef OPENCV_PREFIX /* Name of package */ #undef PACKAGE /* Define to the address where bug reports for this package should be sent. */ #undef PACKAGE_BUGREPORT /* Define to the full name of this package. */ #undef PACKAGE_NAME /* Define to the full name and version of this package. */ #undef PACKAGE_STRING /* Define to the one symbol short name of this package. */ #undef PACKAGE_TARNAME /* Define to the home page for this package. */ #undef PACKAGE_URL /* Define to the version of this package. */ #undef PACKAGE_VERSION /* directory where plugins are located */ #undef PLUGINDIR /* Define to necessary symbol if this constant uses a non-standard name on your system. */ #undef PTHREAD_CREATE_JOINABLE /* The size of `char', as computed by sizeof. */ #undef SIZEOF_CHAR /* The size of `int', as computed by sizeof. */ #undef SIZEOF_INT /* The size of `long', as computed by sizeof. */ #undef SIZEOF_LONG /* The size of `short', as computed by sizeof. */ #undef SIZEOF_SHORT /* The size of `void*', as computed by sizeof. */ #undef SIZEOF_VOIDP /* Define to 1 if you have the ANSI C header files. */ #undef STDC_HEADERS /* the target CPU */ #undef TARGET_CPU /* Define location of timidity.cfg */ #undef TIMIDITY_CFG /* Use Mali FB EGL platform */ #undef USE_EGL_MALI_FB /* Use RPi platform */ #undef USE_EGL_RPI /* Version number of package */ #undef VERSION /* Define WORDS_BIGENDIAN to 1 if your processor stores words with the most significant byte first (like Motorola and SPARC, unlike Intel). */ #if defined AC_APPLE_UNIVERSAL_BUILD # if defined __BIG_ENDIAN__ # define WORDS_BIGENDIAN 1 # endif #else # ifndef WORDS_BIGENDIAN # undef WORDS_BIGENDIAN # endif #endif /* We need at least WinXP SP2 for __stat64 */ #undef __MSVCRT_VERSION__