README: Fix switch settings for am65xx-evm
authorNikhil Devshatwar <nikhil.nd@ti.com>
Wed, 29 Jul 2020 11:48:49 +0000 (17:18 +0530)
committerNikhil Devshatwar <nikhil.nd@ti.com>
Wed, 29 Jul 2020 11:51:02 +0000 (17:21 +0530)
Fix the switch settings for am65xx-evm board
Do not print the switch settings on error, instead ask
to refer to README
Add instructions for USB cable connection on am65xx-evm

Signed-off-by: Nikhil Devshatwar <nikhil.nd@ti.com>
k3-bootswitch/README.rst
k3-bootswitch/dfu-boot.sh

index 7f48aac48405a483420f7a4501808cebeee42f52..c67d2b3e2ac305ae532e9fdd3ec1b5d964c2b7d6 100644 (file)
@@ -9,6 +9,9 @@ Hardware setup
 --------------
 
 * USB cable should be connected from the board to the Linux PC
+* Note that on am65xx-evm, there is an adapter board for PCIe / USB.
+  This should be used for connecting the USB cable.
+  DFU boot is only supported from this port.
 * UART cable should be connected from the main_uart to Linux PC
 * Default switch settings should be for DFU boot mode
 * Power supply to the board should be connected via phidget USB relay
@@ -18,7 +21,7 @@ Switch settings for DFU boot mode
 ---------------------------------
 
 * j721e-evm settings  => SW8 = 1000 0000      SW9 = 0010 0000      SW3 = 0101 00 1010
-* am65xx-evm settings => SW2 = 0001 0000 00   SW3 = 0000 0000 00   SW4 = 11
+* am65xx-evm settings => SW2 = 0000 0000 00   SW3 = 0001 0000 00   SW4 = 11
 
 Usage
 -----
index 72f31c19679d4e1a7fe6b2f5a28fe7dbd23c7260..1dea18f7013575ec2ac70140b4515ae586572589 100755 (executable)
@@ -63,9 +63,8 @@ msg=$1
                sleep 0.2
        done
        >&2 echo "    >>>> ERROR: Timeout waiting for dfu"
-       >&2 echo "    >>>>        Make sure to connect Type-C cable to EVM and host machine"
-       >&2 echo "    >>>>        Bootswitch settings fot DFU boot:"
-       >&2 echo "    SW8 = 1000 0000    SW9 = 0010 0000    SW3 = 0101 00 1010"
+       >&2 echo "    >>>>        Make sure to connect USB cable from EVM to host machine"
+       >&2 echo "    >>>>        Refer to readme for correct switch settings for DFU bootmode:"
        exit 1
 }