0c36c71d3a062ff0028608bb02452d4678b9a1ad
[glsdk/iodelay-config.git] / iodelay-autogen.py
1 #!/usr/bin/python
2 # Python script to automatically generate the IO pad and delay data
3 # Author:- Nikhil Devshatwar
5 # This script uses regdump of the pad registers to figure out the muxmodes
6 # Based on the pad and muxmode, it find out all possible virtual/manual modes
7 # by referring to the PCT XML model. Using the, selection file, script
8 # decides which modes to be selected. Finally it dumps the required array entries
10 # This script depends on following files:-
11 # * XML data files      - Shipped with the DRA7xx PCT tool
12 # * Pad register dump   - Generate using omapconf dump 0x4a003400 0x4a00380c
13 # * selection file      - List of selected virtual/manual modes to be used
15 import xml.etree.ElementTree as ET
16 import re
17 import argparse
19 # Handle the command line arguments
20 parser = argparse.ArgumentParser(prog='iodelay-autogen.py',
21         description='Python script to generate the IOdelay data.\n' \
22                 'This script refers to the XML data and automatically generates\n' \
23                 'PAD and DELAY data for the same use case.\n' \
24                 'Note that only the PADs which are used in the dump are configured.',
25         epilog='Generate the pad and delay data using pad regdump')
27 parser.add_argument('-d', '--debug', dest='debug',
28         action='store', type=int, choices=[0, 1, 2], default=0,
29         help='set the debug level')
31 parser.add_argument('-i', '--interactive', dest='interactive',
32         action='store', type=int, choices=[0, 1], default=1,
33         help='run interactively with menus for resolving conflicts')
35 parser.add_argument('-f', '--format', dest='format',
36         action='store', type=str, choices=["linux", "uboot", "bios"], default="uboot",
37         help='select the output format to be used')
39 parser.add_argument('-r', '--revision', dest='revision',
40         action='store', type=str, choices=["1.1", "2.0"], default="1.1",
41         help='select the silicon revision')
43 parser.add_argument('-m', '--module', dest='module',
44         action='store', type=str, default="",
45         help='generate only for this module')
47 parser.add_argument('-s', '--strict', dest='strict',
48         action='store_true',
49         help='strict mode - ask for each pad of the group, do not save selection.\n' \
50                 'For some peripherals, same delaymode cannot be used for all the pads.\n' \
51                 'Use this mode to select different modes for each pad')
53 parser.add_argument('-g', '--gpio', dest='gpio',
54         action='store_true',
55         help='generate script to read pad data from GPIO')
57 parser.add_argument('-c', '--check', dest='check_xml',
58         action='store_true',
59         help='check consistency of the XML files and other data')
61 args = parser.parse_args()
62 # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # #
64 PCT_VERSION = "v1.0.7"
65 pad_data_xml = "XMLFiles/CTRL_MODULE_CORE.xml"
66 iod_data_xml = "XMLFiles/IODELAYCONFIG.xml"
67 model_data_xml = "XMLFiles/model_DRA75x_DRA74x_SR" + args.revision + "_" + PCT_VERSION + ".xml"
69 modehelp_file = "guidelines.txt"
70 pad_file = "ctrl-core.dump"
71 sel_file = "selected-modes.txt"
73 # Read the XML file database for pad and delay registers
74 pad_xml = ET.parse(pad_data_xml).getroot()
75 iod_xml = ET.parse(iod_data_xml).getroot()
76 model_xml = ET.parse(model_data_xml).getroot()
78 # Functions to parse the input files and build data structures
79 def read_guidelines(fname):
80         modehelp = {}
81         pattern = re.compile('(.+\w)\t+(.+)')
82         f = open(fname)
83         for line in f.readlines():
84                 list = re.match(pattern, line)
85                 if ( list == None):
86                         continue
87                 mode = list.groups(0)[0]
88                 info = list.groups(0)[1]
89                 modehelp[mode] = info
90                 if (args.debug >= 2):
91                         print "Help: Mode '%s' is used for '%s'" % (mode, info)
92         return modehelp
94 def read_selmodes(fname):
95         sel = {}
96         pattern = re.compile('(\w+)\W*,\W*(\w*)')
97         f = open(fname)
98         for line in f.readlines():
99                 list = re.match(pattern, line)
100                 if ( list == None):
101                         continue
102                 module = list.groups(0)[0]
103                 mode = list.groups(0)[1]
104                 sel[module] = mode
105                 if (args.debug >= 2):
106                         print "INFO: Select '%s' for '%s'" % (mode, module)
107         return sel
109 def read_pad_dump(file):
110         regmap = {}
111         pattern = re.compile('.*(0x[0-9A-F]+).*(0x[0-9A-F]+).*')
112         f = open(file, 'r')
113         for line in f:
114                 list = re.match(pattern, line)
115                 if ( list == None):
116                         continue
117                 addr = int(list.groups(0)[0], 16)
118                 val = int(list.groups(0)[1], 16)
119                 #print "PADXML: Addr = %08x Value = %08x" % (addr, val)
120                 regmap[addr] = val
121         return regmap
122 # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # #
124 # Helper functions to parse XML nodes and get the desired data
125 # Hugely dependent on the XML format of the PCT files
126 # Uses XPath to search elements with queries and filters
127 # Parse the nodes to generate data in desired format
129 def xml_pad_get_name(offset):
130         padlist = pad_xml.findall("register[@offset='0x%X']" % offset)
131         if (len(padlist) == 0):
132                 return "Unknown"
133         else:
134                 return padlist[0].get("id")
136 def xml_pad_get_pin(offset, muxmode):
137         padlist = pad_xml.findall("register[@offset='0x%X']" % offset)
138         if (len(padlist) == 0):
139                 return "Unknown"
140         else:
141                 mux_field = padlist[0].findall("./bitfield[@end='0']")
142                 if (len(mux_field) == 0):
143                         return "Unknown"
144                 modes = mux_field[0].findall("./bitenum[@value='%d']" % muxmode)
145                 if (len(modes) == 0):
146                         return "Unknown"
147                 return modes[0].get("id")
149 def xml_iodelay_get_reg(name):
150         delaylist = iod_xml.findall("register[@id='%s']" % name)
151         if (len(delaylist) == 0):
152                 return 0
153         else:
154                 offset = delaylist[0].get("offset")
155                 #print "IOD: Name = %s Offset = %s" % (del_reg, offset)
156                 return int(offset, 16)
158 def xml_get_virtual(mode):
159         vmodes = {}
160         signal = mode.findtext("signal")
161         for virt in mode.findall("virtualmode/mode"):
162                 virt_mode = virt.findtext("value")
163                 virt_name = virt.findtext("name")
164                 if (virt_name == "NA"):
165                         continue
166                 virt_mode = int(virt_mode)
167                 vmodes[virt_name] = virt_mode
168                 if (args.debug >= 1):
169                         print ("    * VIRTUAL: %s [%s] => delaymode = %d" % (signal, virt_name, virt_mode))
170         return vmodes
172 def xml_get_manual(mode):
173         mmodes = {}
174         signal = mode.findtext("signal")
175         for man in mode.findall("manualmode"):
176                 regname = man.findtext("cfgreg/name")
177                 for sel in man.findall("cfgreg/mode"):
178                         adel = sel.findtext("adelay")
179                         gdel = sel.findtext("gdelay")
180                         man_name = sel.findtext("name")
181                         if (man_name == "NA"):
182                                 continue
183                         adel = int(adel)
184                         gdel = int(gdel)
185                         if (man_name not in mmodes.keys()):
186                                 mmodes[man_name] = []
187                         mmodes[man_name].append((regname, adel, gdel))
188                         if (args.debug >= 1):
189                                 print ("    * MANUAL: %s [%s] => delay[%s] = %d, %d" % (signal, man_name, regname, adel, gdel))
190         return mmodes
192 def xml_find_delaymodes(pad_name, muxmode):
193         padlist = model_xml.findall("padDB/clockNode/type/pad")
194         for pad in padlist:
195                 if (pad_name == pad.findtext("confregisters/regbit/register")):
196                         muxmodes = pad.findall("muxmode")
197                         break
198         if not muxmodes:
199                 return None
200         for mode in muxmodes:
201                 if ("%d" % muxmode == mode.findtext("mode")):
202                         virt = xml_get_virtual(mode)
203                         man = xml_get_manual(mode)
204                         return (virt, man)
205         return None
207 def xml_check_correctness(modehelp):
208         if(args.check_xml == False):
209                 return
211         print "###########################################"
212         print "XML correctness checks:"
213         padcore_list = []
214         padmodel_list = []
215         modes = {}
217         # Fint all the pads in core XML
218         pad_list = pad_xml.findall("register")
219         for i in pad_list:
220                 name = i.get("id")
221                 if (re.match("CTRL_CORE_PAD_.*", name) == None):
222                         continue
223                 padcore_list.append(name)
224         print ">> Total pads defined in core XML = %d" % len(padcore_list)
226         # Find all the pads in model XML
227         pad_list = model_xml.findall("padDB/clockNode/type/pad/confregisters/regbit")
228         for i in pad_list:
229                 name = i.findtext("register")
230                 padmodel_list.append(name)
231         print ">> Total pads defined in model XML = %d" % len(padmodel_list)
233         # Find all the manual modes
234         manmode_list = model_xml.findall("padDB/clockNode/type/pad/muxmode/manualmode/cfgreg/mode")
235         for i in manmode_list:
236                 man_name = i.findtext("name")
237                 modes[man_name] = "manual"
238         # Find all the virtual modes
239         virtmode_list = model_xml.findall("padDB/clockNode/type/pad/muxmode/virtualmode/mode")
240         for i in virtmode_list:
241                 virt_name = i.findtext("name")
242                 modes[virt_name] = "virtual"
243         print ">> Total delaymodes defined in model XML = %d" % len(modes)
245         # Print out all the errors found in the tests
246         print "== Pads defined in core XML but not in model XML =="
247         for i in padcore_list:
248                 if (i not in padmodel_list):
249                         print "\t%s" % i
250         print "== Pads defined in model XML but not in core XML =="
251         for i in padmodel_list:
252                 if (i not in padcore_list):
253                         print "\t%s" % i
255         # Check if description for each mode is available
256         print "== Delaymodes missing description in the guidelines.txt =="
257         for i in modes:
258                 if (i not in modehelp):
259                         print "\t%s" % i
261         print "###########################################"
263 # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # #
265 # Decision point of the script
266 # For each pad/pin, decide what delay method is used
267 # Lookup in the selection file or ask user with a menu
268 def select_mode(pad, pin, module, virt, man, modehelp, sel):
269         modelist = []
270         for modename in virt.keys():
271                 modelist.append(modename)
273         for modename in man.keys():
274                 modelist.append(modename)
276         if (len(modelist) == 0):
277                 return "LEGACY"
279         if (module in sel.keys()):
280                 mode = sel[module]
281                 if (mode == "SKIP" or mode in modelist):
282                         return mode
283                 else:
284                         print("ERR: Invalid delaymode '%s' for module '%s'" % (mode, module))
286         if (args.interactive == 0):
287                 print "WARN: No delay modes for %s found, skipping" % module
288                 mode = "SKIP"
289                 sel[module] = mode
290                 return mode
292         # Display the menu and ask user to select the 'right' mode
293         while True:
294                 print ""
295                 print "MENU: Select delay mode for %s -> %s" % (pad, pin)
296                 i = 0
297                 print "MENU: %d: %s \t\t\t%s" % (i, "SKIP", "Skips this module for now")
298                 for mode in modelist:
299                         i += 1
300                         if (mode in modehelp):
301                                 helptext = modehelp[mode]
302                         else:
303                                 helptext = "Unknown"
304                         print "MENU: %d: %s \t\t%s" % (i, mode, helptext)
305                 try:
306                         choice = int(raw_input("Select delay mode #> "))
307                         if (choice == 0):
308                                 mode = "SKIP"
309                                 break
310                         elif (choice >=0 and choice <= len(modelist)):
311                                 mode = modelist[choice - 1]
312                                 break
313                         print "ERROR: Invalid choice"
314                 except ValueError:
315                         print "ERROR: Invalid choice"
316         print "MENU: Selected mode is %s" % mode
317         print ""
319         return mode
320 # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # #
322 # Pad read using GPIO - Specific to linux only
323 # As each pad is muxed with a SoC gpio (for most of the pads)
324 # It's possible to read the pad data using gpio datain registers
325 # Dump the linux commands to read the gpio registers and read the pad data
326 def pad_dump_gpio(padconf, per_padconf):
327         if(args.gpio == False):
328                 return
330         print "# Read pad signals using GPIO DATA-IN registers"
331         print "# Works only for the input signals"
332         gpio_data_addrs = (0, 0x4ae10138, 0x48055138, 0x48057138, 0x48059138, 0x4805b138, 0x4805d138, 0x48051138, 0x48053138)
333         for i in padconf:
334                 (pad_name, pin_name, addr, val, delayinfo) = i
336                 offset = addr - 0x4a002000
337                 gpio_name = xml_pad_get_pin(offset, 14)
338                 matchlist = re.match("GPIO(.)_(.)", gpio_name)
339                 if (matchlist == None):
340                         print "ERR: No GPIO for pad %s" % pad_name
341                         continue
343                 inst = int(matchlist.groups(0)[0])
344                 bit = int(matchlist.groups(0)[1])
345                 gpio_addr = gpio_data_addrs[inst]
347                 print "#Read GPIO%d_%d to sample %s" % (inst, bit, pin_name)
348                 print " echo %d > /sys/class/gpio/export 2>/dev/null;" % ((inst - 1) * 32)
349                 print " val=`omapconf read 0x%x 2>&1 | grep -v \"support\"`;" % gpio_addr
350                 print " status=$((0x$val >> %d & 0x1));" % bit
351                 print " echo -e \"%s (%s)\t = $status\";" % (pin_name, gpio_name)
352                 print ""
353         print ""
354 # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # #
356 # Generate the final pad and delay data in the required format
357 def format_pad_regs(padconf, per_padconf):
358         print "###########################################"
359         print "Pad data output (with the delay modes)"
360         print "###########################################"
361         if (args.format == "uboot"):
362                 uboot_format_pad_regs(padconf, per_padconf)
363         elif (args.format == "linux"):
364                 linux_format_pad_regs(padconf, per_padconf)
365         elif (args.format == "bios"):
366                 bios_format_pad_regs(padconf, per_padconf)
367         else:
368                 print "ERR: Format %s not suppported" % args.format
370 def format_delay_regs(delayconf, per_delayconf):
371         print "#########################################"
372         print "Delay data output (for manual modes)"
373         print "#########################################"
374         if (args.format == "uboot"):
375                 uboot_format_delay_regs(delayconf, per_delayconf)
376         elif (args.format == "linux"):
377                 linux_format_delay_regs(delayconf, per_delayconf)
378         elif (args.format == "bios"):
379                 bios_format_delay_regs(delayconf, per_delayconf)
380         else:
381                 print "ERR: Format %s not suppported" % args.format
383 def get_pin_info(val):
384         inp_en = (val >> 18) & 0x1
385         pulltype = (val >> 17) & 0x1
386         pull_dis = (val >> 16) & 0x1
387         pin = "PIN"
388         if (inp_en):
389                 pin += "_INPUT"
390         else:
391                 pin += "_OUTPUT"
392         if (pull_dis == 0):
393                 if (pulltype):
394                         pin += "_PULLUP"
395                 else:
396                         pin += "_PULLDOWN"
397         return pin
399 # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # #
401 # Generate output in u-boot format
402 def uboot_format_pad_regs(padconf, per_padconf):
403         print "\nconst struct pad_conf_entry dra74x_core_padconf_array[] = {"
404         for i in padconf:
405                 (pad_name, pin_name, addr, val, delayinfo) = i
407                 if (re.match("MMC.*", pin_name) != None):
408                         print "WARN: Skipping MMC padconf in uboot"
409                         continue
411                 muxmode = val & 0xf
412                 (method, data) = delayinfo
413                 if (method == "LEGACY"):
414                         extramode = ""
415                 elif (method == "VIRTUAL"):
416                         delaymode = data
417                         extramode = " | VIRTUAL_MODE%d" % delaymode
418                 elif (method == "MANUAL"):
419                         extramode = " | MANUAL_MODE"
420                 else:
421                         print "ERR: Invalid method %s" % method
423                 pin_info = get_pin_info(val) + extramode
424                 pad_short = re.sub("CTRL_CORE_PAD_", "", pad_name)
425                 comment = (pad_short + "." + pin_name).lower()
427                 print "\t{ %s, (M%d | %s) },\t/* %s */" % (pad_short, muxmode, pin_info, comment)
428         print "};\n"
430 def uboot_format_delay_regs(delayconf, per_delayconf):
431         print "\nconst struct iodelay_cfg_entry dra742_iodelay_cfg_array[] = {"
432         for i in delayconf:
433                 (pad_name, pin_name, regname, del_offset, man_name, adel, gdel) = i
435                 if (re.match("MMC.*", pin_name) != None):
436                         print "WARN: Skipping MMC delayconf in uboot"
437                         continue
439                 print "\t{ 0x%04X, %5d, %5d },\t/* %s */" % (del_offset, adel, gdel, regname)
440         print "};\n"
442 # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # #
444 # Generate output in linux format
445 def linux_format_pad_regs(padconf, per_padconf):
446         print "&dra7_pmx_core {"
447         for per in per_padconf:
449                 if (re.match("MMC.*", per) == None):
450                         print "ERR: Only MMC padconf is recommended in kernel"
451                         continue
453                 dtsnode = ("%s_pins_default" % per).lower()
454                 print ""
455                 print "\t%s: %s {" % (dtsnode, dtsnode)
456                 print "\t\tpinctrl-single,pins = <"
457                 for i in per_padconf[per]:
458                         (pad_name, pin_name, addr, val, delayinfo) = i
460                         muxmode = val & 0xf
461                         (method, data) = delayinfo
462                         if (method == "LEGACY"):
463                                 extramode = ""
464                         elif (method == "VIRTUAL"):
465                                 delaymode = data
466                                 extramode = " | VIRTUAL_MODE%d" % delaymode
467                         elif (method == "MANUAL"):
468                                 extramode = " | MANUAL_MODE"
469                         else:
470                                 print "ERR: Invalid method %s" % method
472                         pin_info = get_pin_info(val) + extramode
473                         pad_short = re.sub("CTRL_CORE_PAD_", "", pad_name)
474                         offset = addr - 0x4a003400
475                         comment = (pad_short + "." + pin_name).lower()
477                         print "\t\t\t0x%03X\t(%s | MUM_MODE%d)\t/* %s */" % (offset, pin_info, muxmode, comment)
478                 print "\t\t>;"
479                 print "\t};"
480         print "};\n"
483 def linux_format_delay_regs(delayconf, per_delayconf):
484         print "&dra7_iodelay_core {"
485         for per in per_delayconf.keys():
487                 if (re.match("MMC.*", per) == None):
488                         print "ERR: Only MMC delayconf is recommended in kernel"
489                         continue
491                 # Get the mode from the first entry
492                 (pad_name, pin_name, regname, del_offset, mode, adel, gdel) = per_delayconf[per][0]
494                 dtsnode = ("%s_iodelay_%s_conf" % (per, mode)).lower()
495                 print "\t%s: %s {" % (dtsnode, dtsnode)
496                 print "\t\tpinctrl-single,pins = <"
497                 for i in per_delayconf[per]:
498                         (pad_name, pin_name, regname, del_offset, mode, adel, gdel) = i
500                         print "\t\t\t0x%03X A_DELAY(%d) | G_DELAY(%d)\t/* %s */" % (del_offset, adel, gdel, regname)
501                 print "\t\t>;"
502                 print "\t};"
503         print "};\n"
505 # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # #
507 # Generate output in bios format
508 def bios_format_pad_regs(padconf, per_padconf):
509         for i in padconf:
510                 (pad_name, pin_name, addr, val, delayinfo) = i
512                 delaylist = []
513                 (method, data) = delayinfo
514                 if (method == "VIRTUAL"):
515                         virt_mode = data
516                         val = val | ( virt_mode<< 4)
517                         val = val | (1 << 8)
518                 elif (method == "MANUAL"):
519                         delaylist = data
520                         val = val | (1 << 8)
522                 offset = addr - 0x4a003400
523                 out_delreg = out_adel = out_gdel = 0
524                 in_delreg  = in_adel  = in_gdel  = 0
525                 oen_delreg = oen_adel = oen_gdel = 0
527                 for j in delaylist:
528                         (regname, adel, gdel) = j
529                         if (re.match(".*_IN", regname) != None):
530                                 in_delreg = xml_iodelay_get_reg(regname)
531                                 in_adel = adel
532                                 in_gdel = gdel
533                         elif (re.match(".*_OEN", regname) != None):
534                                 oen_delreg = xml_iodelay_get_reg(regname)
535                                 oen_adel = adel
536                                 oen_gdel = gdel
537                         elif (re.match(".*_OUT", regname) != None):
538                                 out_delreg = xml_iodelay_get_reg(regname)
539                                 out_adel = adel
540                                 out_gdel = gdel
541                 indel  = "{ 0x%04X, %4d, %4d }" % (in_delreg,  in_adel,  in_gdel)
542                 oendel = "{ 0x%04X, %4d, %4d }" % (oen_delreg, oen_adel, oen_gdel)
543                 outdel = "{ 0x%04X, %4d, %4d }" % (out_delreg, out_adel, out_gdel)
544                 pin_info = get_pin_info(val)
545                 print "\t/* %s -> %s (%s) %s delaymode */" % (pad_name, pin_name, pin_info, method)
546                 print "\t{ 0x%03X, 0x%08X, %s, %s, %s }" % (offset, val, indel, oendel, outdel)
548 def bios_format_delay_regs(delayconf, per_delayconf):
549         print "Manual delays are not configured separately"
550         print "Delays are configured as part of the padconf step only"
552 # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # #
554 # Main execution starts here
555 # * Parse all the XML files - Get the pad data and IOdelay data
556 # * Iterate over the pad register dumps
557 # * For each pad, find out the muxmode being used and the pad direction, etc
558 # * For the muxmode being used, find out available virtual/modes
559 #   - Dump the virtual/manual modes available (based on options)
560 #   - Build up the gpio script to read the pad data using GPIO module
561 # * Select the correct mode to be used
562 #   - Check if the mode is described for the peripheral module, (from selected-modes.txt)
563 #   - Otherwise ask the user (with a menu) to decide the delaymode
564 #     => Update the selection for the whole of the peripheral module
565 #   - Worst case, skip the delaymode for this pad
566 # * Build the pad and delay register information
567 # * Create the dump for pad and delay data in linux/u-boot format
568 # * Dump the delaymode selection for each peripheral
569 # * Dump the GPIO script for each peripheral (all pads grouped together)
572 # Read all the input files and parse the required info
573 modehelp = read_guidelines(modehelp_file)
574 sel = read_selmodes(sel_file)
575 regmap = read_pad_dump(pad_file)
576 reglist = regmap.keys()
578 # List of all the pads being configured
579 padconf = []
580 # List of all the delay registers being configured (for manual mode)
581 delayconf = []
582 # Dictionary of pads grouped by peripheral/module
583 per_padconf = {}
584 # Dictionary of delay registers grouped by peripheral/module
585 per_delayconf = {}
587 xml_check_correctness(modehelp)
588 # Start iterating over each pad
589 for i in range(0, 260):
590         # Find out the muxmode and pad direction, etc
591         addr = 0x4a003400 + i * 4
592         offset = 0x1400 + i * 4
593         dts_offset = offset - 0x1400
595         if (addr not in reglist):
596                 print "WARN: Register dump for pad 0x%X not found" % addr
597                 continue
598         val = regmap[addr]
599         muxmode = val & 0xf
601         # Find out the pin based on the muxmode
602         pad_name = xml_pad_get_name(offset)
603         pin_name = xml_pad_get_pin(offset, muxmode)
604         if (pad_name == "Unknown" or pin_name == "Unknown"):
605                 print "WARN: Cannot find out Pad/Pin name for PAD address 0x%X (%s[%s] = %s)" \
606                 % (addr, pad_name, muxmode, pin_name)
607                 continue
608         if (pin_name == "DRIVER OFF"):
609                 continue
611         # Find out if the delaymode for this module is already selected
612         module = re.match("([^_]+)_.*", pin_name).groups(0)[0]
614         if (args.module != "" and args.module != module):
615                 continue
617         if (args.debug >= 1):
618                 print "\nPAD: %s: Addr= 0x%08X Value = 0x%08X \"%s\"" \
619                 % (pad_name, addr, val, pin_name)
621         # Find out all the possible virtual, manual modes fot the specific pad -> pin combination
622         (virt, man) = xml_find_delaymodes(pad_name, muxmode)
624         # Need to select one out of allowed modes
625         mode = select_mode(pad_name, pin_name, module, virt, man, modehelp, sel)
627         # Remember the selection for that module, for later reuse
628         if (args.strict == False):
629                 sel[module] = mode
631         if (mode == "SKIP"):
632                 continue
633         elif (mode == "LEGACY"):
634                 delayinfo = ("LEGACY", "")
635         elif (mode in virt):
636                 delayinfo = ("VIRTUAL", virt[mode])
637         elif (mode in man):
638                 delayinfo = ("MANUAL", man[mode])
639         else:
640                 print "ERR: Unknown mode '%s' selected" % mode
641                 continue
643         if (args.debug >= 1):
644                 print "  => Using mode %s" % mode
645         paddata = (pad_name, pin_name, addr, val, delayinfo)
646         if (module not in per_padconf.keys()):
647                 per_padconf[module] = []
648         padconf.append(paddata)
649         per_padconf[module].append(paddata)
651         if(mode not in man):
652                 continue
654         # Add the delay data if using manual mode
655         for regval in man[mode]:
656                 (regname, adel, gdel) = regval
657                 del_offset = xml_iodelay_get_reg(regname)
658                 if (del_offset == 0):
659                         print "WARN: Can't find delay offset of register %s" % regname
660                         break
661                 if (args.debug >= 1):
662                         print "  => Manual delay[%s] = (%d, %d)" % (regname, adel, gdel)
663                 delaydata = (pad_name, pin_name, regname, del_offset, mode, adel, gdel)
664                 if (module not in per_delayconf.keys()):
665                         per_delayconf[module] = []
666                 delayconf.append(delaydata)
667                 per_delayconf[module].append(delaydata)
669 print ""
670 print "Total PAD registers: %d" % len(padconf)
671 print "Total DELAY registers: %d" % len(delayconf)
672 print ""
674 format_pad_regs(padconf, per_padconf)
675 format_delay_regs(delayconf, per_delayconf)
676 pad_dump_gpio(padconf, per_padconf)
678 # Dump the final selection for reuse
679 print "Selected modes for each peripheral module\n"
680 for group in sel:
681         print "%s,\t%s" % (group, sel[group])
682 print ""
683 # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # #