script: Correct MMC related warnings in u-boot and kernel
[glsdk/iodelay-config.git] / iodelay-autogen.py
1 #!/usr/bin/python
2 # Python script to automatically generate the IO pad and delay data
3 # Author:- Nikhil Devshatwar
5 # This script uses regdump of the pad registers to figure out the muxmodes
6 # Based on the pad and muxmode, it find out all possible virtual/manual modes
7 # by referring to the PCT XML model. Using the, selection file, script
8 # decides which modes to be selected. Finally it dumps the required array entries
10 # This script depends on following files:-
11 # * XML data files      - Shipped with the DRA7xx PCT tool
12 # * Pad register dump   - Generate using omapconf dump 0x4a003400 0x4a00380c
13 # * selection file      - List of selected virtual/manual modes to be used
15 import xml.etree.ElementTree as ET
16 import re
17 import argparse
19 # Handle the command line arguments
20 parser = argparse.ArgumentParser(prog='iodelay-autogen.py',
21         description='Python script to generate the IOdelay data.\n' \
22                 'This script refers to the XML data and automatically generates\n' \
23                 'PAD and DELAY data for the same use case.\n' \
24                 'Note that only the PADs which are used in the dump are configured.',
25         epilog='Generate the pad and delay data using pad register dumps. For this,\n' \
26                 'Run omapconf dump 0x4a003400 0x4a00380c and save the output')
28 parser.add_argument('-d', '--debug', dest='debug',
29         action='store', type=int, choices=[0, 1, 2], default=0,
30         help='set the debug level')
32 parser.add_argument('-i', '--interactive', dest='interactive',
33         action='store', type=int, choices=[0, 1], default=1,
34         help='run interactively with menus for resolving conflicts')
36 parser.add_argument('-f', '--format', dest='format',
37         action='store', type=str, choices=["linux", "uboot", "bios"], default="uboot",
38         help='select the output format to be used')
40 parser.add_argument('-r', '--revision', dest='revision',
41         action='store', type=str, choices=["1.0", "1.1", "2.0"], default="1.1",
42         help='select the silicon revision')
44 parser.add_argument('-p', '--part', dest='part',
45         action='store', type=str, choices=["dra74x", "dra75x", "dra72x"], default="dra74x",
46         help='select the device part')
48 parser.add_argument('-m', '--module', dest='module',
49         action='store', type=str, default="",
50         help='generate only for modules matching the provided RE')
52 parser.add_argument('-s', '--strict', dest='strict',
53         action='store_true',
54         help='strict mode - ask for each pad of the group, do not save selection.\n' \
55                 'For some peripherals, same delaymode cannot be used for all the pads.\n' \
56                 'Use this mode to select different modes for each pad')
58 parser.add_argument('-g', '--gpio', dest='gpio',
59         action='store_true',
60         help='generate script to read pad data from GPIO')
62 parser.add_argument('-c', '--check', dest='check_xml',
63         action='store_true',
64         help='check consistency of the XML files and other data')
66 args = parser.parse_args()
68 # Some more knobs for developers, Don't want to expose them to cmd line
69 args.resetslew = True
71 # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # #
73 VERSION = "2.4"
75 if (args.part == "dra74x" or args.part == "dra75x"):
76         XML_PATH = "XMLFiles/DRA75x_DRA74x"
77         PART = "DRA75x_DRA74x"
78         PCT_VERSION = "v1.0.10"
79 elif (args.part == "dra72x"):
80         XML_PATH = "XMLFiles/DRA72x"
81         PART = "DRA72x"
82         PCT_VERSION = "v1.0.6"
84 pad_data_xml   = XML_PATH + "/CTRL_MODULE_CORE.xml"
85 iod_data_xml   = XML_PATH + "/IODELAYCONFIG.xml"
86 model_data_xml = XML_PATH + "/model_" + PART + "_SR" + args.revision + "_" + PCT_VERSION + ".xml"
87 modehelp_file  = XML_PATH + "/guidelines.txt"
89 pad_file = "ctrl-core.dump"
90 sel_file = "selected-modes.txt"
92 print "iodelay-autogen.py - Python script to generate the IOdelay data."
93 print "v" + VERSION + " using PCT version " + PCT_VERSION
94 print "Parsing PCT data from " + model_data_xml + "..."
95 print ""
97 # Read the XML file database for pad and delay registers
98 pad_xml = ET.parse(pad_data_xml).getroot()
99 iod_xml = ET.parse(iod_data_xml).getroot()
100 model_xml = ET.parse(model_data_xml).getroot()
102 # Functions to parse the input files and build data structures
103 def read_guidelines(fname):
104         modehelp = {}
105         pattern = re.compile('([^\t.]+\w)\t+(.+)')
106         f = open(fname)
107         for line in f.readlines():
108                 list = re.match(pattern, line)
109                 if ( list == None):
110                         continue
111                 mode = list.groups(0)[0]
112                 info = list.groups(0)[1]
113                 modehelp[mode] = info
114                 if (args.debug >= 2):
115                         print "Help: Mode '%s' is used for '%s'" % (mode, info)
116         return modehelp
118 def read_selmodes(fname):
119         sel = {}
120         pattern = re.compile('(\w+)\W*,\W*(\w*)')
121         f = open(fname)
122         for line in f.readlines():
123                 list = re.match(pattern, line)
124                 if ( list == None):
125                         continue
126                 module = list.groups(0)[0]
127                 mode = list.groups(0)[1]
128                 sel[module] = mode
129                 if (args.debug >= 2):
130                         print "INFO: Select '%s' for '%s'" % (mode, module)
131         return sel
133 def read_pad_dump(file):
134         regmap = {}
135         pattern = re.compile('.*(0x[0-9A-F]+).*(0x[0-9A-F]+).*')
136         f = open(file, 'r')
137         for line in f:
138                 list = re.match(pattern, line)
139                 if ( list == None):
140                         continue
141                 addr = int(list.groups(0)[0], 16)
142                 val = int(list.groups(0)[1], 16)
143                 #print "PADXML: Addr = %08x Value = %08x" % (addr, val)
144                 regmap[addr] = val
145         return regmap
146 # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # #
148 # Helper functions to parse XML nodes and get the desired data
149 # Hugely dependent on the XML format of the PCT files
150 # Uses XPath to search elements with queries and filters
151 # Parse the nodes to generate data in desired format
153 def xml_pad_get_name(offset):
154         padlist = pad_xml.findall("register[@offset='0x%X']" % offset)
155         if (len(padlist) == 0):
156                 return "Unknown"
157         else:
158                 return padlist[0].get("id")
160 def xml_pad_get_slew(offset):
161         padlist = pad_xml.findall("register[@offset='0x%X']" % offset)
162         if (len(padlist) == 0):
163                 return 0x0
164         else:
165                 bitlist = padlist[0].findall("bitfield[@begin='19']")
166                 if (len(bitlist) == 0):
167                         return 0x0
168                 else:
169                         return int(bitlist[0].get("resetval"), 16)
171 def xml_pad_get_pin(offset, muxmode):
172         padlist = pad_xml.findall("register[@offset='0x%X']" % offset)
173         if (len(padlist) == 0):
174                 return "Unknown"
175         else:
176                 mux_field = padlist[0].findall("./bitfield[@end='0']")
177                 if (len(mux_field) == 0):
178                         return "Unknown"
179                 modes = mux_field[0].findall("./bitenum[@value='%d']" % muxmode)
180                 if (len(modes) == 0):
181                         return "Unknown"
182                 return modes[0].get("id")
184 def xml_iodelay_get_reg(name):
185         delaylist = iod_xml.findall("register[@id='%s']" % name)
186         if (len(delaylist) == 0):
187                 return 0
188         else:
189                 offset = delaylist[0].get("offset")
190                 #print "IOD: Name = %s Offset = %s" % (del_reg, offset)
191                 return int(offset, 16)
193 def xml_get_virtual(mode):
194         vmodes = {}
195         signal = mode.findtext("signal")
196         for virt in mode.findall("virtualmode/mode"):
197                 virt_mode = virt.findtext("value")
198                 virt_name = virt.findtext("name")
199                 if (virt_name == "NA"):
200                         continue
201                 virt_mode = int(virt_mode)
202                 vmodes[virt_name] = virt_mode
203                 if (args.debug >= 1):
204                         print ("    * VIRTUAL: %s [%s] => delaymode = %d" % (signal, virt_name, virt_mode))
205         return vmodes
207 def xml_get_manual(mode):
208         mmodes = {}
209         signal = mode.findtext("signal")
210         for man in mode.findall("manualmode"):
211                 regname = man.findtext("cfgreg/name")
212                 for sel in man.findall("cfgreg/mode"):
213                         adel = sel.findtext("adelay")
214                         gdel = sel.findtext("gdelay")
215                         man_name = sel.findtext("name")
216                         if (man_name == "NA"):
217                                 continue
218                         adel = int(adel)
219                         gdel = int(gdel)
220                         if (man_name not in mmodes.keys()):
221                                 mmodes[man_name] = []
222                         mmodes[man_name].append((regname, adel, gdel))
223                         if (args.debug >= 1):
224                                 print ("    * MANUAL: %s [%s] => delay[%s] = %d, %d" % (signal, man_name, regname, adel, gdel))
225         return mmodes
227 def xml_find_delaymodes(pad_name, muxmode):
228         padlist = model_xml.findall("padDB/clockNode/type/pad")
229         for pad in padlist:
230                 if (pad_name == pad.findtext("confregisters/regbit/register")):
231                         muxmodes = pad.findall("muxmode")
232                         break
233         if not muxmodes:
234                 return None
235         for mode in muxmodes:
236                 if ("%d" % muxmode == mode.findtext("mode")):
237                         virt = xml_get_virtual(mode)
238                         man = xml_get_manual(mode)
239                         return (virt, man)
240         return None
242 def xml_check_correctness(modehelp):
243         if(args.check_xml == False):
244                 return
246         print "###########################################"
247         print "XML correctness checks:"
248         padcore_list = []
249         padmodel_list = []
250         modes = {}
252         # Fint all the pads in core XML
253         pad_list = pad_xml.findall("register")
254         for i in pad_list:
255                 name = i.get("id")
256                 if (re.match("CTRL_CORE_PAD_.*", name) == None):
257                         continue
258                 padcore_list.append(name)
259         print ">> Total pads defined in core XML = %d" % len(padcore_list)
261         # Find all the pads in model XML
262         pad_list = model_xml.findall("padDB/clockNode/type/pad/confregisters/regbit")
263         for i in pad_list:
264                 name = i.findtext("register")
265                 padmodel_list.append(name)
266         print ">> Total pads defined in model XML = %d" % len(padmodel_list)
268         # Find all the manual modes
269         manmode_list = model_xml.findall("padDB/clockNode/type/pad/muxmode/manualmode/cfgreg/mode")
270         for i in manmode_list:
271                 man_name = i.findtext("name")
272                 modes[man_name] = "manual"
273         # Find all the virtual modes
274         virtmode_list = model_xml.findall("padDB/clockNode/type/pad/muxmode/virtualmode/mode")
275         for i in virtmode_list:
276                 virt_name = i.findtext("name")
277                 modes[virt_name] = "virtual"
278         print ">> Total delaymodes defined in model XML = %d" % len(modes)
280         # Print out all the errors found in the tests
281         print "== Pads defined in core XML but not in model XML =="
282         for i in padcore_list:
283                 if (i not in padmodel_list):
284                         print "\t%s" % i
285         print "== Pads defined in model XML but not in core XML =="
286         for i in padmodel_list:
287                 if (i not in padcore_list):
288                         print "\t%s" % i
290         # Check if description for each mode is available
291         print "== Delaymodes missing description in the guidelines.txt =="
292         for i in modes:
293                 if (i not in modehelp):
294                         print "\t%s" % i
296         print "###########################################"
298 # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # #
300 # Decision point of the script
301 # For each pad/pin, decide what delay method is used
302 # Lookup in the selection file or ask user with a menu
303 def select_mode(pad, pin, module, virt, man, modehelp, sel):
304         modelist = []
305         for modename in virt.keys():
306                 modelist.append(modename)
308         for modename in man.keys():
309                 modelist.append(modename)
311         if (len(modelist) == 0):
312                 return "LEGACY"
314         if (module in sel.keys()):
315                 mode = sel[module]
316                 if (mode == "SKIP" or mode == "LEGACY" or mode in modelist):
317                         return mode
318                 else:
319                         print("ERR: Invalid delaymode '%s' for module '%s'" % (mode, module))
321         if (args.interactive == 0):
322                 print "WARN: No delay modes for %s found, skipping" % module
323                 mode = "SKIP"
324                 return mode
326         # Display the menu and ask user to select the 'right' mode
327         while True:
328                 print ""
329                 print "MENU: Select delay mode for %s -> %s" % (pad, pin)
330                 i = 0
331                 print "MENU: %d: %s \t\t\t%s" % (i, "SKIP", "Skips this module for now")
332                 i = 1
333                 print "MENU: %d: %s \t\t%s" % (i, "LEGACY", "No external delay config (No virtual/manual needed)")
334                 for mode in modelist:
335                         i += 1
336                         if (mode in modehelp):
337                                 helptext = modehelp[mode]
338                         else:
339                                 helptext = "Unknown"
340                         print "MENU: %d: %s \t\t%s" % (i, mode, helptext)
341                 try:
342                         choice = int(raw_input("Select delay mode #> "))
343                         if (choice == 0):
344                                 mode = "SKIP"
345                                 break
346                         elif (choice == 1):
347                                 mode = "LEGACY"
348                                 break
349                         elif (choice >=2 and choice <= len(modelist) + 1):
350                                 mode = modelist[choice - 2]
351                                 break
352                         print "ERROR: Invalid choice"
353                 except ValueError:
354                         print "ERROR: Invalid choice"
355         print "MENU: Selected mode is %s" % mode
356         print ""
358         return mode
359 # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # #
361 # Pad read using GPIO - Specific to linux only
362 # As each pad is muxed with a SoC gpio (for most of the pads)
363 # It's possible to read the pad data using gpio datain registers
364 # Dump the linux commands to read the gpio registers and read the pad data
365 def pad_dump_gpio(padconf, per_padconf):
366         if(args.gpio == False):
367                 return
369         print "# Read pad signals using GPIO DATA-IN registers"
370         print "# Works only for the input signals"
371         gpio_data_addrs = (0, 0x4ae10138, 0x48055138, 0x48057138, 0x48059138, 0x4805b138, 0x4805d138, 0x48051138, 0x48053138)
372         for i in padconf:
373                 (pad_name, pin_name, addr, val, mode, delayinfo) = i
375                 offset = addr - 0x4a002000
376                 gpio_name = xml_pad_get_pin(offset, 14)
377                 matchlist = re.match("GPIO(.)_(.*)", gpio_name)
378                 if (matchlist == None):
379                         print "ERR: No GPIO for pad %s" % pad_name
380                         continue
382                 inst = int(matchlist.groups(0)[0])
383                 bit = int(matchlist.groups(0)[1])
384                 gpio_addr = gpio_data_addrs[inst]
386                 print "#Read GPIO%d_%d to sample %s" % (inst, bit, pin_name)
387                 print " echo %d > /sys/class/gpio/export 2>/dev/null;" % ((inst - 1) * 32)
388                 print " val=`omapconf read 0x%x 2>&1 | grep -v \"support\"`;" % gpio_addr
389                 print " status=$((0x$val >> %d & 0x1));" % bit
390                 print " echo -e \"%s (%s)\t = $status\";" % (pin_name, gpio_name)
391                 print ""
392         print ""
393 # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # #
395 # Generate the final pad and delay data in the required format
396 def format_pad_regs(padconf, per_padconf):
397         print "###########################################"
398         print "Pad data output (with the delay modes)"
399         print "###########################################"
400         if (args.format == "uboot"):
401                 uboot_format_pad_regs(padconf, per_padconf)
402         elif (args.format == "linux"):
403                 linux_format_pad_regs(padconf, per_padconf)
404         elif (args.format == "bios"):
405                 bios_format_pad_regs(padconf, per_padconf)
406         else:
407                 print "ERR: Format %s not suppported" % args.format
409 def format_delay_regs(delayconf, per_delayconf):
410         print "#########################################"
411         print "Delay data output (for manual modes)"
412         print "#########################################"
413         if (args.format == "uboot"):
414                 uboot_format_delay_regs(delayconf, per_delayconf)
415         elif (args.format == "linux"):
416                 linux_format_delay_regs(delayconf, per_delayconf)
417         elif (args.format == "bios"):
418                 bios_format_delay_regs(delayconf, per_delayconf)
419         else:
420                 print "ERR: Format %s not suppported" % args.format
422 def get_pin_info(val):
423         slew_fast = (val >> 19) & 0x1
424         inp_en = (val >> 18) & 0x1
425         pulltype = (val >> 17) & 0x1
426         pull_dis = (val >> 16) & 0x1
427         pin = "PIN"
428         if (inp_en):
429                 pin += "_INPUT"
430         else:
431                 pin += "_OUTPUT"
432         if (pull_dis == 0):
433                 if (pulltype):
434                         pin += "_PULLUP"
435                 else:
436                         pin += "_PULLDOWN"
437         if (slew_fast):
438                 pin += " | SLEWCONTROL"
439         return pin
441 # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # #
443 # Generate output in u-boot format
444 def uboot_format_pad_regs(padconf, per_padconf):
445         print "\nconst struct pad_conf_entry dra74x_core_padconf_array[] = {"
446         for i in padconf:
447                 (pad_name, pin_name, addr, val, mode, delayinfo) = i
449                 muxmode = val & 0xf
450                 (method, data) = delayinfo
451                 if (method == "LEGACY"):
452                         extramode = ""
453                 elif (method == "VIRTUAL"):
454                         delaymode = data
455                         extramode = " | VIRTUAL_MODE%d" % delaymode
456                 elif (method == "MANUAL"):
457                         extramode = " | MANUAL_MODE"
458                 else:
459                         print "ERR: Invalid method %s" % method
461                 pin_info = get_pin_info(val) + extramode
462                 pad_short = re.sub("CTRL_CORE_PAD_", "", pad_name)
463                 comment = (pad_short + "." + pin_name).lower()
465                 print "\t{ %s, (M%d | %s) },\t/* %s */" % (pad_short, muxmode, pin_info, comment)
466         print "};\n"
468 def uboot_format_delay_regs(delayconf, per_delayconf):
469         manual_del = []
470         for i in delayconf:
471                 (pad_name, pin_name, regname, del_offset, man_name, adel, gdel) = i
473                 entry = (del_offset, adel, gdel, regname, pin_name, man_name)
474                 manual_del.append(entry)
476         es_rev = args.revision.replace('.', '_')
477         print "\nconst struct iodelay_cfg_entry dra742_es" + es_rev + "_iodelay_cfg_array[] = {"
478         for entry in sorted(manual_del):
479                 print "\t{ 0x%04X, %5d, %5d },\t/* %s : %s - %s */" % entry
480         print "};\n"
482 # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # #
484 # Generate output in linux format
485 def linux_format_pad_regs(padconf, per_padconf):
486         print "&dra7_pmx_core {"
487         for per in per_padconf:
489                 if (re.match("MMC.*", per) == None):
490                         print "WARN: Only MMC padconf is recommended in kernel"
492                 # Get the mode from the first entry
493                 (pad_name, pin_name, addr, val, mode, delayinfo) = per_padconf[per][0]
495                 dtsnode = ("%s_pins_%s" % (per, mode)).lower()
496                 print ""
497                 print "\t%s: %s {" % (dtsnode, dtsnode)
498                 print "\t\tpinctrl-single,pins = <"
499                 for i in per_padconf[per]:
500                         (pad_name, pin_name, addr, val, mode, delayinfo) = i
502                         muxmode = val & 0xf
503                         (method, data) = delayinfo
504                         if (method == "LEGACY"):
505                                 extramode = ""
506                         elif (method == "VIRTUAL"):
507                                 delaymode = data
508                                 extramode = " | MUX_VIRTUAL_MODE%d" % delaymode
509                         elif (method == "MANUAL"):
510                                 extramode = " | MANUAL_MODE"
511                         else:
512                                 print "ERR: Invalid method %s" % method
514                         pin_info = get_pin_info(val) + extramode
515                         pad_short = re.sub("CTRL_CORE_PAD_", "", pad_name)
516                         offset = addr - 0x4a003400
517                         comment = (pad_short + "." + pin_name).lower()
519                         print "\t\t\t0x%03X\t(%s | MUX_MODE%d)\t/* %s */" % (offset, pin_info, muxmode, comment)
520                 print "\t\t>;"
521                 print "\t};"
522         print "};\n"
525 def linux_format_delay_regs(delayconf, per_delayconf):
526         print "&dra7_iodelay_core {"
527         for per in per_delayconf.keys():
529                 if (re.match("MMC.*", per) == None):
530                         print "WARN: Only MMC delayconf is recommended in kernel"
532                 # Get the mode from the first entry
533                 (pad_name, pin_name, regname, del_offset, mode, adel, gdel) = per_delayconf[per][0]
535                 dtsnode = ("%s_iodelay_%s_conf" % (per, mode)).lower()
536                 print "\t%s: %s {" % (dtsnode, dtsnode)
537                 print "\t\tpinctrl-single,pins = <"
538                 for i in per_delayconf[per]:
539                         (pad_name, pin_name, regname, del_offset, mode, adel, gdel) = i
541                         print "\t\t\t0x%03X (A_DELAY(%d) | G_DELAY(%d))\t/* %s */" % (del_offset, adel, gdel, regname)
542                 print "\t\t>;"
543                 print "\t};"
544         print "};\n"
546 # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # #
548 # Generate output in bios format
549 def bios_format_pad_regs(padconf, per_padconf):
550         for i in padconf:
551                 (pad_name, pin_name, addr, val, mode, delayinfo) = i
553                 delaylist = []
554                 (method, data) = delayinfo
555                 if (method == "VIRTUAL"):
556                         virt_mode = data
557                         val = val | ( virt_mode<< 4)
558                         val = val | (1 << 8)
559                 elif (method == "MANUAL"):
560                         delaylist = data
561                         val = val | (1 << 8)
563                 offset = addr - 0x4a003400
564                 out_delreg = out_adel = out_gdel = 0
565                 in_delreg  = in_adel  = in_gdel  = 0
566                 oen_delreg = oen_adel = oen_gdel = 0
568                 for j in delaylist:
569                         (regname, adel, gdel) = j
570                         if (re.match(".*_IN", regname) != None):
571                                 in_delreg = xml_iodelay_get_reg(regname)
572                                 in_adel = adel
573                                 in_gdel = gdel
574                         elif (re.match(".*_OEN", regname) != None):
575                                 oen_delreg = xml_iodelay_get_reg(regname)
576                                 oen_adel = adel
577                                 oen_gdel = gdel
578                         elif (re.match(".*_OUT", regname) != None):
579                                 out_delreg = xml_iodelay_get_reg(regname)
580                                 out_adel = adel
581                                 out_gdel = gdel
582                 indel  = "{ 0x%04X, %4d, %4d }" % (in_delreg,  in_adel,  in_gdel)
583                 oendel = "{ 0x%04X, %4d, %4d }" % (oen_delreg, oen_adel, oen_gdel)
584                 outdel = "{ 0x%04X, %4d, %4d }" % (out_delreg, out_adel, out_gdel)
585                 pin_info = get_pin_info(val)
586                 print "\t/* %s -> %s (%s) %s delaymode */" % (pad_name, pin_name, pin_info, method)
587                 print "\t{ 0x%03X, 0x%08X, %s, %s, %s }" % (offset, val, indel, oendel, outdel)
589 def bios_format_delay_regs(delayconf, per_delayconf):
590         print "Manual delays are not configured separately"
591         print "Delays are configured as part of the padconf step only"
593 # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # #
595 # Main execution starts here
596 # * Parse all the XML files - Get the pad data and IOdelay data
597 # * Iterate over the pad register dumps
598 # * For each pad, find out the muxmode being used and the pad direction, etc
599 # * For the muxmode being used, find out available virtual/modes
600 #   - Dump the virtual/manual modes available (based on options)
601 #   - Build up the gpio script to read the pad data using GPIO module
602 # * Select the correct mode to be used
603 #   - Check if the mode is described for the peripheral module, (from selected-modes.txt)
604 #   - Otherwise ask the user (with a menu) to decide the delaymode
605 #     => Update the selection for the whole of the peripheral module
606 #   - Worst case, skip the delaymode for this pad
607 # * Build the pad and delay register information
608 # * Create the dump for pad and delay data in linux/u-boot format
609 # * Dump the delaymode selection for each peripheral
610 # * Dump the GPIO script for each peripheral (all pads grouped together)
613 # Read all the input files and parse the required info
614 modehelp = read_guidelines(modehelp_file)
615 sel = read_selmodes(sel_file)
616 regmap = read_pad_dump(pad_file)
617 reglist = regmap.keys()
619 # List of all the pads being configured
620 padconf = []
621 # List of all the delay registers being configured (for manual mode)
622 delayconf = []
623 # Dictionary of pads grouped by peripheral/module
624 per_padconf = {}
625 # Dictionary of delay registers grouped by peripheral/module
626 per_delayconf = {}
628 xml_check_correctness(modehelp)
630 # Start iterating over each pad
631 for i in range(0, 260):
632         # Find out the muxmode and pad direction, etc
633         addr = 0x4a003400 + i * 4
634         offset = 0x1400 + i * 4
635         dts_offset = offset - 0x1400
637         if (addr not in reglist):
638                 print "WARN: Register dump for pad 0x%X not found" % addr
639                 continue
640         val = regmap[addr]
641         muxmode = val & 0xf
643         # Find out the pin based on the muxmode
644         pad_name = xml_pad_get_name(offset)
645         pin_name = xml_pad_get_pin(offset, muxmode)
646         if (pad_name == "Unknown" or pin_name == "Unknown"):
647                 print "WARN: Cannot find out Pad/Pin name for PAD address 0x%X (%s[%s] = %s)" \
648                 % (addr, pad_name, muxmode, pin_name)
649                 continue
650         if (pin_name == "DRIVER OFF"):
651                 continue
653         # Find out if the delaymode for this module is already selected
654         module = re.match("([^_]+)_.*", pin_name).groups(0)[0]
656         if (args.module != "" and re.match("%s" % args.module, module) == None):
657                 continue
659         # It is recommended to keep the reset value of the slewcontrol bit
660         # Find out the reset value from XML and update if required
661         if (args.resetslew):
662                 val |= (xml_pad_get_slew(offset) & 0x1) << 19
664         if (args.debug >= 1):
665                 print "\nPAD: %s: Addr= 0x%08X Value = 0x%08X \"%s\"" \
666                 % (pad_name, addr, val, pin_name)
668         # Find out all the possible virtual, manual modes fot the specific pad -> pin combination
669         (virt, man) = xml_find_delaymodes(pad_name, muxmode)
671         # Need to select one out of allowed modes
672         mode = select_mode(pad_name, pin_name, module, virt, man, modehelp, sel)
674         # Remember the selection for that module, for later reuse
675         if (args.strict == False and module not in sel.keys()):
676                 sel[module] = mode
678         if (mode == "SKIP"):
679                 continue
680         elif (mode == "LEGACY"):
681                 delayinfo = ("LEGACY", "")
682         elif (mode in virt):
683                 delayinfo = ("VIRTUAL", virt[mode])
684         elif (mode in man):
685                 delayinfo = ("MANUAL", man[mode])
686         else:
687                 print "ERR: Unknown mode '%s' selected" % mode
688                 continue
690         if (args.debug >= 1):
691                 print "  => Using mode %s" % mode
692         paddata = (pad_name, pin_name, addr, val, mode, delayinfo)
693         if (module not in per_padconf.keys()):
694                 per_padconf[module] = []
695         padconf.append(paddata)
696         per_padconf[module].append(paddata)
698         if(mode not in man):
699                 continue
701         # Add the delay data if using manual mode
702         for regval in man[mode]:
703                 (regname, adel, gdel) = regval
704                 del_offset = xml_iodelay_get_reg(regname)
705                 if (del_offset == 0):
706                         print "WARN: Can't find delay offset of register %s" % regname
707                         break
708                 if (args.debug >= 1):
709                         print "  => Manual delay[%s] = (%d, %d)" % (regname, adel, gdel)
710                 delaydata = (pad_name, pin_name, regname, del_offset, mode, adel, gdel)
711                 if (module not in per_delayconf.keys()):
712                         per_delayconf[module] = []
713                 delayconf.append(delaydata)
714                 per_delayconf[module].append(delaydata)
716 print ""
717 print "Total PAD registers: %d" % len(padconf)
718 print "Total DELAY registers: %d" % len(delayconf)
719 print ""
721 format_pad_regs(padconf, per_padconf)
722 format_delay_regs(delayconf, per_delayconf)
723 pad_dump_gpio(padconf, per_padconf)
725 # Dump the final selection for reuse
726 print "Selected modes for each peripheral module\n"
727 for group in sel:
728         print "%s,\t%s" % (group, sel[group])
729 print ""
730 # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # #