393a2d948635358a21e01f892bfc31da6c70fd84
[glsdk/iodelay-config.git] / iodelay-autogen.py
1 #!/usr/bin/python
2 # Python script to automatically generate the IO pad and delay data
3 # Author:- Nikhil Devshatwar
5 # This script uses regdump of the pad registers to figure out the muxmodes
6 # Based on the pad and muxmode, it find out all possible virtual/manual modes
7 # by referring to the PCT XML model. Using the, selection file, script
8 # decides which modes to be selected. Finally it dumps the required array entries
10 # This script depends on following files:-
11 # * XML data files      - Shipped with the DRA7xx PCT tool
12 # * Pad register dump   - Generate using omapconf dump 0x4a003400 0x4a00380c
13 # * selection file      - List of selected virtual/manual modes to be used
15 import xml.etree.ElementTree as ET
16 import re
17 import argparse
19 # Handle the command line arguments
20 parser = argparse.ArgumentParser(prog='iodelay-autogen.py',
21         description='Python script to generate the IOdelay data.\n' \
22                 'This script refers to the XML data and automatically generates\n' \
23                 'PAD and DELAY data for the same use case.\n' \
24                 'Note that only the PADs which are used in the dump are configured.',
25         epilog='Generate the pad and delay data using pad register dumps. For this,\n' \
26                 'Run omapconf dump 0x4a003400 0x4a00380c and save the output')
28 parser.add_argument('-d', '--debug', dest='debug',
29         action='store', type=int, choices=[0, 1, 2], default=0,
30         help='set the debug level')
32 parser.add_argument('-i', '--interactive', dest='interactive',
33         action='store', type=int, choices=[0, 1], default=1,
34         help='run interactively with menus for resolving conflicts')
36 parser.add_argument('-f', '--format', dest='format',
37         action='store', type=str, choices=["linux", "uboot", "bios"], default="uboot",
38         help='select the output format to be used')
40 parser.add_argument('-r', '--revision', dest='revision',
41         action='store', type=str, choices=["1.0", "1.1", "2.0"], default="1.1",
42         help='select the silicon revision')
44 parser.add_argument('-p', '--part', dest='part',
45         action='store', type=str, choices=["dra74x", "dra75x", "dra72x"], default="dra74x",
46         help='select the device part')
48 parser.add_argument('-m', '--module', dest='module',
49         action='store', type=str, default="",
50         help='generate only for this module')
52 parser.add_argument('-s', '--strict', dest='strict',
53         action='store_true',
54         help='strict mode - ask for each pad of the group, do not save selection.\n' \
55                 'For some peripherals, same delaymode cannot be used for all the pads.\n' \
56                 'Use this mode to select different modes for each pad')
58 parser.add_argument('-g', '--gpio', dest='gpio',
59         action='store_true',
60         help='generate script to read pad data from GPIO')
62 parser.add_argument('-c', '--check', dest='check_xml',
63         action='store_true',
64         help='check consistency of the XML files and other data')
66 args = parser.parse_args()
67 # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # #
69 VERSION = "2.4"
71 if (args.part == "dra74x" or args.part == "dra75x"):
72         XML_PATH = "XMLFiles/DRA75x_DRA74x"
73         PART = "DRA75x_DRA74x"
74         PCT_VERSION = "v1.0.9"
75 elif (args.part == "dra72x"):
76         XML_PATH = "XMLFiles/DRA72x"
77         PART = "DRA72x"
78         PCT_VERSION = "v1.0.5"
80 pad_data_xml   = XML_PATH + "/CTRL_MODULE_CORE.xml"
81 iod_data_xml   = XML_PATH + "/IODELAYCONFIG.xml"
82 model_data_xml = XML_PATH + "/model_" + PART + "_SR" + args.revision + "_" + PCT_VERSION + ".xml"
83 modehelp_file  = XML_PATH + "/guidelines.txt"
85 pad_file = "ctrl-core.dump"
86 sel_file = "selected-modes.txt"
88 print "iodelay-autogen.py - Python script to generate the IOdelay data."
89 print "v" + VERSION + " using PCT version " + PCT_VERSION
90 print "Parsing PCT data from " + model_data_xml + "..."
91 print ""
93 # Read the XML file database for pad and delay registers
94 pad_xml = ET.parse(pad_data_xml).getroot()
95 iod_xml = ET.parse(iod_data_xml).getroot()
96 model_xml = ET.parse(model_data_xml).getroot()
98 # Functions to parse the input files and build data structures
99 def read_guidelines(fname):
100         modehelp = {}
101         pattern = re.compile('([^\t.]+\w)\t+(.+)')
102         f = open(fname)
103         for line in f.readlines():
104                 list = re.match(pattern, line)
105                 if ( list == None):
106                         continue
107                 mode = list.groups(0)[0]
108                 info = list.groups(0)[1]
109                 modehelp[mode] = info
110                 if (args.debug >= 2):
111                         print "Help: Mode '%s' is used for '%s'" % (mode, info)
112         return modehelp
114 def read_selmodes(fname):
115         sel = {}
116         pattern = re.compile('(\w+)\W*,\W*(\w*)')
117         f = open(fname)
118         for line in f.readlines():
119                 list = re.match(pattern, line)
120                 if ( list == None):
121                         continue
122                 module = list.groups(0)[0]
123                 mode = list.groups(0)[1]
124                 sel[module] = mode
125                 if (args.debug >= 2):
126                         print "INFO: Select '%s' for '%s'" % (mode, module)
127         return sel
129 def read_pad_dump(file):
130         regmap = {}
131         pattern = re.compile('.*(0x[0-9A-F]+).*(0x[0-9A-F]+).*')
132         f = open(file, 'r')
133         for line in f:
134                 list = re.match(pattern, line)
135                 if ( list == None):
136                         continue
137                 addr = int(list.groups(0)[0], 16)
138                 val = int(list.groups(0)[1], 16)
139                 #print "PADXML: Addr = %08x Value = %08x" % (addr, val)
140                 regmap[addr] = val
141         return regmap
142 # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # #
144 # Helper functions to parse XML nodes and get the desired data
145 # Hugely dependent on the XML format of the PCT files
146 # Uses XPath to search elements with queries and filters
147 # Parse the nodes to generate data in desired format
149 def xml_pad_get_name(offset):
150         padlist = pad_xml.findall("register[@offset='0x%X']" % offset)
151         if (len(padlist) == 0):
152                 return "Unknown"
153         else:
154                 return padlist[0].get("id")
156 def xml_pad_get_pin(offset, muxmode):
157         padlist = pad_xml.findall("register[@offset='0x%X']" % offset)
158         if (len(padlist) == 0):
159                 return "Unknown"
160         else:
161                 mux_field = padlist[0].findall("./bitfield[@end='0']")
162                 if (len(mux_field) == 0):
163                         return "Unknown"
164                 modes = mux_field[0].findall("./bitenum[@value='%d']" % muxmode)
165                 if (len(modes) == 0):
166                         return "Unknown"
167                 return modes[0].get("id")
169 def xml_iodelay_get_reg(name):
170         delaylist = iod_xml.findall("register[@id='%s']" % name)
171         if (len(delaylist) == 0):
172                 return 0
173         else:
174                 offset = delaylist[0].get("offset")
175                 #print "IOD: Name = %s Offset = %s" % (del_reg, offset)
176                 return int(offset, 16)
178 def xml_get_virtual(mode):
179         vmodes = {}
180         signal = mode.findtext("signal")
181         for virt in mode.findall("virtualmode/mode"):
182                 virt_mode = virt.findtext("value")
183                 virt_name = virt.findtext("name")
184                 if (virt_name == "NA"):
185                         continue
186                 virt_mode = int(virt_mode)
187                 vmodes[virt_name] = virt_mode
188                 if (args.debug >= 1):
189                         print ("    * VIRTUAL: %s [%s] => delaymode = %d" % (signal, virt_name, virt_mode))
190         return vmodes
192 def xml_get_manual(mode):
193         mmodes = {}
194         signal = mode.findtext("signal")
195         for man in mode.findall("manualmode"):
196                 regname = man.findtext("cfgreg/name")
197                 for sel in man.findall("cfgreg/mode"):
198                         adel = sel.findtext("adelay")
199                         gdel = sel.findtext("gdelay")
200                         man_name = sel.findtext("name")
201                         if (man_name == "NA"):
202                                 continue
203                         adel = int(adel)
204                         gdel = int(gdel)
205                         if (man_name not in mmodes.keys()):
206                                 mmodes[man_name] = []
207                         mmodes[man_name].append((regname, adel, gdel))
208                         if (args.debug >= 1):
209                                 print ("    * MANUAL: %s [%s] => delay[%s] = %d, %d" % (signal, man_name, regname, adel, gdel))
210         return mmodes
212 def xml_find_delaymodes(pad_name, muxmode):
213         padlist = model_xml.findall("padDB/clockNode/type/pad")
214         for pad in padlist:
215                 if (pad_name == pad.findtext("confregisters/regbit/register")):
216                         muxmodes = pad.findall("muxmode")
217                         break
218         if not muxmodes:
219                 return None
220         for mode in muxmodes:
221                 if ("%d" % muxmode == mode.findtext("mode")):
222                         virt = xml_get_virtual(mode)
223                         man = xml_get_manual(mode)
224                         return (virt, man)
225         return None
227 def xml_check_correctness(modehelp):
228         if(args.check_xml == False):
229                 return
231         print "###########################################"
232         print "XML correctness checks:"
233         padcore_list = []
234         padmodel_list = []
235         modes = {}
237         # Fint all the pads in core XML
238         pad_list = pad_xml.findall("register")
239         for i in pad_list:
240                 name = i.get("id")
241                 if (re.match("CTRL_CORE_PAD_.*", name) == None):
242                         continue
243                 padcore_list.append(name)
244         print ">> Total pads defined in core XML = %d" % len(padcore_list)
246         # Find all the pads in model XML
247         pad_list = model_xml.findall("padDB/clockNode/type/pad/confregisters/regbit")
248         for i in pad_list:
249                 name = i.findtext("register")
250                 padmodel_list.append(name)
251         print ">> Total pads defined in model XML = %d" % len(padmodel_list)
253         # Find all the manual modes
254         manmode_list = model_xml.findall("padDB/clockNode/type/pad/muxmode/manualmode/cfgreg/mode")
255         for i in manmode_list:
256                 man_name = i.findtext("name")
257                 modes[man_name] = "manual"
258         # Find all the virtual modes
259         virtmode_list = model_xml.findall("padDB/clockNode/type/pad/muxmode/virtualmode/mode")
260         for i in virtmode_list:
261                 virt_name = i.findtext("name")
262                 modes[virt_name] = "virtual"
263         print ">> Total delaymodes defined in model XML = %d" % len(modes)
265         # Print out all the errors found in the tests
266         print "== Pads defined in core XML but not in model XML =="
267         for i in padcore_list:
268                 if (i not in padmodel_list):
269                         print "\t%s" % i
270         print "== Pads defined in model XML but not in core XML =="
271         for i in padmodel_list:
272                 if (i not in padcore_list):
273                         print "\t%s" % i
275         # Check if description for each mode is available
276         print "== Delaymodes missing description in the guidelines.txt =="
277         for i in modes:
278                 if (i not in modehelp):
279                         print "\t%s" % i
281         print "###########################################"
283 # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # #
285 # Decision point of the script
286 # For each pad/pin, decide what delay method is used
287 # Lookup in the selection file or ask user with a menu
288 def select_mode(pad, pin, module, virt, man, modehelp, sel):
289         modelist = []
290         for modename in virt.keys():
291                 modelist.append(modename)
293         for modename in man.keys():
294                 modelist.append(modename)
296         if (len(modelist) == 0):
297                 return "LEGACY"
299         if (module in sel.keys()):
300                 mode = sel[module]
301                 if (mode == "SKIP" or mode == "LEGACY" or mode in modelist):
302                         return mode
303                 else:
304                         print("ERR: Invalid delaymode '%s' for module '%s'" % (mode, module))
306         if (args.interactive == 0):
307                 print "WARN: No delay modes for %s found, skipping" % module
308                 mode = "SKIP"
309                 return mode
311         # Display the menu and ask user to select the 'right' mode
312         while True:
313                 print ""
314                 print "MENU: Select delay mode for %s -> %s" % (pad, pin)
315                 i = 0
316                 print "MENU: %d: %s \t\t\t%s" % (i, "SKIP", "Skips this module for now")
317                 i = 1
318                 print "MENU: %d: %s \t\t%s" % (i, "LEGACY", "No external delay config (No virtual/manual needed)")
319                 for mode in modelist:
320                         i += 1
321                         if (mode in modehelp):
322                                 helptext = modehelp[mode]
323                         else:
324                                 helptext = "Unknown"
325                         print "MENU: %d: %s \t\t%s" % (i, mode, helptext)
326                 try:
327                         choice = int(raw_input("Select delay mode #> "))
328                         if (choice == 0):
329                                 mode = "SKIP"
330                                 break
331                         elif (choice == 1):
332                                 mode = "LEGACY"
333                                 break
334                         elif (choice >=2 and choice <= len(modelist) + 1):
335                                 mode = modelist[choice - 2]
336                                 break
337                         print "ERROR: Invalid choice"
338                 except ValueError:
339                         print "ERROR: Invalid choice"
340         print "MENU: Selected mode is %s" % mode
341         print ""
343         return mode
344 # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # #
346 # Pad read using GPIO - Specific to linux only
347 # As each pad is muxed with a SoC gpio (for most of the pads)
348 # It's possible to read the pad data using gpio datain registers
349 # Dump the linux commands to read the gpio registers and read the pad data
350 def pad_dump_gpio(padconf, per_padconf):
351         if(args.gpio == False):
352                 return
354         print "# Read pad signals using GPIO DATA-IN registers"
355         print "# Works only for the input signals"
356         gpio_data_addrs = (0, 0x4ae10138, 0x48055138, 0x48057138, 0x48059138, 0x4805b138, 0x4805d138, 0x48051138, 0x48053138)
357         for i in padconf:
358                 (pad_name, pin_name, addr, val, mode, delayinfo) = i
360                 offset = addr - 0x4a002000
361                 gpio_name = xml_pad_get_pin(offset, 14)
362                 matchlist = re.match("GPIO(.)_(.*)", gpio_name)
363                 if (matchlist == None):
364                         print "ERR: No GPIO for pad %s" % pad_name
365                         continue
367                 inst = int(matchlist.groups(0)[0])
368                 bit = int(matchlist.groups(0)[1])
369                 gpio_addr = gpio_data_addrs[inst]
371                 print "#Read GPIO%d_%d to sample %s" % (inst, bit, pin_name)
372                 print " echo %d > /sys/class/gpio/export 2>/dev/null;" % ((inst - 1) * 32)
373                 print " val=`omapconf read 0x%x 2>&1 | grep -v \"support\"`;" % gpio_addr
374                 print " status=$((0x$val >> %d & 0x1));" % bit
375                 print " echo -e \"%s (%s)\t = $status\";" % (pin_name, gpio_name)
376                 print ""
377         print ""
378 # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # #
380 # Generate the final pad and delay data in the required format
381 def format_pad_regs(padconf, per_padconf):
382         print "###########################################"
383         print "Pad data output (with the delay modes)"
384         print "###########################################"
385         if (args.format == "uboot"):
386                 uboot_format_pad_regs(padconf, per_padconf)
387         elif (args.format == "linux"):
388                 linux_format_pad_regs(padconf, per_padconf)
389         elif (args.format == "bios"):
390                 bios_format_pad_regs(padconf, per_padconf)
391         else:
392                 print "ERR: Format %s not suppported" % args.format
394 def format_delay_regs(delayconf, per_delayconf):
395         print "#########################################"
396         print "Delay data output (for manual modes)"
397         print "#########################################"
398         if (args.format == "uboot"):
399                 uboot_format_delay_regs(delayconf, per_delayconf)
400         elif (args.format == "linux"):
401                 linux_format_delay_regs(delayconf, per_delayconf)
402         elif (args.format == "bios"):
403                 bios_format_delay_regs(delayconf, per_delayconf)
404         else:
405                 print "ERR: Format %s not suppported" % args.format
407 def get_pin_info(val):
408         inp_en = (val >> 18) & 0x1
409         pulltype = (val >> 17) & 0x1
410         pull_dis = (val >> 16) & 0x1
411         pin = "PIN"
412         if (inp_en):
413                 pin += "_INPUT"
414         else:
415                 pin += "_OUTPUT"
416         if (pull_dis == 0):
417                 if (pulltype):
418                         pin += "_PULLUP"
419                 else:
420                         pin += "_PULLDOWN"
421         return pin
423 # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # #
425 # Generate output in u-boot format
426 def uboot_format_pad_regs(padconf, per_padconf):
427         print "\nconst struct pad_conf_entry dra74x_core_padconf_array[] = {"
428         for i in padconf:
429                 (pad_name, pin_name, addr, val, mode, delayinfo) = i
431                 if (re.match("MMC.*", pin_name) != None):
432                         print "WARN: Skipping MMC padconf in uboot"
434                 muxmode = val & 0xf
435                 (method, data) = delayinfo
436                 if (method == "LEGACY"):
437                         extramode = ""
438                 elif (method == "VIRTUAL"):
439                         delaymode = data
440                         extramode = " | VIRTUAL_MODE%d" % delaymode
441                 elif (method == "MANUAL"):
442                         extramode = " | MANUAL_MODE"
443                 else:
444                         print "ERR: Invalid method %s" % method
446                 pin_info = get_pin_info(val) + extramode
447                 pad_short = re.sub("CTRL_CORE_PAD_", "", pad_name)
448                 comment = (pad_short + "." + pin_name).lower()
450                 print "\t{ %s, (M%d | %s) },\t/* %s */" % (pad_short, muxmode, pin_info, comment)
451         print "};\n"
453 def uboot_format_delay_regs(delayconf, per_delayconf):
454         manual_del = []
455         for i in delayconf:
456                 (pad_name, pin_name, regname, del_offset, man_name, adel, gdel) = i
458                 if (re.match("MMC.*", pin_name) != None):
459                         print "WARN: Skipping MMC delayconf in uboot"
460                         continue
462                 entry = (del_offset, adel, gdel, regname, pin_name, man_name)
463                 manual_del.append(entry)
465         es_rev = args.revision.replace('.', '_')
466         print "\nconst struct iodelay_cfg_entry dra742_es" + es_rev + "_iodelay_cfg_array[] = {"
467         for entry in sorted(manual_del):
468                 print "\t{ 0x%04X, %5d, %5d },\t/* %s : %s - %s */" % entry
469         print "};\n"
471 # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # #
473 # Generate output in linux format
474 def linux_format_pad_regs(padconf, per_padconf):
475         print "&dra7_pmx_core {"
476         for per in per_padconf:
478                 if (re.match("MMC.*", per) == None):
479                         print "ERR: Only MMC padconf is recommended in kernel"
480                         continue
482                 # Get the mode from the first entry
483                 (pad_name, pin_name, addr, val, mode, delayinfo) = per_padconf[per][0]
485                 dtsnode = ("%s_pins_%s" % (per, mode)).lower()
486                 print ""
487                 print "\t%s: %s {" % (dtsnode, dtsnode)
488                 print "\t\tpinctrl-single,pins = <"
489                 for i in per_padconf[per]:
490                         (pad_name, pin_name, addr, val, mode, delayinfo) = i
492                         muxmode = val & 0xf
493                         (method, data) = delayinfo
494                         if (method == "LEGACY"):
495                                 extramode = ""
496                         elif (method == "VIRTUAL"):
497                                 delaymode = data
498                                 extramode = " | MUX_VIRTUAL_MODE%d" % delaymode
499                         elif (method == "MANUAL"):
500                                 extramode = " | MANUAL_MODE"
501                         else:
502                                 print "ERR: Invalid method %s" % method
504                         pin_info = get_pin_info(val) + extramode
505                         pad_short = re.sub("CTRL_CORE_PAD_", "", pad_name)
506                         offset = addr - 0x4a003400
507                         comment = (pad_short + "." + pin_name).lower()
509                         print "\t\t\t0x%03X\t(%s | MUX_MODE%d)\t/* %s */" % (offset, pin_info, muxmode, comment)
510                 print "\t\t>;"
511                 print "\t};"
512         print "};\n"
515 def linux_format_delay_regs(delayconf, per_delayconf):
516         print "&dra7_iodelay_core {"
517         for per in per_delayconf.keys():
519                 if (re.match("MMC.*", per) == None):
520                         print "ERR: Only MMC delayconf is recommended in kernel"
521                         continue
523                 # Get the mode from the first entry
524                 (pad_name, pin_name, regname, del_offset, mode, adel, gdel) = per_delayconf[per][0]
526                 dtsnode = ("%s_iodelay_%s_conf" % (per, mode)).lower()
527                 print "\t%s: %s {" % (dtsnode, dtsnode)
528                 print "\t\tpinctrl-single,pins = <"
529                 for i in per_delayconf[per]:
530                         (pad_name, pin_name, regname, del_offset, mode, adel, gdel) = i
532                         print "\t\t\t0x%03X (A_DELAY(%d) | G_DELAY(%d))\t/* %s */" % (del_offset, adel, gdel, regname)
533                 print "\t\t>;"
534                 print "\t};"
535         print "};\n"
537 # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # #
539 # Generate output in bios format
540 def bios_format_pad_regs(padconf, per_padconf):
541         for i in padconf:
542                 (pad_name, pin_name, addr, val, mode, delayinfo) = i
544                 delaylist = []
545                 (method, data) = delayinfo
546                 if (method == "VIRTUAL"):
547                         virt_mode = data
548                         val = val | ( virt_mode<< 4)
549                         val = val | (1 << 8)
550                 elif (method == "MANUAL"):
551                         delaylist = data
552                         val = val | (1 << 8)
554                 offset = addr - 0x4a003400
555                 out_delreg = out_adel = out_gdel = 0
556                 in_delreg  = in_adel  = in_gdel  = 0
557                 oen_delreg = oen_adel = oen_gdel = 0
559                 for j in delaylist:
560                         (regname, adel, gdel) = j
561                         if (re.match(".*_IN", regname) != None):
562                                 in_delreg = xml_iodelay_get_reg(regname)
563                                 in_adel = adel
564                                 in_gdel = gdel
565                         elif (re.match(".*_OEN", regname) != None):
566                                 oen_delreg = xml_iodelay_get_reg(regname)
567                                 oen_adel = adel
568                                 oen_gdel = gdel
569                         elif (re.match(".*_OUT", regname) != None):
570                                 out_delreg = xml_iodelay_get_reg(regname)
571                                 out_adel = adel
572                                 out_gdel = gdel
573                 indel  = "{ 0x%04X, %4d, %4d }" % (in_delreg,  in_adel,  in_gdel)
574                 oendel = "{ 0x%04X, %4d, %4d }" % (oen_delreg, oen_adel, oen_gdel)
575                 outdel = "{ 0x%04X, %4d, %4d }" % (out_delreg, out_adel, out_gdel)
576                 pin_info = get_pin_info(val)
577                 print "\t/* %s -> %s (%s) %s delaymode */" % (pad_name, pin_name, pin_info, method)
578                 print "\t{ 0x%03X, 0x%08X, %s, %s, %s }" % (offset, val, indel, oendel, outdel)
580 def bios_format_delay_regs(delayconf, per_delayconf):
581         print "Manual delays are not configured separately"
582         print "Delays are configured as part of the padconf step only"
584 # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # #
586 # Main execution starts here
587 # * Parse all the XML files - Get the pad data and IOdelay data
588 # * Iterate over the pad register dumps
589 # * For each pad, find out the muxmode being used and the pad direction, etc
590 # * For the muxmode being used, find out available virtual/modes
591 #   - Dump the virtual/manual modes available (based on options)
592 #   - Build up the gpio script to read the pad data using GPIO module
593 # * Select the correct mode to be used
594 #   - Check if the mode is described for the peripheral module, (from selected-modes.txt)
595 #   - Otherwise ask the user (with a menu) to decide the delaymode
596 #     => Update the selection for the whole of the peripheral module
597 #   - Worst case, skip the delaymode for this pad
598 # * Build the pad and delay register information
599 # * Create the dump for pad and delay data in linux/u-boot format
600 # * Dump the delaymode selection for each peripheral
601 # * Dump the GPIO script for each peripheral (all pads grouped together)
604 # Read all the input files and parse the required info
605 modehelp = read_guidelines(modehelp_file)
606 sel = read_selmodes(sel_file)
607 regmap = read_pad_dump(pad_file)
608 reglist = regmap.keys()
610 # List of all the pads being configured
611 padconf = []
612 # List of all the delay registers being configured (for manual mode)
613 delayconf = []
614 # Dictionary of pads grouped by peripheral/module
615 per_padconf = {}
616 # Dictionary of delay registers grouped by peripheral/module
617 per_delayconf = {}
619 xml_check_correctness(modehelp)
621 # Start iterating over each pad
622 for i in range(0, 260):
623         # Find out the muxmode and pad direction, etc
624         addr = 0x4a003400 + i * 4
625         offset = 0x1400 + i * 4
626         dts_offset = offset - 0x1400
628         if (addr not in reglist):
629                 print "WARN: Register dump for pad 0x%X not found" % addr
630                 continue
631         val = regmap[addr]
632         muxmode = val & 0xf
634         # Find out the pin based on the muxmode
635         pad_name = xml_pad_get_name(offset)
636         pin_name = xml_pad_get_pin(offset, muxmode)
637         if (pad_name == "Unknown" or pin_name == "Unknown"):
638                 print "WARN: Cannot find out Pad/Pin name for PAD address 0x%X (%s[%s] = %s)" \
639                 % (addr, pad_name, muxmode, pin_name)
640                 continue
641         if (pin_name == "DRIVER OFF"):
642                 continue
644         # Find out if the delaymode for this module is already selected
645         module = re.match("([^_]+)_.*", pin_name).groups(0)[0]
647         if (args.module != "" and args.module != module):
648                 continue
650         if (args.debug >= 1):
651                 print "\nPAD: %s: Addr= 0x%08X Value = 0x%08X \"%s\"" \
652                 % (pad_name, addr, val, pin_name)
654         # Find out all the possible virtual, manual modes fot the specific pad -> pin combination
655         (virt, man) = xml_find_delaymodes(pad_name, muxmode)
657         # Need to select one out of allowed modes
658         mode = select_mode(pad_name, pin_name, module, virt, man, modehelp, sel)
660         # Remember the selection for that module, for later reuse
661         if (args.strict == False and module not in sel.keys()):
662                 sel[module] = mode
664         if (mode == "SKIP"):
665                 continue
666         elif (mode == "LEGACY"):
667                 delayinfo = ("LEGACY", "")
668         elif (mode in virt):
669                 delayinfo = ("VIRTUAL", virt[mode])
670         elif (mode in man):
671                 delayinfo = ("MANUAL", man[mode])
672         else:
673                 print "ERR: Unknown mode '%s' selected" % mode
674                 continue
676         if (args.debug >= 1):
677                 print "  => Using mode %s" % mode
678         paddata = (pad_name, pin_name, addr, val, mode, delayinfo)
679         if (module not in per_padconf.keys()):
680                 per_padconf[module] = []
681         padconf.append(paddata)
682         per_padconf[module].append(paddata)
684         if(mode not in man):
685                 continue
687         # Add the delay data if using manual mode
688         for regval in man[mode]:
689                 (regname, adel, gdel) = regval
690                 del_offset = xml_iodelay_get_reg(regname)
691                 if (del_offset == 0):
692                         print "WARN: Can't find delay offset of register %s" % regname
693                         break
694                 if (args.debug >= 1):
695                         print "  => Manual delay[%s] = (%d, %d)" % (regname, adel, gdel)
696                 delaydata = (pad_name, pin_name, regname, del_offset, mode, adel, gdel)
697                 if (module not in per_delayconf.keys()):
698                         per_delayconf[module] = []
699                 delayconf.append(delaydata)
700                 per_delayconf[module].append(delaydata)
702 print ""
703 print "Total PAD registers: %d" % len(padconf)
704 print "Total DELAY registers: %d" % len(delayconf)
705 print ""
707 format_pad_regs(padconf, per_padconf)
708 format_delay_regs(delayconf, per_delayconf)
709 pad_dump_gpio(padconf, per_padconf)
711 # Dump the final selection for reuse
712 print "Selected modes for each peripheral module\n"
713 for group in sel:
714         print "%s,\t%s" % (group, sel[group])
715 print ""
716 # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # #