3e887de13df0cc1efd0fbf0c3edaae5c17e5159e
[glsdk/iodelay-config.git] / iodelay-autogen.py
1 #!/usr/bin/python
2 # Python script to automatically generate the IO pad and delay data
3 # Author:- Nikhil Devshatwar
5 # This script uses regdump of the pad registers to figure out the muxmodes
6 # Based on the pad and muxmode, it find out all possible virtual/manual modes
7 # by referring to the PCT XML model. Using the, selection file, script
8 # decides which modes to be selected. Finally it dumps the required array entries
10 # This script depends on following files:-
11 # * XML data files      - Shipped with the DRA7xx PCT tool
12 # * Pad register dump   - Generate using omapconf dump 0x4a003400 0x4a00380c
13 # * selection file      - List of selected virtual/manual modes to be used
15 import xml.etree.ElementTree as ET
16 import re
17 import argparse
19 # Handle the command line arguments
20 parser = argparse.ArgumentParser(prog='iodelay-autogen.py',
21         description='Python script to generate the IOdelay data.\n' \
22                 'This script refers to the XML data and automatically generates\n' \
23                 'PAD and DELAY data for the same use case.\n' \
24                 'Note that only the PADs which are used in the dump are configured.',
25         epilog='Generate the pad and delay data using pad register dumps. For this,\n' \
26                 'Run omapconf dump 0x4a003400 0x4a00380c and save the output')
28 parser.add_argument('-d', '--debug', dest='debug',
29         action='store', type=int, choices=[0, 1, 2], default=0,
30         help='set the debug level')
32 parser.add_argument('-i', '--interactive', dest='interactive',
33         action='store', type=int, choices=[0, 1], default=1,
34         help='run interactively with menus for resolving conflicts')
36 parser.add_argument('-f', '--format', dest='format',
37         action='store', type=str, choices=["linux", "uboot", "bios"], default="uboot",
38         help='select the output format to be used')
40 parser.add_argument('-r', '--revision', dest='revision',
41         action='store', type=str, choices=["1.1", "2.0"], default="1.1",
42         help='select the silicon revision')
44 parser.add_argument('-m', '--module', dest='module',
45         action='store', type=str, default="",
46         help='generate only for this module')
48 parser.add_argument('-s', '--strict', dest='strict',
49         action='store_true',
50         help='strict mode - ask for each pad of the group, do not save selection.\n' \
51                 'For some peripherals, same delaymode cannot be used for all the pads.\n' \
52                 'Use this mode to select different modes for each pad')
54 parser.add_argument('-g', '--gpio', dest='gpio',
55         action='store_true',
56         help='generate script to read pad data from GPIO')
58 parser.add_argument('-c', '--check', dest='check_xml',
59         action='store_true',
60         help='check consistency of the XML files and other data')
62 args = parser.parse_args()
63 # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # #
65 PCT_VERSION = "v1.0.7"
66 pad_data_xml = "XMLFiles/CTRL_MODULE_CORE.xml"
67 iod_data_xml = "XMLFiles/IODELAYCONFIG.xml"
68 model_data_xml = "XMLFiles/model_DRA75x_DRA74x_SR" + args.revision + "_" + PCT_VERSION + ".xml"
70 modehelp_file = "guidelines.txt"
71 pad_file = "ctrl-core.dump"
72 sel_file = "selected-modes.txt"
74 # Read the XML file database for pad and delay registers
75 pad_xml = ET.parse(pad_data_xml).getroot()
76 iod_xml = ET.parse(iod_data_xml).getroot()
77 model_xml = ET.parse(model_data_xml).getroot()
79 # Functions to parse the input files and build data structures
80 def read_guidelines(fname):
81         modehelp = {}
82         pattern = re.compile('(.+\w)\t+(.+)')
83         f = open(fname)
84         for line in f.readlines():
85                 list = re.match(pattern, line)
86                 if ( list == None):
87                         continue
88                 mode = list.groups(0)[0]
89                 info = list.groups(0)[1]
90                 modehelp[mode] = info
91                 if (args.debug >= 2):
92                         print "Help: Mode '%s' is used for '%s'" % (mode, info)
93         return modehelp
95 def read_selmodes(fname):
96         sel = {}
97         pattern = re.compile('(\w+)\W*,\W*(\w*)')
98         f = open(fname)
99         for line in f.readlines():
100                 list = re.match(pattern, line)
101                 if ( list == None):
102                         continue
103                 module = list.groups(0)[0]
104                 mode = list.groups(0)[1]
105                 sel[module] = mode
106                 if (args.debug >= 2):
107                         print "INFO: Select '%s' for '%s'" % (mode, module)
108         return sel
110 def read_pad_dump(file):
111         regmap = {}
112         pattern = re.compile('.*(0x[0-9A-F]+).*(0x[0-9A-F]+).*')
113         f = open(file, 'r')
114         for line in f:
115                 list = re.match(pattern, line)
116                 if ( list == None):
117                         continue
118                 addr = int(list.groups(0)[0], 16)
119                 val = int(list.groups(0)[1], 16)
120                 #print "PADXML: Addr = %08x Value = %08x" % (addr, val)
121                 regmap[addr] = val
122         return regmap
123 # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # #
125 # Helper functions to parse XML nodes and get the desired data
126 # Hugely dependent on the XML format of the PCT files
127 # Uses XPath to search elements with queries and filters
128 # Parse the nodes to generate data in desired format
130 def xml_pad_get_name(offset):
131         padlist = pad_xml.findall("register[@offset='0x%X']" % offset)
132         if (len(padlist) == 0):
133                 return "Unknown"
134         else:
135                 return padlist[0].get("id")
137 def xml_pad_get_pin(offset, muxmode):
138         padlist = pad_xml.findall("register[@offset='0x%X']" % offset)
139         if (len(padlist) == 0):
140                 return "Unknown"
141         else:
142                 mux_field = padlist[0].findall("./bitfield[@end='0']")
143                 if (len(mux_field) == 0):
144                         return "Unknown"
145                 modes = mux_field[0].findall("./bitenum[@value='%d']" % muxmode)
146                 if (len(modes) == 0):
147                         return "Unknown"
148                 return modes[0].get("id")
150 def xml_iodelay_get_reg(name):
151         delaylist = iod_xml.findall("register[@id='%s']" % name)
152         if (len(delaylist) == 0):
153                 return 0
154         else:
155                 offset = delaylist[0].get("offset")
156                 #print "IOD: Name = %s Offset = %s" % (del_reg, offset)
157                 return int(offset, 16)
159 def xml_get_virtual(mode):
160         vmodes = {}
161         signal = mode.findtext("signal")
162         for virt in mode.findall("virtualmode/mode"):
163                 virt_mode = virt.findtext("value")
164                 virt_name = virt.findtext("name")
165                 if (virt_name == "NA"):
166                         continue
167                 virt_mode = int(virt_mode)
168                 vmodes[virt_name] = virt_mode
169                 if (args.debug >= 1):
170                         print ("    * VIRTUAL: %s [%s] => delaymode = %d" % (signal, virt_name, virt_mode))
171         return vmodes
173 def xml_get_manual(mode):
174         mmodes = {}
175         signal = mode.findtext("signal")
176         for man in mode.findall("manualmode"):
177                 regname = man.findtext("cfgreg/name")
178                 for sel in man.findall("cfgreg/mode"):
179                         adel = sel.findtext("adelay")
180                         gdel = sel.findtext("gdelay")
181                         man_name = sel.findtext("name")
182                         if (man_name == "NA"):
183                                 continue
184                         adel = int(adel)
185                         gdel = int(gdel)
186                         if (man_name not in mmodes.keys()):
187                                 mmodes[man_name] = []
188                         mmodes[man_name].append((regname, adel, gdel))
189                         if (args.debug >= 1):
190                                 print ("    * MANUAL: %s [%s] => delay[%s] = %d, %d" % (signal, man_name, regname, adel, gdel))
191         return mmodes
193 def xml_find_delaymodes(pad_name, muxmode):
194         padlist = model_xml.findall("padDB/clockNode/type/pad")
195         for pad in padlist:
196                 if (pad_name == pad.findtext("confregisters/regbit/register")):
197                         muxmodes = pad.findall("muxmode")
198                         break
199         if not muxmodes:
200                 return None
201         for mode in muxmodes:
202                 if ("%d" % muxmode == mode.findtext("mode")):
203                         virt = xml_get_virtual(mode)
204                         man = xml_get_manual(mode)
205                         return (virt, man)
206         return None
208 def xml_check_correctness(modehelp):
209         if(args.check_xml == False):
210                 return
212         print "###########################################"
213         print "XML correctness checks:"
214         padcore_list = []
215         padmodel_list = []
216         modes = {}
218         # Fint all the pads in core XML
219         pad_list = pad_xml.findall("register")
220         for i in pad_list:
221                 name = i.get("id")
222                 if (re.match("CTRL_CORE_PAD_.*", name) == None):
223                         continue
224                 padcore_list.append(name)
225         print ">> Total pads defined in core XML = %d" % len(padcore_list)
227         # Find all the pads in model XML
228         pad_list = model_xml.findall("padDB/clockNode/type/pad/confregisters/regbit")
229         for i in pad_list:
230                 name = i.findtext("register")
231                 padmodel_list.append(name)
232         print ">> Total pads defined in model XML = %d" % len(padmodel_list)
234         # Find all the manual modes
235         manmode_list = model_xml.findall("padDB/clockNode/type/pad/muxmode/manualmode/cfgreg/mode")
236         for i in manmode_list:
237                 man_name = i.findtext("name")
238                 modes[man_name] = "manual"
239         # Find all the virtual modes
240         virtmode_list = model_xml.findall("padDB/clockNode/type/pad/muxmode/virtualmode/mode")
241         for i in virtmode_list:
242                 virt_name = i.findtext("name")
243                 modes[virt_name] = "virtual"
244         print ">> Total delaymodes defined in model XML = %d" % len(modes)
246         # Print out all the errors found in the tests
247         print "== Pads defined in core XML but not in model XML =="
248         for i in padcore_list:
249                 if (i not in padmodel_list):
250                         print "\t%s" % i
251         print "== Pads defined in model XML but not in core XML =="
252         for i in padmodel_list:
253                 if (i not in padcore_list):
254                         print "\t%s" % i
256         # Check if description for each mode is available
257         print "== Delaymodes missing description in the guidelines.txt =="
258         for i in modes:
259                 if (i not in modehelp):
260                         print "\t%s" % i
262         print "###########################################"
264 # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # #
266 # Decision point of the script
267 # For each pad/pin, decide what delay method is used
268 # Lookup in the selection file or ask user with a menu
269 def select_mode(pad, pin, module, virt, man, modehelp, sel):
270         modelist = []
271         for modename in virt.keys():
272                 modelist.append(modename)
274         for modename in man.keys():
275                 modelist.append(modename)
277         if (len(modelist) == 0):
278                 return "LEGACY"
280         if (module in sel.keys()):
281                 mode = sel[module]
282                 if (mode == "SKIP" or mode in modelist):
283                         return mode
284                 else:
285                         print("ERR: Invalid delaymode '%s' for module '%s'" % (mode, module))
287         if (args.interactive == 0):
288                 print "WARN: No delay modes for %s found, skipping" % module
289                 mode = "SKIP"
290                 sel[module] = mode
291                 return mode
293         # Display the menu and ask user to select the 'right' mode
294         while True:
295                 print ""
296                 print "MENU: Select delay mode for %s -> %s" % (pad, pin)
297                 i = 0
298                 print "MENU: %d: %s \t\t\t%s" % (i, "SKIP", "Skips this module for now")
299                 for mode in modelist:
300                         i += 1
301                         if (mode in modehelp):
302                                 helptext = modehelp[mode]
303                         else:
304                                 helptext = "Unknown"
305                         print "MENU: %d: %s \t\t%s" % (i, mode, helptext)
306                 try:
307                         choice = int(raw_input("Select delay mode #> "))
308                         if (choice == 0):
309                                 mode = "SKIP"
310                                 break
311                         elif (choice >=0 and choice <= len(modelist)):
312                                 mode = modelist[choice - 1]
313                                 break
314                         print "ERROR: Invalid choice"
315                 except ValueError:
316                         print "ERROR: Invalid choice"
317         print "MENU: Selected mode is %s" % mode
318         print ""
320         return mode
321 # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # #
323 # Pad read using GPIO - Specific to linux only
324 # As each pad is muxed with a SoC gpio (for most of the pads)
325 # It's possible to read the pad data using gpio datain registers
326 # Dump the linux commands to read the gpio registers and read the pad data
327 def pad_dump_gpio(padconf, per_padconf):
328         if(args.gpio == False):
329                 return
331         print "# Read pad signals using GPIO DATA-IN registers"
332         print "# Works only for the input signals"
333         gpio_data_addrs = (0, 0x4ae10138, 0x48055138, 0x48057138, 0x48059138, 0x4805b138, 0x4805d138, 0x48051138, 0x48053138)
334         for i in padconf:
335                 (pad_name, pin_name, addr, val, delayinfo) = i
337                 offset = addr - 0x4a002000
338                 gpio_name = xml_pad_get_pin(offset, 14)
339                 matchlist = re.match("GPIO(.)_(.*)", gpio_name)
340                 if (matchlist == None):
341                         print "ERR: No GPIO for pad %s" % pad_name
342                         continue
344                 inst = int(matchlist.groups(0)[0])
345                 bit = int(matchlist.groups(0)[1])
346                 gpio_addr = gpio_data_addrs[inst]
348                 print "#Read GPIO%d_%d to sample %s" % (inst, bit, pin_name)
349                 print " echo %d > /sys/class/gpio/export 2>/dev/null;" % ((inst - 1) * 32)
350                 print " val=`omapconf read 0x%x 2>&1 | grep -v \"support\"`;" % gpio_addr
351                 print " status=$((0x$val >> %d & 0x1));" % bit
352                 print " echo -e \"%s (%s)\t = $status\";" % (pin_name, gpio_name)
353                 print ""
354         print ""
355 # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # #
357 # Generate the final pad and delay data in the required format
358 def format_pad_regs(padconf, per_padconf):
359         print "###########################################"
360         print "Pad data output (with the delay modes)"
361         print "###########################################"
362         if (args.format == "uboot"):
363                 uboot_format_pad_regs(padconf, per_padconf)
364         elif (args.format == "linux"):
365                 linux_format_pad_regs(padconf, per_padconf)
366         elif (args.format == "bios"):
367                 bios_format_pad_regs(padconf, per_padconf)
368         else:
369                 print "ERR: Format %s not suppported" % args.format
371 def format_delay_regs(delayconf, per_delayconf):
372         print "#########################################"
373         print "Delay data output (for manual modes)"
374         print "#########################################"
375         if (args.format == "uboot"):
376                 uboot_format_delay_regs(delayconf, per_delayconf)
377         elif (args.format == "linux"):
378                 linux_format_delay_regs(delayconf, per_delayconf)
379         elif (args.format == "bios"):
380                 bios_format_delay_regs(delayconf, per_delayconf)
381         else:
382                 print "ERR: Format %s not suppported" % args.format
384 def get_pin_info(val):
385         inp_en = (val >> 18) & 0x1
386         pulltype = (val >> 17) & 0x1
387         pull_dis = (val >> 16) & 0x1
388         pin = "PIN"
389         if (inp_en):
390                 pin += "_INPUT"
391         else:
392                 pin += "_OUTPUT"
393         if (pull_dis == 0):
394                 if (pulltype):
395                         pin += "_PULLUP"
396                 else:
397                         pin += "_PULLDOWN"
398         return pin
400 # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # #
402 # Generate output in u-boot format
403 def uboot_format_pad_regs(padconf, per_padconf):
404         print "\nconst struct pad_conf_entry dra74x_core_padconf_array[] = {"
405         for i in padconf:
406                 (pad_name, pin_name, addr, val, delayinfo) = i
408                 if (re.match("MMC.*", pin_name) != None):
409                         print "WARN: Skipping MMC padconf in uboot"
410                         continue
412                 muxmode = val & 0xf
413                 (method, data) = delayinfo
414                 if (method == "LEGACY"):
415                         extramode = ""
416                 elif (method == "VIRTUAL"):
417                         delaymode = data
418                         extramode = " | VIRTUAL_MODE%d" % delaymode
419                 elif (method == "MANUAL"):
420                         extramode = " | MANUAL_MODE"
421                 else:
422                         print "ERR: Invalid method %s" % method
424                 pin_info = get_pin_info(val) + extramode
425                 pad_short = re.sub("CTRL_CORE_PAD_", "", pad_name)
426                 comment = (pad_short + "." + pin_name).lower()
428                 print "\t{ %s, (M%d | %s) },\t/* %s */" % (pad_short, muxmode, pin_info, comment)
429         print "};\n"
431 def uboot_format_delay_regs(delayconf, per_delayconf):
432         manual_del = []
433         for i in delayconf:
434                 (pad_name, pin_name, regname, del_offset, man_name, adel, gdel) = i
436                 if (re.match("MMC.*", pin_name) != None):
437                         print "WARN: Skipping MMC delayconf in uboot"
438                         continue
440                 entry = (del_offset, adel, gdel, regname, pin_name, man_name)
441                 manual_del.append(entry)
443         es_rev = args.revision.replace('.', '_')
444         print "\nconst struct iodelay_cfg_entry dra742_es" + es_rev + "_iodelay_cfg_array[] = {"
445         for entry in sorted(manual_del):
446                 print "\t{ 0x%04X, %5d, %5d },\t/* %s : %s - %s */" % entry
447         print "};\n"
449 # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # #
451 # Generate output in linux format
452 def linux_format_pad_regs(padconf, per_padconf):
453         print "&dra7_pmx_core {"
454         for per in per_padconf:
456                 if (re.match("MMC.*", per) == None):
457                         print "ERR: Only MMC padconf is recommended in kernel"
458                         continue
460                 dtsnode = ("%s_pins_default" % per).lower()
461                 print ""
462                 print "\t%s: %s {" % (dtsnode, dtsnode)
463                 print "\t\tpinctrl-single,pins = <"
464                 for i in per_padconf[per]:
465                         (pad_name, pin_name, addr, val, delayinfo) = i
467                         muxmode = val & 0xf
468                         (method, data) = delayinfo
469                         if (method == "LEGACY"):
470                                 extramode = ""
471                         elif (method == "VIRTUAL"):
472                                 delaymode = data
473                                 extramode = " | VIRTUAL_MODE%d" % delaymode
474                         elif (method == "MANUAL"):
475                                 extramode = " | MANUAL_MODE"
476                         else:
477                                 print "ERR: Invalid method %s" % method
479                         pin_info = get_pin_info(val) + extramode
480                         pad_short = re.sub("CTRL_CORE_PAD_", "", pad_name)
481                         offset = addr - 0x4a003400
482                         comment = (pad_short + "." + pin_name).lower()
484                         print "\t\t\t0x%03X\t(%s | MUM_MODE%d)\t/* %s */" % (offset, pin_info, muxmode, comment)
485                 print "\t\t>;"
486                 print "\t};"
487         print "};\n"
490 def linux_format_delay_regs(delayconf, per_delayconf):
491         print "&dra7_iodelay_core {"
492         for per in per_delayconf.keys():
494                 if (re.match("MMC.*", per) == None):
495                         print "ERR: Only MMC delayconf is recommended in kernel"
496                         continue
498                 # Get the mode from the first entry
499                 (pad_name, pin_name, regname, del_offset, mode, adel, gdel) = per_delayconf[per][0]
501                 dtsnode = ("%s_iodelay_%s_conf" % (per, mode)).lower()
502                 print "\t%s: %s {" % (dtsnode, dtsnode)
503                 print "\t\tpinctrl-single,pins = <"
504                 for i in per_delayconf[per]:
505                         (pad_name, pin_name, regname, del_offset, mode, adel, gdel) = i
507                         print "\t\t\t0x%03X (A_DELAY(%d) | G_DELAY(%d))\t/* %s */" % (del_offset, adel, gdel, regname)
508                 print "\t\t>;"
509                 print "\t};"
510         print "};\n"
512 # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # #
514 # Generate output in bios format
515 def bios_format_pad_regs(padconf, per_padconf):
516         for i in padconf:
517                 (pad_name, pin_name, addr, val, delayinfo) = i
519                 delaylist = []
520                 (method, data) = delayinfo
521                 if (method == "VIRTUAL"):
522                         virt_mode = data
523                         val = val | ( virt_mode<< 4)
524                         val = val | (1 << 8)
525                 elif (method == "MANUAL"):
526                         delaylist = data
527                         val = val | (1 << 8)
529                 offset = addr - 0x4a003400
530                 out_delreg = out_adel = out_gdel = 0
531                 in_delreg  = in_adel  = in_gdel  = 0
532                 oen_delreg = oen_adel = oen_gdel = 0
534                 for j in delaylist:
535                         (regname, adel, gdel) = j
536                         if (re.match(".*_IN", regname) != None):
537                                 in_delreg = xml_iodelay_get_reg(regname)
538                                 in_adel = adel
539                                 in_gdel = gdel
540                         elif (re.match(".*_OEN", regname) != None):
541                                 oen_delreg = xml_iodelay_get_reg(regname)
542                                 oen_adel = adel
543                                 oen_gdel = gdel
544                         elif (re.match(".*_OUT", regname) != None):
545                                 out_delreg = xml_iodelay_get_reg(regname)
546                                 out_adel = adel
547                                 out_gdel = gdel
548                 indel  = "{ 0x%04X, %4d, %4d }" % (in_delreg,  in_adel,  in_gdel)
549                 oendel = "{ 0x%04X, %4d, %4d }" % (oen_delreg, oen_adel, oen_gdel)
550                 outdel = "{ 0x%04X, %4d, %4d }" % (out_delreg, out_adel, out_gdel)
551                 pin_info = get_pin_info(val)
552                 print "\t/* %s -> %s (%s) %s delaymode */" % (pad_name, pin_name, pin_info, method)
553                 print "\t{ 0x%03X, 0x%08X, %s, %s, %s }" % (offset, val, indel, oendel, outdel)
555 def bios_format_delay_regs(delayconf, per_delayconf):
556         print "Manual delays are not configured separately"
557         print "Delays are configured as part of the padconf step only"
559 # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # #
561 # Main execution starts here
562 # * Parse all the XML files - Get the pad data and IOdelay data
563 # * Iterate over the pad register dumps
564 # * For each pad, find out the muxmode being used and the pad direction, etc
565 # * For the muxmode being used, find out available virtual/modes
566 #   - Dump the virtual/manual modes available (based on options)
567 #   - Build up the gpio script to read the pad data using GPIO module
568 # * Select the correct mode to be used
569 #   - Check if the mode is described for the peripheral module, (from selected-modes.txt)
570 #   - Otherwise ask the user (with a menu) to decide the delaymode
571 #     => Update the selection for the whole of the peripheral module
572 #   - Worst case, skip the delaymode for this pad
573 # * Build the pad and delay register information
574 # * Create the dump for pad and delay data in linux/u-boot format
575 # * Dump the delaymode selection for each peripheral
576 # * Dump the GPIO script for each peripheral (all pads grouped together)
579 # Read all the input files and parse the required info
580 modehelp = read_guidelines(modehelp_file)
581 sel = read_selmodes(sel_file)
582 regmap = read_pad_dump(pad_file)
583 reglist = regmap.keys()
585 # List of all the pads being configured
586 padconf = []
587 # List of all the delay registers being configured (for manual mode)
588 delayconf = []
589 # Dictionary of pads grouped by peripheral/module
590 per_padconf = {}
591 # Dictionary of delay registers grouped by peripheral/module
592 per_delayconf = {}
594 xml_check_correctness(modehelp)
595 # Start iterating over each pad
596 for i in range(0, 260):
597         # Find out the muxmode and pad direction, etc
598         addr = 0x4a003400 + i * 4
599         offset = 0x1400 + i * 4
600         dts_offset = offset - 0x1400
602         if (addr not in reglist):
603                 print "WARN: Register dump for pad 0x%X not found" % addr
604                 continue
605         val = regmap[addr]
606         muxmode = val & 0xf
608         # Find out the pin based on the muxmode
609         pad_name = xml_pad_get_name(offset)
610         pin_name = xml_pad_get_pin(offset, muxmode)
611         if (pad_name == "Unknown" or pin_name == "Unknown"):
612                 print "WARN: Cannot find out Pad/Pin name for PAD address 0x%X (%s[%s] = %s)" \
613                 % (addr, pad_name, muxmode, pin_name)
614                 continue
615         if (pin_name == "DRIVER OFF"):
616                 continue
618         # Find out if the delaymode for this module is already selected
619         module = re.match("([^_]+)_.*", pin_name).groups(0)[0]
621         if (args.module != "" and args.module != module):
622                 continue
624         if (args.debug >= 1):
625                 print "\nPAD: %s: Addr= 0x%08X Value = 0x%08X \"%s\"" \
626                 % (pad_name, addr, val, pin_name)
628         # Find out all the possible virtual, manual modes fot the specific pad -> pin combination
629         (virt, man) = xml_find_delaymodes(pad_name, muxmode)
631         # Need to select one out of allowed modes
632         mode = select_mode(pad_name, pin_name, module, virt, man, modehelp, sel)
634         # Remember the selection for that module, for later reuse
635         if (args.strict == False):
636                 sel[module] = mode
638         if (mode == "SKIP"):
639                 continue
640         elif (mode == "LEGACY"):
641                 delayinfo = ("LEGACY", "")
642         elif (mode in virt):
643                 delayinfo = ("VIRTUAL", virt[mode])
644         elif (mode in man):
645                 delayinfo = ("MANUAL", man[mode])
646         else:
647                 print "ERR: Unknown mode '%s' selected" % mode
648                 continue
650         if (args.debug >= 1):
651                 print "  => Using mode %s" % mode
652         paddata = (pad_name, pin_name, addr, val, delayinfo)
653         if (module not in per_padconf.keys()):
654                 per_padconf[module] = []
655         padconf.append(paddata)
656         per_padconf[module].append(paddata)
658         if(mode not in man):
659                 continue
661         # Add the delay data if using manual mode
662         for regval in man[mode]:
663                 (regname, adel, gdel) = regval
664                 del_offset = xml_iodelay_get_reg(regname)
665                 if (del_offset == 0):
666                         print "WARN: Can't find delay offset of register %s" % regname
667                         break
668                 if (args.debug >= 1):
669                         print "  => Manual delay[%s] = (%d, %d)" % (regname, adel, gdel)
670                 delaydata = (pad_name, pin_name, regname, del_offset, mode, adel, gdel)
671                 if (module not in per_delayconf.keys()):
672                         per_delayconf[module] = []
673                 delayconf.append(delaydata)
674                 per_delayconf[module].append(delaydata)
676 print ""
677 print "Total PAD registers: %d" % len(padconf)
678 print "Total DELAY registers: %d" % len(delayconf)
679 print ""
681 format_pad_regs(padconf, per_padconf)
682 format_delay_regs(delayconf, per_delayconf)
683 pad_dump_gpio(padconf, per_padconf)
685 # Dump the final selection for reuse
686 print "Selected modes for each peripheral module\n"
687 for group in sel:
688         print "%s,\t%s" % (group, sel[group])
689 print ""
690 # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # #