4123d12331c531174bbdd3935ba12f76da592c5b
[glsdk/iodelay-config.git] / iodelay-autogen.py
1 #!/usr/bin/python
2 # Python script to automatically generate the IO pad and delay data
3 # Author:- Nikhil Devshatwar
5 # This script uses regdump of the pad registers to figure out the muxmodes
6 # Based on the pad and muxmode, it find out all possible virtual/manual modes
7 # by referring to the PCT XML model. Using the, selection file, script
8 # decides which modes to be selected. Finally it dumps the required array entries
10 # This script depends on following files:-
11 # * XML data files      - Shipped with the DRA7xx PCT tool
12 # * Pad register dump   - Generate using omapconf dump 0x4a003400 0x4a00380c
13 # * selection file      - List of selected virtual/manual modes to be used
15 import xml.etree.ElementTree as ET
16 import re
17 import argparse
19 # Handle the command line arguments
20 parser = argparse.ArgumentParser(prog='iodelay-autogen.py',
21         description='Python script to generate the IOdelay data.\n' \
22                 'This script refers to the XML data and automatically generates\n' \
23                 'PAD and DELAY data for the same use case.\n' \
24                 'Note that only the PADs which are used in the dump are configured.',
25         epilog='Generate the pad and delay data using pad register dumps. For this,\n' \
26                 'Run omapconf dump 0x4a003400 0x4a00380c and save the output')
28 parser.add_argument('-d', '--debug', dest='debug',
29         action='store', type=int, choices=[0, 1, 2], default=0,
30         help='set the debug level')
32 parser.add_argument('-i', '--interactive', dest='interactive',
33         action='store', type=int, choices=[0, 1], default=1,
34         help='run interactively with menus for resolving conflicts')
36 parser.add_argument('-f', '--format', dest='format',
37         action='store', type=str, choices=["linux", "uboot", "bios"], default="uboot",
38         help='select the output format to be used')
40 parser.add_argument('-r', '--revision', dest='revision',
41         action='store', type=str, choices=["1.1", "2.0"], default="1.1",
42         help='select the silicon revision')
44 parser.add_argument('-m', '--module', dest='module',
45         action='store', type=str, default="",
46         help='generate only for this module')
48 parser.add_argument('-s', '--strict', dest='strict',
49         action='store_true',
50         help='strict mode - ask for each pad of the group, do not save selection.\n' \
51                 'For some peripherals, same delaymode cannot be used for all the pads.\n' \
52                 'Use this mode to select different modes for each pad')
54 parser.add_argument('-g', '--gpio', dest='gpio',
55         action='store_true',
56         help='generate script to read pad data from GPIO')
58 parser.add_argument('-c', '--check', dest='check_xml',
59         action='store_true',
60         help='check consistency of the XML files and other data')
62 args = parser.parse_args()
63 # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # #
65 VERSION = "2.3"
66 PCT_VERSION = "v1.0.9"
67 pad_data_xml = "XMLFiles/CTRL_MODULE_CORE.xml"
68 iod_data_xml = "XMLFiles/IODELAYCONFIG.xml"
69 model_data_xml = "XMLFiles/model_DRA75x_DRA74x_SR" + args.revision + "_" + PCT_VERSION + ".xml"
71 modehelp_file = "guidelines.txt"
72 pad_file = "ctrl-core.dump"
73 sel_file = "selected-modes.txt"
75 # Read the XML file database for pad and delay registers
76 pad_xml = ET.parse(pad_data_xml).getroot()
77 iod_xml = ET.parse(iod_data_xml).getroot()
78 model_xml = ET.parse(model_data_xml).getroot()
80 # Functions to parse the input files and build data structures
81 def read_guidelines(fname):
82         modehelp = {}
83         pattern = re.compile('(.+\w)\t+(.+)')
84         f = open(fname)
85         for line in f.readlines():
86                 list = re.match(pattern, line)
87                 if ( list == None):
88                         continue
89                 mode = list.groups(0)[0]
90                 info = list.groups(0)[1]
91                 modehelp[mode] = info
92                 if (args.debug >= 2):
93                         print "Help: Mode '%s' is used for '%s'" % (mode, info)
94         return modehelp
96 def read_selmodes(fname):
97         sel = {}
98         pattern = re.compile('(\w+)\W*,\W*(\w*)')
99         f = open(fname)
100         for line in f.readlines():
101                 list = re.match(pattern, line)
102                 if ( list == None):
103                         continue
104                 module = list.groups(0)[0]
105                 mode = list.groups(0)[1]
106                 sel[module] = mode
107                 if (args.debug >= 2):
108                         print "INFO: Select '%s' for '%s'" % (mode, module)
109         return sel
111 def read_pad_dump(file):
112         regmap = {}
113         pattern = re.compile('.*(0x[0-9A-F]+).*(0x[0-9A-F]+).*')
114         f = open(file, 'r')
115         for line in f:
116                 list = re.match(pattern, line)
117                 if ( list == None):
118                         continue
119                 addr = int(list.groups(0)[0], 16)
120                 val = int(list.groups(0)[1], 16)
121                 #print "PADXML: Addr = %08x Value = %08x" % (addr, val)
122                 regmap[addr] = val
123         return regmap
124 # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # #
126 # Helper functions to parse XML nodes and get the desired data
127 # Hugely dependent on the XML format of the PCT files
128 # Uses XPath to search elements with queries and filters
129 # Parse the nodes to generate data in desired format
131 def xml_pad_get_name(offset):
132         padlist = pad_xml.findall("register[@offset='0x%X']" % offset)
133         if (len(padlist) == 0):
134                 return "Unknown"
135         else:
136                 return padlist[0].get("id")
138 def xml_pad_get_pin(offset, muxmode):
139         padlist = pad_xml.findall("register[@offset='0x%X']" % offset)
140         if (len(padlist) == 0):
141                 return "Unknown"
142         else:
143                 mux_field = padlist[0].findall("./bitfield[@end='0']")
144                 if (len(mux_field) == 0):
145                         return "Unknown"
146                 modes = mux_field[0].findall("./bitenum[@value='%d']" % muxmode)
147                 if (len(modes) == 0):
148                         return "Unknown"
149                 return modes[0].get("id")
151 def xml_iodelay_get_reg(name):
152         delaylist = iod_xml.findall("register[@id='%s']" % name)
153         if (len(delaylist) == 0):
154                 return 0
155         else:
156                 offset = delaylist[0].get("offset")
157                 #print "IOD: Name = %s Offset = %s" % (del_reg, offset)
158                 return int(offset, 16)
160 def xml_get_virtual(mode):
161         vmodes = {}
162         signal = mode.findtext("signal")
163         for virt in mode.findall("virtualmode/mode"):
164                 virt_mode = virt.findtext("value")
165                 virt_name = virt.findtext("name")
166                 if (virt_name == "NA"):
167                         continue
168                 virt_mode = int(virt_mode)
169                 vmodes[virt_name] = virt_mode
170                 if (args.debug >= 1):
171                         print ("    * VIRTUAL: %s [%s] => delaymode = %d" % (signal, virt_name, virt_mode))
172         return vmodes
174 def xml_get_manual(mode):
175         mmodes = {}
176         signal = mode.findtext("signal")
177         for man in mode.findall("manualmode"):
178                 regname = man.findtext("cfgreg/name")
179                 for sel in man.findall("cfgreg/mode"):
180                         adel = sel.findtext("adelay")
181                         gdel = sel.findtext("gdelay")
182                         man_name = sel.findtext("name")
183                         if (man_name == "NA"):
184                                 continue
185                         adel = int(adel)
186                         gdel = int(gdel)
187                         if (man_name not in mmodes.keys()):
188                                 mmodes[man_name] = []
189                         mmodes[man_name].append((regname, adel, gdel))
190                         if (args.debug >= 1):
191                                 print ("    * MANUAL: %s [%s] => delay[%s] = %d, %d" % (signal, man_name, regname, adel, gdel))
192         return mmodes
194 def xml_find_delaymodes(pad_name, muxmode):
195         padlist = model_xml.findall("padDB/clockNode/type/pad")
196         for pad in padlist:
197                 if (pad_name == pad.findtext("confregisters/regbit/register")):
198                         muxmodes = pad.findall("muxmode")
199                         break
200         if not muxmodes:
201                 return None
202         for mode in muxmodes:
203                 if ("%d" % muxmode == mode.findtext("mode")):
204                         virt = xml_get_virtual(mode)
205                         man = xml_get_manual(mode)
206                         return (virt, man)
207         return None
209 def xml_check_correctness(modehelp):
210         if(args.check_xml == False):
211                 return
213         print "###########################################"
214         print "XML correctness checks:"
215         padcore_list = []
216         padmodel_list = []
217         modes = {}
219         # Fint all the pads in core XML
220         pad_list = pad_xml.findall("register")
221         for i in pad_list:
222                 name = i.get("id")
223                 if (re.match("CTRL_CORE_PAD_.*", name) == None):
224                         continue
225                 padcore_list.append(name)
226         print ">> Total pads defined in core XML = %d" % len(padcore_list)
228         # Find all the pads in model XML
229         pad_list = model_xml.findall("padDB/clockNode/type/pad/confregisters/regbit")
230         for i in pad_list:
231                 name = i.findtext("register")
232                 padmodel_list.append(name)
233         print ">> Total pads defined in model XML = %d" % len(padmodel_list)
235         # Find all the manual modes
236         manmode_list = model_xml.findall("padDB/clockNode/type/pad/muxmode/manualmode/cfgreg/mode")
237         for i in manmode_list:
238                 man_name = i.findtext("name")
239                 modes[man_name] = "manual"
240         # Find all the virtual modes
241         virtmode_list = model_xml.findall("padDB/clockNode/type/pad/muxmode/virtualmode/mode")
242         for i in virtmode_list:
243                 virt_name = i.findtext("name")
244                 modes[virt_name] = "virtual"
245         print ">> Total delaymodes defined in model XML = %d" % len(modes)
247         # Print out all the errors found in the tests
248         print "== Pads defined in core XML but not in model XML =="
249         for i in padcore_list:
250                 if (i not in padmodel_list):
251                         print "\t%s" % i
252         print "== Pads defined in model XML but not in core XML =="
253         for i in padmodel_list:
254                 if (i not in padcore_list):
255                         print "\t%s" % i
257         # Check if description for each mode is available
258         print "== Delaymodes missing description in the guidelines.txt =="
259         for i in modes:
260                 if (i not in modehelp):
261                         print "\t%s" % i
263         print "###########################################"
265 # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # #
267 # Decision point of the script
268 # For each pad/pin, decide what delay method is used
269 # Lookup in the selection file or ask user with a menu
270 def select_mode(pad, pin, module, virt, man, modehelp, sel):
271         modelist = []
272         for modename in virt.keys():
273                 modelist.append(modename)
275         for modename in man.keys():
276                 modelist.append(modename)
278         if (len(modelist) == 0):
279                 return "LEGACY"
281         if (module in sel.keys()):
282                 mode = sel[module]
283                 if (mode == "SKIP" or mode in modelist):
284                         return mode
285                 else:
286                         print("ERR: Invalid delaymode '%s' for module '%s'" % (mode, module))
288         if (args.interactive == 0):
289                 print "WARN: No delay modes for %s found, skipping" % module
290                 mode = "SKIP"
291                 sel[module] = mode
292                 return mode
294         # Display the menu and ask user to select the 'right' mode
295         while True:
296                 print ""
297                 print "MENU: Select delay mode for %s -> %s" % (pad, pin)
298                 i = 0
299                 print "MENU: %d: %s \t\t\t%s" % (i, "SKIP", "Skips this module for now")
300                 for mode in modelist:
301                         i += 1
302                         if (mode in modehelp):
303                                 helptext = modehelp[mode]
304                         else:
305                                 helptext = "Unknown"
306                         print "MENU: %d: %s \t\t%s" % (i, mode, helptext)
307                 try:
308                         choice = int(raw_input("Select delay mode #> "))
309                         if (choice == 0):
310                                 mode = "SKIP"
311                                 break
312                         elif (choice >=0 and choice <= len(modelist)):
313                                 mode = modelist[choice - 1]
314                                 break
315                         print "ERROR: Invalid choice"
316                 except ValueError:
317                         print "ERROR: Invalid choice"
318         print "MENU: Selected mode is %s" % mode
319         print ""
321         return mode
322 # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # #
324 # Pad read using GPIO - Specific to linux only
325 # As each pad is muxed with a SoC gpio (for most of the pads)
326 # It's possible to read the pad data using gpio datain registers
327 # Dump the linux commands to read the gpio registers and read the pad data
328 def pad_dump_gpio(padconf, per_padconf):
329         if(args.gpio == False):
330                 return
332         print "# Read pad signals using GPIO DATA-IN registers"
333         print "# Works only for the input signals"
334         gpio_data_addrs = (0, 0x4ae10138, 0x48055138, 0x48057138, 0x48059138, 0x4805b138, 0x4805d138, 0x48051138, 0x48053138)
335         for i in padconf:
336                 (pad_name, pin_name, addr, val, delayinfo) = i
338                 offset = addr - 0x4a002000
339                 gpio_name = xml_pad_get_pin(offset, 14)
340                 matchlist = re.match("GPIO(.)_(.*)", gpio_name)
341                 if (matchlist == None):
342                         print "ERR: No GPIO for pad %s" % pad_name
343                         continue
345                 inst = int(matchlist.groups(0)[0])
346                 bit = int(matchlist.groups(0)[1])
347                 gpio_addr = gpio_data_addrs[inst]
349                 print "#Read GPIO%d_%d to sample %s" % (inst, bit, pin_name)
350                 print " echo %d > /sys/class/gpio/export 2>/dev/null;" % ((inst - 1) * 32)
351                 print " val=`omapconf read 0x%x 2>&1 | grep -v \"support\"`;" % gpio_addr
352                 print " status=$((0x$val >> %d & 0x1));" % bit
353                 print " echo -e \"%s (%s)\t = $status\";" % (pin_name, gpio_name)
354                 print ""
355         print ""
356 # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # #
358 # Generate the final pad and delay data in the required format
359 def format_pad_regs(padconf, per_padconf):
360         print "###########################################"
361         print "Pad data output (with the delay modes)"
362         print "###########################################"
363         if (args.format == "uboot"):
364                 uboot_format_pad_regs(padconf, per_padconf)
365         elif (args.format == "linux"):
366                 linux_format_pad_regs(padconf, per_padconf)
367         elif (args.format == "bios"):
368                 bios_format_pad_regs(padconf, per_padconf)
369         else:
370                 print "ERR: Format %s not suppported" % args.format
372 def format_delay_regs(delayconf, per_delayconf):
373         print "#########################################"
374         print "Delay data output (for manual modes)"
375         print "#########################################"
376         if (args.format == "uboot"):
377                 uboot_format_delay_regs(delayconf, per_delayconf)
378         elif (args.format == "linux"):
379                 linux_format_delay_regs(delayconf, per_delayconf)
380         elif (args.format == "bios"):
381                 bios_format_delay_regs(delayconf, per_delayconf)
382         else:
383                 print "ERR: Format %s not suppported" % args.format
385 def get_pin_info(val):
386         inp_en = (val >> 18) & 0x1
387         pulltype = (val >> 17) & 0x1
388         pull_dis = (val >> 16) & 0x1
389         pin = "PIN"
390         if (inp_en):
391                 pin += "_INPUT"
392         else:
393                 pin += "_OUTPUT"
394         if (pull_dis == 0):
395                 if (pulltype):
396                         pin += "_PULLUP"
397                 else:
398                         pin += "_PULLDOWN"
399         return pin
401 # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # #
403 # Generate output in u-boot format
404 def uboot_format_pad_regs(padconf, per_padconf):
405         print "\nconst struct pad_conf_entry dra74x_core_padconf_array[] = {"
406         for i in padconf:
407                 (pad_name, pin_name, addr, val, delayinfo) = i
409                 if (re.match("MMC.*", pin_name) != None):
410                         print "WARN: Skipping MMC padconf in uboot"
411                         continue
413                 muxmode = val & 0xf
414                 (method, data) = delayinfo
415                 if (method == "LEGACY"):
416                         extramode = ""
417                 elif (method == "VIRTUAL"):
418                         delaymode = data
419                         extramode = " | VIRTUAL_MODE%d" % delaymode
420                 elif (method == "MANUAL"):
421                         extramode = " | MANUAL_MODE"
422                 else:
423                         print "ERR: Invalid method %s" % method
425                 pin_info = get_pin_info(val) + extramode
426                 pad_short = re.sub("CTRL_CORE_PAD_", "", pad_name)
427                 comment = (pad_short + "." + pin_name).lower()
429                 print "\t{ %s, (M%d | %s) },\t/* %s */" % (pad_short, muxmode, pin_info, comment)
430         print "};\n"
432 def uboot_format_delay_regs(delayconf, per_delayconf):
433         manual_del = []
434         for i in delayconf:
435                 (pad_name, pin_name, regname, del_offset, man_name, adel, gdel) = i
437                 if (re.match("MMC.*", pin_name) != None):
438                         print "WARN: Skipping MMC delayconf in uboot"
439                         continue
441                 entry = (del_offset, adel, gdel, regname, pin_name, man_name)
442                 manual_del.append(entry)
444         es_rev = args.revision.replace('.', '_')
445         print "\nconst struct iodelay_cfg_entry dra742_es" + es_rev + "_iodelay_cfg_array[] = {"
446         for entry in sorted(manual_del):
447                 print "\t{ 0x%04X, %5d, %5d },\t/* %s : %s - %s */" % entry
448         print "};\n"
450 # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # #
452 # Generate output in linux format
453 def linux_format_pad_regs(padconf, per_padconf):
454         print "&dra7_pmx_core {"
455         for per in per_padconf:
457                 if (re.match("MMC.*", per) == None):
458                         print "ERR: Only MMC padconf is recommended in kernel"
459                         continue
461                 dtsnode = ("%s_pins_default" % per).lower()
462                 print ""
463                 print "\t%s: %s {" % (dtsnode, dtsnode)
464                 print "\t\tpinctrl-single,pins = <"
465                 for i in per_padconf[per]:
466                         (pad_name, pin_name, addr, val, delayinfo) = i
468                         muxmode = val & 0xf
469                         (method, data) = delayinfo
470                         if (method == "LEGACY"):
471                                 extramode = ""
472                         elif (method == "VIRTUAL"):
473                                 delaymode = data
474                                 extramode = " | VIRTUAL_MODE%d" % delaymode
475                         elif (method == "MANUAL"):
476                                 extramode = " | MANUAL_MODE"
477                         else:
478                                 print "ERR: Invalid method %s" % method
480                         pin_info = get_pin_info(val) + extramode
481                         pad_short = re.sub("CTRL_CORE_PAD_", "", pad_name)
482                         offset = addr - 0x4a003400
483                         comment = (pad_short + "." + pin_name).lower()
485                         print "\t\t\t0x%03X\t(%s | MUM_MODE%d)\t/* %s */" % (offset, pin_info, muxmode, comment)
486                 print "\t\t>;"
487                 print "\t};"
488         print "};\n"
491 def linux_format_delay_regs(delayconf, per_delayconf):
492         print "&dra7_iodelay_core {"
493         for per in per_delayconf.keys():
495                 if (re.match("MMC.*", per) == None):
496                         print "ERR: Only MMC delayconf is recommended in kernel"
497                         continue
499                 # Get the mode from the first entry
500                 (pad_name, pin_name, regname, del_offset, mode, adel, gdel) = per_delayconf[per][0]
502                 dtsnode = ("%s_iodelay_%s_conf" % (per, mode)).lower()
503                 print "\t%s: %s {" % (dtsnode, dtsnode)
504                 print "\t\tpinctrl-single,pins = <"
505                 for i in per_delayconf[per]:
506                         (pad_name, pin_name, regname, del_offset, mode, adel, gdel) = i
508                         print "\t\t\t0x%03X (A_DELAY(%d) | G_DELAY(%d))\t/* %s */" % (del_offset, adel, gdel, regname)
509                 print "\t\t>;"
510                 print "\t};"
511         print "};\n"
513 # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # #
515 # Generate output in bios format
516 def bios_format_pad_regs(padconf, per_padconf):
517         for i in padconf:
518                 (pad_name, pin_name, addr, val, delayinfo) = i
520                 delaylist = []
521                 (method, data) = delayinfo
522                 if (method == "VIRTUAL"):
523                         virt_mode = data
524                         val = val | ( virt_mode<< 4)
525                         val = val | (1 << 8)
526                 elif (method == "MANUAL"):
527                         delaylist = data
528                         val = val | (1 << 8)
530                 offset = addr - 0x4a003400
531                 out_delreg = out_adel = out_gdel = 0
532                 in_delreg  = in_adel  = in_gdel  = 0
533                 oen_delreg = oen_adel = oen_gdel = 0
535                 for j in delaylist:
536                         (regname, adel, gdel) = j
537                         if (re.match(".*_IN", regname) != None):
538                                 in_delreg = xml_iodelay_get_reg(regname)
539                                 in_adel = adel
540                                 in_gdel = gdel
541                         elif (re.match(".*_OEN", regname) != None):
542                                 oen_delreg = xml_iodelay_get_reg(regname)
543                                 oen_adel = adel
544                                 oen_gdel = gdel
545                         elif (re.match(".*_OUT", regname) != None):
546                                 out_delreg = xml_iodelay_get_reg(regname)
547                                 out_adel = adel
548                                 out_gdel = gdel
549                 indel  = "{ 0x%04X, %4d, %4d }" % (in_delreg,  in_adel,  in_gdel)
550                 oendel = "{ 0x%04X, %4d, %4d }" % (oen_delreg, oen_adel, oen_gdel)
551                 outdel = "{ 0x%04X, %4d, %4d }" % (out_delreg, out_adel, out_gdel)
552                 pin_info = get_pin_info(val)
553                 print "\t/* %s -> %s (%s) %s delaymode */" % (pad_name, pin_name, pin_info, method)
554                 print "\t{ 0x%03X, 0x%08X, %s, %s, %s }" % (offset, val, indel, oendel, outdel)
556 def bios_format_delay_regs(delayconf, per_delayconf):
557         print "Manual delays are not configured separately"
558         print "Delays are configured as part of the padconf step only"
560 # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # #
562 # Main execution starts here
563 # * Parse all the XML files - Get the pad data and IOdelay data
564 # * Iterate over the pad register dumps
565 # * For each pad, find out the muxmode being used and the pad direction, etc
566 # * For the muxmode being used, find out available virtual/modes
567 #   - Dump the virtual/manual modes available (based on options)
568 #   - Build up the gpio script to read the pad data using GPIO module
569 # * Select the correct mode to be used
570 #   - Check if the mode is described for the peripheral module, (from selected-modes.txt)
571 #   - Otherwise ask the user (with a menu) to decide the delaymode
572 #     => Update the selection for the whole of the peripheral module
573 #   - Worst case, skip the delaymode for this pad
574 # * Build the pad and delay register information
575 # * Create the dump for pad and delay data in linux/u-boot format
576 # * Dump the delaymode selection for each peripheral
577 # * Dump the GPIO script for each peripheral (all pads grouped together)
580 # Read all the input files and parse the required info
581 modehelp = read_guidelines(modehelp_file)
582 sel = read_selmodes(sel_file)
583 regmap = read_pad_dump(pad_file)
584 reglist = regmap.keys()
586 # List of all the pads being configured
587 padconf = []
588 # List of all the delay registers being configured (for manual mode)
589 delayconf = []
590 # Dictionary of pads grouped by peripheral/module
591 per_padconf = {}
592 # Dictionary of delay registers grouped by peripheral/module
593 per_delayconf = {}
595 xml_check_correctness(modehelp)
597 print "iodelay-autogen.py - Python script to generate the IOdelay data."
598 print "v" + VERSION + " using PCT version " + PCT_VERSION
599 print ""
600 # Start iterating over each pad
601 for i in range(0, 260):
602         # Find out the muxmode and pad direction, etc
603         addr = 0x4a003400 + i * 4
604         offset = 0x1400 + i * 4
605         dts_offset = offset - 0x1400
607         if (addr not in reglist):
608                 print "WARN: Register dump for pad 0x%X not found" % addr
609                 continue
610         val = regmap[addr]
611         muxmode = val & 0xf
613         # Find out the pin based on the muxmode
614         pad_name = xml_pad_get_name(offset)
615         pin_name = xml_pad_get_pin(offset, muxmode)
616         if (pad_name == "Unknown" or pin_name == "Unknown"):
617                 print "WARN: Cannot find out Pad/Pin name for PAD address 0x%X (%s[%s] = %s)" \
618                 % (addr, pad_name, muxmode, pin_name)
619                 continue
620         if (pin_name == "DRIVER OFF"):
621                 continue
623         # Find out if the delaymode for this module is already selected
624         module = re.match("([^_]+)_.*", pin_name).groups(0)[0]
626         if (args.module != "" and args.module != module):
627                 continue
629         if (args.debug >= 1):
630                 print "\nPAD: %s: Addr= 0x%08X Value = 0x%08X \"%s\"" \
631                 % (pad_name, addr, val, pin_name)
633         # Find out all the possible virtual, manual modes fot the specific pad -> pin combination
634         (virt, man) = xml_find_delaymodes(pad_name, muxmode)
636         # Need to select one out of allowed modes
637         mode = select_mode(pad_name, pin_name, module, virt, man, modehelp, sel)
639         # Remember the selection for that module, for later reuse
640         if (args.strict == False):
641                 sel[module] = mode
643         if (mode == "SKIP"):
644                 continue
645         elif (mode == "LEGACY"):
646                 delayinfo = ("LEGACY", "")
647         elif (mode in virt):
648                 delayinfo = ("VIRTUAL", virt[mode])
649         elif (mode in man):
650                 delayinfo = ("MANUAL", man[mode])
651         else:
652                 print "ERR: Unknown mode '%s' selected" % mode
653                 continue
655         if (args.debug >= 1):
656                 print "  => Using mode %s" % mode
657         paddata = (pad_name, pin_name, addr, val, delayinfo)
658         if (module not in per_padconf.keys()):
659                 per_padconf[module] = []
660         padconf.append(paddata)
661         per_padconf[module].append(paddata)
663         if(mode not in man):
664                 continue
666         # Add the delay data if using manual mode
667         for regval in man[mode]:
668                 (regname, adel, gdel) = regval
669                 del_offset = xml_iodelay_get_reg(regname)
670                 if (del_offset == 0):
671                         print "WARN: Can't find delay offset of register %s" % regname
672                         break
673                 if (args.debug >= 1):
674                         print "  => Manual delay[%s] = (%d, %d)" % (regname, adel, gdel)
675                 delaydata = (pad_name, pin_name, regname, del_offset, mode, adel, gdel)
676                 if (module not in per_delayconf.keys()):
677                         per_delayconf[module] = []
678                 delayconf.append(delaydata)
679                 per_delayconf[module].append(delaydata)
681 print ""
682 print "Total PAD registers: %d" % len(padconf)
683 print "Total DELAY registers: %d" % len(delayconf)
684 print ""
686 format_pad_regs(padconf, per_padconf)
687 format_delay_regs(delayconf, per_delayconf)
688 pad_dump_gpio(padconf, per_padconf)
690 # Dump the final selection for reuse
691 print "Selected modes for each peripheral module\n"
692 for group in sel:
693         print "%s,\t%s" % (group, sel[group])
694 print ""
695 # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # #