script: Add support for additional mux in model XML
[glsdk/iodelay-config.git] / iodelay-autogen.py
1 #!/usr/bin/python
2 # Python script to automatically generate the IO pad and delay data
3 # Author:- Nikhil Devshatwar
5 # This script uses regdump of the pad registers to figure out the muxmodes
6 # Based on the pad and muxmode, it find out all possible virtual/manual modes
7 # by referring to the PCT XML model. Using the, selection file, script
8 # decides which modes to be selected. Finally it dumps the required array entries
10 # This script depends on following files:-
11 # * XML data files      - Shipped with the DRA7xx PCT tool
12 # * Pad register dump   - Generate using omapconf dump 0x4a003400 0x4a00380c
13 # * selection file      - List of selected virtual/manual modes to be used
15 import xml.etree.ElementTree as ET
16 import re
17 import argparse
19 # Handle the command line arguments
20 parser = argparse.ArgumentParser(prog='iodelay-autogen.py',
21         description='Python script to generate the IOdelay data.\n' \
22                 'This script refers to the XML data and automatically generates\n' \
23                 'PAD and DELAY data for the same use case.\n' \
24                 'Note that only the PADs which are used in the dump are configured.',
25         epilog='Generate the pad and delay data using pad register dumps. For this,\n' \
26                 'Run omapconf dump 0x4a003400 0x4a00380c and save the output')
28 parser.add_argument('-p', '--part', dest='part',
29         action='store', type=str, choices=["dra74x", "dra75x", "dra72x"], default="dra74x",
30         help='select the device part')
32 parser.add_argument('-r', '--revision', dest='revision',
33         action='store', type=str, choices=["1.0", "1.1", "2.0"], default="2.0",
34         help='select the silicon revision')
36 parser.add_argument('-m', '--module', dest='module',
37         action='store', type=str, default="",
38         help='generate only for modules matching the provided RE')
40 parser.add_argument('-f', '--format', dest='format',
41         action='store', type=str, choices=["linux", "uboot", "bios"], default="uboot",
42         help='select the output format to be used')
44 parser.add_argument('-d', '--debug', dest='debug',
45         action='store', type=int, choices=[0, 1, 2, 3, 4], default=0,
46         help='set the debug level - ERR,WARN,INFO,DBG,VERBOSE')
48 parser.add_argument('-i', '--interactive', dest='interactive',
49         action='store', type=int, choices=[0, 1], default=1,
50         help='run interactively with menus for resolving conflicts')
52 parser.add_argument('-s', '--strict', dest='strict',
53         action='store_true',
54         help='strict mode - ask for each pad of the group, do not save selection.\n' \
55                 'For some peripherals, same delaymode cannot be used for all the pads.\n' \
56                 'Use this mode to select different modes for each pad')
58 parser.add_argument('-g', '--gpio', dest='gpio',
59         action='store_true',
60         help='generate script to probe signals using gpio')
62 parser.add_argument('-c', '--check', dest='check_xml',
63         action='store_true',
64         help='check consistency of the XML files and other data')
66 args = parser.parse_args()
68 # Some more knobs for developers, Don't want to expose them to cmd line
69 args.resetslew = True
71 # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # #
73 VERSION = "2.7"
75 if (args.part == "dra74x" or args.part == "dra75x"):
76         if (args.revision == "1.0" or args.revision == "1.1"):
77                 args.revision = "1.x"
78         XML_PATH = "XMLFiles/DRA75x_DRA74x"
79         PART = "DRA75x_DRA74x"
80         PCT_VERSION = "v1.0.16"
81 elif (args.part == "dra72x"):
82         if (args.revision == "1.1"):
83                 print "dra72x doesn't have silicon revision 1.1"
84                 exit()
85         XML_PATH = "XMLFiles/DRA72x"
86         PART = "DRA72x"
87         PCT_VERSION = "v1.0.9"
89 pad_data_xml   = XML_PATH + "/CTRL_MODULE_CORE.xml"
90 iod_data_xml   = XML_PATH + "/IODELAYCONFIG.xml"
91 model_data_xml = XML_PATH + "/model_" + PART + "_SR" + args.revision + "_" + PCT_VERSION + ".xml"
92 modehelp_file  = XML_PATH + "/guidelines_SR" + args.revision + ".txt"
94 pad_file = "ctrl-core.dump"
95 sel_file = "selected-modes.txt"
97 def trace(level, msg):
98         if (args.debug >= level):
99                 print(msg)
100 def verbose(msg):
101         trace(4, "DEBUG: " + msg)
102 def debug(msg, args=None):
103         trace(3, "DEBUG: " + msg)
104 def info(msg):
105         trace(2, "INFO: " + msg)
106 def warn(msg):
107         trace(1, "WARN: " + msg)
108 def error(msg):
109         trace(0, "ERR: " + msg)
110 def fatal(msg):
111         trace(0, "FATAL: " + msg)
112         exit()
114 if (args.interactive):
115         print "iodelay-autogen.py - Python script to generate the IOdelay data."
116         print "v" + VERSION + " using PCT version " + PCT_VERSION
117         print "Parsing PCT data from " + model_data_xml + "..."
118         print ""
120 # Read the XML file database for pad and delay registers
121 pad_xml = ET.parse(pad_data_xml).getroot()
122 iod_xml = ET.parse(iod_data_xml).getroot()
123 model_xml = ET.parse(model_data_xml).getroot()
125 # Functions to parse the input files and build data structures
126 def read_guidelines(fname):
127         modehelp = {}
128         pattern = re.compile('([^\t.]+\w)\t+(.+)')
129         f = open(fname)
130         for line in f.readlines():
131                 list = re.match(pattern, line)
132                 if ( list == None):
133                         continue
134                 mode = list.groups(0)[0]
135                 info = list.groups(0)[1]
136                 modehelp[mode] = info
137                 verbose("Guideline: Mode '%30s' => '%s'" % (mode, info))
138         return modehelp
140 def read_selmodes(fname):
141         sel = {}
142         pattern = re.compile('(\w+)\W*,\W*(\w*)')
143         f = open(fname)
144         for line in f.readlines():
145                 list = re.match(pattern, line)
146                 if ( list == None):
147                         continue
148                 module = list.groups(0)[0]
149                 mode = list.groups(0)[1]
150                 sel[module] = mode
151                 verbose("Input modes: Select '%s' => '%s'" % (mode, module))
152         return sel
154 def read_pad_dump(file):
155         regmap = {}
156         pattern = re.compile('.*(0x[0-9A-Fa-f]+).*(0x[0-9A-Fa-f]+).*')
157         f = open(file, 'r')
158         for line in f:
159                 list = re.match(pattern, line)
160                 if ( list == None):
161                         continue
162                 addr = int(list.groups(0)[0], 16)
163                 val = int(list.groups(0)[1], 16)
164                 verbose("XML pad-reg: Addr = %08x Value = %08x" % (addr, val))
165                 regmap[addr] = val
166         return regmap
168 # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # #
169 # Read all the input files and parse the required info
170 modehelp = read_guidelines(modehelp_file)
171 sel = read_selmodes(sel_file)
172 regmap = read_pad_dump(pad_file)
173 reglist = regmap.keys()
175 # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # #
177 # Helper functions to parse XML nodes and get the desired data
178 # Hugely dependent on the XML format of the PCT files
179 # Uses XPath to search elements with queries and filters
180 # Parse the nodes to generate data in desired format
182 def xml_pad_get_name(offset):
183         padlist = pad_xml.findall("register[@offset='0x%X']" % offset)
184         if (len(padlist) == 0):
185                 return "Unknown"
186         else:
187                 return padlist[0].get("id")
189 def xml_pad_get_offset(name):
190         padlist = pad_xml.findall("register[@id='%s']" % name)
191         if (len(padlist) == 0):
192                 return None
193         else:
194                 return int(padlist[0].get("offset"), 16)
196 def xml_pad_get_slew(offset):
197         padlist = pad_xml.findall("register[@offset='0x%X']" % offset)
198         if (len(padlist) == 0):
199                 return 0x0
200         else:
201                 bitlist = padlist[0].findall("bitfield[@begin='19']")
202                 if (len(bitlist) == 0):
203                         return 0x0
204                 else:
205                         return int(bitlist[0].get("resetval"), 16)
207 # For DRA72x SoC, for "ball compatibility" purpose, some signals have same muxmode.
208 # CTRL_CORE_ALT_SELECT_MUX register allows to select between one of the signals
209 # Its like a board mux has been added inside the SoC, except it uses same muxmode.
210 def resolve_group(muxmode_str):
211         mmlist = muxmode_str.split(" ")
212         mmlen = len(mmlist)
213         if (mmlen == 1):
214                 def_mode = mmlist[0]
215                 return mmlist[0]
216         elif (mmlen == 2):
217                 def_mode = mmlist[0]
218                 grp1_mode = mmlist[1]
219         elif (mmlen == 3):
220                 def_mode = mmlist[0]
221                 grp1_mode = mmlist[1]
222                 grp2_mode = mmlist[2]
223         else:
224                 error("Cannot resolve muxmode group for '%s'" % muxmode_str)
226         #HACK for now
227         warn("Not resolving muxmode %s, assuming default %s" % (muxmode_str, def_mode))
228         return def_mode
230 def xml_model_get_signal(offset, muxmode):
231         padlist = pad_xml.findall("register[@offset='0x%X']" % offset)
232         if (len(padlist) == 0):
233                 return "Unknown"
234         else:
235                 mux_field = padlist[0].findall("./bitfield[@end='0']")
236                 if (len(mux_field) == 0):
237                         return "Unknown"
238                 modes = mux_field[0].findall("./bitenum[@value='%d']" % muxmode)
239                 if (len(modes) == 0):
240                         return "Unknown"
241                 return resolve_group(modes[0].get("id"))
243 def xml_iodelay_get_reg(name):
244         delaylist = iod_xml.findall("register[@id='%s']" % name)
245         if (len(delaylist) == 0):
246                 return 0
247         else:
248                 offset = delaylist[0].get("offset")
249                 verbose("XML delay-reg: Name = %s Offset = %s" % (name, offset))
250                 return int(offset, 16)
252 def xml_get_virtual(mode):
253         vmodes = {}
254         signal = mode.findtext("signal")
255         for virt in mode.findall("virtualmode/mode"):
256                 virt_mode = virt.findtext("value")
257                 virt_name = virt.findtext("name")
258                 if (virt_name == "NA"):
259                         continue
260                 virt_mode = int(virt_mode)
261                 vmodes[virt_name] = virt_mode
262                 debug("    * VIRTUAL: %s [%s] => delaymode = %d" % (signal, virt_name, virt_mode))
263         return vmodes
265 def xml_get_manual(mode):
266         mmodes = {}
267         signal = mode.findtext("signal")
268         for man in mode.findall("manualmode"):
269                 regname = man.findtext("cfgreg/name")
270                 for sel in man.findall("cfgreg/mode"):
271                         adel = sel.findtext("adelay")
272                         gdel = sel.findtext("gdelay")
273                         man_name = sel.findtext("name")
274                         if (man_name == "NA"):
275                                 continue
276                         adel = int(adel)
277                         gdel = int(gdel)
278                         if (man_name not in mmodes.keys()):
279                                 mmodes[man_name] = []
280                         mmodes[man_name].append((regname, adel, gdel))
281                         debug("    * MANUAL: %s [%s] => delay[%s] = %d, %d" % (signal, man_name, regname, adel, gdel))
282         return mmodes
284 def xml_get_additional_mode(orig):
285         additional_mux = orig.findall("additionalMux/confregisters")
286         if (len(additional_mux) == 0):
287                 return orig
288         else:
289                 additional_mux = additional_mux[0]
290                 mux_reg_name = additional_mux.findtext("register")
291                 offset = xml_pad_get_offset(mux_reg_name)
293                 if (offset == None):
294                         error("Could not find register address for register '%s'" % mux_reg_name)
295                         fatal("This pin may have virtual/manual modes, Fix XML file")
297                 addr = 0x4a002000 + offset
298                 if (addr not in reglist):
299                         error("register dump lacks data for additional muxes")
300                         warn("using default values")
301                         muxval = 0x0
302                 else:
303                         muxval = regmap[addr]
305                 values = additional_mux.findall("value")
306                 for value in values:
308                         option = int(value.findtext("option"))
309                         fieldpos = value.findtext("fieldPos")
310                         signal = value.findtext("signal").upper()
311                         matchlist = re.match("([0-9]+)[:]*([0-9]*)", fieldpos)
313                         verbose("++++ Additional mux %s possible" % signal)
314                         end = int(matchlist.groups(0)[0])
315                         if (matchlist.groups(0)[1] == ""):
316                                 start = end
317                         else:
318                                 start = int(matchlist.groups(0)[1])
320                         muxval = muxval & (1 << end)
321                         muxval = muxval >> start
323                         if (muxval == option):
324                                 debug(">>>> Additional mux %s[%s] = %d" % (mux_reg_name, fieldpos, option))
325                                 debug(">>>> Effective signal = %s" % signal)
326                                 return value
327                 error("None of the additional Mux value matched, using default")
328                 return values[0]
330 def xml_find_delaymodes(pad_name, muxmode):
331         padlist = model_xml.findall("padDB/clockNode/type/pad")
332         for pad in padlist:
333                 if (pad_name == pad.findtext("confregisters/regbit/register")):
334                         muxmodes = pad.findall("muxmode")
335                         break
336         if not muxmodes:
337                 return None
338         for mode in muxmodes:
339                 if ("%d" % muxmode == mode.findtext("mode")):
340                         mode = xml_get_additional_mode(mode)
341                         virt = xml_get_virtual(mode)
342                         man = xml_get_manual(mode)
343                         return (virt, man)
344         return None
346 def xml_check_correctness(modehelp):
348         print "###########################################"
349         print "XML correctness checks:"
350         padcore_list = []
351         padmodel_list = []
352         modes = {}
354         # Find all the pads in core XML
355         pad_list = pad_xml.findall("register")
356         for i in pad_list:
357                 name = i.get("id")
358                 if (re.match("CTRL_CORE_PAD_.*", name) == None):
359                         continue
360                 padcore_list.append(name)
361         print ">> Total pads defined in core XML = %d" % len(padcore_list)
363         # Find all the pads in model XML
364         pad_list = model_xml.findall("padDB/clockNode/type/pad/confregisters/regbit")
365         for i in pad_list:
366                 name = i.findtext("register")
367                 padmodel_list.append(name)
368         print ">> Total pads defined in model XML = %d" % len(padmodel_list)
370         # Find all the manual modes
371         manmode_list = model_xml.findall("padDB/clockNode/type/pad/muxmode/manualmode/cfgreg/mode")
372         for i in manmode_list:
373                 man_name = i.findtext("name")
374                 modes[man_name] = "manual"
375         # Find all the virtual modes
376         virtmode_list = model_xml.findall("padDB/clockNode/type/pad/muxmode/virtualmode/mode")
377         for i in virtmode_list:
378                 virt_name = i.findtext("name")
379                 modes[virt_name] = "virtual"
380         print ">> Total delaymodes defined in model XML = %d" % len(modes)
382         # Print out all the errors found in the tests
383         print "== Pads defined in core XML but not in model XML =="
384         for i in padcore_list:
385                 if (i not in padmodel_list):
386                         print "\t%s" % i
387         print "== Pads defined in model XML but not in core XML =="
388         for i in padmodel_list:
389                 if (i not in padcore_list):
390                         print "\t%s" % i
392         # Check if description for each mode is available
393         print "== Delaymodes missing description in the guidelines.txt =="
394         for i in modes:
395                 if (i not in modehelp):
396                         print "\t%s" % i
398         # Check if description for unknown mode is documented
399         print "== Delaymodes unused from guidelines.txt =="
400         for i in modehelp:
401                 if (i not in modes):
402                         print "\t%s" % i
404         print "###########################################"
406 # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # #
408 # Decision point of the script
409 # For each pad/pin, decide what delay method is used
410 # Lookup in the selection file or ask user with a menu
411 def select_mode(pad, pin, module, virt, man, modehelp, sel):
412         modelist = []
413         for modename in virt.keys():
414                 modelist.append(modename)
416         for modename in man.keys():
417                 modelist.append(modename)
419         if (len(modelist) == 0):
420                 return "LEGACY"
422         if (module in sel.keys()):
423                 mode = sel[module]
424                 if (mode == "SKIP" or mode == "LEGACY" or mode in modelist):
425                         return mode
426                 else:
427                         error("Invalid delaymode '%s' for module '%s'" % (mode, module))
429         if (args.interactive == 0):
430                 warn("No delay modes for %s found, skipping" % module)
431                 mode = "SKIP"
432                 return mode
434         # Display the menu and ask user to select the 'right' mode
435         while True:
436                 print ""
437                 print "MENU: Select delay mode for %s -> %s" % (pad, pin)
438                 i = 0
439                 print "MENU: %d: %s \t\t\t%s" % (i, "SKIP", "Skips this module for now")
440                 i = 1
441                 print "MENU: %d: %s \t\t%s" % (i, "LEGACY", "No external delay config (No virtual/manual needed)")
442                 for mode in modelist:
443                         i += 1
444                         if (mode in modehelp):
445                                 helptext = modehelp[mode]
446                         else:
447                                 helptext = "Unknown"
448                         print "MENU: %d: %s \t\t%s" % (i, mode, helptext)
449                 try:
450                         choice = int(raw_input("Select delay mode #> "))
451                         if (choice == 0):
452                                 mode = "SKIP"
453                                 break
454                         elif (choice == 1):
455                                 mode = "LEGACY"
456                                 break
457                         elif (choice >=2 and choice <= len(modelist) + 1):
458                                 mode = modelist[choice - 2]
459                                 break
460                         print "ERROR: Invalid choice"
461                 except ValueError:
462                         print "ERROR: Invalid choice"
463         print "MENU: Selected mode is %s" % mode
464         print ""
466         return mode
467 # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # #
469 # Pad read using GPIO - Specific to linux only
470 # As each pad is muxed with a SoC gpio (for most of the pads)
471 # It's possible to read the pad data using gpio datain registers
472 # Change pad register to enable input path and export sysfs
473 # Use sysfs to read the status of GPIO and print in a loop
474 def pad_dump_gpio(padconf, per_padconf):
475         gpio_data_addrs = (0, 0x4ae10138, 0x48055138, 0x48057138, 0x48059138, 0x4805b138, 0x4805d138, 0x48051138, 0x48053138)
476         module = args.module
478         # script header
479         gen_header = "###########################################\n" + \
480                      "# Read %s signals using GPIO sysfs\n" % module + \
481                      "###########################################\n\n"
482         gen_data = "%s_data=(\n" % module
484         for i in padconf:
485                 (pad_name, pin_name, addr, val, mode, delayinfo) = i
487                 offset = addr - 0x4a002000
488                 gpio_name = xml_model_get_signal(offset, 14)
489                 matchlist = re.match("GPIO(.)_(.*)", gpio_name)
490                 if (matchlist == None):
491                         error("No GPIO for pad %s - cannot read from script" % pad_name)
492                         continue
494                 inst = int(matchlist.groups(0)[0])
495                 bit = int(matchlist.groups(0)[1])
496                 gpio_addr = gpio_data_addrs[inst]
497                 ngpio = (inst - 1) * 32 + bit
498                 pin_short = re.match(".+_(.*)", pin_name).groups(0)[0]
500                 gen_data += "\t%s:0x%x:%s:%d:0x%x:%d\n" % (pin_short, addr, gpio_name, ngpio, gpio_addr, bit)
502         gen_data += ")\n\n"
504         # Main script to probe the signal
505         gen_main = "echo; echo Probing %s signals\n\n" % module + \
506                    "for data in ${%s_data[@]}\n" % module + \
507                    "do\n" + \
508                    "    pin=`echo $data | cut -d ':' -f1`\n" + \
509                    "    pad=`echo $data | cut -d ':' -f2`\n" + \
510                    "    ngpio=`echo $data | cut -d ':' -f4`\n" + \
511                    "    echo $ngpio > /sys/class/gpio/export 2>/dev/null\n" + \
512                    "    omapconf set bit $pad 18 1>/dev/null 2>/dev/null\n" + \
513                    "    printf \"%8s\" $pin\n" + \
514                    "done\n" + \
515                    "echo\n\n"
517         gen_main += "while true;\n" + \
518                     "do\n" + \
519                     "    for data in ${%s_data[@]}\n" % module + \
520                     "    do\n" + \
521                     "#       pin=`echo $data | cut -d ':' -f1`\n" + \
522                     "#        pad=`echo $data | cut -d ':' -f2`\n" + \
523                     "#       gpio=`echo $data | cut -d ':' -f3`\n" + \
524                     "        ngpio=`echo $data | cut -d ':' -f4`\n" + \
525                     "#       addr=`echo $data | cut -d ':' -f5`\n" + \
526                     "#       bit=`echo $data | cut -d ':' -f6`\n" + \
527                     "        val=`cat /sys/class/gpio/gpio$ngpio/value`\n" + \
528                     "        printf %8d $val \n" + \
529                     "    done\n" + \
530                     "    echo\n" + \
531                     "done\n\n"
533         gen_footer = "###########################################\n"
535         # Generate the shell script
536         gen_script = gen_header + gen_data + gen_main + gen_footer
537         filename = ("./%s-probe.sh" % module).lower()
538         print "Generating '%s' script..." % filename
539         gen_file = open(filename, "w+")
540         gen_file.write(gen_script)
542 # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # #
544 # Generate the final pad and delay data in the required format
545 def format_pad_regs(padconf, per_padconf):
546         print "######## Pad data output ########"
547         if (args.format == "uboot"):
548                 uboot_format_pad_regs(padconf, per_padconf)
549         elif (args.format == "linux"):
550                 linux_format_pad_regs(padconf, per_padconf)
551         elif (args.format == "bios"):
552                 bios_format_pad_regs(padconf, per_padconf)
553         else:
554                 error("Format %s not suppported" % args.format)
556 def format_delay_regs(delayconf, per_delayconf):
557         print "######## Delay data output ########"
558         if (args.format == "uboot"):
559                 uboot_format_delay_regs(delayconf, per_delayconf)
560         elif (args.format == "linux"):
561                 linux_format_delay_regs(delayconf, per_delayconf)
562         elif (args.format == "bios"):
563                 bios_format_delay_regs(delayconf, per_delayconf)
564         else:
565                 error("Format %s not suppported" % args.format)
567 def get_pin_info(val):
568         slew_fast = (val >> 19) & 0x1
569         inp_en = (val >> 18) & 0x1
570         pulltype = (val >> 17) & 0x1
571         pull_dis = (val >> 16) & 0x1
572         pin = "PIN"
573         if (inp_en):
574                 pin += "_INPUT"
575         else:
576                 pin += "_OUTPUT"
577         if (pull_dis == 0):
578                 if (pulltype):
579                         pin += "_PULLUP"
580                 else:
581                         pin += "_PULLDOWN"
582         if (slew_fast):
583                 pin += " | SLEWCONTROL"
584         return pin
586 # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # #
588 # Generate output in u-boot format
589 def uboot_format_pad_regs(padconf, per_padconf):
590         print "\nconst struct pad_conf_entry dra74x_core_padconf_array[] = {"
591         for i in padconf:
592                 (pad_name, pin_name, addr, val, mode, delayinfo) = i
594                 muxmode = val & 0xf
595                 (method, data) = delayinfo
596                 if (method == "LEGACY"):
597                         extramode = ""
598                 elif (method == "VIRTUAL"):
599                         delaymode = data
600                         extramode = " | VIRTUAL_MODE%d" % delaymode
601                 elif (method == "MANUAL"):
602                         extramode = " | MANUAL_MODE"
603                 else:
604                         error("Invalid delay method %s" % method)
606                 pin_info = get_pin_info(val) + extramode
607                 pad_short = re.sub("CTRL_CORE_PAD_", "", pad_name)
608                 comment = (pad_short + "." + pin_name).lower()
610                 print "\t{ %s, (M%d | %s) },\t/* %s */" % (pad_short, muxmode, pin_info, comment)
611         print "};\n"
613 def uboot_format_delay_regs(delayconf, per_delayconf):
614         manual_del = []
615         for i in delayconf:
616                 (pad_name, pin_name, regname, del_offset, man_name, adel, gdel) = i
618                 entry = (del_offset, adel, gdel, regname, pin_name, man_name)
619                 manual_del.append(entry)
621         es_rev = args.revision.replace('.', '_')
622         print "\nconst struct iodelay_cfg_entry dra742_es" + es_rev + "_iodelay_cfg_array[] = {"
623         for entry in sorted(manual_del):
624                 print "\t{ 0x%04X, %5d, %5d },\t/* %s : %s - %s */" % entry
625         print "};\n"
627 # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # #
629 # Generate output in linux format
630 def linux_format_pad_regs(padconf, per_padconf):
631         print "&dra7_pmx_core {"
632         for per in per_padconf:
634                 if (re.match("MMC.*", per) == None):
635                         warn("Only MMC padconf is recommended in kernel")
637                 # Get the mode from the first entry
638                 (pad_name, pin_name, addr, val, mode, delayinfo) = per_padconf[per][0]
640                 dtsnode = ("%s_pins_%s" % (per, mode)).lower()
641                 print ""
642                 print "\t%s: %s {" % (dtsnode, dtsnode)
643                 print "\t\tpinctrl-single,pins = <"
644                 for i in per_padconf[per]:
645                         (pad_name, pin_name, addr, val, mode, delayinfo) = i
647                         muxmode = val & 0xf
648                         (method, data) = delayinfo
649                         if (method == "LEGACY"):
650                                 extramode = ""
651                         elif (method == "VIRTUAL"):
652                                 delaymode = data
653                                 extramode = " | MUX_VIRTUAL_MODE%d" % delaymode
654                         elif (method == "MANUAL"):
655                                 extramode = " | MANUAL_MODE"
656                         else:
657                                 warn("Invalid method %s" % method)
659                         pin_info = get_pin_info(val) + extramode
660                         pad_short = re.sub("CTRL_CORE_PAD_", "", pad_name)
661                         offset = addr - 0x4a003400
662                         comment = (pad_short + "." + pin_name).lower()
664                         print "\t\t\t0x%03X\t(%s | MUX_MODE%d)\t/* %s */" % (offset, pin_info, muxmode, comment)
665                 print "\t\t>;"
666                 print "\t};"
667         print "};\n"
670 def linux_format_delay_regs(delayconf, per_delayconf):
671         print "&dra7_iodelay_core {"
672         for per in per_delayconf.keys():
674                 if (re.match("MMC.*", per) == None):
675                         warn("Only MMC delayconf is recommended in kernel")
677                 # Get the mode from the first entry
678                 (pad_name, pin_name, regname, del_offset, mode, adel, gdel) = per_delayconf[per][0]
680                 dtsnode = ("%s_iodelay_%s_conf" % (per, mode)).lower()
681                 print "\t%s: %s {" % (dtsnode, dtsnode)
682                 print "\t\tpinctrl-single,pins = <"
683                 for i in per_delayconf[per]:
684                         (pad_name, pin_name, regname, del_offset, mode, adel, gdel) = i
686                         print "\t\t\t0x%03X (A_DELAY(%d) | G_DELAY(%d))\t/* %s */" % (del_offset, adel, gdel, regname)
687                 print "\t\t>;"
688                 print "\t};"
689         print "};\n"
691 # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # #
693 # Generate output in bios format
694 def bios_format_pad_regs(padconf, per_padconf):
695         for i in padconf:
696                 (pad_name, pin_name, addr, val, mode, delayinfo) = i
698                 delaylist = []
699                 (method, data) = delayinfo
700                 if (method == "VIRTUAL"):
701                         virt_mode = data
702                         val = val | ( virt_mode<< 4)
703                         val = val | (1 << 8)
704                 elif (method == "MANUAL"):
705                         delaylist = data
706                         val = val | (1 << 8)
708                 offset = addr - 0x4a003400
709                 out_delreg = out_adel = out_gdel = 0
710                 in_delreg  = in_adel  = in_gdel  = 0
711                 oen_delreg = oen_adel = oen_gdel = 0
713                 for j in delaylist:
714                         (regname, adel, gdel) = j
715                         if (re.match(".*_IN", regname) != None):
716                                 in_delreg = xml_iodelay_get_reg(regname)
717                                 in_adel = adel
718                                 in_gdel = gdel
719                         elif (re.match(".*_OEN", regname) != None):
720                                 oen_delreg = xml_iodelay_get_reg(regname)
721                                 oen_adel = adel
722                                 oen_gdel = gdel
723                         elif (re.match(".*_OUT", regname) != None):
724                                 out_delreg = xml_iodelay_get_reg(regname)
725                                 out_adel = adel
726                                 out_gdel = gdel
727                 indel  = "{ 0x%04X, %4d, %4d , 0}" % (in_delreg,  in_adel,  in_gdel)
728                 oendel = "{ 0x%04X, %4d, %4d , 0}" % (oen_delreg, oen_adel, oen_gdel)
729                 outdel = "{ 0x%04X, %4d, %4d , 0}" % (out_delreg, out_adel, out_gdel)
730                 pin_info = get_pin_info(val)
731                 print "\t/* %s -> %s (%s) %s delaymode */" % (pad_name, pin_name, pin_info, method)
732                 print "\t{ 0x%03X, 0x%08X, %s, %s, %s }" % (offset, val, indel, oendel, outdel)
734 def bios_format_delay_regs(delayconf, per_delayconf):
735         debug("Manual delays are not configured separately")
736         debug("Delays are configured as part of the padconf step only")
738 # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # #
740 # Main execution starts here
741 # * Parse all the XML files - Get the pad data and IOdelay data
742 # * Iterate over the pad register dumps
743 # * For each pad, find out the muxmode being used and the pad direction, etc
744 # * For the muxmode being used, find out available virtual/modes
745 #   - Dump the virtual/manual modes available (based on options)
746 #   - Build up the gpio script to read the pad data using GPIO module
747 # * Select the correct mode to be used
748 #   - Check if the mode is described for the peripheral module, (from selected-modes.txt)
749 #   - Otherwise ask the user (with a menu) to decide the delaymode
750 #     => Update the selection for the whole of the peripheral module
751 #   - Worst case, skip the delaymode for this pad
752 # * Build the pad and delay register information
753 # * Create the dump for pad and delay data in linux/u-boot format
754 # * Dump the delaymode selection for each peripheral
755 # * Dump the GPIO script for each peripheral (all pads grouped together)
758 # List of all the pads being configured
759 padconf = []
760 # List of all the delay registers being configured (for manual mode)
761 delayconf = []
762 # Dictionary of pads grouped by peripheral/module
763 per_padconf = {}
764 # Dictionary of delay registers grouped by peripheral/module
765 per_delayconf = {}
767 if(args.check_xml):
768         xml_check_correctness(modehelp)
769         exit()
771 # Start iterating over each pad
772 for i in range(0, 260):
773         # Find out the muxmode and pad direction, etc
774         addr = 0x4a003400 + i * 4
775         offset = 0x1400 + i * 4
776         dts_offset = offset - 0x1400
778         if (addr not in reglist):
779                 warn("Register dump for pad 0x%X not found" % addr)
780                 continue
781         val = regmap[addr]
782         muxmode = val & 0xf
784         # Find out the pin based on the muxmode
785         pad_name = xml_pad_get_name(offset)
786         pin_name = xml_model_get_signal(offset, muxmode)
787         if (pad_name == "Unknown" or pin_name == "Unknown"):
788                 warn("Cannot find out Pad/Pin name for PAD address 0x%X (%s[%s] = %s)" \
789                 % (addr, pad_name, muxmode, pin_name))
790                 continue
791         if (pin_name == "DRIVER"):
792                 continue
794         # Find out if the delaymode for this module is already selected
795         match = re.match("([^_]+)_.*", pin_name)
796         if (match):
797                 module = match.groups(0)[0]
798         else:
799                 module = pin_name
801         if (args.module != "" and re.match("%s" % args.module, module) == None):
802                 continue
804         # It is recommended to keep the reset value of the slewcontrol bit
805         # Find out the reset value from XML and update if required
806         if (args.resetslew):
807                 val |= (xml_pad_get_slew(offset) & 0x1) << 19
809         debug("PAD: %s: Addr= 0x%08X Value = 0x%08X \"%s\"" \
810                 % (pad_name, addr, val, pin_name))
812         # Find out all the possible virtual, manual modes fot the specific pad -> pin combination
813         (virt, man) = xml_find_delaymodes(pad_name, muxmode)
815         if (args.gpio == True):
816                 mode = "LEGACY"
817         else:
818                 # Need to select one out of allowed modes
819                 mode = select_mode(pad_name, pin_name, module, virt, man, modehelp, sel)
821         # Remember the selection for that module, for later reuse
822         if (args.strict == False and module not in sel.keys()):
823                 sel[module] = mode
825         if (mode == "SKIP"):
826                 continue
827         elif (mode == "LEGACY"):
828                 delayinfo = ("LEGACY", "")
829         elif (mode in virt):
830                 delayinfo = ("VIRTUAL", virt[mode])
831         elif (mode in man):
832                 delayinfo = ("MANUAL", man[mode])
833         else:
834                 error("Unknown mode '%s' selected" % mode)
835                 continue
837         debug("  => Using mode %s" % mode)
838         paddata = (pad_name, pin_name, addr, val, mode, delayinfo)
839         if (module not in per_padconf.keys()):
840                 per_padconf[module] = []
841         padconf.append(paddata)
842         per_padconf[module].append(paddata)
844         if(mode not in man):
845                 continue
847         # Add the delay data if using manual mode
848         for regval in man[mode]:
849                 (regname, adel, gdel) = regval
850                 del_offset = xml_iodelay_get_reg(regname)
851                 if (del_offset == 0):
852                         error("Can't find delay offset of register %s" % regname)
853                         break
854                 debug("  => Manual delay[%s] = (%d, %d)" % (regname, adel, gdel))
855                 delaydata = (pad_name, pin_name, regname, del_offset, mode, adel, gdel)
856                 if (module not in per_delayconf.keys()):
857                         per_delayconf[module] = []
858                 delayconf.append(delaydata)
859                 per_delayconf[module].append(delaydata)
861 if(args.gpio == True):
862         pad_dump_gpio(padconf, per_padconf)
863         exit()
865 format_pad_regs(padconf, per_padconf)
866 format_delay_regs(delayconf, per_delayconf)
868 if (args.interactive):
869         # Summary of the generated data
870         print ""
871         print "Total PAD registers: %d" % len(padconf)
872         print "Total DELAY registers: %d" % len(delayconf)
873         print ""
874         # Dump the final selection for reuse
875         print "Selected modes for each peripheral module\n"
876         for group in sel:
877                 print "%s,\t%s" % (group, sel[group])
878         print ""
879 # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # #