XML: PCT: Update DRA75x SR2.0 XML files
[glsdk/iodelay-config.git] / iodelay-autogen.py
1 #!/usr/bin/python
2 # Python script to automatically generate the IO pad and delay data
3 # Author:- Nikhil Devshatwar
5 # This script uses regdump of the pad registers to figure out the muxmodes
6 # Based on the pad and muxmode, it find out all possible virtual/manual modes
7 # by referring to the PCT XML model. Using the, selection file, script
8 # decides which modes to be selected. Finally it dumps the required array entries
10 # This script depends on following files:-
11 # * XML data files      - Shipped with the DRA7xx PCT tool
12 # * Pad register dump   - Generate using omapconf dump 0x4a003400 0x4a00380c
13 # * selection file      - List of selected virtual/manual modes to be used
15 import xml.etree.ElementTree as ET
16 import re
17 import argparse
19 # Handle the command line arguments
20 parser = argparse.ArgumentParser(prog='iodelay-autogen.py',
21         description='Python script to generate the IOdelay data.\n' \
22                 'This script refers to the XML data and automatically generates\n' \
23                 'PAD and DELAY data for the same use case.\n' \
24                 'Note that only the PADs which are used in the dump are configured.',
25         epilog='Generate the pad and delay data using pad register dumps. For this,\n' \
26                 'Run omapconf dump 0x4a003400 0x4a00380c and save the output')
28 parser.add_argument('-p', '--part', dest='part',
29         action='store', type=str, choices=["dra74x", "dra75x", "dra72x"], default="dra74x",
30         help='select the device part')
32 parser.add_argument('-r', '--revision', dest='revision',
33         action='store', type=str, choices=["1.0", "1.1", "2.0"], default="1.1",
34         help='select the silicon revision')
36 parser.add_argument('-m', '--module', dest='module',
37         action='store', type=str, default="",
38         help='generate only for modules matching the provided RE')
40 parser.add_argument('-f', '--format', dest='format',
41         action='store', type=str, choices=["linux", "uboot", "bios"], default="uboot",
42         help='select the output format to be used')
44 parser.add_argument('-d', '--debug', dest='debug',
45         action='store', type=int, choices=[0, 1, 2, 3, 4], default=0,
46         help='set the debug level - ERR,WARN,INFO,DBG,VERBOSE')
48 parser.add_argument('-i', '--interactive', dest='interactive',
49         action='store', type=int, choices=[0, 1], default=1,
50         help='run interactively with menus for resolving conflicts')
52 parser.add_argument('-s', '--strict', dest='strict',
53         action='store_true',
54         help='strict mode - ask for each pad of the group, do not save selection.\n' \
55                 'For some peripherals, same delaymode cannot be used for all the pads.\n' \
56                 'Use this mode to select different modes for each pad')
58 parser.add_argument('-g', '--gpio', dest='gpio',
59         action='store_true',
60         help='generate script to probe signals using gpio')
62 parser.add_argument('-c', '--check', dest='check_xml',
63         action='store_true',
64         help='check consistency of the XML files and other data')
66 args = parser.parse_args()
68 # Some more knobs for developers, Don't want to expose them to cmd line
69 args.resetslew = True
71 # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # #
73 VERSION = "2.6"
75 if (args.part == "dra74x" or args.part == "dra75x"):
76         if (args.revision == "1.0" or args.revision == "1.1"):
77                 args.revision = "1.x"
78         XML_PATH = "XMLFiles/DRA75x_DRA74x"
79         PART = "DRA75x_DRA74x"
80         PCT_VERSION = "v1.0.16"
81 elif (args.part == "dra72x"):
82         if (args.revision == "1.1"):
83                 print "dra72x doesn't have silicon revision 1.1"
84                 exit()
85         XML_PATH = "XMLFiles/DRA72x"
86         PART = "DRA72x"
87         PCT_VERSION = "v1.0.7"
89 pad_data_xml   = XML_PATH + "/CTRL_MODULE_CORE.xml"
90 iod_data_xml   = XML_PATH + "/IODELAYCONFIG.xml"
91 model_data_xml = XML_PATH + "/model_" + PART + "_SR" + args.revision + "_" + PCT_VERSION + ".xml"
92 modehelp_file  = XML_PATH + "/guidelines_SR" + args.revision + ".txt"
94 pad_file = "ctrl-core.dump"
95 sel_file = "selected-modes.txt"
97 def trace(level, msg):
98         if (args.debug >= level):
99                 print(msg)
100 def verbose(msg):
101         trace(4, "DEBUG: " + msg)
102 def debug(msg, args=None):
103         trace(3, "DEBUG: " + msg)
104 def info(msg):
105         trace(2, "INFO: " + msg)
106 def warn(msg):
107         trace(1, "WARN: " + msg)
108 def error(msg):
109         trace(0, "ERR: " + msg)
111 if (args.interactive):
112         print "iodelay-autogen.py - Python script to generate the IOdelay data."
113         print "v" + VERSION + " using PCT version " + PCT_VERSION
114         print "Parsing PCT data from " + model_data_xml + "..."
115         print ""
117 # Read the XML file database for pad and delay registers
118 pad_xml = ET.parse(pad_data_xml).getroot()
119 iod_xml = ET.parse(iod_data_xml).getroot()
120 model_xml = ET.parse(model_data_xml).getroot()
122 # Functions to parse the input files and build data structures
123 def read_guidelines(fname):
124         modehelp = {}
125         pattern = re.compile('([^\t.]+\w)\t+(.+)')
126         f = open(fname)
127         for line in f.readlines():
128                 list = re.match(pattern, line)
129                 if ( list == None):
130                         continue
131                 mode = list.groups(0)[0]
132                 info = list.groups(0)[1]
133                 modehelp[mode] = info
134                 verbose("Guideline: Mode '%30s' => '%s'" % (mode, info))
135         return modehelp
137 def read_selmodes(fname):
138         sel = {}
139         pattern = re.compile('(\w+)\W*,\W*(\w*)')
140         f = open(fname)
141         for line in f.readlines():
142                 list = re.match(pattern, line)
143                 if ( list == None):
144                         continue
145                 module = list.groups(0)[0]
146                 mode = list.groups(0)[1]
147                 sel[module] = mode
148                 verbose("Input modes: Select '%s' => '%s'" % (mode, module))
149         return sel
151 def read_pad_dump(file):
152         regmap = {}
153         pattern = re.compile('.*(0x[0-9A-F]+).*(0x[0-9A-F]+).*')
154         f = open(file, 'r')
155         for line in f:
156                 list = re.match(pattern, line)
157                 if ( list == None):
158                         continue
159                 addr = int(list.groups(0)[0], 16)
160                 val = int(list.groups(0)[1], 16)
161                 verbose("XML pad-reg: Addr = %08x Value = %08x" % (addr, val))
162                 regmap[addr] = val
163         return regmap
164 # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # #
166 # Helper functions to parse XML nodes and get the desired data
167 # Hugely dependent on the XML format of the PCT files
168 # Uses XPath to search elements with queries and filters
169 # Parse the nodes to generate data in desired format
171 def xml_pad_get_name(offset):
172         padlist = pad_xml.findall("register[@offset='0x%X']" % offset)
173         if (len(padlist) == 0):
174                 return "Unknown"
175         else:
176                 return padlist[0].get("id")
178 def xml_pad_get_slew(offset):
179         padlist = pad_xml.findall("register[@offset='0x%X']" % offset)
180         if (len(padlist) == 0):
181                 return 0x0
182         else:
183                 bitlist = padlist[0].findall("bitfield[@begin='19']")
184                 if (len(bitlist) == 0):
185                         return 0x0
186                 else:
187                         return int(bitlist[0].get("resetval"), 16)
189 # For DRA72x SoC, for "ball compatibility" purpose, some signals have same muxmode.
190 # CTRL_CORE_ALT_SELECT_MUX register allows to select between one of the signals
191 # Its like a board mux has been added inside the SoC, except it uses same muxmode.
192 def resolve_group(muxmode_str):
193         mmlist = muxmode_str.split(" ")
194         mmlen = len(mmlist)
195         if (mmlen == 1):
196                 def_mode = mmlist[0]
197                 return mmlist[0]
198         elif (mmlen == 2):
199                 def_mode = mmlist[0]
200                 grp1_mode = mmlist[1]
201         elif (mmlen == 3):
202                 def_mode = mmlist[0]
203                 grp1_mode = mmlist[1]
204                 grp2_mode = mmlist[2]
205         else:
206                 error("Cannot resolve muxmode group for '%s'" % muxmode_str)
208         #HACK for now
209         warn("Not resolving muxmode %s, assuming default %s" % (muxmode_str, def_mode))
210         return def_mode
212 def xml_model_get_signal(offset, muxmode):
213         padlist = pad_xml.findall("register[@offset='0x%X']" % offset)
214         if (len(padlist) == 0):
215                 return "Unknown"
216         else:
217                 mux_field = padlist[0].findall("./bitfield[@end='0']")
218                 if (len(mux_field) == 0):
219                         return "Unknown"
220                 modes = mux_field[0].findall("./bitenum[@value='%d']" % muxmode)
221                 if (len(modes) == 0):
222                         return "Unknown"
223                 return resolve_group(modes[0].get("id"))
225 def xml_iodelay_get_reg(name):
226         delaylist = iod_xml.findall("register[@id='%s']" % name)
227         if (len(delaylist) == 0):
228                 return 0
229         else:
230                 offset = delaylist[0].get("offset")
231                 verbose("XML delay-reg: Name = %s Offset = %s" % (name, offset))
232                 return int(offset, 16)
234 def xml_get_virtual(mode):
235         vmodes = {}
236         signal = mode.findtext("signal")
237         for virt in mode.findall("virtualmode/mode"):
238                 virt_mode = virt.findtext("value")
239                 virt_name = virt.findtext("name")
240                 if (virt_name == "NA"):
241                         continue
242                 virt_mode = int(virt_mode)
243                 vmodes[virt_name] = virt_mode
244                 debug("    * VIRTUAL: %s [%s] => delaymode = %d" % (signal, virt_name, virt_mode))
245         return vmodes
247 def xml_get_manual(mode):
248         mmodes = {}
249         signal = mode.findtext("signal")
250         for man in mode.findall("manualmode"):
251                 regname = man.findtext("cfgreg/name")
252                 for sel in man.findall("cfgreg/mode"):
253                         adel = sel.findtext("adelay")
254                         gdel = sel.findtext("gdelay")
255                         man_name = sel.findtext("name")
256                         if (man_name == "NA"):
257                                 continue
258                         adel = int(adel)
259                         gdel = int(gdel)
260                         if (man_name not in mmodes.keys()):
261                                 mmodes[man_name] = []
262                         mmodes[man_name].append((regname, adel, gdel))
263                         debug("    * MANUAL: %s [%s] => delay[%s] = %d, %d" % (signal, man_name, regname, adel, gdel))
264         return mmodes
266 def xml_find_delaymodes(pad_name, muxmode):
267         padlist = model_xml.findall("padDB/clockNode/type/pad")
268         for pad in padlist:
269                 if (pad_name == pad.findtext("confregisters/regbit/register")):
270                         muxmodes = pad.findall("muxmode")
271                         break
272         if not muxmodes:
273                 return None
274         for mode in muxmodes:
275                 if ("%d" % muxmode == mode.findtext("mode")):
276                         virt = xml_get_virtual(mode)
277                         man = xml_get_manual(mode)
278                         return (virt, man)
279         return None
281 def xml_check_correctness(modehelp):
283         print "###########################################"
284         print "XML correctness checks:"
285         padcore_list = []
286         padmodel_list = []
287         modes = {}
289         # Find all the pads in core XML
290         pad_list = pad_xml.findall("register")
291         for i in pad_list:
292                 name = i.get("id")
293                 if (re.match("CTRL_CORE_PAD_.*", name) == None):
294                         continue
295                 padcore_list.append(name)
296         print ">> Total pads defined in core XML = %d" % len(padcore_list)
298         # Find all the pads in model XML
299         pad_list = model_xml.findall("padDB/clockNode/type/pad/confregisters/regbit")
300         for i in pad_list:
301                 name = i.findtext("register")
302                 padmodel_list.append(name)
303         print ">> Total pads defined in model XML = %d" % len(padmodel_list)
305         # Find all the manual modes
306         manmode_list = model_xml.findall("padDB/clockNode/type/pad/muxmode/manualmode/cfgreg/mode")
307         for i in manmode_list:
308                 man_name = i.findtext("name")
309                 modes[man_name] = "manual"
310         # Find all the virtual modes
311         virtmode_list = model_xml.findall("padDB/clockNode/type/pad/muxmode/virtualmode/mode")
312         for i in virtmode_list:
313                 virt_name = i.findtext("name")
314                 modes[virt_name] = "virtual"
315         print ">> Total delaymodes defined in model XML = %d" % len(modes)
317         # Print out all the errors found in the tests
318         print "== Pads defined in core XML but not in model XML =="
319         for i in padcore_list:
320                 if (i not in padmodel_list):
321                         print "\t%s" % i
322         print "== Pads defined in model XML but not in core XML =="
323         for i in padmodel_list:
324                 if (i not in padcore_list):
325                         print "\t%s" % i
327         # Check if description for each mode is available
328         print "== Delaymodes missing description in the guidelines.txt =="
329         for i in modes:
330                 if (i not in modehelp):
331                         print "\t%s" % i
333         # Check if description for unknown mode is documented
334         print "== Delaymodes unused from guidelines.txt =="
335         for i in modehelp:
336                 if (i not in modes):
337                         print "\t%s" % i
339         print "###########################################"
341 # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # #
343 # Decision point of the script
344 # For each pad/pin, decide what delay method is used
345 # Lookup in the selection file or ask user with a menu
346 def select_mode(pad, pin, module, virt, man, modehelp, sel):
347         modelist = []
348         for modename in virt.keys():
349                 modelist.append(modename)
351         for modename in man.keys():
352                 modelist.append(modename)
354         if (len(modelist) == 0):
355                 return "LEGACY"
357         if (module in sel.keys()):
358                 mode = sel[module]
359                 if (mode == "SKIP" or mode == "LEGACY" or mode in modelist):
360                         return mode
361                 else:
362                         error("Invalid delaymode '%s' for module '%s'" % (mode, module))
364         if (args.interactive == 0):
365                 warn("No delay modes for %s found, skipping" % module)
366                 mode = "SKIP"
367                 return mode
369         # Display the menu and ask user to select the 'right' mode
370         while True:
371                 print ""
372                 print "MENU: Select delay mode for %s -> %s" % (pad, pin)
373                 i = 0
374                 print "MENU: %d: %s \t\t\t%s" % (i, "SKIP", "Skips this module for now")
375                 i = 1
376                 print "MENU: %d: %s \t\t%s" % (i, "LEGACY", "No external delay config (No virtual/manual needed)")
377                 for mode in modelist:
378                         i += 1
379                         if (mode in modehelp):
380                                 helptext = modehelp[mode]
381                         else:
382                                 helptext = "Unknown"
383                         print "MENU: %d: %s \t\t%s" % (i, mode, helptext)
384                 try:
385                         choice = int(raw_input("Select delay mode #> "))
386                         if (choice == 0):
387                                 mode = "SKIP"
388                                 break
389                         elif (choice == 1):
390                                 mode = "LEGACY"
391                                 break
392                         elif (choice >=2 and choice <= len(modelist) + 1):
393                                 mode = modelist[choice - 2]
394                                 break
395                         print "ERROR: Invalid choice"
396                 except ValueError:
397                         print "ERROR: Invalid choice"
398         print "MENU: Selected mode is %s" % mode
399         print ""
401         return mode
402 # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # #
404 # Pad read using GPIO - Specific to linux only
405 # As each pad is muxed with a SoC gpio (for most of the pads)
406 # It's possible to read the pad data using gpio datain registers
407 # Change pad register to enable input path and export sysfs
408 # Use sysfs to read the status of GPIO and print in a loop
409 def pad_dump_gpio(padconf, per_padconf):
410         gpio_data_addrs = (0, 0x4ae10138, 0x48055138, 0x48057138, 0x48059138, 0x4805b138, 0x4805d138, 0x48051138, 0x48053138)
411         module = args.module
413         # script header
414         gen_header = "###########################################\n" + \
415                      "# Read %s signals using GPIO sysfs\n" % module + \
416                      "###########################################\n\n"
417         gen_data = "%s_data=(\n" % module
419         for i in padconf:
420                 (pad_name, pin_name, addr, val, mode, delayinfo) = i
422                 offset = addr - 0x4a002000
423                 gpio_name = xml_model_get_signal(offset, 14)
424                 matchlist = re.match("GPIO(.)_(.*)", gpio_name)
425                 if (matchlist == None):
426                         error("No GPIO for pad %s - cannot read from script" % pad_name)
427                         continue
429                 inst = int(matchlist.groups(0)[0])
430                 bit = int(matchlist.groups(0)[1])
431                 gpio_addr = gpio_data_addrs[inst]
432                 ngpio = (inst - 1) * 32 + bit
433                 pin_short = re.match(".+_(.*)", pin_name).groups(0)[0]
435                 gen_data += "\t%s:0x%x:%s:%d:0x%x:%d\n" % (pin_short, addr, gpio_name, ngpio, gpio_addr, bit)
437         gen_data += ")\n\n"
439         # Main script to probe the signal
440         gen_main = "echo; echo Probing %s signals\n\n" % module + \
441                    "for data in ${%s_data[@]}\n" % module + \
442                    "do\n" + \
443                    "    pin=`echo $data | cut -d ':' -f1`\n" + \
444                    "    pad=`echo $data | cut -d ':' -f2`\n" + \
445                    "    ngpio=`echo $data | cut -d ':' -f4`\n" + \
446                    "    echo $ngpio > /sys/class/gpio/export 2>/dev/null\n" + \
447                    "    omapconf set bit $pad 18 1>/dev/null 2>/dev/null\n" + \
448                    "    printf \"%8s\" $pin\n" + \
449                    "done\n" + \
450                    "echo\n\n"
452         gen_main += "while true;\n" + \
453                     "do\n" + \
454                     "    for data in ${%s_data[@]}\n" % module + \
455                     "    do\n" + \
456                     "#       pin=`echo $data | cut -d ':' -f1`\n" + \
457                     "#        pad=`echo $data | cut -d ':' -f2`\n" + \
458                     "#       gpio=`echo $data | cut -d ':' -f3`\n" + \
459                     "        ngpio=`echo $data | cut -d ':' -f4`\n" + \
460                     "#       addr=`echo $data | cut -d ':' -f5`\n" + \
461                     "#       bit=`echo $data | cut -d ':' -f6`\n" + \
462                     "        val=`cat /sys/class/gpio/gpio$ngpio/value`\n" + \
463                     "        printf %8d $val \n" + \
464                     "    done\n" + \
465                     "    echo\n" + \
466                     "done\n\n"
468         gen_footer = "###########################################\n"
470         # Generate the shell script
471         gen_script = gen_header + gen_data + gen_main + gen_footer
472         filename = ("./%s-probe.sh" % module).lower()
473         print "Generating '%s' script..." % filename
474         gen_file = open(filename, "w+")
475         gen_file.write(gen_script)
477 # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # #
479 # Generate the final pad and delay data in the required format
480 def format_pad_regs(padconf, per_padconf):
481         print "######## Pad data output ########"
482         if (args.format == "uboot"):
483                 uboot_format_pad_regs(padconf, per_padconf)
484         elif (args.format == "linux"):
485                 linux_format_pad_regs(padconf, per_padconf)
486         elif (args.format == "bios"):
487                 bios_format_pad_regs(padconf, per_padconf)
488         else:
489                 error("Format %s not suppported" % args.format)
491 def format_delay_regs(delayconf, per_delayconf):
492         print "######## Delay data output ########"
493         if (args.format == "uboot"):
494                 uboot_format_delay_regs(delayconf, per_delayconf)
495         elif (args.format == "linux"):
496                 linux_format_delay_regs(delayconf, per_delayconf)
497         elif (args.format == "bios"):
498                 bios_format_delay_regs(delayconf, per_delayconf)
499         else:
500                 error("Format %s not suppported" % args.format)
502 def get_pin_info(val):
503         slew_fast = (val >> 19) & 0x1
504         inp_en = (val >> 18) & 0x1
505         pulltype = (val >> 17) & 0x1
506         pull_dis = (val >> 16) & 0x1
507         pin = "PIN"
508         if (inp_en):
509                 pin += "_INPUT"
510         else:
511                 pin += "_OUTPUT"
512         if (pull_dis == 0):
513                 if (pulltype):
514                         pin += "_PULLUP"
515                 else:
516                         pin += "_PULLDOWN"
517         if (slew_fast):
518                 pin += " | SLEWCONTROL"
519         return pin
521 # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # #
523 # Generate output in u-boot format
524 def uboot_format_pad_regs(padconf, per_padconf):
525         print "\nconst struct pad_conf_entry dra74x_core_padconf_array[] = {"
526         for i in padconf:
527                 (pad_name, pin_name, addr, val, mode, delayinfo) = i
529                 muxmode = val & 0xf
530                 (method, data) = delayinfo
531                 if (method == "LEGACY"):
532                         extramode = ""
533                 elif (method == "VIRTUAL"):
534                         delaymode = data
535                         extramode = " | VIRTUAL_MODE%d" % delaymode
536                 elif (method == "MANUAL"):
537                         extramode = " | MANUAL_MODE"
538                 else:
539                         error("Invalid delay method %s" % method)
541                 pin_info = get_pin_info(val) + extramode
542                 pad_short = re.sub("CTRL_CORE_PAD_", "", pad_name)
543                 comment = (pad_short + "." + pin_name).lower()
545                 print "\t{ %s, (M%d | %s) },\t/* %s */" % (pad_short, muxmode, pin_info, comment)
546         print "};\n"
548 def uboot_format_delay_regs(delayconf, per_delayconf):
549         manual_del = []
550         for i in delayconf:
551                 (pad_name, pin_name, regname, del_offset, man_name, adel, gdel) = i
553                 entry = (del_offset, adel, gdel, regname, pin_name, man_name)
554                 manual_del.append(entry)
556         es_rev = args.revision.replace('.', '_')
557         print "\nconst struct iodelay_cfg_entry dra742_es" + es_rev + "_iodelay_cfg_array[] = {"
558         for entry in sorted(manual_del):
559                 print "\t{ 0x%04X, %5d, %5d },\t/* %s : %s - %s */" % entry
560         print "};\n"
562 # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # #
564 # Generate output in linux format
565 def linux_format_pad_regs(padconf, per_padconf):
566         print "&dra7_pmx_core {"
567         for per in per_padconf:
569                 if (re.match("MMC.*", per) == None):
570                         warn("Only MMC padconf is recommended in kernel")
572                 # Get the mode from the first entry
573                 (pad_name, pin_name, addr, val, mode, delayinfo) = per_padconf[per][0]
575                 dtsnode = ("%s_pins_%s" % (per, mode)).lower()
576                 print ""
577                 print "\t%s: %s {" % (dtsnode, dtsnode)
578                 print "\t\tpinctrl-single,pins = <"
579                 for i in per_padconf[per]:
580                         (pad_name, pin_name, addr, val, mode, delayinfo) = i
582                         muxmode = val & 0xf
583                         (method, data) = delayinfo
584                         if (method == "LEGACY"):
585                                 extramode = ""
586                         elif (method == "VIRTUAL"):
587                                 delaymode = data
588                                 extramode = " | MUX_VIRTUAL_MODE%d" % delaymode
589                         elif (method == "MANUAL"):
590                                 extramode = " | MANUAL_MODE"
591                         else:
592                                 warn("Invalid method %s" % method)
594                         pin_info = get_pin_info(val) + extramode
595                         pad_short = re.sub("CTRL_CORE_PAD_", "", pad_name)
596                         offset = addr - 0x4a003400
597                         comment = (pad_short + "." + pin_name).lower()
599                         print "\t\t\t0x%03X\t(%s | MUX_MODE%d)\t/* %s */" % (offset, pin_info, muxmode, comment)
600                 print "\t\t>;"
601                 print "\t};"
602         print "};\n"
605 def linux_format_delay_regs(delayconf, per_delayconf):
606         print "&dra7_iodelay_core {"
607         for per in per_delayconf.keys():
609                 if (re.match("MMC.*", per) == None):
610                         warn("Only MMC delayconf is recommended in kernel")
612                 # Get the mode from the first entry
613                 (pad_name, pin_name, regname, del_offset, mode, adel, gdel) = per_delayconf[per][0]
615                 dtsnode = ("%s_iodelay_%s_conf" % (per, mode)).lower()
616                 print "\t%s: %s {" % (dtsnode, dtsnode)
617                 print "\t\tpinctrl-single,pins = <"
618                 for i in per_delayconf[per]:
619                         (pad_name, pin_name, regname, del_offset, mode, adel, gdel) = i
621                         print "\t\t\t0x%03X (A_DELAY(%d) | G_DELAY(%d))\t/* %s */" % (del_offset, adel, gdel, regname)
622                 print "\t\t>;"
623                 print "\t};"
624         print "};\n"
626 # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # #
628 # Generate output in bios format
629 def bios_format_pad_regs(padconf, per_padconf):
630         for i in padconf:
631                 (pad_name, pin_name, addr, val, mode, delayinfo) = i
633                 delaylist = []
634                 (method, data) = delayinfo
635                 if (method == "VIRTUAL"):
636                         virt_mode = data
637                         val = val | ( virt_mode<< 4)
638                         val = val | (1 << 8)
639                 elif (method == "MANUAL"):
640                         delaylist = data
641                         val = val | (1 << 8)
643                 offset = addr - 0x4a003400
644                 out_delreg = out_adel = out_gdel = 0
645                 in_delreg  = in_adel  = in_gdel  = 0
646                 oen_delreg = oen_adel = oen_gdel = 0
648                 for j in delaylist:
649                         (regname, adel, gdel) = j
650                         if (re.match(".*_IN", regname) != None):
651                                 in_delreg = xml_iodelay_get_reg(regname)
652                                 in_adel = adel
653                                 in_gdel = gdel
654                         elif (re.match(".*_OEN", regname) != None):
655                                 oen_delreg = xml_iodelay_get_reg(regname)
656                                 oen_adel = adel
657                                 oen_gdel = gdel
658                         elif (re.match(".*_OUT", regname) != None):
659                                 out_delreg = xml_iodelay_get_reg(regname)
660                                 out_adel = adel
661                                 out_gdel = gdel
662                 indel  = "{ 0x%04X, %4d, %4d , 0}" % (in_delreg,  in_adel,  in_gdel)
663                 oendel = "{ 0x%04X, %4d, %4d , 0}" % (oen_delreg, oen_adel, oen_gdel)
664                 outdel = "{ 0x%04X, %4d, %4d , 0}" % (out_delreg, out_adel, out_gdel)
665                 pin_info = get_pin_info(val)
666                 print "\t/* %s -> %s (%s) %s delaymode */" % (pad_name, pin_name, pin_info, method)
667                 print "\t{ 0x%03X, 0x%08X, %s, %s, %s }" % (offset, val, indel, oendel, outdel)
669 def bios_format_delay_regs(delayconf, per_delayconf):
670         debug("Manual delays are not configured separately")
671         debug("Delays are configured as part of the padconf step only")
673 # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # #
675 # Main execution starts here
676 # * Parse all the XML files - Get the pad data and IOdelay data
677 # * Iterate over the pad register dumps
678 # * For each pad, find out the muxmode being used and the pad direction, etc
679 # * For the muxmode being used, find out available virtual/modes
680 #   - Dump the virtual/manual modes available (based on options)
681 #   - Build up the gpio script to read the pad data using GPIO module
682 # * Select the correct mode to be used
683 #   - Check if the mode is described for the peripheral module, (from selected-modes.txt)
684 #   - Otherwise ask the user (with a menu) to decide the delaymode
685 #     => Update the selection for the whole of the peripheral module
686 #   - Worst case, skip the delaymode for this pad
687 # * Build the pad and delay register information
688 # * Create the dump for pad and delay data in linux/u-boot format
689 # * Dump the delaymode selection for each peripheral
690 # * Dump the GPIO script for each peripheral (all pads grouped together)
693 # Read all the input files and parse the required info
694 modehelp = read_guidelines(modehelp_file)
695 sel = read_selmodes(sel_file)
696 regmap = read_pad_dump(pad_file)
697 reglist = regmap.keys()
699 # List of all the pads being configured
700 padconf = []
701 # List of all the delay registers being configured (for manual mode)
702 delayconf = []
703 # Dictionary of pads grouped by peripheral/module
704 per_padconf = {}
705 # Dictionary of delay registers grouped by peripheral/module
706 per_delayconf = {}
708 if(args.check_xml):
709         xml_check_correctness(modehelp)
710         exit()
712 # Start iterating over each pad
713 for i in range(0, 260):
714         # Find out the muxmode and pad direction, etc
715         addr = 0x4a003400 + i * 4
716         offset = 0x1400 + i * 4
717         dts_offset = offset - 0x1400
719         if (addr not in reglist):
720                 warn("Register dump for pad 0x%X not found" % addr)
721                 continue
722         val = regmap[addr]
723         muxmode = val & 0xf
725         # Find out the pin based on the muxmode
726         pad_name = xml_pad_get_name(offset)
727         pin_name = xml_model_get_signal(offset, muxmode)
728         if (pad_name == "Unknown" or pin_name == "Unknown"):
729                 warn("Cannot find out Pad/Pin name for PAD address 0x%X (%s[%s] = %s)" \
730                 % (addr, pad_name, muxmode, pin_name))
731                 continue
732         if (pin_name == "DRIVER"):
733                 continue
735         # Find out if the delaymode for this module is already selected
736         match = re.match("([^_]+)_.*", pin_name)
737         if (match):
738                 module = match.groups(0)[0]
739         else:
740                 module = pin_name
742         if (args.module != "" and re.match("%s" % args.module, module) == None):
743                 continue
745         # It is recommended to keep the reset value of the slewcontrol bit
746         # Find out the reset value from XML and update if required
747         if (args.resetslew):
748                 val |= (xml_pad_get_slew(offset) & 0x1) << 19
750         debug("\nPAD: %s: Addr= 0x%08X Value = 0x%08X \"%s\"" \
751                 % (pad_name, addr, val, pin_name))
753         # Find out all the possible virtual, manual modes fot the specific pad -> pin combination
754         (virt, man) = xml_find_delaymodes(pad_name, muxmode)
756         if (args.gpio == True):
757                 mode = "LEGACY"
758         else:
759                 # Need to select one out of allowed modes
760                 mode = select_mode(pad_name, pin_name, module, virt, man, modehelp, sel)
762         # Remember the selection for that module, for later reuse
763         if (args.strict == False and module not in sel.keys()):
764                 sel[module] = mode
766         if (mode == "SKIP"):
767                 continue
768         elif (mode == "LEGACY"):
769                 delayinfo = ("LEGACY", "")
770         elif (mode in virt):
771                 delayinfo = ("VIRTUAL", virt[mode])
772         elif (mode in man):
773                 delayinfo = ("MANUAL", man[mode])
774         else:
775                 error("Unknown mode '%s' selected" % mode)
776                 continue
778         debug("  => Using mode %s" % mode)
779         paddata = (pad_name, pin_name, addr, val, mode, delayinfo)
780         if (module not in per_padconf.keys()):
781                 per_padconf[module] = []
782         padconf.append(paddata)
783         per_padconf[module].append(paddata)
785         if(mode not in man):
786                 continue
788         # Add the delay data if using manual mode
789         for regval in man[mode]:
790                 (regname, adel, gdel) = regval
791                 del_offset = xml_iodelay_get_reg(regname)
792                 if (del_offset == 0):
793                         error("Can't find delay offset of register %s" % regname)
794                         break
795                 debug("  => Manual delay[%s] = (%d, %d)" % (regname, adel, gdel))
796                 delaydata = (pad_name, pin_name, regname, del_offset, mode, adel, gdel)
797                 if (module not in per_delayconf.keys()):
798                         per_delayconf[module] = []
799                 delayconf.append(delaydata)
800                 per_delayconf[module].append(delaydata)
802 if(args.gpio == True):
803         pad_dump_gpio(padconf, per_padconf)
804         exit()
806 format_pad_regs(padconf, per_padconf)
807 format_delay_regs(delayconf, per_delayconf)
809 if (args.interactive):
810         # Summary of the generated data
811         print ""
812         print "Total PAD registers: %d" % len(padconf)
813         print "Total DELAY registers: %d" % len(delayconf)
814         print ""
815         # Dump the final selection for reuse
816         print "Selected modes for each peripheral module\n"
817         for group in sel:
818                 print "%s,\t%s" % (group, sel[group])
819         print ""
820 # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # #