script: Add support for all DRA7xx parts
[glsdk/iodelay-config.git] / iodelay-autogen.py
1 #!/usr/bin/python
2 # Python script to automatically generate the IO pad and delay data
3 # Author:- Nikhil Devshatwar
5 # This script uses regdump of the pad registers to figure out the muxmodes
6 # Based on the pad and muxmode, it find out all possible virtual/manual modes
7 # by referring to the PCT XML model. Using the, selection file, script
8 # decides which modes to be selected. Finally it dumps the required array entries
10 # This script depends on following files:-
11 # * XML data files      - Shipped with the DRA7xx PCT tool
12 # * Pad register dump   - Generate using omapconf dump 0x4a003400 0x4a00380c
13 # * selection file      - List of selected virtual/manual modes to be used
15 import xml.etree.ElementTree as ET
16 import re
17 import argparse
19 # Handle the command line arguments
20 parser = argparse.ArgumentParser(prog='iodelay-autogen.py',
21         description='Python script to generate the IOdelay data.\n' \
22                 'This script refers to the XML data and automatically generates\n' \
23                 'PAD and DELAY data for the same use case.\n' \
24                 'Note that only the PADs which are used in the dump are configured.',
25         epilog='Generate the pad and delay data using pad register dumps. For this,\n' \
26                 'Run omapconf dump 0x4a003400 0x4a00380c and save the output')
28 parser.add_argument('-d', '--debug', dest='debug',
29         action='store', type=int, choices=[0, 1, 2], default=0,
30         help='set the debug level')
32 parser.add_argument('-i', '--interactive', dest='interactive',
33         action='store', type=int, choices=[0, 1], default=1,
34         help='run interactively with menus for resolving conflicts')
36 parser.add_argument('-f', '--format', dest='format',
37         action='store', type=str, choices=["linux", "uboot", "bios"], default="uboot",
38         help='select the output format to be used')
40 parser.add_argument('-r', '--revision', dest='revision',
41         action='store', type=str, choices=["1.0", "1.1", "2.0"], default="1.1",
42         help='select the silicon revision')
44 parser.add_argument('-p', '--part', dest='part',
45         action='store', type=str, choices=["dra74x", "dra75x", "dra72x"], default="dra74x",
46         help='select the device part')
48 parser.add_argument('-m', '--module', dest='module',
49         action='store', type=str, default="",
50         help='generate only for this module')
52 parser.add_argument('-s', '--strict', dest='strict',
53         action='store_true',
54         help='strict mode - ask for each pad of the group, do not save selection.\n' \
55                 'For some peripherals, same delaymode cannot be used for all the pads.\n' \
56                 'Use this mode to select different modes for each pad')
58 parser.add_argument('-g', '--gpio', dest='gpio',
59         action='store_true',
60         help='generate script to read pad data from GPIO')
62 parser.add_argument('-c', '--check', dest='check_xml',
63         action='store_true',
64         help='check consistency of the XML files and other data')
66 args = parser.parse_args()
67 # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # #
69 VERSION = "2.4"
71 if (args.part == "dra74x" or args.part == "dra75x"):
72         XML_PATH = "XMLFiles/DRA75x_DRA74x"
73         PART = "DRA75x_DRA74x"
74         PCT_VERSION = "v1.0.9"
75 elif (args.part == "dra72x"):
76         XML_PATH = "XMLFiles/DRA72x"
77         PART = "DRA72x"
78         PCT_VERSION = "v1.0.5"
80 pad_data_xml   = XML_PATH + "/CTRL_MODULE_CORE.xml"
81 iod_data_xml   = XML_PATH + "/IODELAYCONFIG.xml"
82 model_data_xml = XML_PATH + "/model_" + PART + "_SR" + args.revision + "_" + PCT_VERSION + ".xml"
84 modehelp_file = "guidelines.txt"
85 pad_file = "ctrl-core.dump"
86 sel_file = "selected-modes.txt"
88 print "iodelay-autogen.py - Python script to generate the IOdelay data."
89 print "v" + VERSION + " using PCT version " + PCT_VERSION
90 print ""
92 # Read the XML file database for pad and delay registers
93 if (args.debug >= 1):
94         print ("Parsing PCT data from " + model_data_xml)
95 pad_xml = ET.parse(pad_data_xml).getroot()
96 iod_xml = ET.parse(iod_data_xml).getroot()
97 model_xml = ET.parse(model_data_xml).getroot()
99 # Functions to parse the input files and build data structures
100 def read_guidelines(fname):
101         modehelp = {}
102         pattern = re.compile('(.+\w)\t+(.+)')
103         f = open(fname)
104         for line in f.readlines():
105                 list = re.match(pattern, line)
106                 if ( list == None):
107                         continue
108                 mode = list.groups(0)[0]
109                 info = list.groups(0)[1]
110                 modehelp[mode] = info
111                 if (args.debug >= 2):
112                         print "Help: Mode '%s' is used for '%s'" % (mode, info)
113         return modehelp
115 def read_selmodes(fname):
116         sel = {}
117         pattern = re.compile('(\w+)\W*,\W*(\w*)')
118         f = open(fname)
119         for line in f.readlines():
120                 list = re.match(pattern, line)
121                 if ( list == None):
122                         continue
123                 module = list.groups(0)[0]
124                 mode = list.groups(0)[1]
125                 sel[module] = mode
126                 if (args.debug >= 2):
127                         print "INFO: Select '%s' for '%s'" % (mode, module)
128         return sel
130 def read_pad_dump(file):
131         regmap = {}
132         pattern = re.compile('.*(0x[0-9A-F]+).*(0x[0-9A-F]+).*')
133         f = open(file, 'r')
134         for line in f:
135                 list = re.match(pattern, line)
136                 if ( list == None):
137                         continue
138                 addr = int(list.groups(0)[0], 16)
139                 val = int(list.groups(0)[1], 16)
140                 #print "PADXML: Addr = %08x Value = %08x" % (addr, val)
141                 regmap[addr] = val
142         return regmap
143 # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # #
145 # Helper functions to parse XML nodes and get the desired data
146 # Hugely dependent on the XML format of the PCT files
147 # Uses XPath to search elements with queries and filters
148 # Parse the nodes to generate data in desired format
150 def xml_pad_get_name(offset):
151         padlist = pad_xml.findall("register[@offset='0x%X']" % offset)
152         if (len(padlist) == 0):
153                 return "Unknown"
154         else:
155                 return padlist[0].get("id")
157 def xml_pad_get_pin(offset, muxmode):
158         padlist = pad_xml.findall("register[@offset='0x%X']" % offset)
159         if (len(padlist) == 0):
160                 return "Unknown"
161         else:
162                 mux_field = padlist[0].findall("./bitfield[@end='0']")
163                 if (len(mux_field) == 0):
164                         return "Unknown"
165                 modes = mux_field[0].findall("./bitenum[@value='%d']" % muxmode)
166                 if (len(modes) == 0):
167                         return "Unknown"
168                 return modes[0].get("id")
170 def xml_iodelay_get_reg(name):
171         delaylist = iod_xml.findall("register[@id='%s']" % name)
172         if (len(delaylist) == 0):
173                 return 0
174         else:
175                 offset = delaylist[0].get("offset")
176                 #print "IOD: Name = %s Offset = %s" % (del_reg, offset)
177                 return int(offset, 16)
179 def xml_get_virtual(mode):
180         vmodes = {}
181         signal = mode.findtext("signal")
182         for virt in mode.findall("virtualmode/mode"):
183                 virt_mode = virt.findtext("value")
184                 virt_name = virt.findtext("name")
185                 if (virt_name == "NA"):
186                         continue
187                 virt_mode = int(virt_mode)
188                 vmodes[virt_name] = virt_mode
189                 if (args.debug >= 1):
190                         print ("    * VIRTUAL: %s [%s] => delaymode = %d" % (signal, virt_name, virt_mode))
191         return vmodes
193 def xml_get_manual(mode):
194         mmodes = {}
195         signal = mode.findtext("signal")
196         for man in mode.findall("manualmode"):
197                 regname = man.findtext("cfgreg/name")
198                 for sel in man.findall("cfgreg/mode"):
199                         adel = sel.findtext("adelay")
200                         gdel = sel.findtext("gdelay")
201                         man_name = sel.findtext("name")
202                         if (man_name == "NA"):
203                                 continue
204                         adel = int(adel)
205                         gdel = int(gdel)
206                         if (man_name not in mmodes.keys()):
207                                 mmodes[man_name] = []
208                         mmodes[man_name].append((regname, adel, gdel))
209                         if (args.debug >= 1):
210                                 print ("    * MANUAL: %s [%s] => delay[%s] = %d, %d" % (signal, man_name, regname, adel, gdel))
211         return mmodes
213 def xml_find_delaymodes(pad_name, muxmode):
214         padlist = model_xml.findall("padDB/clockNode/type/pad")
215         for pad in padlist:
216                 if (pad_name == pad.findtext("confregisters/regbit/register")):
217                         muxmodes = pad.findall("muxmode")
218                         break
219         if not muxmodes:
220                 return None
221         for mode in muxmodes:
222                 if ("%d" % muxmode == mode.findtext("mode")):
223                         virt = xml_get_virtual(mode)
224                         man = xml_get_manual(mode)
225                         return (virt, man)
226         return None
228 def xml_check_correctness(modehelp):
229         if(args.check_xml == False):
230                 return
232         print "###########################################"
233         print "XML correctness checks:"
234         padcore_list = []
235         padmodel_list = []
236         modes = {}
238         # Fint all the pads in core XML
239         pad_list = pad_xml.findall("register")
240         for i in pad_list:
241                 name = i.get("id")
242                 if (re.match("CTRL_CORE_PAD_.*", name) == None):
243                         continue
244                 padcore_list.append(name)
245         print ">> Total pads defined in core XML = %d" % len(padcore_list)
247         # Find all the pads in model XML
248         pad_list = model_xml.findall("padDB/clockNode/type/pad/confregisters/regbit")
249         for i in pad_list:
250                 name = i.findtext("register")
251                 padmodel_list.append(name)
252         print ">> Total pads defined in model XML = %d" % len(padmodel_list)
254         # Find all the manual modes
255         manmode_list = model_xml.findall("padDB/clockNode/type/pad/muxmode/manualmode/cfgreg/mode")
256         for i in manmode_list:
257                 man_name = i.findtext("name")
258                 modes[man_name] = "manual"
259         # Find all the virtual modes
260         virtmode_list = model_xml.findall("padDB/clockNode/type/pad/muxmode/virtualmode/mode")
261         for i in virtmode_list:
262                 virt_name = i.findtext("name")
263                 modes[virt_name] = "virtual"
264         print ">> Total delaymodes defined in model XML = %d" % len(modes)
266         # Print out all the errors found in the tests
267         print "== Pads defined in core XML but not in model XML =="
268         for i in padcore_list:
269                 if (i not in padmodel_list):
270                         print "\t%s" % i
271         print "== Pads defined in model XML but not in core XML =="
272         for i in padmodel_list:
273                 if (i not in padcore_list):
274                         print "\t%s" % i
276         # Check if description for each mode is available
277         print "== Delaymodes missing description in the guidelines.txt =="
278         for i in modes:
279                 if (i not in modehelp):
280                         print "\t%s" % i
282         print "###########################################"
284 # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # #
286 # Decision point of the script
287 # For each pad/pin, decide what delay method is used
288 # Lookup in the selection file or ask user with a menu
289 def select_mode(pad, pin, module, virt, man, modehelp, sel):
290         modelist = []
291         for modename in virt.keys():
292                 modelist.append(modename)
294         for modename in man.keys():
295                 modelist.append(modename)
297         if (len(modelist) == 0):
298                 return "LEGACY"
300         if (module in sel.keys()):
301                 mode = sel[module]
302                 if (mode == "SKIP" or mode in modelist):
303                         return mode
304                 else:
305                         print("ERR: Invalid delaymode '%s' for module '%s'" % (mode, module))
307         if (args.interactive == 0):
308                 print "WARN: No delay modes for %s found, skipping" % module
309                 mode = "SKIP"
310                 sel[module] = mode
311                 return mode
313         # Display the menu and ask user to select the 'right' mode
314         while True:
315                 print ""
316                 print "MENU: Select delay mode for %s -> %s" % (pad, pin)
317                 i = 0
318                 print "MENU: %d: %s \t\t\t%s" % (i, "SKIP", "Skips this module for now")
319                 for mode in modelist:
320                         i += 1
321                         if (mode in modehelp):
322                                 helptext = modehelp[mode]
323                         else:
324                                 helptext = "Unknown"
325                         print "MENU: %d: %s \t\t%s" % (i, mode, helptext)
326                 try:
327                         choice = int(raw_input("Select delay mode #> "))
328                         if (choice == 0):
329                                 mode = "SKIP"
330                                 break
331                         elif (choice >=0 and choice <= len(modelist)):
332                                 mode = modelist[choice - 1]
333                                 break
334                         print "ERROR: Invalid choice"
335                 except ValueError:
336                         print "ERROR: Invalid choice"
337         print "MENU: Selected mode is %s" % mode
338         print ""
340         return mode
341 # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # #
343 # Pad read using GPIO - Specific to linux only
344 # As each pad is muxed with a SoC gpio (for most of the pads)
345 # It's possible to read the pad data using gpio datain registers
346 # Dump the linux commands to read the gpio registers and read the pad data
347 def pad_dump_gpio(padconf, per_padconf):
348         if(args.gpio == False):
349                 return
351         print "# Read pad signals using GPIO DATA-IN registers"
352         print "# Works only for the input signals"
353         gpio_data_addrs = (0, 0x4ae10138, 0x48055138, 0x48057138, 0x48059138, 0x4805b138, 0x4805d138, 0x48051138, 0x48053138)
354         for i in padconf:
355                 (pad_name, pin_name, addr, val, delayinfo) = i
357                 offset = addr - 0x4a002000
358                 gpio_name = xml_pad_get_pin(offset, 14)
359                 matchlist = re.match("GPIO(.)_(.*)", gpio_name)
360                 if (matchlist == None):
361                         print "ERR: No GPIO for pad %s" % pad_name
362                         continue
364                 inst = int(matchlist.groups(0)[0])
365                 bit = int(matchlist.groups(0)[1])
366                 gpio_addr = gpio_data_addrs[inst]
368                 print "#Read GPIO%d_%d to sample %s" % (inst, bit, pin_name)
369                 print " echo %d > /sys/class/gpio/export 2>/dev/null;" % ((inst - 1) * 32)
370                 print " val=`omapconf read 0x%x 2>&1 | grep -v \"support\"`;" % gpio_addr
371                 print " status=$((0x$val >> %d & 0x1));" % bit
372                 print " echo -e \"%s (%s)\t = $status\";" % (pin_name, gpio_name)
373                 print ""
374         print ""
375 # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # #
377 # Generate the final pad and delay data in the required format
378 def format_pad_regs(padconf, per_padconf):
379         print "###########################################"
380         print "Pad data output (with the delay modes)"
381         print "###########################################"
382         if (args.format == "uboot"):
383                 uboot_format_pad_regs(padconf, per_padconf)
384         elif (args.format == "linux"):
385                 linux_format_pad_regs(padconf, per_padconf)
386         elif (args.format == "bios"):
387                 bios_format_pad_regs(padconf, per_padconf)
388         else:
389                 print "ERR: Format %s not suppported" % args.format
391 def format_delay_regs(delayconf, per_delayconf):
392         print "#########################################"
393         print "Delay data output (for manual modes)"
394         print "#########################################"
395         if (args.format == "uboot"):
396                 uboot_format_delay_regs(delayconf, per_delayconf)
397         elif (args.format == "linux"):
398                 linux_format_delay_regs(delayconf, per_delayconf)
399         elif (args.format == "bios"):
400                 bios_format_delay_regs(delayconf, per_delayconf)
401         else:
402                 print "ERR: Format %s not suppported" % args.format
404 def get_pin_info(val):
405         inp_en = (val >> 18) & 0x1
406         pulltype = (val >> 17) & 0x1
407         pull_dis = (val >> 16) & 0x1
408         pin = "PIN"
409         if (inp_en):
410                 pin += "_INPUT"
411         else:
412                 pin += "_OUTPUT"
413         if (pull_dis == 0):
414                 if (pulltype):
415                         pin += "_PULLUP"
416                 else:
417                         pin += "_PULLDOWN"
418         return pin
420 # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # #
422 # Generate output in u-boot format
423 def uboot_format_pad_regs(padconf, per_padconf):
424         print "\nconst struct pad_conf_entry dra74x_core_padconf_array[] = {"
425         for i in padconf:
426                 (pad_name, pin_name, addr, val, delayinfo) = i
428                 if (re.match("MMC.*", pin_name) != None):
429                         print "WARN: Skipping MMC padconf in uboot"
430                         continue
432                 muxmode = val & 0xf
433                 (method, data) = delayinfo
434                 if (method == "LEGACY"):
435                         extramode = ""
436                 elif (method == "VIRTUAL"):
437                         delaymode = data
438                         extramode = " | VIRTUAL_MODE%d" % delaymode
439                 elif (method == "MANUAL"):
440                         extramode = " | MANUAL_MODE"
441                 else:
442                         print "ERR: Invalid method %s" % method
444                 pin_info = get_pin_info(val) + extramode
445                 pad_short = re.sub("CTRL_CORE_PAD_", "", pad_name)
446                 comment = (pad_short + "." + pin_name).lower()
448                 print "\t{ %s, (M%d | %s) },\t/* %s */" % (pad_short, muxmode, pin_info, comment)
449         print "};\n"
451 def uboot_format_delay_regs(delayconf, per_delayconf):
452         manual_del = []
453         for i in delayconf:
454                 (pad_name, pin_name, regname, del_offset, man_name, adel, gdel) = i
456                 if (re.match("MMC.*", pin_name) != None):
457                         print "WARN: Skipping MMC delayconf in uboot"
458                         continue
460                 entry = (del_offset, adel, gdel, regname, pin_name, man_name)
461                 manual_del.append(entry)
463         es_rev = args.revision.replace('.', '_')
464         print "\nconst struct iodelay_cfg_entry dra742_es" + es_rev + "_iodelay_cfg_array[] = {"
465         for entry in sorted(manual_del):
466                 print "\t{ 0x%04X, %5d, %5d },\t/* %s : %s - %s */" % entry
467         print "};\n"
469 # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # #
471 # Generate output in linux format
472 def linux_format_pad_regs(padconf, per_padconf):
473         print "&dra7_pmx_core {"
474         for per in per_padconf:
476                 if (re.match("MMC.*", per) == None):
477                         print "ERR: Only MMC padconf is recommended in kernel"
478                         continue
480                 dtsnode = ("%s_pins_default" % per).lower()
481                 print ""
482                 print "\t%s: %s {" % (dtsnode, dtsnode)
483                 print "\t\tpinctrl-single,pins = <"
484                 for i in per_padconf[per]:
485                         (pad_name, pin_name, addr, val, delayinfo) = i
487                         muxmode = val & 0xf
488                         (method, data) = delayinfo
489                         if (method == "LEGACY"):
490                                 extramode = ""
491                         elif (method == "VIRTUAL"):
492                                 delaymode = data
493                                 extramode = " | VIRTUAL_MODE%d" % delaymode
494                         elif (method == "MANUAL"):
495                                 extramode = " | MANUAL_MODE"
496                         else:
497                                 print "ERR: Invalid method %s" % method
499                         pin_info = get_pin_info(val) + extramode
500                         pad_short = re.sub("CTRL_CORE_PAD_", "", pad_name)
501                         offset = addr - 0x4a003400
502                         comment = (pad_short + "." + pin_name).lower()
504                         print "\t\t\t0x%03X\t(%s | MUM_MODE%d)\t/* %s */" % (offset, pin_info, muxmode, comment)
505                 print "\t\t>;"
506                 print "\t};"
507         print "};\n"
510 def linux_format_delay_regs(delayconf, per_delayconf):
511         print "&dra7_iodelay_core {"
512         for per in per_delayconf.keys():
514                 if (re.match("MMC.*", per) == None):
515                         print "ERR: Only MMC delayconf is recommended in kernel"
516                         continue
518                 # Get the mode from the first entry
519                 (pad_name, pin_name, regname, del_offset, mode, adel, gdel) = per_delayconf[per][0]
521                 dtsnode = ("%s_iodelay_%s_conf" % (per, mode)).lower()
522                 print "\t%s: %s {" % (dtsnode, dtsnode)
523                 print "\t\tpinctrl-single,pins = <"
524                 for i in per_delayconf[per]:
525                         (pad_name, pin_name, regname, del_offset, mode, adel, gdel) = i
527                         print "\t\t\t0x%03X (A_DELAY(%d) | G_DELAY(%d))\t/* %s */" % (del_offset, adel, gdel, regname)
528                 print "\t\t>;"
529                 print "\t};"
530         print "};\n"
532 # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # #
534 # Generate output in bios format
535 def bios_format_pad_regs(padconf, per_padconf):
536         for i in padconf:
537                 (pad_name, pin_name, addr, val, delayinfo) = i
539                 delaylist = []
540                 (method, data) = delayinfo
541                 if (method == "VIRTUAL"):
542                         virt_mode = data
543                         val = val | ( virt_mode<< 4)
544                         val = val | (1 << 8)
545                 elif (method == "MANUAL"):
546                         delaylist = data
547                         val = val | (1 << 8)
549                 offset = addr - 0x4a003400
550                 out_delreg = out_adel = out_gdel = 0
551                 in_delreg  = in_adel  = in_gdel  = 0
552                 oen_delreg = oen_adel = oen_gdel = 0
554                 for j in delaylist:
555                         (regname, adel, gdel) = j
556                         if (re.match(".*_IN", regname) != None):
557                                 in_delreg = xml_iodelay_get_reg(regname)
558                                 in_adel = adel
559                                 in_gdel = gdel
560                         elif (re.match(".*_OEN", regname) != None):
561                                 oen_delreg = xml_iodelay_get_reg(regname)
562                                 oen_adel = adel
563                                 oen_gdel = gdel
564                         elif (re.match(".*_OUT", regname) != None):
565                                 out_delreg = xml_iodelay_get_reg(regname)
566                                 out_adel = adel
567                                 out_gdel = gdel
568                 indel  = "{ 0x%04X, %4d, %4d }" % (in_delreg,  in_adel,  in_gdel)
569                 oendel = "{ 0x%04X, %4d, %4d }" % (oen_delreg, oen_adel, oen_gdel)
570                 outdel = "{ 0x%04X, %4d, %4d }" % (out_delreg, out_adel, out_gdel)
571                 pin_info = get_pin_info(val)
572                 print "\t/* %s -> %s (%s) %s delaymode */" % (pad_name, pin_name, pin_info, method)
573                 print "\t{ 0x%03X, 0x%08X, %s, %s, %s }" % (offset, val, indel, oendel, outdel)
575 def bios_format_delay_regs(delayconf, per_delayconf):
576         print "Manual delays are not configured separately"
577         print "Delays are configured as part of the padconf step only"
579 # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # #
581 # Main execution starts here
582 # * Parse all the XML files - Get the pad data and IOdelay data
583 # * Iterate over the pad register dumps
584 # * For each pad, find out the muxmode being used and the pad direction, etc
585 # * For the muxmode being used, find out available virtual/modes
586 #   - Dump the virtual/manual modes available (based on options)
587 #   - Build up the gpio script to read the pad data using GPIO module
588 # * Select the correct mode to be used
589 #   - Check if the mode is described for the peripheral module, (from selected-modes.txt)
590 #   - Otherwise ask the user (with a menu) to decide the delaymode
591 #     => Update the selection for the whole of the peripheral module
592 #   - Worst case, skip the delaymode for this pad
593 # * Build the pad and delay register information
594 # * Create the dump for pad and delay data in linux/u-boot format
595 # * Dump the delaymode selection for each peripheral
596 # * Dump the GPIO script for each peripheral (all pads grouped together)
599 # Read all the input files and parse the required info
600 modehelp = read_guidelines(modehelp_file)
601 sel = read_selmodes(sel_file)
602 regmap = read_pad_dump(pad_file)
603 reglist = regmap.keys()
605 # List of all the pads being configured
606 padconf = []
607 # List of all the delay registers being configured (for manual mode)
608 delayconf = []
609 # Dictionary of pads grouped by peripheral/module
610 per_padconf = {}
611 # Dictionary of delay registers grouped by peripheral/module
612 per_delayconf = {}
614 xml_check_correctness(modehelp)
616 # Start iterating over each pad
617 for i in range(0, 260):
618         # Find out the muxmode and pad direction, etc
619         addr = 0x4a003400 + i * 4
620         offset = 0x1400 + i * 4
621         dts_offset = offset - 0x1400
623         if (addr not in reglist):
624                 print "WARN: Register dump for pad 0x%X not found" % addr
625                 continue
626         val = regmap[addr]
627         muxmode = val & 0xf
629         # Find out the pin based on the muxmode
630         pad_name = xml_pad_get_name(offset)
631         pin_name = xml_pad_get_pin(offset, muxmode)
632         if (pad_name == "Unknown" or pin_name == "Unknown"):
633                 print "WARN: Cannot find out Pad/Pin name for PAD address 0x%X (%s[%s] = %s)" \
634                 % (addr, pad_name, muxmode, pin_name)
635                 continue
636         if (pin_name == "DRIVER OFF"):
637                 continue
639         # Find out if the delaymode for this module is already selected
640         module = re.match("([^_]+)_.*", pin_name).groups(0)[0]
642         if (args.module != "" and args.module != module):
643                 continue
645         if (args.debug >= 1):
646                 print "\nPAD: %s: Addr= 0x%08X Value = 0x%08X \"%s\"" \
647                 % (pad_name, addr, val, pin_name)
649         # Find out all the possible virtual, manual modes fot the specific pad -> pin combination
650         (virt, man) = xml_find_delaymodes(pad_name, muxmode)
652         # Need to select one out of allowed modes
653         mode = select_mode(pad_name, pin_name, module, virt, man, modehelp, sel)
655         # Remember the selection for that module, for later reuse
656         if (args.strict == False):
657                 sel[module] = mode
659         if (mode == "SKIP"):
660                 continue
661         elif (mode == "LEGACY"):
662                 delayinfo = ("LEGACY", "")
663         elif (mode in virt):
664                 delayinfo = ("VIRTUAL", virt[mode])
665         elif (mode in man):
666                 delayinfo = ("MANUAL", man[mode])
667         else:
668                 print "ERR: Unknown mode '%s' selected" % mode
669                 continue
671         if (args.debug >= 1):
672                 print "  => Using mode %s" % mode
673         paddata = (pad_name, pin_name, addr, val, delayinfo)
674         if (module not in per_padconf.keys()):
675                 per_padconf[module] = []
676         padconf.append(paddata)
677         per_padconf[module].append(paddata)
679         if(mode not in man):
680                 continue
682         # Add the delay data if using manual mode
683         for regval in man[mode]:
684                 (regname, adel, gdel) = regval
685                 del_offset = xml_iodelay_get_reg(regname)
686                 if (del_offset == 0):
687                         print "WARN: Can't find delay offset of register %s" % regname
688                         break
689                 if (args.debug >= 1):
690                         print "  => Manual delay[%s] = (%d, %d)" % (regname, adel, gdel)
691                 delaydata = (pad_name, pin_name, regname, del_offset, mode, adel, gdel)
692                 if (module not in per_delayconf.keys()):
693                         per_delayconf[module] = []
694                 delayconf.append(delaydata)
695                 per_delayconf[module].append(delaydata)
697 print ""
698 print "Total PAD registers: %d" % len(padconf)
699 print "Total DELAY registers: %d" % len(delayconf)
700 print ""
702 format_pad_regs(padconf, per_padconf)
703 format_delay_regs(delayconf, per_delayconf)
704 pad_dump_gpio(padconf, per_padconf)
706 # Dump the final selection for reuse
707 print "Selected modes for each peripheral module\n"
708 for group in sel:
709         print "%s,\t%s" % (group, sel[group])
710 print ""
711 # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # #