c472a5ddc82284036fe193a0265d3182a6af3722
[glsdk/iodelay-config.git] / iodelay-autogen.py
1 #!/usr/bin/python
2 # Python script to automatically generate the IO pad and delay data
3 # Author:- Nikhil Devshatwar
5 # This script uses regdump of the pad registers to figure out the muxmodes
6 # Based on the pad and muxmode, it find out all possible virtual/manual modes
7 # by referring to the PCT XML model. Using the, selection file, script
8 # decides which modes to be selected. Finally it dumps the required array entries
10 # This script depends on following files:-
11 # * XML data files      - Shipped with the DRA7xx PCT tool
12 # * Pad register dump   - Generate using omapconf dump 0x4a003400 0x4a00380c
13 # * selection file      - List of selected virtual/manual modes to be used
15 import xml.etree.ElementTree as ET
16 import re
17 import argparse
19 # Handle the command line arguments
20 parser = argparse.ArgumentParser(prog='iodelay-autogen.py',
21         description='Python script to generate the IOdelay data.\n' \
22                 'This script refers to the XML data and automatically generates\n' \
23                 'PAD and DELAY data for the same use case.\n' \
24                 'Note that only the PADs which are used in the dump are configured.',
25         epilog='Generate the pad and delay data using pad regdump')
27 parser.add_argument('-d', '--debug', dest='debug',
28         action='store', type=int, choices=[0, 1, 2], default=0,
29         help='set the debug level')
31 parser.add_argument('-i', '--interactive', dest='interactive',
32         action='store', type=int, choices=[0, 1], default=1,
33         help='run interactively with menus for resolving conflicts')
35 parser.add_argument('-f', '--format', dest='format',
36         action='store', type=str, choices=["linux", "uboot", "bios"], default="uboot",
37         help='select the output format to be used')
39 parser.add_argument('-r', '--revision', dest='revision',
40         action='store', type=str, choices=["1.1", "2.0"], default="1.1",
41         help='select the silicon revision')
43 parser.add_argument('-m', '--module', dest='module',
44         action='store', type=str, default="",
45         help='generate only for this module')
47 parser.add_argument('-g', '--gpio', dest='gpio',
48         action='store_true',
49         help='generate script to read pad data from GPIO')
51 parser.add_argument('-c', '--check', dest='check_xml',
52         action='store_true',
53         help='check consistency of the XML files and other data')
55 args = parser.parse_args()
56 # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # #
58 PCT_VERSION = "v1.0.7"
59 pad_data_xml = "XMLFiles/CTRL_MODULE_CORE.xml"
60 iod_data_xml = "XMLFiles/IODELAYCONFIG.xml"
61 model_data_xml = "XMLFiles/model_DRA75x_DRA74x_SR" + args.revision + "_" + PCT_VERSION + ".xml"
63 modehelp_file = "guidelines.txt"
64 pad_file = "ctrl-core.dump"
65 sel_file = "selected-modes.txt"
67 # Read the XML file database for pad and delay registers
68 pad_xml = ET.parse(pad_data_xml).getroot()
69 iod_xml = ET.parse(iod_data_xml).getroot()
70 model_xml = ET.parse(model_data_xml).getroot()
72 # Functions to parse the input files and build data structures
73 def read_guidelines(fname):
74         modehelp = {}
75         pattern = re.compile('(.+\w)\t+(.+)')
76         f = open(fname)
77         for line in f.readlines():
78                 list = re.match(pattern, line)
79                 if ( list == None):
80                         continue
81                 mode = list.groups(0)[0]
82                 info = list.groups(0)[1]
83                 modehelp[mode] = info
84                 if (args.debug >= 2):
85                         print "Help: Mode '%s' is used for '%s'" % (mode, info)
86         return modehelp
88 def read_selmodes(fname):
89         sel = {}
90         pattern = re.compile('(\w+)\W*,\W*(\w*)')
91         f = open(fname)
92         for line in f.readlines():
93                 list = re.match(pattern, line)
94                 if ( list == None):
95                         continue
96                 module = list.groups(0)[0]
97                 mode = list.groups(0)[1]
98                 sel[module] = mode
99                 if (args.debug >= 2):
100                         print "INFO: Select '%s' for '%s'" % (mode, module)
101         return sel
103 def read_pad_dump(file):
104         regmap = {}
105         pattern = re.compile('.*(0x[0-9A-F]+).*(0x[0-9A-F]+).*')
106         f = open(file, 'r')
107         for line in f:
108                 list = re.match(pattern, line)
109                 if ( list == None):
110                         continue
111                 addr = int(list.groups(0)[0], 16)
112                 val = int(list.groups(0)[1], 16)
113                 #print "PADXML: Addr = %08x Value = %08x" % (addr, val)
114                 regmap[addr] = val
115         return regmap
116 # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # #
118 # Helper functions to parse XML nodes and get the desired data
119 # Hugely dependent on the XML format of the PCT files
120 # Uses XPath to search elements with queries and filters
121 # Parse the nodes to generate data in desired format
123 def xml_pad_get_name(offset):
124         padlist = pad_xml.findall("register[@offset='0x%X']" % offset)
125         if (len(padlist) == 0):
126                 return "Unknown"
127         else:
128                 return padlist[0].get("id")
130 def xml_pad_get_pin(offset, muxmode):
131         padlist = pad_xml.findall("register[@offset='0x%X']" % offset)
132         if (len(padlist) == 0):
133                 return "Unknown"
134         else:
135                 mux_field = padlist[0].findall("./bitfield[@end='0']")
136                 if (len(mux_field) == 0):
137                         return "Unknown"
138                 modes = mux_field[0].findall("./bitenum[@value='%d']" % muxmode)
139                 if (len(modes) == 0):
140                         return "Unknown"
141                 return modes[0].get("id")
143 def xml_iodelay_get_reg(name):
144         delaylist = iod_xml.findall("register[@id='%s']" % name)
145         if (len(delaylist) == 0):
146                 return 0
147         else:
148                 offset = delaylist[0].get("offset")
149                 #print "IOD: Name = %s Offset = %s" % (del_reg, offset)
150                 return int(offset, 16)
152 def xml_get_virtual(mode):
153         vmodes = {}
154         signal = mode.findtext("signal")
155         for virt in mode.findall("virtualmode/mode"):
156                 virt_mode = virt.findtext("value")
157                 virt_name = virt.findtext("name")
158                 if (virt_name == "NA"):
159                         continue
160                 virt_mode = int(virt_mode)
161                 vmodes[virt_name] = virt_mode
162                 if (args.debug >= 1):
163                         print ("    * VIRTUAL: %s [%s] => delaymode = %d" % (signal, virt_name, virt_mode))
164         return vmodes
166 def xml_get_manual(mode):
167         mmodes = {}
168         signal = mode.findtext("signal")
169         for man in mode.findall("manualmode"):
170                 regname = man.findtext("cfgreg/name")
171                 for sel in man.findall("cfgreg/mode"):
172                         adel = sel.findtext("adelay")
173                         gdel = sel.findtext("gdelay")
174                         man_name = sel.findtext("name")
175                         if (man_name == "NA"):
176                                 continue
177                         adel = int(adel)
178                         gdel = int(gdel)
179                         if (man_name not in mmodes.keys()):
180                                 mmodes[man_name] = []
181                         mmodes[man_name].append((regname, adel, gdel))
182                         if (args.debug >= 1):
183                                 print ("    * MANUAL: %s [%s] => delay[%s] = %d, %d" % (signal, man_name, regname, adel, gdel))
184         return mmodes
186 def xml_find_delaymodes(pad_name, muxmode):
187         padlist = model_xml.findall("padDB/clockNode/type/pad")
188         for pad in padlist:
189                 if (pad_name == pad.findtext("confregisters/regbit/register")):
190                         muxmodes = pad.findall("muxmode")
191                         break
192         if not muxmodes:
193                 return None
194         for mode in muxmodes:
195                 if ("%d" % muxmode == mode.findtext("mode")):
196                         virt = xml_get_virtual(mode)
197                         man = xml_get_manual(mode)
198                         return (virt, man)
199         return None
201 def xml_check_correctness(modehelp):
202         if(args.check_xml == False):
203                 return
205         print "###########################################"
206         print "XML correctness checks:"
207         padcore_list = []
208         padmodel_list = []
209         modes = {}
211         # Fint all the pads in core XML
212         pad_list = pad_xml.findall("register")
213         for i in pad_list:
214                 name = i.get("id")
215                 if (re.match("CTRL_CORE_PAD_.*", name) == None):
216                         continue
217                 padcore_list.append(name)
218         print ">> Total pads defined in core XML = %d" % len(padcore_list)
220         # Find all the pads in model XML
221         pad_list = model_xml.findall("padDB/clockNode/type/pad/confregisters/regbit")
222         for i in pad_list:
223                 name = i.findtext("register")
224                 padmodel_list.append(name)
225         print ">> Total pads defined in model XML = %d" % len(padmodel_list)
227         # Find all the manual modes
228         manmode_list = model_xml.findall("padDB/clockNode/type/pad/muxmode/manualmode/cfgreg/mode")
229         for i in manmode_list:
230                 man_name = i.findtext("name")
231                 modes[man_name] = "manual"
232         # Find all the virtual modes
233         virtmode_list = model_xml.findall("padDB/clockNode/type/pad/muxmode/virtualmode/mode")
234         for i in virtmode_list:
235                 virt_name = i.findtext("name")
236                 modes[virt_name] = "virtual"
237         print ">> Total delaymodes defined in model XML = %d" % len(modes)
239         # Print out all the errors found in the tests
240         print "== Pads defined in core XML but not in model XML =="
241         for i in padcore_list:
242                 if (i not in padmodel_list):
243                         print "\t%s" % i
244         print "== Pads defined in model XML but not in core XML =="
245         for i in padmodel_list:
246                 if (i not in padcore_list):
247                         print "\t%s" % i
249         # Check if description for each mode is available
250         print "== Delaymodes missing description in the guidelines.txt =="
251         for i in modes:
252                 if (i not in modehelp):
253                         print "\t%s" % i
255         print "###########################################"
257 # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # #
259 # Decision point of the script
260 # For each pad/pin, decide what delay method is used
261 # Lookup in the selection file or ask user with a menu
262 def select_mode(pad, pin, module, virt, man, modehelp, sel):
263         modelist = []
264         for modename in virt.keys():
265                 modelist.append(modename)
267         for modename in man.keys():
268                 modelist.append(modename)
270         if (len(modelist) == 0):
271                 return "LEGACY"
273         if (module in sel.keys()):
274                 mode = sel[module]
275                 if (mode == "SKIP" or mode in modelist):
276                         return mode
277                 else:
278                         print("ERR: Invalid delaymode '%s' for module '%s'" % (mode, module))
280         if (args.interactive == 0):
281                 print "WARN: No delay modes for %s found, skipping" % module
282                 mode = "SKIP"
283                 sel[module] = mode
284                 return mode
286         # Display the menu and ask user to select the 'right' mode
287         while True:
288                 print ""
289                 print "MENU: Select delay mode for %s -> %s" % (pad, pin)
290                 i = 0
291                 print "MENU: %d: %s \t\t\t%s" % (i, "SKIP", "Skips this module for now")
292                 for mode in modelist:
293                         i += 1
294                         if (mode in modehelp):
295                                 helptext = modehelp[mode]
296                         else:
297                                 helptext = "Unknown"
298                         print "MENU: %d: %s \t\t%s" % (i, mode, helptext)
299                 try:
300                         choice = int(raw_input("Select delay mode #> "))
301                         if (choice == 0):
302                                 mode = "SKIP"
303                                 break
304                         elif (choice >=0 and choice <= len(modelist)):
305                                 mode = modelist[choice - 1]
306                                 break
307                         print "ERROR: Invalid choice"
308                 except ValueError:
309                         print "ERROR: Invalid choice"
310         print "MENU: Selected mode is %s" % mode
311         print ""
313         # Remember the selection for that module, for later reuse
314         sel[module] = mode
315         return mode
316 # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # #
318 # Pad read using GPIO - Specific to linux only
319 # As each pad is muxed with a SoC gpio (for most of the pads)
320 # It's possible to read the pad data using gpio datain registers
321 # Dump the linux commands to read the gpio registers and read the pad data
322 def pad_dump_gpio(padconf, per_padconf):
323         if(args.gpio == False):
324                 return
326         print "# Read pad signals using GPIO DATA-IN registers"
327         print "# Works only for the input signals"
328         gpio_data_addrs = (0, 0x4ae10138, 0x48055138, 0x48057138, 0x48059138, 0x4805b138, 0x4805d138, 0x48051138, 0x48053138)
329         for i in padconf:
330                 (pad_name, pin_name, addr, val, delayinfo) = i
332                 offset = addr - 0x4a002000
333                 gpio_name = xml_pad_get_pin(offset, 14)
334                 matchlist = re.match("GPIO(.)_(.)", gpio_name)
335                 if (matchlist == None):
336                         print "ERR: No GPIO for pad %s" % pad_name
337                         continue
339                 inst = int(matchlist.groups(0)[0])
340                 bit = int(matchlist.groups(0)[1])
341                 gpio_addr = gpio_data_addrs[inst]
343                 print "#Read GPIO%d_%d to sample %s" % (inst, bit, pin_name)
344                 print " echo %d > /sys/class/gpio/export 2>/dev/null;" % ((inst - 1) * 32)
345                 print " val=`omapconf read 0x%x 2>&1 | grep -v \"support\"`;" % gpio_addr
346                 print " status=$((0x$val >> %d & 0x1));" % bit
347                 print " echo -e \"%s (%s)\t = $status\";" % (pin_name, gpio_name)
348                 print ""
349         print ""
350 # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # #
352 # Generate the final pad and delay data in the required format
353 def format_pad_regs(padconf, per_padconf):
354         print "###########################################"
355         print "Pad data output (with the delay modes)"
356         print "###########################################"
357         if (args.format == "uboot"):
358                 uboot_format_pad_regs(padconf, per_padconf)
359         elif (args.format == "linux"):
360                 linux_format_pad_regs(padconf, per_padconf)
361         elif (args.format == "bios"):
362                 bios_format_pad_regs(padconf, per_padconf)
363         else:
364                 print "ERR: Format %s not suppported" % args.format
366 def format_delay_regs(delayconf, per_delayconf):
367         print "#########################################"
368         print "Delay data output (for manual modes)"
369         print "#########################################"
370         if (args.format == "uboot"):
371                 uboot_format_delay_regs(delayconf, per_delayconf)
372         elif (args.format == "linux"):
373                 linux_format_delay_regs(delayconf, per_delayconf)
374         elif (args.format == "bios"):
375                 bios_format_delay_regs(delayconf, per_delayconf)
376         else:
377                 print "ERR: Format %s not suppported" % args.format
379 def get_pin_info(val):
380         inp_en = (val >> 18) & 0x1
381         pulltype = (val >> 17) & 0x1
382         pull_dis = (val >> 16) & 0x1
383         pin = "PIN"
384         if (inp_en):
385                 pin += "_INPUT"
386         else:
387                 pin += "_OUTPUT"
388         if (pull_dis == 0):
389                 if (pulltype):
390                         pin += "_PULLUP"
391                 else:
392                         pin += "_PULLDOWN"
393         return pin
395 # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # #
397 # Generate output in u-boot format
398 def uboot_format_pad_regs(padconf, per_padconf):
399         print "\nconst struct pad_conf_entry dra74x_core_padconf_array[] = {"
400         for i in padconf:
401                 (pad_name, pin_name, addr, val, delayinfo) = i
403                 if (re.match("MMC.*", pin_name) != None):
404                         print "WARN: Skipping MMC padconf in uboot"
405                         continue
407                 muxmode = val & 0xf
408                 (method, data) = delayinfo
409                 if (method == "LEGACY"):
410                         extramode = ""
411                 elif (method == "VIRTUAL"):
412                         delaymode = data
413                         extramode = " | VIRTUAL_MODE%d" % delaymode
414                 elif (method == "MANUAL"):
415                         extramode = " | MANUAL_MODE"
416                 else:
417                         print "ERR: Invalid method %s" % method
419                 pin_info = get_pin_info(val) + extramode
420                 pad_short = re.sub("CTRL_CORE_PAD_", "", pad_name)
421                 comment = (pad_short + "." + pin_name).lower()
423                 print "\t{ %s, (M%d | %s) },\t/* %s */" % (pad_short, muxmode, pin_info, comment)
424         print "};\n"
426 def uboot_format_delay_regs(delayconf, per_delayconf):
427         print "\nconst struct iodelay_cfg_entry dra742_iodelay_cfg_array[] = {"
428         for i in delayconf:
429                 (pad_name, pin_name, regname, del_offset, man_name, adel, gdel) = i
431                 if (re.match("MMC.*", pin_name) != None):
432                         print "WARN: Skipping MMC padconf in uboot"
433                         continue
435                 print "\t{ 0x%04X, %5d, %5d },\t/* %s */" % (del_offset, adel, gdel, regname)
436         print "};\n"
438 # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # #
440 # Generate output in linux format
441 def linux_format_pad_regs(padconf, per_padconf):
442         print "&dra7_pmx_core {"
443         for per in per_padconf:
445                 if (re.match("MMC.*", per) == None):
446                         print "ERR: Only MMC padconf is recommended in kernel"
447                         continue
449                 dtsnode = ("%s_pins_default" % per).lower()
450                 print ""
451                 print "\t%s: %s {" % (dtsnode, dtsnode)
452                 print "\t\tpinctrl-single,pins = <"
453                 for i in per_padconf[per]:
454                         (pad_name, pin_name, addr, val, delayinfo) = i
456                         muxmode = val & 0xf
457                         (method, data) = delayinfo
458                         if (method == "LEGACY"):
459                                 extramode = ""
460                         elif (method == "VIRTUAL"):
461                                 delaymode = data
462                                 extramode = " | VIRTUAL_MODE%d" % delaymode
463                         elif (method == "MANUAL"):
464                                 extramode = " | MANUAL_MODE"
465                         else:
466                                 print "ERR: Invalid method %s" % method
468                         pin_info = get_pin_info(val) + extramode
469                         pad_short = re.sub("CTRL_CORE_PAD_", "", pad_name)
470                         offset = addr - 0x4a003400
471                         comment = (pad_short + "." + pin_name).lower()
473                         print "\t\t\t0x%03X\t(%s | MUM_MODE%d)\t/* %s */" % (offset, pin_info, muxmode, comment)
474                 print "\t\t>;"
475                 print "\t};"
476         print "};\n"
479 def linux_format_delay_regs(delayconf, per_delayconf):
480         print "&dra7_iodelay_core {"
481         for per in per_delayconf.keys():
483                 if (re.match("MMC.*", per) == None):
484                         print "ERR: Only MMC delayconf is recommended in kernel"
485                         continue
487                 # Get the mode from the first entry
488                 (pad_name, pin_name, regname, del_offset, mode, adel, gdel) = per_delayconf[per][0]
490                 dtsnode = ("%s_iodelay_%s_conf" % (per, mode)).lower()
491                 print "\t%s: %s {" % (dtsnode, dtsnode)
492                 print "\t\tpinctrl-single,pins = <"
493                 for i in per_delayconf[per]:
494                         (pad_name, pin_name, regname, del_offset, mode, adel, gdel) = i
496                         print "\t\t\t0x%03X A_DELAY(%d) | G_DELAY(%d)\t/* %s */" % (del_offset, adel, gdel, regname)
497                 print "\t\t>;"
498                 print "\t};"
499         print "};\n"
501 # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # #
503 # Generate output in bios format
504 def bios_format_pad_regs(padconf, per_padconf):
505         for i in padconf:
506                 (pad_name, pin_name, addr, val, delayinfo) = i
508                 delaylist = []
509                 (method, data) = delayinfo
510                 if (method == "VIRTUAL"):
511                         virt_mode = data
512                         val = val | ( virt_mode<< 4)
513                         val = val | (1 << 8)
514                 elif (method == "MANUAL"):
515                         delaylist = data
516                         val = val | (1 << 8)
518                 offset = addr - 0x4a003400
519                 out_delreg = out_adel = out_gdel = 0
520                 in_delreg  = in_adel  = in_gdel  = 0
521                 oen_delreg = oen_adel = oen_gdel = 0
523                 for j in delaylist:
524                         (regname, adel, gdel) = j
525                         if (re.match(".*_IN", regname) != None):
526                                 in_delreg = xml_iodelay_get_reg(regname)
527                                 in_adel = adel
528                                 in_gdel = gdel
529                         elif (re.match(".*_OEN", regname) != None):
530                                 oen_delreg = xml_iodelay_get_reg(regname)
531                                 oen_adel = adel
532                                 oen_gdel = gdel
533                         elif (re.match(".*_OUT", regname) != None):
534                                 out_delreg = xml_iodelay_get_reg(regname)
535                                 out_adel = adel
536                                 out_gdel = gdel
537                 indel  = "{ 0x%04X, %4d, %4d }" % (in_delreg,  in_adel,  in_gdel)
538                 oendel = "{ 0x%04X, %4d, %4d }" % (oen_delreg, oen_adel, oen_gdel)
539                 outdel = "{ 0x%04X, %4d, %4d }" % (out_delreg, out_adel, out_gdel)
540                 pin_info = get_pin_info(val)
541                 print "\t/* %s -> %s (%s) %s delaymode */" % (pad_name, pin_name, pin_info, method)
542                 print "\t{ 0x%03X, 0x%08X, %s, %s, %s }" % (offset, val, indel, oendel, outdel)
544 def bios_format_delay_regs(delayconf, per_delayconf):
545         print "Manual delays are not configured separately"
546         print "Delays are configured as part of the padconf step only"
548 # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # #
550 # Main execution starts here
551 # * Parse all the XML files - Get the pad data and IOdelay data
552 # * Iterate over the pad register dumps
553 # * For each pad, find out the muxmode being used and the pad direction, etc
554 # * For the muxmode being used, find out available virtual/modes
555 #   - Dump the virtual/manual modes available (based on options)
556 #   - Build up the gpio script to read the pad data using GPIO module
557 # * Select the correct mode to be used
558 #   - Check if the mode is described for the peripheral module, (from selected-modes.txt)
559 #   - Otherwise ask the user (with a menu) to decide the delaymode
560 #     => Update the selection for the whole of the peripheral module
561 #   - Worst case, skip the delaymode for this pad
562 # * Build the pad and delay register information
563 # * Create the dump for pad and delay data in linux/u-boot format
564 # * Dump the delaymode selection for each peripheral
565 # * Dump the GPIO script for each peripheral (all pads grouped together)
568 # Read all the input files and parse the required info
569 modehelp = read_guidelines(modehelp_file)
570 sel = read_selmodes(sel_file)
571 regmap = read_pad_dump(pad_file)
572 reglist = regmap.keys()
574 # List of all the pads being configured
575 padconf = []
576 # List of all the delay registers being configured (for manual mode)
577 delayconf = []
578 # Dictionary of pads grouped by peripheral/module
579 per_padconf = {}
580 # Dictionary of delay registers grouped by peripheral/module
581 per_delayconf = {}
583 xml_check_correctness(modehelp)
584 # Start iterating over each pad
585 for i in range(0, 260):
586         # Find out the muxmode and pad direction, etc
587         addr = 0x4a003400 + i * 4
588         offset = 0x1400 + i * 4
589         dts_offset = offset - 0x1400
591         if (addr not in reglist):
592                 print "WARN: Register dump for pad 0x%X not found" % addr
593                 continue
594         val = regmap[addr]
595         muxmode = val & 0xf
597         # Find out the pin based on the muxmode
598         pad_name = xml_pad_get_name(offset)
599         pin_name = xml_pad_get_pin(offset, muxmode)
600         if (pad_name == "Unknown" or pin_name == "Unknown"):
601                 print "WARN: Cannot find out Pad/Pin name for PAD address 0x%X (%s[%s] = %s)" \
602                 % (addr, pad_name, muxmode, pin_name)
603                 continue
604         if (pin_name == "DRIVER OFF"):
605                 continue
607         # Find out if the delaymode for this module is already selected
608         module = re.match("([^_]+)_.*", pin_name).groups(0)[0]
610         if (args.module != "" and args.module != module):
611                 continue
613         if (args.debug >= 1):
614                 print "\nPAD: %s: Addr= 0x%08X Value = 0x%08X \"%s\"" \
615                 % (pad_name, addr, val, pin_name)
617         # Find out all the possible virtual, manual modes fot the specific pad -> pin combination
618         (virt, man) = xml_find_delaymodes(pad_name, muxmode)
620         # Need to select one out of allowed modes
621         mode = select_mode(pad_name, pin_name, module, virt, man, modehelp, sel)
622         if (mode == "SKIP"):
623                 continue
625         if (mode == "LEGACY"):
626                 delayinfo = ("LEGACY", "")
627         elif (mode in virt):
628                 delayinfo = ("VIRTUAL", virt[mode])
629         elif (mode in man):
630                 delayinfo = ("MANUAL", man[mode])
631         else:
632                 print "ERR: Unknown mode '%s' selected" % mode
633                 continue
635         if (args.debug >= 1):
636                 print "  => Using mode %s" % mode
637         paddata = (pad_name, pin_name, addr, val, delayinfo)
638         if (module not in per_padconf.keys()):
639                 per_padconf[module] = []
640         padconf.append(paddata)
641         per_padconf[module].append(paddata)
643         if(mode not in man):
644                 continue
646         # Add the delay data if using manual mode
647         for regval in man[mode]:
648                 (regname, adel, gdel) = regval
649                 del_offset = xml_iodelay_get_reg(regname)
650                 if (del_offset == 0):
651                         print "WARN: Can't find delay offset of register %s" % regname
652                         break
653                 if (args.debug >= 1):
654                         print "  => Manual delay[%s] = (%d, %d)" % (regname, adel, gdel)
655                 delaydata = (pad_name, pin_name, regname, del_offset, mode, adel, gdel)
656                 if (module not in per_delayconf.keys()):
657                         per_delayconf[module] = []
658                 delayconf.append(delaydata)
659                 per_delayconf[module].append(delaydata)
661 print ""
662 print "Total PAD registers: %d" % len(padconf)
663 print "Total DELAY registers: %d" % len(delayconf)
664 print ""
666 format_pad_regs(padconf, per_padconf)
667 format_delay_regs(delayconf, per_delayconf)
668 pad_dump_gpio(padconf, per_padconf)
670 # Dump the final selection for reuse
671 print "Selected modes for each peripheral module\n"
672 for group in sel:
673         print "%s,\t%s" % (group, sel[group])
674 print ""
675 # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # #