]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - glsdk/iodelay-config.git/blob - iodelay-autogen.py
script: Handle invalid muxmodes
[glsdk/iodelay-config.git] / iodelay-autogen.py
1 #!/usr/bin/python
2 # Python script to automatically generate the IO pad and delay data
3 # Author:- Nikhil Devshatwar
5 # This script uses regdump of the pad registers to figure out the muxmodes
6 # Based on the pad and muxmode, it find out all possible virtual/manual modes
7 # by referring to the PCT XML model. Using the, selection file, script
8 # decides which modes to be selected. Finally it dumps the required array entries
10 # This script depends on following files:-
11 # * XML data files      - Shipped with the DRA7xx PCT tool
12 # * Pad register dump   - Generate using omapconf dump 0x4a003400 0x4a00380c
13 # * selection file      - List of selected virtual/manual modes to be used
15 import xml.etree.ElementTree as ET
16 import re
17 import argparse
19 # Handle the command line arguments
20 parser = argparse.ArgumentParser(prog='iodelay-autogen.py',
21         description='Python script to generate the IOdelay data.\n' \
22                 'This script refers to the XML data and automatically generates\n' \
23                 'PAD and DELAY data for the same use case.\n' \
24                 'Note that only the PADs which are used in the dump are configured.',
25         epilog='Generate the pad and delay data using pad register dumps. For this,\n' \
26                 'Run omapconf dump 0x4a003400 0x4a00380c and save the output')
28 parser.add_argument('-p', '--part', dest='part',
29         action='store', type=str, choices=["dra74x", "dra75x", "dra72x"], default="dra74x",
30         help='select the device part')
32 parser.add_argument('-r', '--revision', dest='revision',
33         action='store', type=str, choices=["1.0", "1.1", "2.0"], default="2.0",
34         help='select the silicon revision')
36 parser.add_argument('-m', '--module', dest='module',
37         action='store', type=str, default="",
38         help='generate only for modules matching the provided RE')
40 parser.add_argument('-f', '--format', dest='format',
41         action='store', type=str, choices=["linux", "uboot", "bios"], default="uboot",
42         help='select the output format to be used')
44 parser.add_argument('-d', '--debug', dest='debug',
45         action='store', type=int, choices=[0, 1, 2, 3, 4], default=0,
46         help='set the debug level - ERR,WARN,INFO,DBG,VERBOSE')
48 parser.add_argument('-i', '--interactive', dest='interactive',
49         action='store', type=int, choices=[0, 1], default=1,
50         help='run interactively with menus for resolving conflicts')
52 parser.add_argument('-s', '--strict', dest='strict',
53         action='store_true',
54         help='strict mode - ask for each pad of the group, do not save selection.\n' \
55                 'For some peripherals, same delaymode cannot be used for all the pads.\n' \
56                 'Use this mode to select different modes for each pad')
58 parser.add_argument('-g', '--gpio', dest='gpio',
59         action='store_true',
60         help='generate script to probe signals using gpio')
62 parser.add_argument('-c', '--check', dest='check_xml',
63         action='store_true',
64         help='check consistency of the XML files and other data')
66 args = parser.parse_args()
68 # Some more knobs for developers, Don't want to expose them to cmd line
69 args.resetslew = True
71 # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # #
73 VERSION = "2.8"
75 if (args.part == "dra74x" or args.part == "dra75x"):
76         if (args.revision == "1.0" or args.revision == "1.1"):
77                 args.revision = "1.x"
78         XML_PATH = "XMLFiles/DRA75x_DRA74x"
79         PART = "DRA75x_DRA74x"
80         PCT_VERSION = "v1.0.16"
81 elif (args.part == "dra72x"):
82         if (args.revision == "1.1"):
83                 print "dra72x doesn't have silicon revision 1.1"
84                 exit()
85         XML_PATH = "XMLFiles/DRA72x"
86         PART = "DRA72x"
87         PCT_VERSION = "v1.0.9"
89 pad_data_xml   = XML_PATH + "/CTRL_MODULE_CORE.xml"
90 iod_data_xml   = XML_PATH + "/IODELAYCONFIG.xml"
91 model_data_xml = XML_PATH + "/model_" + PART + "_SR" + args.revision + "_" + PCT_VERSION + ".xml"
92 modehelp_file  = XML_PATH + "/guidelines_SR" + args.revision + ".txt"
94 pad_file = "ctrl-core.dump"
95 sel_file = "selected-modes.txt"
97 def trace(level, msg):
98         if (args.debug >= level):
99                 print(msg)
100 def verbose(msg):
101         trace(4, "DEBUG: " + msg)
102 def debug(msg, args=None):
103         trace(3, "DEBUG: " + msg)
104 def info(msg):
105         trace(2, "INFO: " + msg)
106 def warn(msg):
107         trace(1, "WARN: " + msg)
108 def error(msg):
109         trace(0, "ERR: " + msg)
110 def fatal(msg):
111         trace(0, "FATAL: " + msg)
112         exit()
114 if (args.interactive):
115         print "iodelay-autogen.py - Python script to generate the IOdelay data."
116         print "v" + VERSION + " using PCT version " + PCT_VERSION
117         print "Parsing PCT data from " + model_data_xml + "..."
118         print ""
120 # Read the XML file database for pad and delay registers
121 pad_xml = ET.parse(pad_data_xml).getroot()
122 iod_xml = ET.parse(iod_data_xml).getroot()
123 model_xml = ET.parse(model_data_xml).getroot()
125 # Functions to parse the input files and build data structures
126 def read_guidelines(fname):
127         modehelp = {}
128         pattern = re.compile('([^\t.]+\w)\t+(.+)')
129         f = open(fname)
130         for line in f.readlines():
131                 list = re.match(pattern, line)
132                 if ( list == None):
133                         continue
134                 mode = list.groups(0)[0]
135                 info = list.groups(0)[1]
136                 modehelp[mode] = info
137                 verbose("Guideline: Mode '%30s' => '%s'" % (mode, info))
138         return modehelp
140 def read_selmodes(fname):
141         sel = {}
142         pattern = re.compile('(\w+)\W*,\W*(\w*)')
143         f = open(fname)
144         for line in f.readlines():
145                 list = re.match(pattern, line)
146                 if ( list == None):
147                         continue
148                 module = list.groups(0)[0]
149                 mode = list.groups(0)[1]
150                 sel[module] = mode
151                 verbose("Input modes: Select '%s' => '%s'" % (mode, module))
152         return sel
154 def read_pad_dump(file):
155         regmap = {}
156         pattern = re.compile('.*(0x[0-9A-Fa-f]+).*(0x[0-9A-Fa-f]+).*')
157         f = open(file, 'r')
158         for line in f:
159                 list = re.match(pattern, line)
160                 if ( list == None):
161                         continue
162                 addr = int(list.groups(0)[0], 16)
163                 val = int(list.groups(0)[1], 16)
164                 verbose("XML pad-reg: Addr = %08x Value = %08x" % (addr, val))
165                 regmap[addr] = val
166         return regmap
168 # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # #
169 # Read all the input files and parse the required info
170 modehelp = read_guidelines(modehelp_file)
171 sel = read_selmodes(sel_file)
172 regmap = read_pad_dump(pad_file)
173 reglist = regmap.keys()
175 # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # #
177 # Helper functions to parse XML nodes and get the desired data
178 # Hugely dependent on the XML format of the PCT files
179 # Uses XPath to search elements with queries and filters
180 # Parse the nodes to generate data in desired format
182 def xml_pad_get_name(offset):
183         padlist = pad_xml.findall("register[@offset='0x%X']" % offset)
184         if (len(padlist) == 0):
185                 return "Unknown"
186         else:
187                 return padlist[0].get("id")
189 def xml_pad_get_offset(name):
190         padlist = pad_xml.findall("register[@id='%s']" % name)
191         if (len(padlist) == 0):
192                 return None
193         else:
194                 return int(padlist[0].get("offset"), 16)
196 def xml_pad_get_slew(offset):
197         padlist = pad_xml.findall("register[@offset='0x%X']" % offset)
198         if (len(padlist) == 0):
199                 return 0x0
200         else:
201                 bitlist = padlist[0].findall("bitfield[@begin='19']")
202                 if (len(bitlist) == 0):
203                         return 0x0
204                 else:
205                         return int(bitlist[0].get("resetval"), 16)
207 # For DRA72x SoC, for "ball compatibility" purpose, some signals have same muxmode.
208 # CTRL_CORE_ALT_SELECT_MUX register allows to select between one of the signals
209 # Its like a board mux has been added inside the SoC, except it uses same muxmode.
210 def resolve_group(muxmode_str):
211         if (muxmode_str == "DRIVER OFF"):
212                 return muxmode_str
213         mmlist = muxmode_str.split(" ")
214         mmlen = len(mmlist)
215         if (mmlen == 1):
216                 def_mode = mmlist[0]
217                 return mmlist[0]
218         elif (mmlen == 2):
219                 def_mode = mmlist[0]
220                 grp1_mode = mmlist[1]
221         elif (mmlen == 3):
222                 def_mode = mmlist[0]
223                 grp1_mode = mmlist[1]
224                 grp2_mode = mmlist[2]
225         else:
226                 error("Cannot resolve muxmode group for '%s'" % muxmode_str)
228         #HACK for now
229         warn("Not resolving muxmode %s, assuming default %s" % (muxmode_str, def_mode))
230         return def_mode
232 def xml_model_get_signal(offset, muxmode):
233         padlist = pad_xml.findall("register[@offset='0x%X']" % offset)
234         if (len(padlist) == 0):
235                 return "Unknown"
236         else:
237                 mux_field = padlist[0].findall("./bitfield[@end='0']")
238                 if (len(mux_field) == 0):
239                         return "Unknown"
240                 modes = mux_field[0].findall("./bitenum[@value='%d']" % muxmode)
241                 if (len(modes) == 0):
242                         return "Unknown"
243                 return resolve_group(modes[0].get("id"))
245 def xml_iodelay_get_reg(name):
246         delaylist = iod_xml.findall("register[@id='%s']" % name)
247         if (len(delaylist) == 0):
248                 return 0
249         else:
250                 offset = delaylist[0].get("offset")
251                 verbose("XML delay-reg: Name = %s Offset = %s" % (name, offset))
252                 return int(offset, 16)
254 def xml_get_virtual(mode):
255         vmodes = {}
256         signal = mode.findtext("signal")
257         for virt in mode.findall("virtualmode/mode"):
258                 virt_mode = virt.findtext("value")
259                 virt_name = virt.findtext("name")
260                 if (virt_name == "NA"):
261                         continue
262                 virt_mode = int(virt_mode)
263                 vmodes[virt_name] = virt_mode
264                 debug("    * VIRTUAL: %s [%s] => delaymode = %d" % (signal, virt_name, virt_mode))
265         return vmodes
267 def xml_get_manual(mode):
268         mmodes = {}
269         signal = mode.findtext("signal")
270         for man in mode.findall("manualmode"):
271                 regname = man.findtext("cfgreg/name")
272                 for sel in man.findall("cfgreg/mode"):
273                         adel = sel.findtext("adelay")
274                         gdel = sel.findtext("gdelay")
275                         man_name = sel.findtext("name")
276                         if (man_name == "NA"):
277                                 continue
278                         adel = int(adel)
279                         gdel = int(gdel)
280                         if (man_name not in mmodes.keys()):
281                                 mmodes[man_name] = []
282                         mmodes[man_name].append((regname, adel, gdel))
283                         debug("    * MANUAL: %s [%s] => delay[%s] = %d, %d" % (signal, man_name, regname, adel, gdel))
284         return mmodes
286 def xml_get_additional_mode(orig):
287         additional_mux = orig.findall("additionalMux/confregisters")
288         if (len(additional_mux) == 0):
289                 return orig
290         else:
291                 additional_mux = additional_mux[0]
292                 mux_reg_name = additional_mux.findtext("register")
293                 offset = xml_pad_get_offset(mux_reg_name)
295                 if (offset == None):
296                         error("Could not find register address for register '%s'" % mux_reg_name)
297                         fatal("This pin may have virtual/manual modes, Fix XML file")
299                 addr = 0x4a002000 + offset
300                 if (addr not in reglist):
301                         error("register dump lacks data for additional muxes")
302                         warn("using default values")
303                         muxval = 0x0
304                 else:
305                         muxval = regmap[addr]
307                 values = additional_mux.findall("value")
308                 for value in values:
310                         option = int(value.findtext("option"))
311                         fieldpos = value.findtext("fieldPos")
312                         signal = value.findtext("signal").upper()
313                         matchlist = re.match("([0-9]+)[:]*([0-9]*)", fieldpos)
315                         verbose("++++ Additional mux %s possible" % signal)
316                         end = int(matchlist.groups(0)[0])
317                         if (matchlist.groups(0)[1] == ""):
318                                 start = end
319                         else:
320                                 start = int(matchlist.groups(0)[1])
322                         muxval = muxval & (1 << end)
323                         muxval = muxval >> start
325                         if (muxval == option):
326                                 debug(">>>> Additional mux %s[%s] = %d" % (mux_reg_name, fieldpos, option))
327                                 debug(">>>> Effective signal = %s" % signal)
328                                 return value
329                 error("None of the additional Mux value matched, using default")
330                 return values[0]
332 def xml_find_delaymodes(pad_name, muxmode):
333         print pad_name
334         print muxmode
335         virt = {}
336         man = {}
337         padlist = model_xml.findall("padDB/clockNode/type/pad")
338         for pad in padlist:
339                 if (pad_name == pad.findtext("confregisters/regbit/register")):
340                         muxmodes = pad.findall("muxmode")
341                         break
342         if not muxmodes:
343                 return None
344         for mode in muxmodes:
345                 if ("%d" % muxmode == mode.findtext("mode")):
346                         mode = xml_get_additional_mode(mode)
347                         virt = xml_get_virtual(mode)
348                         man = xml_get_manual(mode)
349                         return (virt, man)
350         return (virt, man)
352 def xml_check_correctness(modehelp):
354         print "###########################################"
355         print "XML correctness checks:"
356         padcore_list = []
357         padmodel_list = []
358         modes = {}
360         # Find all the pads in core XML
361         pad_list = pad_xml.findall("register")
362         for i in pad_list:
363                 name = i.get("id")
364                 if (re.match("CTRL_CORE_PAD_.*", name) == None):
365                         continue
366                 padcore_list.append(name)
367         print ">> Total pads defined in core XML = %d" % len(padcore_list)
369         # Find all the pads in model XML
370         pad_list = model_xml.findall("padDB/clockNode/type/pad/confregisters/regbit")
371         for i in pad_list:
372                 name = i.findtext("register")
373                 padmodel_list.append(name)
374         print ">> Total pads defined in model XML = %d" % len(padmodel_list)
376         # Find all the manual modes
377         manmode_list = model_xml.findall("padDB/clockNode/type/pad/muxmode/manualmode/cfgreg/mode")
378         for i in manmode_list:
379                 man_name = i.findtext("name")
380                 modes[man_name] = "manual"
381         # Find all the additional manual modes
382         manmode_list = model_xml.findall("padDB/clockNode/type/pad/muxmode/additionalMux/confregisters/value/manualmode/cfgreg/mode")
383         for i in manmode_list:
384                 man_name = i.findtext("name")
385                 modes[man_name] = "manual"
386         # Find all the virtual modes
387         virtmode_list = model_xml.findall("padDB/clockNode/type/pad/muxmode/virtualmode/mode")
388         for i in virtmode_list:
389                 virt_name = i.findtext("name")
390                 modes[virt_name] = "virtual"
391         # Find all the additional virtual modes
392         virtmode_list = model_xml.findall("padDB/clockNode/type/pad/muxmode/additionalMux/confregisters/value/virtualmode/mode")
393         for i in virtmode_list:
394                 virt_name = i.findtext("name")
395                 modes[virt_name] = "virtual"
396         print ">> Total delaymodes defined in model XML = %d" % len(modes)
398         # Print out all the errors found in the tests
399         print "== Pads defined in core XML but not in model XML =="
400         for i in padcore_list:
401                 if (i not in padmodel_list):
402                         print "\t%s" % i
403         print "== Pads defined in model XML but not in core XML =="
404         for i in padmodel_list:
405                 if (i not in padcore_list):
406                         print "\t%s" % i
408         # Check if description for each mode is available
409         print "== Delaymodes missing description in the guidelines.txt =="
410         for i in modes:
411                 if (i not in modehelp):
412                         print "\t%s" % i
414         # Check if description for unknown mode is documented
415         print "== Delaymodes unused from guidelines.txt =="
416         for i in modehelp:
417                 if (i not in modes):
418                         print "\t%s" % i
420         print "###########################################"
422 # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # #
424 # Decision point of the script
425 # For each pad/pin, decide what delay method is used
426 # Lookup in the selection file or ask user with a menu
427 def select_mode(pad, pin, module, virt, man, modehelp, sel):
428         modelist = []
429         for modename in virt.keys():
430                 modelist.append(modename)
432         for modename in man.keys():
433                 modelist.append(modename)
435         if (len(modelist) == 0):
436                 return "LEGACY"
438         if (module in sel.keys()):
439                 mode = sel[module]
440                 if (mode == "SKIP" or mode == "LEGACY" or mode in modelist):
441                         return mode
442                 else:
443                         error("Invalid delaymode '%s' for module '%s'" % (mode, module))
445         if (args.interactive == 0):
446                 warn("No delay modes for %s found, skipping" % module)
447                 mode = "SKIP"
448                 return mode
450         # Display the menu and ask user to select the 'right' mode
451         while True:
452                 print ""
453                 print "MENU: Select delay mode for %s -> %s" % (pad, pin)
454                 i = 0
455                 print "MENU: %d: %s \t\t\t%s" % (i, "SKIP", "Skips this module for now")
456                 i = 1
457                 print "MENU: %d: %s \t\t%s" % (i, "LEGACY", "No external delay config (No virtual/manual needed)")
458                 for mode in modelist:
459                         i += 1
460                         if (mode in modehelp):
461                                 helptext = modehelp[mode]
462                         else:
463                                 helptext = "Unknown"
464                         print "MENU: %d: %s \t\t%s" % (i, mode, helptext)
465                 try:
466                         choice = int(raw_input("Select delay mode #> "))
467                         if (choice == 0):
468                                 mode = "SKIP"
469                                 break
470                         elif (choice == 1):
471                                 mode = "LEGACY"
472                                 break
473                         elif (choice >=2 and choice <= len(modelist) + 1):
474                                 mode = modelist[choice - 2]
475                                 break
476                         print "ERROR: Invalid choice"
477                 except ValueError:
478                         print "ERROR: Invalid choice"
479         print "MENU: Selected mode is %s" % mode
480         print ""
482         return mode
483 # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # #
485 # Pad read using GPIO - Specific to linux only
486 # As each pad is muxed with a SoC gpio (for most of the pads)
487 # It's possible to read the pad data using gpio datain registers
488 # Change pad register to enable input path and export sysfs
489 # Use sysfs to read the status of GPIO and print in a loop
490 def pad_dump_gpio(padconf, per_padconf):
491         gpio_data_addrs = (0, 0x4ae10138, 0x48055138, 0x48057138, 0x48059138, 0x4805b138, 0x4805d138, 0x48051138, 0x48053138)
492         module = args.module
494         # script header
495         gen_header = "###########################################\n" + \
496                      "# Read %s signals using GPIO sysfs\n" % module + \
497                      "###########################################\n\n"
498         gen_data = "%s_data=(\n" % module
500         for i in padconf:
501                 (pad_name, pin_name, addr, val, mode, delayinfo) = i
503                 offset = addr - 0x4a002000
504                 gpio_name = xml_model_get_signal(offset, 14)
505                 matchlist = re.match("GPIO(.)_(.*)", gpio_name)
506                 if (matchlist == None):
507                         error("No GPIO for pad %s - cannot read from script" % pad_name)
508                         continue
510                 inst = int(matchlist.groups(0)[0])
511                 bit = int(matchlist.groups(0)[1])
512                 gpio_addr = gpio_data_addrs[inst]
513                 ngpio = (inst - 1) * 32 + bit
514                 pin_short = re.match(".+_(.*)", pin_name).groups(0)[0]
516                 gen_data += "\t%s:0x%x:%s:%d:0x%x:%d\n" % (pin_short, addr, gpio_name, ngpio, gpio_addr, bit)
518         gen_data += ")\n\n"
520         # Main script to probe the signal
521         gen_main = "echo; echo Probing %s signals\n\n" % module + \
522                    "for data in ${%s_data[@]}\n" % module + \
523                    "do\n" + \
524                    "    pin=`echo $data | cut -d ':' -f1`\n" + \
525                    "    pad=`echo $data | cut -d ':' -f2`\n" + \
526                    "    ngpio=`echo $data | cut -d ':' -f4`\n" + \
527                    "    echo $ngpio > /sys/class/gpio/export 2>/dev/null\n" + \
528                    "    omapconf set bit $pad 18 1>/dev/null 2>/dev/null\n" + \
529                    "    printf \"%8s\" $pin\n" + \
530                    "done\n" + \
531                    "echo\n\n"
533         gen_main += "while true;\n" + \
534                     "do\n" + \
535                     "    for data in ${%s_data[@]}\n" % module + \
536                     "    do\n" + \
537                     "#       pin=`echo $data | cut -d ':' -f1`\n" + \
538                     "#        pad=`echo $data | cut -d ':' -f2`\n" + \
539                     "#       gpio=`echo $data | cut -d ':' -f3`\n" + \
540                     "        ngpio=`echo $data | cut -d ':' -f4`\n" + \
541                     "#       addr=`echo $data | cut -d ':' -f5`\n" + \
542                     "#       bit=`echo $data | cut -d ':' -f6`\n" + \
543                     "        val=`cat /sys/class/gpio/gpio$ngpio/value`\n" + \
544                     "        printf %8d $val \n" + \
545                     "    done\n" + \
546                     "    echo\n" + \
547                     "done\n\n"
549         gen_footer = "###########################################\n"
551         # Generate the shell script
552         gen_script = gen_header + gen_data + gen_main + gen_footer
553         filename = ("./%s-probe.sh" % module).lower()
554         print "Generating '%s' script..." % filename
555         gen_file = open(filename, "w+")
556         gen_file.write(gen_script)
558 # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # #
560 # Generate the final pad and delay data in the required format
561 def format_pad_regs(padconf, per_padconf):
562         print "######## Pad data output ########"
563         if (args.format == "uboot"):
564                 uboot_format_pad_regs(padconf, per_padconf)
565         elif (args.format == "linux"):
566                 linux_format_pad_regs(padconf, per_padconf)
567         elif (args.format == "bios"):
568                 bios_format_pad_regs(padconf, per_padconf)
569         else:
570                 error("Format %s not suppported" % args.format)
572 def format_delay_regs(delayconf, per_delayconf):
573         print "######## Delay data output ########"
574         if (args.format == "uboot"):
575                 uboot_format_delay_regs(delayconf, per_delayconf)
576         elif (args.format == "linux"):
577                 linux_format_delay_regs(delayconf, per_delayconf)
578         elif (args.format == "bios"):
579                 bios_format_delay_regs(delayconf, per_delayconf)
580         else:
581                 error("Format %s not suppported" % args.format)
583 def get_pin_info(val):
584         slew_fast = (val >> 19) & 0x1
585         inp_en = (val >> 18) & 0x1
586         pulltype = (val >> 17) & 0x1
587         pull_dis = (val >> 16) & 0x1
588         pin = "PIN"
589         if (inp_en):
590                 pin += "_INPUT"
591         else:
592                 pin += "_OUTPUT"
593         if (pull_dis == 0):
594                 if (pulltype):
595                         pin += "_PULLUP"
596                 else:
597                         pin += "_PULLDOWN"
598         if (slew_fast):
599                 pin += " | SLEWCONTROL"
600         return pin
602 # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # #
604 # Generate output in u-boot format
605 def uboot_format_pad_regs(padconf, per_padconf):
606         print "\nconst struct pad_conf_entry dra74x_core_padconf_array[] = {"
607         for i in padconf:
608                 (pad_name, pin_name, addr, val, mode, delayinfo) = i
610                 muxmode = val & 0xf
611                 (method, data) = delayinfo
612                 if (method == "LEGACY"):
613                         extramode = ""
614                 elif (method == "VIRTUAL"):
615                         delaymode = data
616                         extramode = " | VIRTUAL_MODE%d" % delaymode
617                 elif (method == "MANUAL"):
618                         extramode = " | MANUAL_MODE"
619                 else:
620                         error("Invalid delay method %s" % method)
622                 pin_info = get_pin_info(val) + extramode
623                 pad_short = re.sub("CTRL_CORE_PAD_", "", pad_name)
624                 comment = (pad_short + "." + pin_name).lower()
626                 print "\t{ %s, (M%d | %s) },\t/* %s */" % (pad_short, muxmode, pin_info, comment)
627         print "};\n"
629 def uboot_format_delay_regs(delayconf, per_delayconf):
630         manual_del = []
631         for i in delayconf:
632                 (pad_name, pin_name, regname, del_offset, man_name, adel, gdel) = i
634                 entry = (del_offset, adel, gdel, regname, pin_name, man_name)
635                 manual_del.append(entry)
637         es_rev = args.revision.replace('.', '_')
638         print "\nconst struct iodelay_cfg_entry dra742_es" + es_rev + "_iodelay_cfg_array[] = {"
639         for entry in sorted(manual_del):
640                 print "\t{ 0x%04X, %5d, %5d },\t/* %s : %s - %s */" % entry
641         print "};\n"
643 # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # #
645 # Generate output in linux format
646 def linux_format_pad_regs(padconf, per_padconf):
647         print "&dra7_pmx_core {"
648         for per in per_padconf:
650                 if (re.match("MMC.*", per) == None):
651                         warn("Only MMC padconf is recommended in kernel")
653                 # Get the mode from the first entry
654                 (pad_name, pin_name, addr, val, mode, delayinfo) = per_padconf[per][0]
656                 dtsnode = ("%s_pins_%s" % (per, mode)).lower()
657                 print ""
658                 print "\t%s: %s {" % (dtsnode, dtsnode)
659                 print "\t\tpinctrl-single,pins = <"
660                 for i in per_padconf[per]:
661                         (pad_name, pin_name, addr, val, mode, delayinfo) = i
663                         muxmode = val & 0xf
664                         (method, data) = delayinfo
665                         if (method == "LEGACY"):
666                                 extramode = ""
667                         elif (method == "VIRTUAL"):
668                                 delaymode = data
669                                 extramode = " | MUX_VIRTUAL_MODE%d" % delaymode
670                         elif (method == "MANUAL"):
671                                 extramode = " | MANUAL_MODE"
672                         else:
673                                 warn("Invalid method %s" % method)
675                         pin_info = get_pin_info(val) + extramode
676                         pad_short = re.sub("CTRL_CORE_PAD_", "", pad_name)
677                         offset = addr - 0x4a003400
678                         comment = (pad_short + "." + pin_name).lower()
680                         print "\t\t\t0x%03X\t(%s | MUX_MODE%d)\t/* %s */" % (offset, pin_info, muxmode, comment)
681                 print "\t\t>;"
682                 print "\t};"
683         print "};\n"
686 def linux_format_delay_regs(delayconf, per_delayconf):
687         print "&dra7_iodelay_core {"
688         for per in per_delayconf.keys():
690                 if (re.match("MMC.*", per) == None):
691                         warn("Only MMC delayconf is recommended in kernel")
693                 # Get the mode from the first entry
694                 (pad_name, pin_name, regname, del_offset, mode, adel, gdel) = per_delayconf[per][0]
696                 dtsnode = ("%s_iodelay_%s_conf" % (per, mode)).lower()
697                 print "\t%s: %s {" % (dtsnode, dtsnode)
698                 print "\t\tpinctrl-single,pins = <"
699                 for i in per_delayconf[per]:
700                         (pad_name, pin_name, regname, del_offset, mode, adel, gdel) = i
702                         print "\t\t\t0x%03X (A_DELAY(%d) | G_DELAY(%d))\t/* %s */" % (del_offset, adel, gdel, regname)
703                 print "\t\t>;"
704                 print "\t};"
705         print "};\n"
707 # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # #
709 # Generate output in bios format
710 def bios_format_pad_regs(padconf, per_padconf):
711         for i in padconf:
712                 (pad_name, pin_name, addr, val, mode, delayinfo) = i
714                 delaylist = []
715                 (method, data) = delayinfo
716                 if (method == "VIRTUAL"):
717                         virt_mode = data
718                         val = val | ( virt_mode<< 4)
719                         val = val | (1 << 8)
720                 elif (method == "MANUAL"):
721                         delaylist = data
722                         val = val | (1 << 8)
724                 offset = addr - 0x4a003400
725                 out_delreg = out_adel = out_gdel = 0
726                 in_delreg  = in_adel  = in_gdel  = 0
727                 oen_delreg = oen_adel = oen_gdel = 0
729                 for j in delaylist:
730                         (regname, adel, gdel) = j
731                         if (re.match(".*_IN", regname) != None):
732                                 in_delreg = xml_iodelay_get_reg(regname)
733                                 in_adel = adel
734                                 in_gdel = gdel
735                         elif (re.match(".*_OEN", regname) != None):
736                                 oen_delreg = xml_iodelay_get_reg(regname)
737                                 oen_adel = adel
738                                 oen_gdel = gdel
739                         elif (re.match(".*_OUT", regname) != None):
740                                 out_delreg = xml_iodelay_get_reg(regname)
741                                 out_adel = adel
742                                 out_gdel = gdel
743                 indel  = "{ 0x%04X, %4d, %4d , 0}" % (in_delreg,  in_adel,  in_gdel)
744                 oendel = "{ 0x%04X, %4d, %4d , 0}" % (oen_delreg, oen_adel, oen_gdel)
745                 outdel = "{ 0x%04X, %4d, %4d , 0}" % (out_delreg, out_adel, out_gdel)
746                 pin_info = get_pin_info(val)
747                 print "\t/* %s -> %s (%s) %s delaymode */" % (pad_name, pin_name, pin_info, method)
748                 print "\t{ 0x%03X, 0x%08X, %s, %s, %s }" % (offset, val, indel, oendel, outdel)
750 def bios_format_delay_regs(delayconf, per_delayconf):
751         debug("Manual delays are not configured separately")
752         debug("Delays are configured as part of the padconf step only")
754 # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # #
756 # Main execution starts here
757 # * Parse all the XML files - Get the pad data and IOdelay data
758 # * Iterate over the pad register dumps
759 # * For each pad, find out the muxmode being used and the pad direction, etc
760 # * For the muxmode being used, find out available virtual/modes
761 #   - Dump the virtual/manual modes available (based on options)
762 #   - Build up the gpio script to read the pad data using GPIO module
763 # * Select the correct mode to be used
764 #   - Check if the mode is described for the peripheral module, (from selected-modes.txt)
765 #   - Otherwise ask the user (with a menu) to decide the delaymode
766 #     => Update the selection for the whole of the peripheral module
767 #   - Worst case, skip the delaymode for this pad
768 # * Build the pad and delay register information
769 # * Create the dump for pad and delay data in linux/u-boot format
770 # * Dump the delaymode selection for each peripheral
771 # * Dump the GPIO script for each peripheral (all pads grouped together)
774 # List of all the pads being configured
775 padconf = []
776 # List of all the delay registers being configured (for manual mode)
777 delayconf = []
778 # Dictionary of pads grouped by peripheral/module
779 per_padconf = {}
780 # Dictionary of delay registers grouped by peripheral/module
781 per_delayconf = {}
783 if(args.check_xml):
784         xml_check_correctness(modehelp)
785         exit()
787 # Start iterating over each pad
788 for i in range(0, 260):
789         # Find out the muxmode and pad direction, etc
790         addr = 0x4a003400 + i * 4
791         offset = 0x1400 + i * 4
792         dts_offset = offset - 0x1400
794         if (addr not in reglist):
795                 warn("Register dump for pad 0x%X not found" % addr)
796                 continue
797         val = regmap[addr]
798         muxmode = val & 0xf
800         # Find out the pin based on the muxmode
801         pad_name = xml_pad_get_name(offset)
802         pin_name = xml_model_get_signal(offset, muxmode)
803         if (pad_name == "Unknown" or pin_name == "Unknown"):
804                 warn("Cannot find out Pad/Pin name for PAD address 0x%X (%s[%s] = %s)" \
805                 % (addr, pad_name, muxmode, pin_name))
806                 continue
807         if (pin_name == "DRIVER"):
808                 continue
810         # Find out if the delaymode for this module is already selected
811         match = re.match("([^_]+)_.*", pin_name)
812         if (match):
813                 module = match.groups(0)[0]
814         else:
815                 module = pin_name
817         if (args.module != "" and re.match("%s" % args.module, module) == None):
818                 continue
820         # It is recommended to keep the reset value of the slewcontrol bit
821         # Find out the reset value from XML and update if required
822         if (args.resetslew):
823                 val |= (xml_pad_get_slew(offset) & 0x1) << 19
825         debug("PAD: %s: Addr= 0x%08X Value = 0x%08X \"%s\"" \
826                 % (pad_name, addr, val, pin_name))
828         # Find out all the possible virtual, manual modes fot the specific pad -> pin combination
829         (virt, man) = xml_find_delaymodes(pad_name, muxmode)
831         if (args.gpio == True):
832                 mode = "LEGACY"
833         else:
834                 # Need to select one out of allowed modes
835                 mode = select_mode(pad_name, pin_name, module, virt, man, modehelp, sel)
837         # Remember the selection for that module, for later reuse
838         if (args.strict == False and module not in sel.keys()):
839                 sel[module] = mode
841         if (mode == "SKIP"):
842                 continue
843         elif (mode == "LEGACY"):
844                 delayinfo = ("LEGACY", "")
845         elif (mode in virt):
846                 delayinfo = ("VIRTUAL", virt[mode])
847         elif (mode in man):
848                 delayinfo = ("MANUAL", man[mode])
849         else:
850                 error("Unknown mode '%s' selected" % mode)
851                 continue
853         debug("  => Using mode %s" % mode)
854         paddata = (pad_name, pin_name, addr, val, mode, delayinfo)
855         if (module not in per_padconf.keys()):
856                 per_padconf[module] = []
857         padconf.append(paddata)
858         per_padconf[module].append(paddata)
860         if(mode not in man):
861                 continue
863         # Add the delay data if using manual mode
864         for regval in man[mode]:
865                 (regname, adel, gdel) = regval
866                 del_offset = xml_iodelay_get_reg(regname)
867                 if (del_offset == 0):
868                         error("Can't find delay offset of register %s" % regname)
869                         break
870                 debug("  => Manual delay[%s] = (%d, %d)" % (regname, adel, gdel))
871                 delaydata = (pad_name, pin_name, regname, del_offset, mode, adel, gdel)
872                 if (module not in per_delayconf.keys()):
873                         per_delayconf[module] = []
874                 delayconf.append(delaydata)
875                 per_delayconf[module].append(delaydata)
877 if(args.gpio == True):
878         pad_dump_gpio(padconf, per_padconf)
879         exit()
881 format_pad_regs(padconf, per_padconf)
882 format_delay_regs(delayconf, per_delayconf)
884 if (args.interactive):
885         # Summary of the generated data
886         print ""
887         print "Total PAD registers: %d" % len(padconf)
888         print "Total DELAY registers: %d" % len(delayconf)
889         print ""
890         # Dump the final selection for reuse
891         print "Selected modes for each peripheral module\n"
892         for group in sel:
893                 print "%s,\t%s" % (group, sel[group])
894         print ""
895 # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # # #