+++++ Python Script to generate the IOdelay values +++++ IODELAY CONFIGURATION ===================== When migrating to adapt to the IOdelay framework on DRA7xx SoCs, * All the pinmuxing is performed from the bootloader ** Allows to select the muxmode and pad direction ** LEGACY_MODE padmux * For some pads, along with mux mode, extra delay mode has to be configured ** Allows to select one of the precoded delays from the ROM ** VIRTUAL_MODE delay * For some pads, additional registers have to be written with delays ** Allows to manually set input/output delays per pad ** MANUAL_MODE delay DESCRIPTION =========== This script is used for generating the padmux and IO delay data for the existing use cases based on group selection of delay modes. For each pad, depending on the muxmode that is being used, there can be multiple choices of choosing the delay - LEGACY, VIRTUAL_MODE or MANUAL_MODE For LEGACY_MODE, nothing special has to be done. Depending on the way the pad is being used, a specific delay mode has to be chosen out of the multiple possibilities. This script uses the register dump of the PAD registers from a running kernel. From this, it derives the muxmode and pad directions used in the system. Now the only thing that the script needs to add is the delay information. Using PCT(Pad Configuration Tool) XML files as reference, the script finds out all the possible options for VIRTUAL and MANUAL mode delays. Depending on the way the hardware is used, user has to choose a specific mode. User has to only select the delay mode to be used by a PAD group so that the script selects them whenever in conflict. Optionally, the script can run interactively to build up this data via menu based selection. FILES ===== iodelay-autogen.py - Python script guidelines.txt - Describes when a specific delay mode is to be used XMLFiles/*.xml - XML data from Pad Config Tool Contains available delay modes and values selected-modes.txt - User selected delay modes to be used by script ctrl-core.dump - Register dump of all the PAD registers generate-all-modes.sh - Helper script to generate all modes of a peripheral EXAMPLES ======== ## For getting the register dump of the PAD registers from "linux" system:- - Run this command on target "omapconf dump 0x4a003400 0x4a00380c" and save the output to a file called ctrl-core.dump - Please refer to the usage and help message for more info. $> ./iodelay-autogen.py --help ## For getting the register dump of the PAD registers from "bios" system:- - For bios use cases, omapconf is not available. Use the CCS tool to create the dump of pad registers using gel script 'get-pad-dump.gel' #1 For generating the IOdelay values from the old kernel interactively:- - Run the script interactively with -i option (default). - Select the delay mode for the PAD group in conflict. Refer to the guidelines.txt for description about that delay mode. - For the peripherals in doubt, you can skip the entire PAD group - Selection of each PAD group and the selected mode is printed at end. - e.g. to generate the pad/delay data first time, run $> ./iodelay-autogen.py -i 1 $> ./iodelay-autogen.py #2 For generating the IOdelay values for a specific module only:- - Use the module filter to specify the desired module. The script would only generate output wrt the module specified. - e.g. to generate the pad/delay data only for VIN3A interface, run $> ./iodelay-autogen.py -m VIN3A #3 For generating the IOdelay values for kernel format:- - Use the format option -f to specify the output format. - e.g. for generating pad/delay data for MMC1 in DTS format, run $> ./iodelay-autogen.py -m MMC1 -f linux #4 For generating MMC data in kernel DTS format:- - Use the generate-all-modes.sh helper similar to the python tool. - e.g. for generating MMC1 for J6eco SR1.0, run #> ./generate-all-modes.sh -p dra72x -m MMC1 -r 1.0 -f linux #5 For generating signal probe script for VIN1A signals:- - Use the module filter for to specify the module. - Enable '--gpio' option #> ./iodelay-autogen.py -m VIN1A --gpio - This would create vin1a-probe.sh which can be used on target TODO ==== SUPPORT AND BUGS ================ - Some PAD registers are hidden in the XML, so warnings for them are expected - I2C1 PADs do not have mux mode names, so errors for them are expected For any queries and support on this script, please write to "Nikhil Devshatwar"