index 1e7fd8a6731e33882ac8643f22f75d80b0fe196f..41f251650e6e8b474ecd8ff04e49364ada927218 100644 (file)
--- a/README
+++ b/README
selected-modes.txt - User selected delay modes to be used by script
ctrl-core.dump - Register dump of all the PAD registers
-config-iodelay-autogen - Turn on/off common options for the script
+generate-all-modes.sh - Helper script to generate all modes of a peripheral
EXAMPLES
#0 For getting the register dump of the PAD registers:-
- Run this command on target "omapconf dump 0x4a003400 0x4a00380c"
and save the output to a file called ctrl-core.dump
+ - Please refer to the usage and help message for more info.
+ $> ./iodelay-autogen.py --help
#1 For generating the IOdelay values from the old kernel interactively:-
- - Set interactive = 1 in the config-iodelay-autogen and run
- $> python iodelay-autogen.py
+ - Run the script interactively with -i option (default).
- Select the delay mode for the PAD group in conflict. Refer to the
guidelines.txt for description about that delay mode.
- For the peripherals in doubt, you can skip the entire PAD group
- Selection of each PAD group and the selected mode is printed at end.
+ - e.g. to generate the pad/delay data first time, run
+ $> ./iodelay-autogen.py -i 1
+ $> ./iodelay-autogen.py
#2 For generating the IOdelay values for a specific module only:-
- - Update the selected-modes.txt with an entry for the correct delay mode
- to be used for the specific module.
- - Set interactive = 0 in the config-iodelay-autogen and run
- $> python iodelay-autogen.py | grep "PAD:" #Dumps all pad entries
- $> python iodelay-autogen.py | grep "DELAY:" #Dumps all manual delays
-
-#3 For generating the IOdelay values for all of the pads:-
- - Create the selected-modes.txt either by following step #1 or
- by referring to the guidelines.txt
- - Set auto_decide = 1 in config-iodelay-autogen and run
- $> python iodelay-autogen.py
- - All the PAD and DELAY registers are dumped including the LEGACY_MODE
- for which no manual/virtual modes are needed.
+ - Use the module filter to specify the desired module.
+ The script would only generate output wrt the module specified.
+ - e.g. to generate the pad/delay data only for VIN3A interface, run
+ $> ./iodelay-autogen.py -m VIN3A
+
+#3 For generating the IOdelay values for kernel format:-
+ - Use the format option -f to specify the output format.
+ - e.g. for generating pad/delay data for MMC1 in DTS format, run
+ $> ./iodelay-autogen.py -m MMC1 -f linux
+
+#4 For generating MMC data in kernel DTS format:-
+ - Use the generate-all-modes.sh helper similar to the python tool.
+ - e.g. for generating MMC1 for J6eco SR1.0, run
+ #> ./generate-all-modes.sh -p dra72x -m MMC1 -r 1.0 -f linux
TODO
====
-- Do not dump the data immediately, save in a list and dump later
-- Create output in u-boot or kernel format
-- Dump data sorted by register address or by PAD group
-
SUPPORT AND BUGS
================