PCT XML: Add support for ES2.0 silicon revision
[glsdk/iodelay-config.git] / README
diff --git a/README b/README
index 1e7fd8a6731e33882ac8643f22f75d80b0fe196f..93f5b3c702ee8ecb43c73fe07474330281f3bcb7 100644 (file)
--- a/README
+++ b/README
@@ -50,7 +50,6 @@ XMLFiles/*.xml           - XML data from Pad Config Tool
 
 selected-modes.txt       - User selected delay modes to be used by script
 ctrl-core.dump           - Register dump of all the PAD registers
-config-iodelay-autogen   - Turn on/off common options for the script
 
 
 EXAMPLES
@@ -58,36 +57,32 @@ EXAMPLES
 #0 For getting the register dump of the PAD registers:-
     - Run this command on target "omapconf dump 0x4a003400 0x4a00380c"
       and save the output to a file called ctrl-core.dump
+    - Please refer to the usage and help message for more info.
+      $> ./iodelay-autogen.py --help
 
 #1 For generating the IOdelay values from the old kernel interactively:-
-    - Set interactive = 1 in the config-iodelay-autogen and run
-      $> python iodelay-autogen.py
+    - Run the script interactively with -i option (default).
     - Select the delay mode for the PAD group in conflict. Refer to the
       guidelines.txt for description about that delay mode.
     - For the peripherals in doubt, you can skip the entire PAD group
     - Selection of each PAD group and the selected mode is printed at end.
+    - e.g. to generate the pad/delay data first time, run
+      $> ./iodelay-autogen.py -i 1
+      $> ./iodelay-autogen.py
 
 #2 For generating the IOdelay values for a specific module only:-
-    - Update the selected-modes.txt with an entry for the correct delay mode
-      to be used for the specific module.
-    - Set interactive = 0 in the config-iodelay-autogen and run
-      $> python iodelay-autogen.py | grep "PAD:"     #Dumps all pad entries
-      $> python iodelay-autogen.py | grep "DELAY:"   #Dumps all manual delays
-
-#3 For generating the IOdelay values for all of the pads:-
-    - Create the selected-modes.txt either by following step #1 or
-      by referring to the guidelines.txt
-    - Set auto_decide = 1 in config-iodelay-autogen and run
-      $> python iodelay-autogen.py
-    - All the PAD and DELAY registers are dumped including the LEGACY_MODE
-      for which no manual/virtual modes are needed.
+    - Use the module filter to specify the desired module.
+      The script would only generate output wrt the module specified.
+    - e.g. to generate the pad/delay data only for VIN3A interface, run
+      $> ./iodelay-autogen.py -m VIN3A
+
+#3 For generating the IOdelay values for kernel format:-
+    - Use the format option -f to specify the output format.
+    - e.g. for generating pad/delay data for MMC1 in DTS format, run
+      $> ./iodelay-autogen.py -m MMC1 -f linux
 
 TODO
 ====
-- Do not dump the data immediately, save in a list and dump later
-- Create output in u-boot or kernel format
-- Dump data sorted by register address or by PAD group
-
 
 SUPPORT AND BUGS
 ================