[GLP] Libdce linux implementation
authorSathishkumar <x0203598@ti.com>
Tue, 30 Jul 2013 05:50:14 +0000 (11:20 +0530)
committerSaurabh Bipin Chandra <a0131926@ti.com>
Tue, 27 Aug 2013 21:12:42 +0000 (02:42 +0530)
commitf71e00630af23f1dd7d2a0df87d9b5b524c823a8
tree956d57896e212423862da2031aabaa50ba2d7f01
parent17668bcb5a1f7f9db2ba225b1825bc55365c3e66
[GLP] Libdce linux implementation

make install & libdce.c issue fix

1. make install has been fixed. libdce.h will be installed in /usr/include,
   libdce.so files in /usr/lib and libdce.pc in /usr/lib/pkgconfig on using
   --prefix=/usr. By default the prefix is /usr/local.
2. init and deinit calls are removed from libdce.h
3. dce_set_fd and dce_get_fd calls are implemented in libdce.c
4. configure.ac checks for libmmrpc and makefile.am modified to link with libmmrpc.

configure.ac and makefile.am modified

1. Codec_engine,xdctolls,framework_components,ipc,xdctools and xdaias paths needs
   to be exported. Configure.ac checks for the exported paths.
2. Makefile.am is modified to have the exported paths in the include directories list
   for the compiler.

Modifications done after review

1. Comments added in memplugin_linux.c. White spaces removed manually and cleaned up
   libdce.c, memplugin.h. dce_priv.h is modified to have File and line number in the
   logs. linux/dce.h file is removed.

Libdce modifications for linux

Linux Specific libdce functionality added.
1. memplugin calls specific to linux are added in memplugin_linux.c
2. Error and debug logs implementation for linux in dce_priv.h
3. xll and wayland specific files are moved to linux folder

Change-Id: Ib41e6a52d902376cdabbb939dee7585944720d92
Signed-off-by: Saurabh Bipin Chandra <a0131926@ti.com>
Signed-off-by: Sathishkumar <x0203598@ti.com>
12 files changed:
Makefile.am [new file with mode: 0644]
autogen.sh [new file with mode: 0755]
configure.ac [new file with mode: 0644]
dce_priv.h
libdce.c
libdce.h
libdce.pc.in [new file with mode: 0644]
linux/libdce-x11.c [new file with mode: 0644]
linux/wayland-drm-client-protocol.h [new file with mode: 0644]
linux/wayland-drm-protocol.c [new file with mode: 0644]
memplugin.h
memplugin_linux.c [new file with mode: 0644]