]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - glsdk/libdrm.git/blob - README
man: convert manpages to XML instead of plain troff
[glsdk/libdrm.git] / README
1 libdrm - userspace library for drm
3 This  is libdrm,  a userspace  library for  accessing the  DRM, direct
4 rendering  manager, on  Linux,  BSD and  other  operating systes  that
5 support the  ioctl interface.  The library  provides wrapper functions
6 for the  ioctls to avoid  exposing the kernel interface  directly, and
7 for chipsets with drm memory manager, support for tracking relocations
8 and  buffers.   libdrm  is  a  low-level library,  typically  used  by
9 graphics drivers  such as the Mesa  DRI drivers, the  X drivers, libva
10 and  similar projects.  New  functionality in  the kernel  DRM drivers
11 typically requires  a new  libdrm, but a  new libdrm will  always work
12 with an older kernel.
15 Compiling
16 ---------
18 libdrm  is  a  standard  autotools  packages and  follows  the  normal
19 configure, build  and install steps.   The first step is  to configure
20 the package, which is done by running the configure shell script:
22         ./configure
24 By default, libdrm  will install into the /usr/local/  prefix.  If you
25 want  to  install   this  DRM  to  replace  your   system  copy,  pass
26 --prefix=/usr and  --exec-prefix=/ to configure.  If  you are building
27 libdrm  from a  git checkout,  you first  need to  run  the autogen.sh
28 script.  You can  pass any options to autogen.sh  that you would other
29 wise  pass to configure,  or you  can just  re-run configure  with the
30 options you need once autogen.sh finishes.
32 Next step is to build libdrm:
34         make
36 and once make finishes successfully, install the package using
38         make install
40 If you are install into a system location, you will need to be root to
41 perform the install step.