]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - glsdk/libdrm.git/blob - RELEASING
radeon: don't force stencil tile split to 0
[glsdk/libdrm.git] / RELEASING
1 The release criteria for libdrm is essentially "if you need a release,
2 make one".  There is no designated release engineer or maintainer.
3 Anybody is free to make a release if there's a certain feature or bug
4 fix they need in a released version of libdrm.
6 When new ioctl definitions are merged into drm-next, we will add
7 support to libdrm, at which point we typically create a new release.
8 However, this is up to whoever is driving the feature in question.
10 Follow these steps to release a new version of libdrm:
12   1) Ensure that there are no local, uncommitted/unpushed
13      modifications. You're probably in a good state if both "git diff
14      HEAD" and "git log master..origin/master" give no output.
16   3) Bump the version number in configure.ac. We seem to have settled
17      for 2.4.x as the versioning scheme for libdrm, so just bump the
18      micro version.
20   4) Run autoconf and then re-run ./configure so the build system
21      picks up the new version number.
23   5) Verify that the code passes "make distcheck".  libdrm is tricky
24      to distcheck since the test suite will need to become drm master.
25      This means that you need to run it outside X, that is, in text
26      mode (KMS or no KMS doesn't matter).
28      Running "make distcheck" should result in no warnings or errors
29      and end with a message of the form:
31         =============================================
32         libdrm-X.Y.Z archives ready for distribution:
33         libdrm-X.Y.Z.tar.gz
34         libdrm-X.Y.Z.tar.bz2
35         =============================================
37      Make sure that the version number reported by distcheck and in
38      the tarball names matches the number you bumped to in configure.ac.
40   6) Commit the configure.ac change and make an annotated tag for that
41      commit with the version number of the release as the name and a
42      message of "libdrm X.Y.Z".  For example, for the 2.4.16 release
43      the command is:
45         git tag -a 2.4.16 -m "libdrm 2.4.16"
47   7) Push the commit and tag by saying
49         git push --tags origin master
51      assuming the remote for the upstream libdrm repo is called origin.
53   6) Use the release.sh script from the xorg/util/modular repo to
54      upload the tarballs to the freedesktop.org download area and
55      create an annouce email template.  The script takes three
56      arguments: a "section", the previous tag and the new tag we just
57      created.  For 2.4.16 again, the command is:
59         ../modular/release.sh libdrm 2.4.15 2.4.16
61      This copies the two tarballs to freedesktop.org and creates
62      libdrm-2.4.16.announce which has a detailed summary of the
63      changes, links to the tarballs, MD5 and SHA1 sums and pre-filled
64      out email headers.  Fill out the blank between the email headers
65      and the list of changes with a brief message of what changed or
66      what prompted this release.  Send out the email and you're done!