]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - glsdk/libdrm.git/blob - exynos/exynos_drm.c
DEBIAN: debianization
[glsdk/libdrm.git] / exynos / exynos_drm.c
1 /*
2  * Copyright (C) 2012 Samsung Electronics Co., Ltd.
3  *
4  * Permission is hereby granted, free of charge, to any person obtaining a
5  * copy of this software and associated documentation files (the "Software"),
6  * to deal in the Software without restriction, including without limitation
7  * the rights to use, copy, modify, merge, publish, distribute, sublicense,
8  * and/or sell copies of the Software, and to permit persons to whom the
9  * Software is furnished to do so, subject to the following conditions:
10  *
11  * The above copyright notice and this permission notice (including the next
12  * paragraph) shall be included in all copies or substantial portions of the
13  * Software.
14  *
15  * THE SOFTWARE IS PROVIDED "AS IS", WITHOUT WARRANTY OF ANY KIND, EXPRESS OR
16  * IMPLIED, INCLUDING BUT NOT LIMITED TO THE WARRANTIES OF MERCHANTABILITY,
17  * FITNESS FOR A PARTICULAR PURPOSE AND NONINFRINGEMENT.  IN NO EVENT SHALL
18  * THE AUTHORS OR COPYRIGHT HOLDERS BE LIABLE FOR ANY CLAIM, DAMAGES OR OTHER
19  * LIABILITY, WHETHER IN AN ACTION OF CONTRACT, TORT OR OTHERWISE, ARISING FROM,
20  * OUT OF OR IN CONNECTION WITH THE SOFTWARE OR THE USE OR OTHER DEALINGS IN THE
21  * SOFTWARE.
22  *
23  * Authors:
24  *    Inki Dae <inki.dae@samsung.com>
25  */
27 #ifdef HAVE_CONFIG_H
28 #include "config.h"
29 #endif
31 #include <stdlib.h>
32 #include <stdio.h>
33 #include <string.h>
34 #include <errno.h>
36 #include <sys/mman.h>
37 #include <linux/stddef.h>
39 #include <xf86drm.h>
41 #include "exynos_drm.h"
42 #include "exynos_drmif.h"
44 /*
45  * Create exynos drm device object.
46  *
47  * @fd: file descriptor to exynos drm driver opened.
48  *
49  * if true, return the device object else NULL.
50  */
51 struct exynos_device * exynos_device_create(int fd)
52 {
53         struct exynos_device *dev;
55         dev = calloc(sizeof(*dev), 1);
56         if (!dev) {
57                 fprintf(stderr, "failed to create device[%s].\n",
58                                 strerror(errno));
59                 return NULL;
60         }
62         dev->fd = fd;
64         return dev;
65 }
67 /*
68  * Destroy exynos drm device object
69  *
70  * @dev: exynos drm device object.
71  */
72 void exynos_device_destroy(struct exynos_device *dev)
73 {
74         free(dev);
75 }
77 /*
78  * Create a exynos buffer object to exynos drm device.
79  *
80  * @dev: exynos drm device object.
81  * @size: user-desired size.
82  * flags: user-desired memory type.
83  *      user can set one or more types among several types to memory
84  *      allocation and cache attribute types. and as default,
85  *      EXYNOS_BO_NONCONTIG and EXYNOS-BO_NONCACHABLE types would
86  *      be used.
87  *
88  * if true, return a exynos buffer object else NULL.
89  */
90 struct exynos_bo * exynos_bo_create(struct exynos_device *dev,
91                                                 size_t size, uint32_t flags)
92 {
93         struct exynos_bo *bo;
94         struct drm_exynos_gem_create req = {
95                 .size = size,
96                 .flags = flags,
97         };
99         if (size == 0) {
100                 fprintf(stderr, "invalid size.\n");
101                 goto fail;
102         }
104         bo = calloc(sizeof(*bo), 1);
105         if (!bo) {
106                 fprintf(stderr, "failed to create bo[%s].\n",
107                                 strerror(errno));
108                 goto err_free_bo;
109         }
111         bo->dev = dev;
113         if (drmIoctl(dev->fd, DRM_IOCTL_EXYNOS_GEM_CREATE, &req)){
114                 fprintf(stderr, "failed to create gem object[%s].\n",
115                                 strerror(errno));
116                 goto err_free_bo;
117         }
119         bo->handle = req.handle;
120         bo->size = size;
121         bo->flags = flags;
123         return bo;
125 err_free_bo:
126         free(bo);
127 fail:
128         return NULL;
131 /*
132  * Get information to gem region allocated.
133  *
134  * @dev: exynos drm device object.
135  * @handle: gem handle to request gem info.
136  * @size: size to gem object and returned by kernel side.
137  * @flags: gem flags to gem object and returned by kernel side.
138  *
139  * with this function call, you can get flags and size to gem handle
140  * through bo object.
141  *
142  * if true, return 0 else negative.
143  */
144 int exynos_bo_get_info(struct exynos_device *dev, uint32_t handle,
145                         size_t *size, uint32_t *flags)
147         int ret;
148         struct drm_exynos_gem_info req = {
149                 .handle = handle,
150         };
152         ret = drmIoctl(dev->fd, DRM_IOCTL_EXYNOS_GEM_GET, &req);
153         if (ret < 0) {
154                 fprintf(stderr, "failed to get gem object information[%s].\n",
155                                 strerror(errno));
156                 return ret;
157         }
159         *size = req.size;
160         *flags = req.flags;
162         return 0;
165 /*
166  * Destroy a exynos buffer object.
167  *
168  * @bo: a exynos buffer object to be destroyed.
169  */
170 void exynos_bo_destroy(struct exynos_bo *bo)
172         if (!bo)
173                 return;
175         if (bo->vaddr)
176                 munmap(bo->vaddr, bo->size);
178         if (bo->handle) {
179                 struct drm_gem_close req = {
180                         .handle = bo->handle,
181                 };
183                 drmIoctl(bo->dev->fd, DRM_IOCTL_GEM_CLOSE, &req);
184         }
186         free(bo);
190 /*
191  * Get a exynos buffer object from a gem global object name.
192  *
193  * @dev: a exynos device object.
194  * @name: a gem global object name exported by another process.
195  *
196  * this interface is used to get a exynos buffer object from a gem
197  * global object name sent by another process for buffer sharing.
198  *
199  * if true, return a exynos buffer object else NULL.
200  *
201  */
202 struct exynos_bo * exynos_bo_from_name(struct exynos_device *dev, uint32_t name)
204         struct exynos_bo *bo;
205         struct drm_gem_open req = {
206                 .name = name,
207         };
209         bo = calloc(sizeof(*bo), 1);
210         if (!bo) {
211                 fprintf(stderr, "failed to allocate bo[%s].\n",
212                                 strerror(errno));
213                 return NULL;
214         }
216         if (drmIoctl(dev->fd, DRM_IOCTL_GEM_OPEN, &req)) {
217                 fprintf(stderr, "failed to open gem object[%s].\n",
218                                 strerror(errno));
219                 goto err_free_bo;
220         }
222         bo->dev = dev;
223         bo->name = name;
224         bo->handle = req.handle;
226         return bo;
228 err_free_bo:
229         free(bo);
230         return NULL;
233 /*
234  * Get a gem global object name from a gem object handle.
235  *
236  * @bo: a exynos buffer object including gem handle.
237  * @name: a gem global object name to be got by kernel driver.
238  *
239  * this interface is used to get a gem global object name from a gem object
240  * handle to a buffer that wants to share it with another process.
241  *
242  * if true, return 0 else negative.
243  */
244 int exynos_bo_get_name(struct exynos_bo *bo, uint32_t *name)
246         if (!bo->name) {
247                 struct drm_gem_flink req = {
248                         .handle = bo->handle,
249                 };
250                 int ret;
252                 ret = drmIoctl(bo->dev->fd, DRM_IOCTL_GEM_FLINK, &req);
253                 if (ret) {
254                         fprintf(stderr, "failed to get gem global name[%s].\n",
255                                         strerror(errno));
256                         return ret;
257                 }
259                 bo->name = req.name;
260         }
262         *name = bo->name;
264         return 0;
267 uint32_t exynos_bo_handle(struct exynos_bo *bo)
269         return bo->handle;
272 /*
273  * Mmap a buffer to user space.
274  *
275  * @bo: a exynos buffer object including a gem object handle to be mmapped
276  *      to user space.
277  *
278  * if true, user pointer mmaped else NULL.
279  */
280 void *exynos_bo_map(struct exynos_bo *bo)
282         if (!bo->vaddr) {
283                 struct exynos_device *dev = bo->dev;
284                 struct drm_exynos_gem_mmap req = {
285                         .handle = bo->handle,
286                         .size   = bo->size,
287                 };
288                 int ret;
290                 ret = drmIoctl(dev->fd, DRM_IOCTL_EXYNOS_GEM_MMAP, &req);
291                 if (ret) {
292                         fprintf(stderr, "failed to mmap[%s].\n",
293                                 strerror(errno));
294                         return NULL;
295                 }
297                 bo->vaddr = req.mapped;
298         }
300         return bo->vaddr;
303 /*
304  * Export gem object to dmabuf as file descriptor.
305  *
306  * @dev: a exynos device object.
307  * @handle: gem handle to be exported into dmabuf as file descriptor.
308  * @fd: file descriptor to dmabuf exported from gem handle and
309  *      returned by kernel side.
310  *
311  * if true, return 0 else negative.
312  */
313 int exynos_prime_handle_to_fd(struct exynos_device *dev, uint32_t handle,
314                                         int *fd)
316         int ret;
317         struct drm_prime_handle req = {
318                 .handle = handle,
319         };
321         ret = drmIoctl(dev->fd, DRM_IOCTL_PRIME_HANDLE_TO_FD, &req);
322         if (ret) {
323                 fprintf(stderr, "failed to mmap[%s].\n",
324                         strerror(errno));
325                 return ret;
326         }
328         *fd = req.fd;
329         return 0;
332 /*
333  * Import file descriptor into gem handle.
334  *
335  * @dev: a exynos device object.
336  * @fd: file descriptor exported into dmabuf.
337  * @handle: gem handle to gem object imported from file descriptor
338  *      and returned by kernel side.
339  *
340  * if true, return 0 else negative.
341  */
342 int exynos_prime_fd_to_handle(struct exynos_device *dev, int fd,
343                                         uint32_t *handle)
345         int ret;
346         struct drm_prime_handle req = {
347                 .fd     = fd,
348         };
350         ret = drmIoctl(dev->fd, DRM_IOCTL_PRIME_FD_TO_HANDLE, &req);
351         if (ret) {
352                 fprintf(stderr, "failed to mmap[%s].\n",
353                         strerror(errno));
354                 return ret;
355         }
357         *handle = req.handle;
358         return 0;
363 /*
364  * Request Wireless Display connection or disconnection.
365  *
366  * @dev: a exynos device object.
367  * @connect: indicate whether connectoin or disconnection request.
368  * @ext: indicate whether edid data includes extentions data or not.
369  * @edid: a pointer to edid data from Wireless Display device.
370  *
371  * this interface is used to request Virtual Display driver connection or
372  * disconnection. for this, user should get a edid data from the Wireless
373  * Display device and then send that data to kernel driver with connection
374  * request
375  *
376  * if true, return 0 else negative.
377  */
378 int exynos_vidi_connection(struct exynos_device *dev, uint32_t connect,
379                                 uint32_t ext, void *edid)
381         struct drm_exynos_vidi_connection req = {
382                 .connection     = connect,
383                 .extensions     = ext,
384                 .edid           = edid,
385         };
386         int ret;
388         ret = drmIoctl(dev->fd, DRM_IOCTL_EXYNOS_VIDI_CONNECTION, &req);
389         if (ret) {
390                 fprintf(stderr, "failed to request vidi connection[%s].\n",
391                                 strerror(errno));
392                 return ret;
393         }
395         return 0;