1 /*
2 * Copyright © 2008 Intel Corporation
3 *
4 * Permission is hereby granted, free of charge, to any person obtaining a
5 * copy of this software and associated documentation files (the "Software"),
6 * to deal in the Software without restriction, including without limitation
7 * the rights to use, copy, modify, merge, publish, distribute, sublicense,
8 * and/or sell copies of the Software, and to permit persons to whom the
9 * Software is furnished to do so, subject to the following conditions:
10 *
11 * The above copyright notice and this permission notice (including the next
12 * paragraph) shall be included in all copies or substantial portions of the
13 * Software.
14 *
15 * THE SOFTWARE IS PROVIDED "AS IS", WITHOUT WARRANTY OF ANY KIND, EXPRESS OR
16 * IMPLIED, INCLUDING BUT NOT LIMITED TO THE WARRANTIES OF MERCHANTABILITY,
17 * FITNESS FOR A PARTICULAR PURPOSE AND NONINFRINGEMENT. IN NO EVENT SHALL
18 * THE AUTHORS OR COPYRIGHT HOLDERS BE LIABLE FOR ANY CLAIM, DAMAGES OR OTHER
19 * LIABILITY, WHETHER IN AN ACTION OF CONTRACT, TORT OR OTHERWISE, ARISING
20 * FROM, OUT OF OR IN CONNECTION WITH THE SOFTWARE OR THE USE OR OTHER DEALINGS
21 * IN THE SOFTWARE.
22 *
23 * Authors:
24 * Eric Anholt <eric@anholt.net>
25 *
26 */
28 /**
29 * @file intel_bufmgr_priv.h
30 *
31 * Private definitions of Intel-specific bufmgr functions and structures.
32 */
34 #ifndef INTEL_BUFMGR_PRIV_H
35 #define INTEL_BUFMGR_PRIV_H
37 /**
38 * Context for a buffer manager instance.
39 *
40 * Contains public methods followed by private storage for the buffer manager.
41 */
42 struct _drm_intel_bufmgr {
43 /**
44 * Allocate a buffer object.
45 *
46 * Buffer objects are not necessarily initially mapped into CPU virtual
47 * address space or graphics device aperture. They must be mapped
48 * using bo_map() or drm_intel_gem_bo_map_gtt() to be used by the CPU.
49 */
50 drm_intel_bo *(*bo_alloc) (drm_intel_bufmgr *bufmgr, const char *name,
51 unsigned long size, unsigned int alignment);
53 /**
54 * Allocate a buffer object, hinting that it will be used as a
55 * render target.
56 *
57 * This is otherwise the same as bo_alloc.
58 */
59 drm_intel_bo *(*bo_alloc_for_render) (drm_intel_bufmgr *bufmgr,
60 const char *name,
61 unsigned long size,
62 unsigned int alignment);
64 /**
65 * Allocate a tiled buffer object.
66 *
67 * Alignment for tiled objects is set automatically; the 'flags'
68 * argument provides a hint about how the object will be used initially.
69 *
70 * Valid tiling formats are:
71 * I915_TILING_NONE
72 * I915_TILING_X
73 * I915_TILING_Y
74 *
75 * Note the tiling format may be rejected; callers should check the
76 * 'tiling_mode' field on return, as well as the pitch value, which
77 * may have been rounded up to accommodate for tiling restrictions.
78 */
79 drm_intel_bo *(*bo_alloc_tiled) (drm_intel_bufmgr *bufmgr,
80 const char *name,
81 int x, int y, int cpp,
82 uint32_t *tiling_mode,
83 unsigned long *pitch,
84 unsigned long flags);
86 /** Takes a reference on a buffer object */
87 void (*bo_reference) (drm_intel_bo *bo);
89 /**
90 * Releases a reference on a buffer object, freeing the data if
91 * no references remain.
92 */
93 void (*bo_unreference) (drm_intel_bo *bo);
95 /**
96 * Maps the buffer into userspace.
97 *
98 * This function will block waiting for any existing execution on the
99 * buffer to complete, first. The resulting mapping is available at
100 * buf->virtual.
101 */
102 int (*bo_map) (drm_intel_bo *bo, int write_enable);
104 /**
105 * Reduces the refcount on the userspace mapping of the buffer
106 * object.
107 */
108 int (*bo_unmap) (drm_intel_bo *bo);
110 /**
111 * Write data into an object.
112 *
113 * This is an optional function, if missing,
114 * drm_intel_bo will map/memcpy/unmap.
115 */
116 int (*bo_subdata) (drm_intel_bo *bo, unsigned long offset,
117 unsigned long size, const void *data);
119 /**
120 * Read data from an object
121 *
122 * This is an optional function, if missing,
123 * drm_intel_bo will map/memcpy/unmap.
124 */
125 int (*bo_get_subdata) (drm_intel_bo *bo, unsigned long offset,
126 unsigned long size, void *data);
128 /**
129 * Waits for rendering to an object by the GPU to have completed.
130 *
131 * This is not required for any access to the BO by bo_map,
132 * bo_subdata, etc. It is merely a way for the driver to implement
133 * glFinish.
134 */
135 void (*bo_wait_rendering) (drm_intel_bo *bo);
137 /**
138 * Tears down the buffer manager instance.
139 */
140 void (*destroy) (drm_intel_bufmgr *bufmgr);
142 /**
143 * Add relocation entry in reloc_buf, which will be updated with the
144 * target buffer's real offset on on command submission.
145 *
146 * Relocations remain in place for the lifetime of the buffer object.
147 *
148 * \param bo Buffer to write the relocation into.
149 * \param offset Byte offset within reloc_bo of the pointer to
150 * target_bo.
151 * \param target_bo Buffer whose offset should be written into the
152 * relocation entry.
153 * \param target_offset Constant value to be added to target_bo's
154 * offset in relocation entry.
155 * \param read_domains GEM read domains which the buffer will be
156 * read into by the command that this relocation
157 * is part of.
158 * \param write_domains GEM read domains which the buffer will be
159 * dirtied in by the command that this
160 * relocation is part of.
161 */
162 int (*bo_emit_reloc) (drm_intel_bo *bo, uint32_t offset,
163 drm_intel_bo *target_bo, uint32_t target_offset,
164 uint32_t read_domains, uint32_t write_domain);
165 int (*bo_emit_reloc_fence)(drm_intel_bo *bo, uint32_t offset,
166 drm_intel_bo *target_bo,
167 uint32_t target_offset,
168 uint32_t read_domains,
169 uint32_t write_domain);
171 /** Executes the command buffer pointed to by bo. */
172 int (*bo_exec) (drm_intel_bo *bo, int used,
173 drm_clip_rect_t *cliprects, int num_cliprects,
174 int DR4);
176 /** Executes the command buffer pointed to by bo on the selected
177 * ring buffer
178 */
179 int (*bo_mrb_exec) (drm_intel_bo *bo, int used,
180 drm_clip_rect_t *cliprects, int num_cliprects,
181 int DR4, unsigned flags);
183 /**
184 * Pin a buffer to the aperture and fix the offset until unpinned
185 *
186 * \param buf Buffer to pin
187 * \param alignment Required alignment for aperture, in bytes
188 */
189 int (*bo_pin) (drm_intel_bo *bo, uint32_t alignment);
191 /**
192 * Unpin a buffer from the aperture, allowing it to be removed
193 *
194 * \param buf Buffer to unpin
195 */
196 int (*bo_unpin) (drm_intel_bo *bo);
198 /**
199 * Ask that the buffer be placed in tiling mode
200 *
201 * \param buf Buffer to set tiling mode for
202 * \param tiling_mode desired, and returned tiling mode
203 */
204 int (*bo_set_tiling) (drm_intel_bo *bo, uint32_t * tiling_mode,
205 uint32_t stride);
207 /**
208 * Get the current tiling (and resulting swizzling) mode for the bo.
209 *
210 * \param buf Buffer to get tiling mode for
211 * \param tiling_mode returned tiling mode
212 * \param swizzle_mode returned swizzling mode
213 */
214 int (*bo_get_tiling) (drm_intel_bo *bo, uint32_t * tiling_mode,
215 uint32_t * swizzle_mode);
217 /**
218 * Create a visible name for a buffer which can be used by other apps
219 *
220 * \param buf Buffer to create a name for
221 * \param name Returned name
222 */
223 int (*bo_flink) (drm_intel_bo *bo, uint32_t * name);
225 /**
226 * Returns 1 if mapping the buffer for write could cause the process
227 * to block, due to the object being active in the GPU.
228 */
229 int (*bo_busy) (drm_intel_bo *bo);
231 /**
232 * Specify the volatility of the buffer.
233 * \param bo Buffer to create a name for
234 * \param madv The purgeable status
235 *
236 * Use I915_MADV_DONTNEED to mark the buffer as purgeable, and it will be
237 * reclaimed under memory pressure. If you subsequently require the buffer,
238 * then you must pass I915_MADV_WILLNEED to mark the buffer as required.
239 *
240 * Returns 1 if the buffer was retained, or 0 if it was discarded whilst
241 * marked as I915_MADV_DONTNEED.
242 */
243 int (*bo_madvise) (drm_intel_bo *bo, int madv);
245 int (*check_aperture_space) (drm_intel_bo ** bo_array, int count);
247 /**
248 * Disable buffer reuse for buffers which will be shared in some way,
249 * as with scanout buffers. When the buffer reference count goes to
250 * zero, it will be freed and not placed in the reuse list.
251 *
252 * \param bo Buffer to disable reuse for
253 */
254 int (*bo_disable_reuse) (drm_intel_bo *bo);
256 /**
257 * Query whether a buffer is reusable.
258 *
259 * \param bo Buffer to query
260 */
261 int (*bo_is_reusable) (drm_intel_bo *bo);
263 /**
264 *
265 * Return the pipe associated with a crtc_id so that vblank
266 * synchronization can use the correct data in the request.
267 * This is only supported for KMS and gem at this point, when
268 * unsupported, this function returns -1 and leaves the decision
269 * of what to do in that case to the caller
270 *
271 * \param bufmgr the associated buffer manager
272 * \param crtc_id the crtc identifier
273 */
274 int (*get_pipe_from_crtc_id) (drm_intel_bufmgr *bufmgr, int crtc_id);
276 /** Returns true if target_bo is in the relocation tree rooted at bo. */
277 int (*bo_references) (drm_intel_bo *bo, drm_intel_bo *target_bo);
279 /**< Enables verbose debugging printouts */
280 int debug;
281 };
283 struct _drm_intel_context {
284 unsigned int ctx_id;
285 struct _drm_intel_bufmgr *bufmgr;
286 };
288 #define ALIGN(value, alignment) ((value + alignment - 1) & ~(alignment - 1))
289 #define ROUND_UP_TO(x, y) (((x) + (y) - 1) / (y) * (y))
290 #define ROUND_UP_TO_MB(x) ROUND_UP_TO((x), 1024*1024)
292 #endif /* INTEL_BUFMGR_PRIV_H */