omap: fix license header
[glsdk/libdrm.git] / omap / omap_drm.h
1 /* -*- mode: C; c-file-style: "k&r"; tab-width 4; indent-tabs-mode: t; -*- */
3 /*
4  * Copyright (C) 2011 Texas Instruments, Inc
5  *
6  * Permission is hereby granted, free of charge, to any person obtaining a
7  * copy of this software and associated documentation files (the "Software"),
8  * to deal in the Software without restriction, including without limitation
9  * the rights to use, copy, modify, merge, publish, distribute, sublicense,
10  * and/or sell copies of the Software, and to permit persons to whom the
11  * Software is furnished to do so, subject to the following conditions:
12  *
13  * The above copyright notice and this permission notice (including the next
14  * paragraph) shall be included in all copies or substantial portions of the
15  * Software.
16  *
17  * THE SOFTWARE IS PROVIDED "AS IS", WITHOUT WARRANTY OF ANY KIND, EXPRESS OR
18  * IMPLIED, INCLUDING BUT NOT LIMITED TO THE WARRANTIES OF MERCHANTABILITY,
19  * FITNESS FOR A PARTICULAR PURPOSE AND NONINFRINGEMENT.  IN NO EVENT SHALL
20  * THE AUTHORS OR COPYRIGHT HOLDERS BE LIABLE FOR ANY CLAIM, DAMAGES OR OTHER
21  * LIABILITY, WHETHER IN AN ACTION OF CONTRACT, TORT OR OTHERWISE, ARISING FROM,
22  * OUT OF OR IN CONNECTION WITH THE SOFTWARE OR THE USE OR OTHER DEALINGS IN THE
23  * SOFTWARE.
24  *
25  * Authors:
26  *    Rob Clark <rob@ti.com>
27  */
29 #ifndef __OMAP_DRM_H__
30 #define __OMAP_DRM_H__
32 #include "drm.h"
34 /* Please note that modifications to all structs defined here are
35  * subject to backwards-compatibility constraints.
36  */
38 #define OMAP_PARAM_CHIPSET_ID   1       /* ie. 0x3430, 0x4430, etc */
40 struct drm_omap_param {
41         uint64_t param;                 /* in */
42         uint64_t value;                 /* in (set_param), out (get_param) */
43 };
45 struct drm_omap_get_base {
46         char plugin_name[64];           /* in */
47         uint32_t ioctl_base;            /* out */
48         uint32_t __pad;
49 };
51 #define OMAP_BO_SCANOUT         0x00000001      /* scanout capable (phys contiguous) */
52 #define OMAP_BO_CACHE_MASK      0x00000006      /* cache type mask, see cache modes */
53 #define OMAP_BO_TILED_MASK      0x00000f00      /* tiled mapping mask, see tiled modes */
55 /* cache modes */
56 #define OMAP_BO_CACHED          0x00000000      /* default */
57 #define OMAP_BO_WC              0x00000002      /* write-combine */
58 #define OMAP_BO_UNCACHED        0x00000004      /* strongly-ordered (uncached) */
60 /* tiled modes */
61 #define OMAP_BO_TILED_8         0x00000100
62 #define OMAP_BO_TILED_16        0x00000200
63 #define OMAP_BO_TILED_32        0x00000300
64 #define OMAP_BO_TILED           (OMAP_BO_TILED_8 | OMAP_BO_TILED_16 | OMAP_BO_TILED_32)
66 union omap_gem_size {
67         uint32_t bytes;         /* (for non-tiled formats) */
68         struct {
69                 uint16_t width;
70                 uint16_t height;
71         } tiled;                /* (for tiled formats) */
72 };
74 struct drm_omap_gem_new {
75         union omap_gem_size size;       /* in */
76         uint32_t flags;                 /* in */
77         uint32_t handle;                /* out */
78         uint32_t __pad;
79 };
81 /* mask of operations: */
82 enum omap_gem_op {
83         OMAP_GEM_READ = 0x01,
84         OMAP_GEM_WRITE = 0x02,
85 };
87 struct drm_omap_gem_cpu_prep {
88         uint32_t handle;                /* buffer handle (in) */
89         uint32_t op;                    /* mask of omap_gem_op (in) */
90 };
92 struct drm_omap_gem_cpu_fini {
93         uint32_t handle;                /* buffer handle (in) */
94         uint32_t op;                    /* mask of omap_gem_op (in) */
95         /* TODO maybe here we pass down info about what regions are touched
96          * by sw so we can be clever about cache ops?  For now a placeholder,
97          * set to zero and we just do full buffer flush..
98          */
99         uint32_t nregions;
100         uint32_t __pad;
101 };
103 struct drm_omap_gem_info {
104         uint32_t handle;                /* buffer handle (in) */
105         uint32_t pad;
106         uint64_t offset;                /* mmap offset (out) */
107         /* note: in case of tiled buffers, the user virtual size can be
108          * different from the physical size (ie. how many pages are needed
109          * to back the object) which is returned in DRM_IOCTL_GEM_OPEN..
110          * This size here is the one that should be used if you want to
111          * mmap() the buffer:
112          */
113         uint32_t size;                  /* virtual size for mmap'ing (out) */
114         uint32_t __pad;
115 };
117 #define DRM_OMAP_GET_PARAM              0x00
118 #define DRM_OMAP_SET_PARAM              0x01
119 #define DRM_OMAP_GET_BASE               0x02
120 #define DRM_OMAP_GEM_NEW                0x03
121 #define DRM_OMAP_GEM_CPU_PREP           0x04
122 #define DRM_OMAP_GEM_CPU_FINI           0x05
123 #define DRM_OMAP_GEM_INFO               0x06
124 #define DRM_OMAP_NUM_IOCTLS             0x07
126 #define DRM_IOCTL_OMAP_GET_PARAM        DRM_IOWR(DRM_COMMAND_BASE + DRM_OMAP_GET_PARAM, struct drm_omap_param)
127 #define DRM_IOCTL_OMAP_SET_PARAM        DRM_IOW (DRM_COMMAND_BASE + DRM_OMAP_SET_PARAM, struct drm_omap_param)
128 #define DRM_IOCTL_OMAP_GET_BASE         DRM_IOWR(DRM_COMMAND_BASE + DRM_OMAP_GET_BASE, struct drm_omap_get_base)
129 #define DRM_IOCTL_OMAP_GEM_NEW          DRM_IOWR(DRM_COMMAND_BASE + DRM_OMAP_GEM_NEW, struct drm_omap_gem_new)
130 #define DRM_IOCTL_OMAP_GEM_CPU_PREP     DRM_IOW (DRM_COMMAND_BASE + DRM_OMAP_GEM_CPU_PREP, struct drm_omap_gem_cpu_prep)
131 #define DRM_IOCTL_OMAP_GEM_CPU_FINI     DRM_IOW (DRM_COMMAND_BASE + DRM_OMAP_GEM_CPU_FINI, struct drm_omap_gem_cpu_fini)
132 #define DRM_IOCTL_OMAP_GEM_INFO         DRM_IOWR(DRM_COMMAND_BASE + DRM_OMAP_GEM_INFO, struct drm_omap_gem_info)
134 #endif /* __OMAP_DRM_H__ */