/* * Copyright 2012 Red Hat Inc. * * Permission is hereby granted, free of charge, to any person obtaining a * copy of this software and associated documentation files (the "Software"), * to deal in the Software without restriction, including without limitation * the rights to use, copy, modify, merge, publish, distribute, sublicense, * and/or sell copies of the Software, and to permit persons to whom the * Software is furnished to do so, subject to the following conditions: * * The above copyright notice and this permission notice shall be included in * all copies or substantial portions of the Software. * * THE SOFTWARE IS PROVIDED "AS IS", WITHOUT WARRANTY OF ANY KIND, EXPRESS OR * IMPLIED, INCLUDING BUT NOT LIMITED TO THE WARRANTIES OF MERCHANTABILITY, * FITNESS FOR A PARTICULAR PURPOSE AND NONINFRINGEMENT. IN NO EVENT SHALL * THE COPYRIGHT HOLDER(S) OR AUTHOR(S) BE LIABLE FOR ANY CLAIM, DAMAGES OR * OTHER LIABILITY, WHETHER IN AN ACTION OF CONTRACT, TORT OR OTHERWISE, * ARISING FROM, OUT OF OR IN CONNECTION WITH THE SOFTWARE OR THE USE OR * OTHER DEALINGS IN THE SOFTWARE. * * Authors: Ben Skeggs */ #ifdef HAVE_CONFIG_H #include #endif #include #include #include #include #include #include #include #include #include #include #include "libdrm_lists.h" #include "nouveau_drm.h" #include "nouveau.h" #include "private.h" #ifdef DEBUG uint32_t nouveau_debug = 0; static void debug_init(char *args) { if (args) { int n = strtol(args, NULL, 0); if (n >= 0) nouveau_debug = n; } } #endif /* this is the old libdrm's version of nouveau_device_wrap(), the symbol * is kept here to prevent AIGLX from crashing if the DDX is linked against * the new libdrm, but the DRI driver against the old */ int nouveau_device_open_existing(struct nouveau_device **pdev, int close, int fd, drm_context_t ctx) { return -EACCES; } int nouveau_device_wrap(int fd, int close, struct nouveau_device **pdev) { struct nouveau_device_priv *nvdev = calloc(1, sizeof(*nvdev)); struct nouveau_device *dev = &nvdev->base; uint64_t chipset, vram, gart, bousage; drmVersionPtr ver; int ret; #ifdef DEBUG debug_init(getenv("NOUVEAU_LIBDRM_DEBUG")); #endif if (!nvdev) return -ENOMEM; nvdev->base.fd = fd; ver = drmGetVersion(fd); if (ver) dev->drm_version = (ver->version_major << 24) | (ver->version_minor << 8) | ver->version_patchlevel; drmFreeVersion(ver); if ( dev->drm_version != 0x00000010 && (dev->drm_version < 0x01000000 || dev->drm_version >= 0x02000000)) { nouveau_device_del(&dev); return -EINVAL; } ret = nouveau_getparam(dev, NOUVEAU_GETPARAM_CHIPSET_ID, &chipset); if (ret == 0) ret = nouveau_getparam(dev, NOUVEAU_GETPARAM_FB_SIZE, &vram); if (ret == 0) ret = nouveau_getparam(dev, NOUVEAU_GETPARAM_AGP_SIZE, &gart); if (ret) { nouveau_device_del(&dev); return ret; } ret = nouveau_getparam(dev, NOUVEAU_GETPARAM_HAS_BO_USAGE, &bousage); if (ret == 0) nvdev->have_bo_usage = (bousage != 0); nvdev->close = close; DRMINITLISTHEAD(&nvdev->bo_list); nvdev->base.object.oclass = NOUVEAU_DEVICE_CLASS; nvdev->base.lib_version = 0x01000000; nvdev->base.chipset = chipset; nvdev->base.vram_size = vram; nvdev->base.gart_size = gart; nvdev->base.vram_limit = (nvdev->base.vram_size * 80) / 100; nvdev->base.gart_limit = (nvdev->base.gart_size * 80) / 100; *pdev = &nvdev->base; return 0; } int nouveau_device_open(const char *busid, struct nouveau_device **pdev) { int ret = -ENODEV, fd = drmOpen("nouveau", busid); if (fd >= 0) { ret = nouveau_device_wrap(fd, 1, pdev); if (ret) drmClose(fd); } return ret; } void nouveau_device_del(struct nouveau_device **pdev) { struct nouveau_device_priv *nvdev = nouveau_device(*pdev); if (nvdev) { if (nvdev->close) drmClose(nvdev->base.fd); free(nvdev->client); free(nvdev); *pdev = NULL; } } int nouveau_getparam(struct nouveau_device *dev, uint64_t param, uint64_t *value) { struct drm_nouveau_getparam r = { param, 0 }; int fd = dev->fd, ret = drmCommandWriteRead(fd, DRM_NOUVEAU_GETPARAM, &r, sizeof(r)); *value = r.value; return ret; } int nouveau_setparam(struct nouveau_device *dev, uint64_t param, uint64_t value) { struct drm_nouveau_setparam r = { param, value }; return drmCommandWrite(dev->fd, DRM_NOUVEAU_SETPARAM, &r, sizeof(r)); } int nouveau_client_new(struct nouveau_device *dev, struct nouveau_client **pclient) { struct nouveau_device_priv *nvdev = nouveau_device(dev); struct nouveau_client_priv *pcli; int id = 0, i, ret = -ENOMEM; uint32_t *clients; for (i = 0; i < nvdev->nr_client; i++) { id = ffs(nvdev->client[i]) - 1; if (id >= 0) goto out; } clients = realloc(nvdev->client, sizeof(uint32_t) * (i + 1)); if (!clients) return ret; nvdev->client = clients; nvdev->client[i] = 0; nvdev->nr_client++; out: pcli = calloc(1, sizeof(*pcli)); if (pcli) { nvdev->client[i] |= (1 << id); pcli->base.device = dev; pcli->base.id = (i * 32) + id; ret = 0; } *pclient = &pcli->base; return ret; } void nouveau_client_del(struct nouveau_client **pclient) { struct nouveau_client_priv *pcli = nouveau_client(*pclient); struct nouveau_device_priv *nvdev; if (pcli) { int id = pcli->base.id; nvdev = nouveau_device(pcli->base.device); nvdev->client[id / 32] &= ~(1 << (id % 32)); free(pcli->kref); free(pcli); } } int nouveau_object_new(struct nouveau_object *parent, uint64_t handle, uint32_t oclass, void *data, uint32_t length, struct nouveau_object **pobj) { struct nouveau_device *dev; struct nouveau_object *obj; int ret = -EINVAL; if (length == 0) length = sizeof(struct nouveau_object *); obj = malloc(sizeof(*obj) + length); obj->parent = parent; obj->handle = handle; obj->oclass = oclass; obj->length = length; obj->data = obj + 1; if (data) memcpy(obj->data, data, length); *(struct nouveau_object **)obj->data = obj; dev = nouveau_object_find(obj, NOUVEAU_DEVICE_CLASS); switch (parent->oclass) { case NOUVEAU_DEVICE_CLASS: switch (obj->oclass) { case NOUVEAU_FIFO_CHANNEL_CLASS: { if (dev->chipset < 0xc0) ret = abi16_chan_nv04(obj); else ret = abi16_chan_nvc0(obj); } break; default: break; } break; case NOUVEAU_FIFO_CHANNEL_CLASS: switch (obj->oclass) { case NOUVEAU_NOTIFIER_CLASS: ret = abi16_ntfy(obj); break; default: ret = abi16_engobj(obj); break; } default: break; } if (ret) { free(obj); return ret; } *pobj = obj; return 0; } void nouveau_object_del(struct nouveau_object **pobj) { struct nouveau_object *obj = *pobj; struct nouveau_device *dev; if (obj) { dev = nouveau_object_find(obj, NOUVEAU_DEVICE_CLASS); if (obj->oclass == NOUVEAU_FIFO_CHANNEL_CLASS) { struct drm_nouveau_channel_free req; req.channel = obj->handle; drmCommandWrite(dev->fd, DRM_NOUVEAU_CHANNEL_FREE, &req, sizeof(req)); } else { struct drm_nouveau_gpuobj_free req; req.channel = obj->parent->handle; req.handle = obj->handle; drmCommandWrite(dev->fd, DRM_NOUVEAU_GPUOBJ_FREE, &req, sizeof(req)); } } free(obj); *pobj = NULL; } void * nouveau_object_find(struct nouveau_object *obj, uint32_t pclass) { while (obj && obj->oclass != pclass) { obj = obj->parent; if (pclass == NOUVEAU_PARENT_CLASS) break; } return obj; } static void nouveau_bo_del(struct nouveau_bo *bo) { struct nouveau_bo_priv *nvbo = nouveau_bo(bo); struct drm_gem_close req = { bo->handle }; DRMLISTDEL(&nvbo->head); if (bo->map) munmap(bo->map, bo->size); drmIoctl(bo->device->fd, DRM_IOCTL_GEM_CLOSE, &req); free(nvbo); } int nouveau_bo_new(struct nouveau_device *dev, uint32_t flags, uint32_t align, uint64_t size, union nouveau_bo_config *config, struct nouveau_bo **pbo) { struct nouveau_device_priv *nvdev = nouveau_device(dev); struct nouveau_bo_priv *nvbo = calloc(1, sizeof(*nvbo)); struct nouveau_bo *bo = &nvbo->base; int ret; if (!nvbo) return -ENOMEM; atomic_set(&nvbo->refcnt, 1); bo->device = dev; bo->flags = flags; bo->size = size; ret = abi16_bo_init(bo, align, config); if (ret) { free(nvbo); return ret; } DRMLISTADD(&nvbo->head, &nvdev->bo_list); *pbo = bo; return 0; } int nouveau_bo_wrap(struct nouveau_device *dev, uint32_t handle, struct nouveau_bo **pbo) { struct nouveau_device_priv *nvdev = nouveau_device(dev); struct drm_nouveau_gem_info req = { .handle = handle }; struct nouveau_bo_priv *nvbo; int ret; DRMLISTFOREACHENTRY(nvbo, &nvdev->bo_list, head) { if (nvbo->base.handle == handle) { *pbo = NULL; nouveau_bo_ref(&nvbo->base, pbo); return 0; } } ret = drmCommandWriteRead(dev->fd, DRM_NOUVEAU_GEM_INFO, &req, sizeof(req)); if (ret) return ret; nvbo = calloc(1, sizeof(*nvbo)); if (nvbo) { atomic_set(&nvbo->refcnt, 1); nvbo->base.device = dev; abi16_bo_info(&nvbo->base, &req); DRMLISTADD(&nvbo->head, &nvdev->bo_list); *pbo = &nvbo->base; return 0; } return -ENOMEM; } int nouveau_bo_name_ref(struct nouveau_device *dev, uint32_t name, struct nouveau_bo **pbo) { struct nouveau_device_priv *nvdev = nouveau_device(dev); struct nouveau_bo_priv *nvbo; struct drm_gem_open req = { .name = name }; int ret; DRMLISTFOREACHENTRY(nvbo, &nvdev->bo_list, head) { if (nvbo->name == name) { *pbo = NULL; nouveau_bo_ref(&nvbo->base, pbo); return 0; } } ret = drmIoctl(dev->fd, DRM_IOCTL_GEM_OPEN, &req); if (ret == 0) { ret = nouveau_bo_wrap(dev, req.handle, pbo); nouveau_bo((*pbo))->name = name; } return ret; } int nouveau_bo_name_get(struct nouveau_bo *bo, uint32_t *name) { struct drm_gem_flink req = { .handle = bo->handle }; struct nouveau_bo_priv *nvbo = nouveau_bo(bo); if (!nvbo->name) { int ret = drmIoctl(bo->device->fd, DRM_IOCTL_GEM_FLINK, &req); if (ret) return ret; nvbo->name = req.name; } *name = nvbo->name; return 0; } void nouveau_bo_ref(struct nouveau_bo *bo, struct nouveau_bo **pref) { struct nouveau_bo *ref = *pref; if (bo) { atomic_inc(&nouveau_bo(bo)->refcnt); } if (ref) { if (atomic_dec_and_test(&nouveau_bo(ref)->refcnt)) nouveau_bo_del(ref); } *pref = bo; } int nouveau_bo_wait(struct nouveau_bo *bo, uint32_t access, struct nouveau_client *client) { struct nouveau_bo_priv *nvbo = nouveau_bo(bo); struct drm_nouveau_gem_cpu_prep req; struct nouveau_pushbuf *push; int ret = 0; if (!(access & NOUVEAU_BO_RDWR)) return 0; push = cli_push_get(client, bo); if (push && push->channel) nouveau_pushbuf_kick(push, push->channel); if (!nvbo->name && !(nvbo->access & NOUVEAU_BO_WR) && !( access & NOUVEAU_BO_WR)) return 0; req.handle = bo->handle; req.flags = 0; if (access & NOUVEAU_BO_WR) req.flags |= NOUVEAU_GEM_CPU_PREP_WRITE; if (access & NOUVEAU_BO_NOBLOCK) req.flags |= NOUVEAU_GEM_CPU_PREP_NOWAIT; ret = drmCommandWrite(bo->device->fd, DRM_NOUVEAU_GEM_CPU_PREP, &req, sizeof(req)); if (ret == 0) nvbo->access = 0; return ret; } int nouveau_bo_map(struct nouveau_bo *bo, uint32_t access, struct nouveau_client *client) { struct nouveau_bo_priv *nvbo = nouveau_bo(bo); if (bo->map == NULL) { bo->map = mmap(0, bo->size, PROT_READ | PROT_WRITE, MAP_SHARED, bo->device->fd, nvbo->map_handle); if (bo->map == MAP_FAILED) { bo->map = NULL; return -errno; } } return nouveau_bo_wait(bo, access, client); }