#ifndef __NOUVEAU_H__ #define __NOUVEAU_H__ #include #include #define NOUVEAU_DEVICE_CLASS 0x80000000 #define NOUVEAU_FIFO_CHANNEL_CLASS 0x80000001 #define NOUVEAU_NOTIFIER_CLASS 0x80000002 #define NOUVEAU_PARENT_CLASS 0xffffffff struct nouveau_list { struct nouveau_list *prev; struct nouveau_list *next; }; struct nouveau_object { struct nouveau_object *parent; uint64_t handle; uint32_t oclass; uint32_t length; void *data; }; struct nouveau_fifo { struct nouveau_object *object; uint32_t channel; uint32_t pushbuf; uint64_t unused1[3]; }; struct nv04_fifo { struct nouveau_fifo base; uint32_t vram; uint32_t gart; uint32_t notify; }; struct nvc0_fifo { struct nouveau_fifo base; uint32_t notify; }; #define NVE0_FIFO_ENGINE_GR 0x00000001 #define NVE0_FIFO_ENGINE_VP 0x00000002 #define NVE0_FIFO_ENGINE_PPP 0x00000004 #define NVE0_FIFO_ENGINE_BSP 0x00000008 #define NVE0_FIFO_ENGINE_CE0 0x00000010 #define NVE0_FIFO_ENGINE_CE1 0x00000020 #define NVE0_FIFO_ENGINE_ENC 0x00000040 struct nve0_fifo { struct { struct nouveau_fifo base; uint32_t notify; }; uint32_t engine; }; struct nv04_notify { struct nouveau_object *object; uint32_t offset; uint32_t length; }; int nouveau_object_new(struct nouveau_object *parent, uint64_t handle, uint32_t oclass, void *data, uint32_t length, struct nouveau_object **); void nouveau_object_del(struct nouveau_object **); void *nouveau_object_find(struct nouveau_object *, uint32_t parent_class); struct nouveau_device { struct nouveau_object object; int fd; uint32_t lib_version; uint32_t drm_version; uint32_t chipset; uint64_t vram_size; uint64_t gart_size; uint64_t vram_limit; uint64_t gart_limit; }; int nouveau_device_wrap(int fd, int close, struct nouveau_device **); int nouveau_device_open(const char *busid, struct nouveau_device **); void nouveau_device_del(struct nouveau_device **); int nouveau_getparam(struct nouveau_device *, uint64_t param, uint64_t *value); int nouveau_setparam(struct nouveau_device *, uint64_t param, uint64_t value); struct nouveau_client { struct nouveau_device *device; int id; }; int nouveau_client_new(struct nouveau_device *, struct nouveau_client **); void nouveau_client_del(struct nouveau_client **); union nouveau_bo_config { struct { #define NV04_BO_16BPP 0x00000001 #define NV04_BO_32BPP 0x00000002 #define NV04_BO_ZETA 0x00000004 uint32_t surf_flags; uint32_t surf_pitch; } nv04; struct { uint32_t memtype; uint32_t tile_mode; } nv50; struct { uint32_t memtype; uint32_t tile_mode; } nvc0; uint32_t data[8]; }; #define NOUVEAU_BO_VRAM 0x00000001 #define NOUVEAU_BO_GART 0x00000002 #define NOUVEAU_BO_APER (NOUVEAU_BO_VRAM | NOUVEAU_BO_GART) #define NOUVEAU_BO_RD 0x00000100 #define NOUVEAU_BO_WR 0x00000200 #define NOUVEAU_BO_RDWR (NOUVEAU_BO_RD | NOUVEAU_BO_WR) #define NOUVEAU_BO_NOBLOCK 0x00000400 #define NOUVEAU_BO_LOW 0x00001000 #define NOUVEAU_BO_HIGH 0x00002000 #define NOUVEAU_BO_OR 0x00004000 #define NOUVEAU_BO_MAP 0x80000000 #define NOUVEAU_BO_CONTIG 0x40000000 #define NOUVEAU_BO_NOSNOOP 0x20000000 struct nouveau_bo { struct nouveau_device *device; uint32_t handle; uint64_t size; uint32_t flags; uint64_t offset; void *map; union nouveau_bo_config config; }; int nouveau_bo_new(struct nouveau_device *, uint32_t flags, uint32_t align, uint64_t size, union nouveau_bo_config *, struct nouveau_bo **); int nouveau_bo_wrap(struct nouveau_device *, uint32_t handle, struct nouveau_bo **); int nouveau_bo_name_ref(struct nouveau_device *dev, uint32_t name, struct nouveau_bo **); int nouveau_bo_name_get(struct nouveau_bo *, uint32_t *name); void nouveau_bo_ref(struct nouveau_bo *, struct nouveau_bo **); int nouveau_bo_map(struct nouveau_bo *, uint32_t access, struct nouveau_client *); int nouveau_bo_wait(struct nouveau_bo *, uint32_t access, struct nouveau_client *); int nouveau_bo_prime_handle_ref(struct nouveau_device *dev, int prime_fd, struct nouveau_bo **); int nouveau_bo_set_prime(struct nouveau_bo *bo, int *prime_fd); struct nouveau_bufref { struct nouveau_list thead; struct nouveau_bo *bo; uint32_t packet; uint32_t flags; uint32_t data; uint32_t vor; uint32_t tor; uint32_t priv_data; void *priv; }; struct nouveau_bufctx { struct nouveau_client *client; struct nouveau_list head; struct nouveau_list pending; struct nouveau_list current; int relocs; }; int nouveau_bufctx_new(struct nouveau_client *, int bins, struct nouveau_bufctx **); void nouveau_bufctx_del(struct nouveau_bufctx **); struct nouveau_bufref * nouveau_bufctx_refn(struct nouveau_bufctx *, int bin, struct nouveau_bo *, uint32_t flags); struct nouveau_bufref * nouveau_bufctx_mthd(struct nouveau_bufctx *, int bin, uint32_t packet, struct nouveau_bo *, uint64_t data, uint32_t flags, uint32_t vor, uint32_t tor); void nouveau_bufctx_reset(struct nouveau_bufctx *, int bin); struct nouveau_pushbuf_krec; struct nouveau_pushbuf { struct nouveau_client *client; struct nouveau_object *channel; struct nouveau_bufctx *bufctx; void (*kick_notify)(struct nouveau_pushbuf *); void *user_priv; uint32_t rsvd_kick; uint32_t flags; uint32_t *cur; uint32_t *end; }; struct nouveau_pushbuf_refn { struct nouveau_bo *bo; uint32_t flags; }; int nouveau_pushbuf_new(struct nouveau_client *, struct nouveau_object *channel, int nr, uint32_t size, bool immediate, struct nouveau_pushbuf **); void nouveau_pushbuf_del(struct nouveau_pushbuf **); int nouveau_pushbuf_space(struct nouveau_pushbuf *, uint32_t dwords, uint32_t relocs, uint32_t pushes); void nouveau_pushbuf_data(struct nouveau_pushbuf *, struct nouveau_bo *, uint64_t offset, uint64_t length); int nouveau_pushbuf_refn(struct nouveau_pushbuf *, struct nouveau_pushbuf_refn *, int nr); /* Emits a reloc into the push buffer at the current position, you *must* * have previously added the referenced buffer to a buffer context, and * validated it against the current push buffer. */ void nouveau_pushbuf_reloc(struct nouveau_pushbuf *, struct nouveau_bo *, uint32_t data, uint32_t flags, uint32_t vor, uint32_t tor); int nouveau_pushbuf_validate(struct nouveau_pushbuf *); uint32_t nouveau_pushbuf_refd(struct nouveau_pushbuf *, struct nouveau_bo *); int nouveau_pushbuf_kick(struct nouveau_pushbuf *, struct nouveau_object *channel); struct nouveau_bufctx * nouveau_pushbuf_bufctx(struct nouveau_pushbuf *, struct nouveau_bufctx *); #endif