diff --git a/configure.ac b/configure.ac
index 97bbcb72dbd57a67c4ff63ed16fd4373d82d51a3..8c28107a9a674226b954cba46dc575a5ae3c2d13 100644 (file)
--- a/configure.ac
+++ b/configure.ac
AC_PREREQ([2.63])
AC_INIT([libdrm],
- [2.4.31],
+ [2.4.39],
[https://bugs.freedesktop.org/enter_bug.cgi?product=DRI],
[libdrm])
# Enable quiet compiles on automake 1.11.
m4_ifdef([AM_SILENT_RULES], [AM_SILENT_RULES([yes])])
+if test x$LIB_MAN_SUFFIX = x ; then
+ LIB_MAN_SUFFIX=3
+fi
+if test x$LIB_MAN_DIR = x ; then
+ LIB_MAN_DIR='$(mandir)/man$(LIB_MAN_SUFFIX)'
+fi
+AC_SUBST([LIB_MAN_SUFFIX])
+AC_SUBST([LIB_MAN_DIR])
+
+MAN_SUBSTS="\
+ -e 's|__vendorversion__|\"\$(PACKAGE_STRING)\" |' \
+ -e 's|__projectroot__|\$(prefix)|g' \
+ -e 's|__apploaddir__|\$(appdefaultdir)|g' \
+ -e 's|__appmansuffix__|\$(APP_MAN_SUFFIX)|g' \
+ -e 's|__drivermansuffix__|\$(DRIVER_MAN_SUFFIX)|g' \
+ -e 's|__adminmansuffix__|\$(ADMIN_MAN_SUFFIX)|g' \
+ -e 's|__libmansuffix__|\$(LIB_MAN_SUFFIX)|g' \
+ -e 's|__miscmansuffix__|\$(MISC_MAN_SUFFIX)|g' \
+ -e 's|__filemansuffix__|\$(FILE_MAN_SUFFIX)|g'"
+AC_SUBST([MAN_SUBSTS])
+
# Check for programs
AC_PROG_CC
AC_SUBST(PTHREADSTUBS_CFLAGS)
AC_SUBST(PTHREADSTUBS_LIBS)
-PKG_CHECK_MODULES(PCIACCESS, [pciaccess >= 0.10])
-AC_SUBST(PCIACCESS_CFLAGS)
-AC_SUBST(PCIACCESS_LIBS)
-
pkgconfigdir=${libdir}/pkgconfig
AC_SUBST(pkgconfigdir)
AC_ARG_ENABLE([udev],
[Enable support for radeon's KMS API (default: auto)]),
[RADEON=$enableval], [RADEON=auto])
-AC_ARG_ENABLE(vmwgfx-experimental-api,
- AS_HELP_STRING([--enable-vmwgfx-experimental-api],
- [Install vmwgfx's experimental kernel API header (default: disabled)]),
- [VMWGFX=$enableval], [VMWGFX=no])
+AC_ARG_ENABLE(nouveau,
+ AS_HELP_STRING([--disable-nouveau],
+ [Enable support for nouveau's KMS API (default: auto)]),
+ [NOUVEAU=$enableval], [NOUVEAU=auto])
-AC_ARG_ENABLE(nouveau-experimental-api,
- AS_HELP_STRING([--enable-nouveau-experimental-api],
- [Enable support for nouveau's experimental API (default: disabled)]),
- [NOUVEAU=$enableval], [NOUVEAU=no])
+AC_ARG_ENABLE(vmwgfx,
+ AS_HELP_STRING([--disable-vmwgfx],
+ [Enable support for vmwgfx's KMS API (default: yes)]),
+ [VMWGFX=$enableval], [VMWGFX=yes])
+AC_ARG_ENABLE(omap-experimental-api,
+ AS_HELP_STRING([--enable-omap-experimental-api],
+ [Enable support for OMAP's experimental API (default: disabled)]),
+ [OMAP=$enableval], [OMAP=no])
+
+AC_ARG_ENABLE(exynos-experimental-api,
+ AS_HELP_STRING([--enable-exynos-experimental-api],
+ [Enable support for EXYNOS's experimental API (default: disabled)]),
+ [EXYNOS=$enableval], [EXYNOS=no])
dnl ===========================================================================
dnl check compiler flags
-Wpointer-arith -Wwrite-strings -Wstrict-prototypes \
-Wmissing-prototypes -Wmissing-declarations -Wnested-externs \
-Wpacked -Wswitch-enum -Wmissing-format-attribute \
--Wstrict-aliasing=2 -Winit-self -Wunsafe-loop-optimizations \
+-Wstrict-aliasing=2 -Winit-self \
-Wdeclaration-after-statement -Wold-style-definition \
-Wno-missing-field-initializers -Wno-unused-parameter \
-Wno-attributes -Wno-long-long -Winline"
AC_DEFINE(HAVE_NOUVEAU, 1, [Have nouveau (nvidia) support])
fi
+AM_CONDITIONAL(HAVE_OMAP, [test "x$OMAP" = xyes])
+if test "x$OMAP" = xyes; then
+ AC_DEFINE(HAVE_OMAP, 1, [Have OMAP support])
+fi
+
+AM_CONDITIONAL(HAVE_EXYNOS, [test "x$EXYNOS" = xyes])
+if test "x$EXYNOS" = xyes; then
+ AC_DEFINE(HAVE_EXYNOS, 1, [Have EXYNOS support])
+fi
+
+AC_ARG_ENABLE([cairo-tests],
+ [AS_HELP_STRING([--enable-cairo-tests],
+ [Enable support for Cairo rendering in tests (default: auto)])],
+ [CAIRO=$enableval], [CAIRO=auto])
PKG_CHECK_MODULES(CAIRO, cairo, [HAVE_CAIRO=yes], [HAVE_CAIRO=no])
-if test "x$HAVE_CAIRO" = xyes; then
- AC_DEFINE(HAVE_CAIRO, 1, [Have cairo support])
+AC_MSG_CHECKING([whether to enable Cairo tests])
+if test "x$CAIRO" = xauto; then
+ CAIRO="$HAVE_CAIRO"
fi
-AM_CONDITIONAL(HAVE_CAIRO, [test "x$HAVE_CAIRO" = xyes])
+if test "x$CAIRO" = xyes; then
+ if ! test "x$HAVE_CAIRO" = xyes; then
+ AC_MSG_ERROR([Cairo support required but not present])
+ fi
+ AC_DEFINE(HAVE_CAIRO, 1, [Have Cairo support])
+fi
+AC_MSG_RESULT([$CAIRO])
+AM_CONDITIONAL(HAVE_CAIRO, [test "x$CAIRO" = xyes])
# For enumerating devices in test case
PKG_CHECK_MODULES(LIBUDEV, libudev, [HAVE_LIBUDEV=yes], [HAVE_LIBUDEV=no])
fi
AM_CONDITIONAL(HAVE_LIBUDEV, [test "x$HAVE_LIBUDEV" = xyes])
-if test "x$INTEL" != "xno" -o "x$RADEON" != "xno"; then
+if test "x$INTEL" != "xno" -o "x$RADEON" != "xno" -o "x$NOUVEAU" != "xno" -o "x$OMAP" != "xno"; then
# Check for atomic intrinsics
AC_CACHE_CHECK([for native atomic primitives], drm_cv_atomic_primitives,
[
AC_MSG_WARN([Disabling libdrm_radeon. It depends on atomic operations, which were not found for your compiler/cpu. Try compiling with -march=native, or install the libatomics-op-dev package.])
RADEON=no
fi
-
+ if test "x$NOUVEAU" != "xauto"; then
+ if test "x$NOUVEAU" != "xno"; then
+ AC_MSG_ERROR([libdrm_nouveau depends upon atomic operations, which were not found for your compiler/cpu. Try compiling with -march=native, or install the libatomics-op-dev package, or, failing both of those, disable support for NVIDIA GPUs by passing --disable-nouveau to ./configure])
+ fi
+ else
+ AC_MSG_WARN([Disabling libdrm_nouveau. It depends on atomic operations, which were not found for your compiler/cpu. Try compiling with -march=native, or install the libatomics-op-dev package.])
+ NOUVEAU=no
+ fi
else
if test "x$INTEL" != "xno"; then
case $host_cpu in
if test "x$RADEON" != "xno"; then
RADEON=yes
fi
+ if test "x$NOUVEAU" != "xno"; then
+ NOUVEAU=yes
+ fi
fi
fi
+if test "x$INTEL" != "xno"; then
+ PKG_CHECK_MODULES(PCIACCESS, [pciaccess >= 0.10])
+fi
+AC_SUBST(PCIACCESS_CFLAGS)
+AC_SUBST(PCIACCESS_LIBS)
+
PKG_CHECK_MODULES(VALGRIND, [valgrind], [have_valgrind=yes], [have_valgrind=no])
if test "x$have_valgrind" = "xyes"; then
AC_DEFINE([HAVE_VALGRIND], 1, [Use valgrind intrinsics to suppress false warnings])
AM_CONDITIONAL(HAVE_INTEL, [test "x$INTEL" != "xno"])
AM_CONDITIONAL(HAVE_RADEON, [test "x$RADEON" != "xno"])
+AM_CONDITIONAL(HAVE_NOUVEAU, [test "x$NOUVEAU" != "xno"])
if test "x$RADEON" = xyes; then
AC_DEFINE(HAVE_RADEON, 1, [Have radeon support])
fi
radeon/libdrm_radeon.pc
nouveau/Makefile
nouveau/libdrm_nouveau.pc
+ omap/Makefile
+ omap/libdrm_omap.pc
+ exynos/Makefile
+ exynos/libdrm_exynos.pc
tests/Makefile
tests/modeprint/Makefile
tests/modetest/Makefile
tests/vbltest/Makefile
include/Makefile
include/drm/Makefile
+ man/Makefile
libdrm.pc])
AC_OUTPUT
echo " vmwgfx API $VMWGFX"
echo " Radeon API $RADEON"
echo " Nouveau API $NOUVEAU"
+echo " OMAP API $OMAP"
+echo " EXYNOS API $EXYNOS"
echo ""