index b4a005659f6c09bfded6dc28b4fa4a7d9ed7aa79..187e8ec9ca8684b5c99cbcb50f72fd095fbe2879 100644 (file)
--- a/intel/intel_bufmgr_gem.c
+++ b/intel/intel_bufmgr_gem.c
#endif
#include <xf86drm.h>
+#include <xf86atomic.h>
#include <fcntl.h>
#include <stdio.h>
#include <stdlib.h>
#include <sys/mman.h>
#include <sys/stat.h>
#include <sys/types.h>
+#include <stdbool.h>
#include "errno.h"
#include "libdrm_lists.h"
-#include "intel_atomic.h"
#include "intel_bufmgr.h"
#include "intel_bufmgr_priv.h"
#include "intel_chipset.h"
fprintf(stderr, __VA_ARGS__); \
} while (0)
+#define ARRAY_SIZE(x) (sizeof(x) / sizeof((x)[0]))
+
typedef struct _drm_intel_bo_gem drm_intel_bo_gem;
struct drm_intel_gem_bo_bucket {
unsigned long size;
};
-/* Only cache objects up to 64MB. Bigger than that, and the rounding of the
- * size makes many operations fail that wouldn't otherwise.
- */
-#define DRM_INTEL_GEM_BO_BUCKETS 14
typedef struct _drm_intel_bufmgr_gem {
drm_intel_bufmgr bufmgr;
int exec_count;
/** Array of lists of cached gem objects of power-of-two sizes */
- struct drm_intel_gem_bo_bucket cache_bucket[DRM_INTEL_GEM_BO_BUCKETS];
+ struct drm_intel_gem_bo_bucket cache_bucket[14 * 4];
+ int num_buckets;
+ time_t time;
+
+ drmMMListHead named;
+ drmMMListHead vma_cache;
+ int vma_count, vma_open, vma_max;
uint64_t gtt_size;
int available_fences;
int pci_device;
- char bo_reuse;
- char fenced_relocs;
+ int gen;
+ unsigned int has_bsd : 1;
+ unsigned int has_blt : 1;
+ unsigned int has_relaxed_fencing : 1;
+ unsigned int has_llc : 1;
+ unsigned int bo_reuse : 1;
+ bool fenced_relocs;
} drm_intel_bufmgr_gem;
#define DRM_INTEL_RELOC_FENCE (1<<0)
* Kenel-assigned global name for this object
*/
unsigned int global_name;
+ drmMMListHead name_list;
/**
* Index of the buffer within the validation list while preparing a
*/
uint32_t tiling_mode;
uint32_t swizzle_mode;
+ unsigned long stride;
time_t free_time;
void *mem_virtual;
/** GTT virtual address for the buffer, saved across map/unmap cycles */
void *gtt_virtual;
+ int map_count;
+ drmMMListHead vma_list;
/** BO cache list */
drmMMListHead head;
* Boolean of whether this BO and its children have been included in
* the current drm_intel_bufmgr_check_aperture_space() total.
*/
- char included_in_check_aperture;
+ bool included_in_check_aperture;
/**
* Boolean of whether this buffer has been used as a relocation
* target and had its size accounted for, and thus can't have any
* further relocations added to it.
*/
- char used_as_reloc_target;
+ bool used_as_reloc_target;
/**
* Boolean of whether we have encountered an error whilst building the relocation tree.
*/
- char has_error;
+ bool has_error;
/**
* Boolean of whether this buffer can be re-used
*/
- char reusable;
+ bool reusable;
/**
* Size in bytes of this buffer and its relocation descendents.
* relocations.
*/
int reloc_tree_fences;
+
+ /** Flags that we may need to do the SW_FINSIH ioctl on unmap. */
+ bool mapped_cpu_write;
};
static unsigned int
uint32_t * swizzle_mode);
static int
-drm_intel_gem_bo_set_tiling(drm_intel_bo *bo, uint32_t * tiling_mode,
- uint32_t stride);
+drm_intel_gem_bo_set_tiling_internal(drm_intel_bo *bo,
+ uint32_t tiling_mode,
+ uint32_t stride);
static void drm_intel_gem_bo_unreference_locked_timed(drm_intel_bo *bo,
time_t time);
@@ -221,11 +239,11 @@ drm_intel_gem_bo_tile_size(drm_intel_bufmgr_gem *bufmgr_gem, unsigned long size,
return size;
/* 965+ just need multiples of page size for tiling */
- if (!IS_GEN2(bufmgr_gem) && !IS_GEN3(bufmgr_gem))
+ if (bufmgr_gem->gen >= 4)
return ROUND_UP_TO(size, 4096);
/* Older chips need powers of two, of at least 512k or 1M */
- if (!IS_GEN2(bufmgr_gem)) {
+ if (bufmgr_gem->gen == 3) {
min_size = 1024*1024;
max_size = 128*1024*1024;
} else {
@@ -238,6 +256,10 @@ drm_intel_gem_bo_tile_size(drm_intel_bufmgr_gem *bufmgr_gem, unsigned long size,
return size;
}
+ /* Do we need to allocate every page for the fence? */
+ if (bufmgr_gem->has_relaxed_fencing)
+ return ROUND_UP_TO(size, 4096);
+
for (i = min_size; i < size; i <<= 1)
;
@@ -251,18 +273,36 @@ drm_intel_gem_bo_tile_size(drm_intel_bufmgr_gem *bufmgr_gem, unsigned long size,
*/
static unsigned long
drm_intel_gem_bo_tile_pitch(drm_intel_bufmgr_gem *bufmgr_gem,
- unsigned long pitch, uint32_t tiling_mode)
+ unsigned long pitch, uint32_t *tiling_mode)
{
- unsigned long tile_width = 512;
+ unsigned long tile_width;
unsigned long i;
- if (tiling_mode == I915_TILING_NONE)
- return ROUND_UP_TO(pitch, tile_width);
+ /* If untiled, then just align it so that we can do rendering
+ * to it with the 3D engine.
+ */
+ if (*tiling_mode == I915_TILING_NONE)
+ return ALIGN(pitch, 64);
+
+ if (*tiling_mode == I915_TILING_X
+ || (IS_915(bufmgr_gem->pci_device)
+ && *tiling_mode == I915_TILING_Y))
+ tile_width = 512;
+ else
+ tile_width = 128;
/* 965 is flexible */
- if (!IS_GEN2(bufmgr_gem) && !IS_GEN3(bufmgr_gem))
+ if (bufmgr_gem->gen >= 4)
return ROUND_UP_TO(pitch, tile_width);
+ /* The older hardware has a maximum pitch of 8192 with tiled
+ * surfaces, so fallback to untiled if it's too large.
+ */
+ if (pitch > 8192) {
+ *tiling_mode = I915_TILING_NONE;
+ return ALIGN(pitch, 64);
+ }
+
/* Pre-965 needs power of two tile width */
for (i = tile_width; i < pitch; i <<= 1)
;
{
int i;
- for (i = 0; i < DRM_INTEL_GEM_BO_BUCKETS; i++) {
+ for (i = 0; i < bufmgr_gem->num_buckets; i++) {
struct drm_intel_gem_bo_bucket *bucket =
&bufmgr_gem->cache_bucket[i];
if (bucket->size >= size) {
{
drm_intel_bo_gem *bo_gem = (drm_intel_bo_gem *) bo;
- assert(atomic_read(&bo_gem->refcount) > 0);
atomic_inc(&bo_gem->refcount);
}
drm_intel_bo_gem *bo_gem = (drm_intel_bo_gem *)bo;
int index;
- if (bo_gem->validate_index != -1)
+ if (bo_gem->validate_index != -1) {
+ if (need_fence)
+ bufmgr_gem->exec2_objects[bo_gem->validate_index].flags |=
+ EXEC_OBJECT_NEEDS_FENCE;
return;
+ }
/* Extend the array of validation entries as necessary. */
if (bufmgr_gem->exec_count == bufmgr_gem->exec_size) {
* aperture. Optimal packing is for wimps.
*/
size = bo_gem->bo.size;
- if ((IS_GEN2(bufmgr_gem) || IS_GEN3(bufmgr_gem))
- && bo_gem->tiling_mode != I915_TILING_NONE)
- size *= 2;
+ if (bufmgr_gem->gen < 4 && bo_gem->tiling_mode != I915_TILING_NONE) {
+ int min_size;
+
+ if (bufmgr_gem->has_relaxed_fencing) {
+ if (bufmgr_gem->gen == 3)
+ min_size = 1024*1024;
+ else
+ min_size = 512*1024;
+
+ while (min_size < size)
+ min_size *= 2;
+ } else
+ min_size = size;
+
+ /* Account for worst-case alignment. */
+ size = 2 * min_size;
+ }
bo_gem->reloc_tree_size = size;
}
bo_gem->relocs = malloc(max_relocs *
sizeof(struct drm_i915_gem_relocation_entry));
bo_gem->reloc_target_info = malloc(max_relocs *
- sizeof(drm_intel_reloc_target *));
+ sizeof(drm_intel_reloc_target));
if (bo_gem->relocs == NULL || bo_gem->reloc_target_info == NULL) {
- bo_gem->has_error = 1;
+ bo_gem->has_error = true;
free (bo_gem->relocs);
bo_gem->relocs = NULL;
memset(&busy, 0, sizeof(busy));
busy.handle = bo_gem->gem_handle;
- do {
- ret = ioctl(bufmgr_gem->fd, DRM_IOCTL_I915_GEM_BUSY, &busy);
- } while (ret == -1 && errno == EINTR);
+ ret = drmIoctl(bufmgr_gem->fd, DRM_IOCTL_I915_GEM_BUSY, &busy);
return (ret == 0 && busy.busy);
}
madv.handle = bo_gem->gem_handle;
madv.madv = state;
madv.retained = 1;
- ioctl(bufmgr_gem->fd, DRM_IOCTL_I915_GEM_MADVISE, &madv);
+ drmIoctl(bufmgr_gem->fd, DRM_IOCTL_I915_GEM_MADVISE, &madv);
return madv.retained;
}
drm_intel_gem_bo_alloc_internal(drm_intel_bufmgr *bufmgr,
const char *name,
unsigned long size,
- unsigned long flags)
+ unsigned long flags,
+ uint32_t tiling_mode,
+ unsigned long stride)
{
drm_intel_bufmgr_gem *bufmgr_gem = (drm_intel_bufmgr_gem *) bufmgr;
drm_intel_bo_gem *bo_gem;
unsigned int page_size = getpagesize();
int ret;
struct drm_intel_gem_bo_bucket *bucket;
- int alloc_from_cache;
+ bool alloc_from_cache;
unsigned long bo_size;
- int for_render = 0;
+ bool for_render = false;
if (flags & BO_ALLOC_FOR_RENDER)
- for_render = 1;
+ for_render = true;
/* Round the allocated size up to a power of two number of pages. */
bucket = drm_intel_gem_bo_bucket_for_size(bufmgr_gem, size);
pthread_mutex_lock(&bufmgr_gem->lock);
/* Get a buffer out of the cache if available */
retry:
- alloc_from_cache = 0;
+ alloc_from_cache = false;
if (bucket != NULL && !DRMLISTEMPTY(&bucket->head)) {
if (for_render) {
/* Allocate new render-target BOs from the tail (MRU)
bo_gem = DRMLISTENTRY(drm_intel_bo_gem,
bucket->head.prev, head);
DRMLISTDEL(&bo_gem->head);
- alloc_from_cache = 1;
+ alloc_from_cache = true;
} else {
/* For non-render-target BOs (where we're probably
* going to map it first thing in order to fill it
bo_gem = DRMLISTENTRY(drm_intel_bo_gem,
bucket->head.next, head);
if (!drm_intel_gem_bo_busy(&bo_gem->bo)) {
- alloc_from_cache = 1;
+ alloc_from_cache = true;
DRMLISTDEL(&bo_gem->head);
}
}
bucket);
goto retry;
}
+
+ if (drm_intel_gem_bo_set_tiling_internal(&bo_gem->bo,
+ tiling_mode,
+ stride)) {
+ drm_intel_gem_bo_free(&bo_gem->bo);
+ goto retry;
+ }
}
}
pthread_mutex_unlock(&bufmgr_gem->lock);
memset(&create, 0, sizeof(create));
create.size = bo_size;
- do {
- ret = ioctl(bufmgr_gem->fd,
- DRM_IOCTL_I915_GEM_CREATE,
- &create);
- } while (ret == -1 && errno == EINTR);
+ ret = drmIoctl(bufmgr_gem->fd,
+ DRM_IOCTL_I915_GEM_CREATE,
+ &create);
bo_gem->gem_handle = create.handle;
bo_gem->bo.handle = bo_gem->gem_handle;
if (ret != 0) {
return NULL;
}
bo_gem->bo.bufmgr = bufmgr;
+
+ bo_gem->tiling_mode = I915_TILING_NONE;
+ bo_gem->swizzle_mode = I915_BIT_6_SWIZZLE_NONE;
+ bo_gem->stride = 0;
+
+ if (drm_intel_gem_bo_set_tiling_internal(&bo_gem->bo,
+ tiling_mode,
+ stride)) {
+ drm_intel_gem_bo_free(&bo_gem->bo);
+ return NULL;
+ }
+
+ DRMINITLISTHEAD(&bo_gem->name_list);
+ DRMINITLISTHEAD(&bo_gem->vma_list);
}
bo_gem->name = name;
atomic_set(&bo_gem->refcount, 1);
bo_gem->validate_index = -1;
bo_gem->reloc_tree_fences = 0;
- bo_gem->used_as_reloc_target = 0;
- bo_gem->has_error = 0;
- bo_gem->tiling_mode = I915_TILING_NONE;
- bo_gem->swizzle_mode = I915_BIT_6_SWIZZLE_NONE;
- bo_gem->reusable = 1;
+ bo_gem->used_as_reloc_target = false;
+ bo_gem->has_error = false;
+ bo_gem->reusable = true;
drm_intel_bo_gem_set_in_aperture_size(bufmgr_gem, bo_gem);
unsigned int alignment)
{
return drm_intel_gem_bo_alloc_internal(bufmgr, name, size,
- BO_ALLOC_FOR_RENDER);
+ BO_ALLOC_FOR_RENDER,
+ I915_TILING_NONE, 0);
}
static drm_intel_bo *
unsigned long size,
unsigned int alignment)
{
- return drm_intel_gem_bo_alloc_internal(bufmgr, name, size, 0);
+ return drm_intel_gem_bo_alloc_internal(bufmgr, name, size, 0,
+ I915_TILING_NONE, 0);
}
static drm_intel_bo *
unsigned long *pitch, unsigned long flags)
{
drm_intel_bufmgr_gem *bufmgr_gem = (drm_intel_bufmgr_gem *)bufmgr;
- drm_intel_bo *bo;
- unsigned long size, stride, aligned_y = y;
- int ret;
-
- if (*tiling_mode == I915_TILING_NONE)
- aligned_y = ALIGN(y, 2);
- else if (*tiling_mode == I915_TILING_X)
- aligned_y = ALIGN(y, 8);
- else if (*tiling_mode == I915_TILING_Y)
- aligned_y = ALIGN(y, 32);
-
- stride = x * cpp;
- stride = drm_intel_gem_bo_tile_pitch(bufmgr_gem, stride, *tiling_mode);
- size = stride * aligned_y;
- size = drm_intel_gem_bo_tile_size(bufmgr_gem, size, tiling_mode);
-
- bo = drm_intel_gem_bo_alloc_internal(bufmgr, name, size, flags);
- if (!bo)
- return NULL;
-
- ret = drm_intel_gem_bo_set_tiling(bo, tiling_mode, stride);
- if (ret != 0) {
- drm_intel_gem_bo_unreference(bo);
- return NULL;
- }
+ unsigned long size, stride;
+ uint32_t tiling;
+ do {
+ unsigned long aligned_y, height_alignment;
+
+ tiling = *tiling_mode;
+
+ /* If we're tiled, our allocations are in 8 or 32-row blocks,
+ * so failure to align our height means that we won't allocate
+ * enough pages.
+ *
+ * If we're untiled, we still have to align to 2 rows high
+ * because the data port accesses 2x2 blocks even if the
+ * bottom row isn't to be rendered, so failure to align means
+ * we could walk off the end of the GTT and fault. This is
+ * documented on 965, and may be the case on older chipsets
+ * too so we try to be careful.
+ */
+ aligned_y = y;
+ height_alignment = 2;
+
+ if ((bufmgr_gem->gen == 2) && tiling != I915_TILING_NONE)
+ height_alignment = 16;
+ else if (tiling == I915_TILING_X
+ || (IS_915(bufmgr_gem->pci_device)
+ && tiling == I915_TILING_Y))
+ height_alignment = 8;
+ else if (tiling == I915_TILING_Y)
+ height_alignment = 32;
+ aligned_y = ALIGN(y, height_alignment);
+
+ stride = x * cpp;
+ stride = drm_intel_gem_bo_tile_pitch(bufmgr_gem, stride, tiling_mode);
+ size = stride * aligned_y;
+ size = drm_intel_gem_bo_tile_size(bufmgr_gem, size, tiling_mode);
+ } while (*tiling_mode != tiling);
*pitch = stride;
- return bo;
+ if (tiling == I915_TILING_NONE)
+ stride = 0;
+
+ return drm_intel_gem_bo_alloc_internal(bufmgr, name, size, flags,
+ tiling, stride);
}
/**
int ret;
struct drm_gem_open open_arg;
struct drm_i915_gem_get_tiling get_tiling;
+ drmMMListHead *list;
+
+ /* At the moment most applications only have a few named bo.
+ * For instance, in a DRI client only the render buffers passed
+ * between X and the client are named. And since X returns the
+ * alternating names for the front/back buffer a linear search
+ * provides a sufficiently fast match.
+ */
+ for (list = bufmgr_gem->named.next;
+ list != &bufmgr_gem->named;
+ list = list->next) {
+ bo_gem = DRMLISTENTRY(drm_intel_bo_gem, list, name_list);
+ if (bo_gem->global_name == handle) {
+ drm_intel_gem_bo_reference(&bo_gem->bo);
+ return &bo_gem->bo;
+ }
+ }
bo_gem = calloc(1, sizeof(*bo_gem));
if (!bo_gem)
memset(&open_arg, 0, sizeof(open_arg));
open_arg.name = handle;
- do {
- ret = ioctl(bufmgr_gem->fd,
- DRM_IOCTL_GEM_OPEN,
- &open_arg);
- } while (ret == -1 && errno == EINTR);
+ ret = drmIoctl(bufmgr_gem->fd,
+ DRM_IOCTL_GEM_OPEN,
+ &open_arg);
if (ret != 0) {
- fprintf(stderr, "Couldn't reference %s handle 0x%08x: %s\n",
- name, handle, strerror(errno));
+ DBG("Couldn't reference %s handle 0x%08x: %s\n",
+ name, handle, strerror(errno));
free(bo_gem);
return NULL;
}
atomic_set(&bo_gem->refcount, 1);
bo_gem->validate_index = -1;
bo_gem->gem_handle = open_arg.handle;
+ bo_gem->bo.handle = open_arg.handle;
bo_gem->global_name = handle;
- bo_gem->reusable = 0;
+ bo_gem->reusable = false;
memset(&get_tiling, 0, sizeof(get_tiling));
get_tiling.handle = bo_gem->gem_handle;
- ret = ioctl(bufmgr_gem->fd, DRM_IOCTL_I915_GEM_GET_TILING, &get_tiling);
+ ret = drmIoctl(bufmgr_gem->fd,
+ DRM_IOCTL_I915_GEM_GET_TILING,
+ &get_tiling);
if (ret != 0) {
drm_intel_gem_bo_unreference(&bo_gem->bo);
return NULL;
}
bo_gem->tiling_mode = get_tiling.tiling_mode;
bo_gem->swizzle_mode = get_tiling.swizzle_mode;
+ /* XXX stride is unknown */
drm_intel_bo_gem_set_in_aperture_size(bufmgr_gem, bo_gem);
+ DRMINITLISTHEAD(&bo_gem->vma_list);
+ DRMLISTADDTAIL(&bo_gem->name_list, &bufmgr_gem->named);
DBG("bo_create_from_handle: %d (%s)\n", handle, bo_gem->name);
return &bo_gem->bo;
struct drm_gem_close close;
int ret;
- if (bo_gem->mem_virtual)
+ DRMLISTDEL(&bo_gem->vma_list);
+ if (bo_gem->mem_virtual) {
munmap(bo_gem->mem_virtual, bo_gem->bo.size);
- if (bo_gem->gtt_virtual)
+ bufmgr_gem->vma_count--;
+ }
+ if (bo_gem->gtt_virtual) {
munmap(bo_gem->gtt_virtual, bo_gem->bo.size);
+ bufmgr_gem->vma_count--;
+ }
/* Close this object */
memset(&close, 0, sizeof(close));
close.handle = bo_gem->gem_handle;
- ret = ioctl(bufmgr_gem->fd, DRM_IOCTL_GEM_CLOSE, &close);
+ ret = drmIoctl(bufmgr_gem->fd, DRM_IOCTL_GEM_CLOSE, &close);
if (ret != 0) {
- fprintf(stderr,
- "DRM_IOCTL_GEM_CLOSE %d failed (%s): %s\n",
- bo_gem->gem_handle, bo_gem->name, strerror(errno));
+ DBG("DRM_IOCTL_GEM_CLOSE %d failed (%s): %s\n",
+ bo_gem->gem_handle, bo_gem->name, strerror(errno));
}
free(bo);
}
{
int i;
- for (i = 0; i < DRM_INTEL_GEM_BO_BUCKETS; i++) {
+ if (bufmgr_gem->time == time)
+ return;
+
+ for (i = 0; i < bufmgr_gem->num_buckets; i++) {
struct drm_intel_gem_bo_bucket *bucket =
&bufmgr_gem->cache_bucket[i];
drm_intel_gem_bo_free(&bo_gem->bo);
}
}
+
+ bufmgr_gem->time = time;
+}
+
+static void drm_intel_gem_bo_purge_vma_cache(drm_intel_bufmgr_gem *bufmgr_gem)
+{
+ int limit;
+
+ DBG("%s: cached=%d, open=%d, limit=%d\n", __FUNCTION__,
+ bufmgr_gem->vma_count, bufmgr_gem->vma_open, bufmgr_gem->vma_max);
+
+ if (bufmgr_gem->vma_max < 0)
+ return;
+
+ /* We may need to evict a few entries in order to create new mmaps */
+ limit = bufmgr_gem->vma_max - 2*bufmgr_gem->vma_open;
+ if (limit < 0)
+ limit = 0;
+
+ while (bufmgr_gem->vma_count > limit) {
+ drm_intel_bo_gem *bo_gem;
+
+ bo_gem = DRMLISTENTRY(drm_intel_bo_gem,
+ bufmgr_gem->vma_cache.next,
+ vma_list);
+ assert(bo_gem->map_count == 0);
+ DRMLISTDELINIT(&bo_gem->vma_list);
+
+ if (bo_gem->mem_virtual) {
+ munmap(bo_gem->mem_virtual, bo_gem->bo.size);
+ bo_gem->mem_virtual = NULL;
+ bufmgr_gem->vma_count--;
+ }
+ if (bo_gem->gtt_virtual) {
+ munmap(bo_gem->gtt_virtual, bo_gem->bo.size);
+ bo_gem->gtt_virtual = NULL;
+ bufmgr_gem->vma_count--;
+ }
+ }
+}
+
+static void drm_intel_gem_bo_close_vma(drm_intel_bufmgr_gem *bufmgr_gem,
+ drm_intel_bo_gem *bo_gem)
+{
+ bufmgr_gem->vma_open--;
+ DRMLISTADDTAIL(&bo_gem->vma_list, &bufmgr_gem->vma_cache);
+ if (bo_gem->mem_virtual)
+ bufmgr_gem->vma_count++;
+ if (bo_gem->gtt_virtual)
+ bufmgr_gem->vma_count++;
+ drm_intel_gem_bo_purge_vma_cache(bufmgr_gem);
+}
+
+static void drm_intel_gem_bo_open_vma(drm_intel_bufmgr_gem *bufmgr_gem,
+ drm_intel_bo_gem *bo_gem)
+{
+ bufmgr_gem->vma_open++;
+ DRMLISTDEL(&bo_gem->vma_list);
+ if (bo_gem->mem_virtual)
+ bufmgr_gem->vma_count--;
+ if (bo_gem->gtt_virtual)
+ bufmgr_gem->vma_count--;
+ drm_intel_gem_bo_purge_vma_cache(bufmgr_gem);
}
static void
drm_intel_bufmgr_gem *bufmgr_gem = (drm_intel_bufmgr_gem *) bo->bufmgr;
drm_intel_bo_gem *bo_gem = (drm_intel_bo_gem *) bo;
struct drm_intel_gem_bo_bucket *bucket;
- uint32_t tiling_mode;
int i;
/* Unreference all the target buffers */
for (i = 0; i < bo_gem->reloc_count; i++) {
- drm_intel_gem_bo_unreference_locked_timed(bo_gem->
- reloc_target_info[i].bo,
- time);
+ if (bo_gem->reloc_target_info[i].bo != bo) {
+ drm_intel_gem_bo_unreference_locked_timed(bo_gem->
+ reloc_target_info[i].bo,
+ time);
+ }
}
bo_gem->reloc_count = 0;
- bo_gem->used_as_reloc_target = 0;
+ bo_gem->used_as_reloc_target = false;
DBG("bo_unreference final: %d (%s)\n",
bo_gem->gem_handle, bo_gem->name);
bo_gem->relocs = NULL;
}
+ /* Clear any left-over mappings */
+ if (bo_gem->map_count) {
+ DBG("bo freed with non-zero map-count %d\n", bo_gem->map_count);
+ bo_gem->map_count = 0;
+ drm_intel_gem_bo_close_vma(bufmgr_gem, bo_gem);
+ }
+
+ DRMLISTDEL(&bo_gem->name_list);
+
bucket = drm_intel_gem_bo_bucket_for_size(bufmgr_gem, bo->size);
/* Put the buffer into our internal cache for reuse if we can. */
- tiling_mode = I915_TILING_NONE;
if (bufmgr_gem->bo_reuse && bo_gem->reusable && bucket != NULL &&
- drm_intel_gem_bo_set_tiling(bo, &tiling_mode, 0) == 0 &&
drm_intel_gem_bo_madvise_internal(bufmgr_gem, bo_gem,
I915_MADV_DONTNEED)) {
bo_gem->free_time = time;
bo_gem->validate_index = -1;
DRMLISTADDTAIL(&bo_gem->head, &bucket->head);
-
- drm_intel_gem_cleanup_bo_cache(bufmgr_gem, time);
} else {
drm_intel_gem_bo_free(bo);
}
pthread_mutex_lock(&bufmgr_gem->lock);
drm_intel_gem_bo_unreference_final(bo, time.tv_sec);
+ drm_intel_gem_cleanup_bo_cache(bufmgr_gem, time.tv_sec);
pthread_mutex_unlock(&bufmgr_gem->lock);
}
}
pthread_mutex_lock(&bufmgr_gem->lock);
- /* Allow recursive mapping. Mesa may recursively map buffers with
- * nested display loops.
- */
+ if (bo_gem->map_count++ == 0)
+ drm_intel_gem_bo_open_vma(bufmgr_gem, bo_gem);
+
if (!bo_gem->mem_virtual) {
struct drm_i915_gem_mmap mmap_arg;
- DBG("bo_map: %d (%s)\n", bo_gem->gem_handle, bo_gem->name);
+ DBG("bo_map: %d (%s), map_count=%d\n",
+ bo_gem->gem_handle, bo_gem->name, bo_gem->map_count);
memset(&mmap_arg, 0, sizeof(mmap_arg));
mmap_arg.handle = bo_gem->gem_handle;
mmap_arg.offset = 0;
mmap_arg.size = bo->size;
- do {
- ret = ioctl(bufmgr_gem->fd,
- DRM_IOCTL_I915_GEM_MMAP,
- &mmap_arg);
- } while (ret == -1 && errno == EINTR);
+ ret = drmIoctl(bufmgr_gem->fd,
+ DRM_IOCTL_I915_GEM_MMAP,
+ &mmap_arg);
if (ret != 0) {
ret = -errno;
- fprintf(stderr,
- "%s:%d: Error mapping buffer %d (%s): %s .\n",
- __FILE__, __LINE__, bo_gem->gem_handle,
- bo_gem->name, strerror(errno));
+ DBG("%s:%d: Error mapping buffer %d (%s): %s .\n",
+ __FILE__, __LINE__, bo_gem->gem_handle,
+ bo_gem->name, strerror(errno));
+ if (--bo_gem->map_count == 0)
+ drm_intel_gem_bo_close_vma(bufmgr_gem, bo_gem);
pthread_mutex_unlock(&bufmgr_gem->lock);
return ret;
}
set_domain.write_domain = I915_GEM_DOMAIN_CPU;
else
set_domain.write_domain = 0;
- do {
- ret = ioctl(bufmgr_gem->fd,
- DRM_IOCTL_I915_GEM_SET_DOMAIN,
- &set_domain);
- } while (ret == -1 && errno == EINTR);
+ ret = drmIoctl(bufmgr_gem->fd,
+ DRM_IOCTL_I915_GEM_SET_DOMAIN,
+ &set_domain);
if (ret != 0) {
- ret = -errno;
- fprintf(stderr, "%s:%d: Error setting to CPU domain %d: %s\n",
- __FILE__, __LINE__, bo_gem->gem_handle,
- strerror(errno));
- pthread_mutex_unlock(&bufmgr_gem->lock);
- return ret;
+ DBG("%s:%d: Error setting to CPU domain %d: %s\n",
+ __FILE__, __LINE__, bo_gem->gem_handle,
+ strerror(errno));
}
+ if (write_enable)
+ bo_gem->mapped_cpu_write = true;
+
pthread_mutex_unlock(&bufmgr_gem->lock);
return 0;
pthread_mutex_lock(&bufmgr_gem->lock);
+ if (bo_gem->map_count++ == 0)
+ drm_intel_gem_bo_open_vma(bufmgr_gem, bo_gem);
+
/* Get a mapping of the buffer if we haven't before. */
if (bo_gem->gtt_virtual == NULL) {
struct drm_i915_gem_mmap_gtt mmap_arg;
- DBG("bo_map_gtt: mmap %d (%s)\n", bo_gem->gem_handle,
- bo_gem->name);
+ DBG("bo_map_gtt: mmap %d (%s), map_count=%d\n",
+ bo_gem->gem_handle, bo_gem->name, bo_gem->map_count);
memset(&mmap_arg, 0, sizeof(mmap_arg));
mmap_arg.handle = bo_gem->gem_handle;
/* Get the fake offset back... */
- do {
- ret = ioctl(bufmgr_gem->fd,
- DRM_IOCTL_I915_GEM_MMAP_GTT,
- &mmap_arg);
- } while (ret == -1 && errno == EINTR);
+ ret = drmIoctl(bufmgr_gem->fd,
+ DRM_IOCTL_I915_GEM_MMAP_GTT,
+ &mmap_arg);
if (ret != 0) {
ret = -errno;
- fprintf(stderr,
- "%s:%d: Error preparing buffer map %d (%s): %s .\n",
- __FILE__, __LINE__,
- bo_gem->gem_handle, bo_gem->name,
- strerror(errno));
+ DBG("%s:%d: Error preparing buffer map %d (%s): %s .\n",
+ __FILE__, __LINE__,
+ bo_gem->gem_handle, bo_gem->name,
+ strerror(errno));
+ if (--bo_gem->map_count == 0)
+ drm_intel_gem_bo_close_vma(bufmgr_gem, bo_gem);
pthread_mutex_unlock(&bufmgr_gem->lock);
return ret;
}
if (bo_gem->gtt_virtual == MAP_FAILED) {
bo_gem->gtt_virtual = NULL;
ret = -errno;
- fprintf(stderr,
- "%s:%d: Error mapping buffer %d (%s): %s .\n",
- __FILE__, __LINE__,
- bo_gem->gem_handle, bo_gem->name,
- strerror(errno));
+ DBG("%s:%d: Error mapping buffer %d (%s): %s .\n",
+ __FILE__, __LINE__,
+ bo_gem->gem_handle, bo_gem->name,
+ strerror(errno));
+ if (--bo_gem->map_count == 0)
+ drm_intel_gem_bo_close_vma(bufmgr_gem, bo_gem);
pthread_mutex_unlock(&bufmgr_gem->lock);
return ret;
}
set_domain.handle = bo_gem->gem_handle;
set_domain.read_domains = I915_GEM_DOMAIN_GTT;
set_domain.write_domain = I915_GEM_DOMAIN_GTT;
- do {
- ret = ioctl(bufmgr_gem->fd,
- DRM_IOCTL_I915_GEM_SET_DOMAIN,
- &set_domain);
- } while (ret == -1 && errno == EINTR);
-
+ ret = drmIoctl(bufmgr_gem->fd,
+ DRM_IOCTL_I915_GEM_SET_DOMAIN,
+ &set_domain);
if (ret != 0) {
- ret = -errno;
- fprintf(stderr, "%s:%d: Error setting domain %d: %s\n",
- __FILE__, __LINE__, bo_gem->gem_handle,
- strerror(errno));
+ DBG("%s:%d: Error setting domain %d: %s\n",
+ __FILE__, __LINE__, bo_gem->gem_handle,
+ strerror(errno));
}
pthread_mutex_unlock(&bufmgr_gem->lock);
- return ret;
+ return 0;
}
-int drm_intel_gem_bo_unmap_gtt(drm_intel_bo *bo)
+static int drm_intel_gem_bo_unmap(drm_intel_bo *bo)
{
drm_intel_bufmgr_gem *bufmgr_gem = (drm_intel_bufmgr_gem *) bo->bufmgr;
drm_intel_bo_gem *bo_gem = (drm_intel_bo_gem *) bo;
+ struct drm_i915_gem_sw_finish sw_finish;
int ret = 0;
if (bo == NULL)
return 0;
- assert(bo_gem->gtt_virtual != NULL);
-
pthread_mutex_lock(&bufmgr_gem->lock);
- bo->virtual = NULL;
- pthread_mutex_unlock(&bufmgr_gem->lock);
-
- return ret;
-}
-
-static int drm_intel_gem_bo_unmap(drm_intel_bo *bo)
-{
- drm_intel_bufmgr_gem *bufmgr_gem = (drm_intel_bufmgr_gem *) bo->bufmgr;
- drm_intel_bo_gem *bo_gem = (drm_intel_bo_gem *) bo;
- struct drm_i915_gem_sw_finish sw_finish;
- int ret;
- if (bo == NULL)
+ if (bo_gem->map_count <= 0) {
+ DBG("attempted to unmap an unmapped bo\n");
+ pthread_mutex_unlock(&bufmgr_gem->lock);
+ /* Preserve the old behaviour of just treating this as a
+ * no-op rather than reporting the error.
+ */
return 0;
+ }
- assert(bo_gem->mem_virtual != NULL);
+ if (bo_gem->mapped_cpu_write) {
+ /* Cause a flush to happen if the buffer's pinned for
+ * scanout, so the results show up in a timely manner.
+ * Unlike GTT set domains, this only does work if the
+ * buffer should be scanout-related.
+ */
+ sw_finish.handle = bo_gem->gem_handle;
+ ret = drmIoctl(bufmgr_gem->fd,
+ DRM_IOCTL_I915_GEM_SW_FINISH,
+ &sw_finish);
+ ret = ret == -1 ? -errno : 0;
- pthread_mutex_lock(&bufmgr_gem->lock);
+ bo_gem->mapped_cpu_write = false;
+ }
- /* Cause a flush to happen if the buffer's pinned for scanout, so the
- * results show up in a timely manner.
+ /* We need to unmap after every innovation as we cannot track
+ * an open vma for every bo as that will exhaasut the system
+ * limits and cause later failures.
*/
- sw_finish.handle = bo_gem->gem_handle;
- do {
- ret = ioctl(bufmgr_gem->fd,
- DRM_IOCTL_I915_GEM_SW_FINISH,
- &sw_finish);
- } while (ret == -1 && errno == EINTR);
-
- bo->virtual = NULL;
+ if (--bo_gem->map_count == 0) {
+ drm_intel_gem_bo_close_vma(bufmgr_gem, bo_gem);
+ bo->virtual = NULL;
+ }
pthread_mutex_unlock(&bufmgr_gem->lock);
- return 0;
+
+ return ret;
+}
+
+int drm_intel_gem_bo_unmap_gtt(drm_intel_bo *bo)
+{
+ return drm_intel_gem_bo_unmap(bo);
}
static int
pwrite.offset = offset;
pwrite.size = size;
pwrite.data_ptr = (uint64_t) (uintptr_t) data;
- do {
- ret = ioctl(bufmgr_gem->fd,
- DRM_IOCTL_I915_GEM_PWRITE,
- &pwrite);
- } while (ret == -1 && errno == EINTR);
+ ret = drmIoctl(bufmgr_gem->fd,
+ DRM_IOCTL_I915_GEM_PWRITE,
+ &pwrite);
if (ret != 0) {
- fprintf(stderr,
- "%s:%d: Error writing data to buffer %d: (%d %d) %s .\n",
- __FILE__, __LINE__, bo_gem->gem_handle, (int)offset,
- (int)size, strerror(errno));
+ ret = -errno;
+ DBG("%s:%d: Error writing data to buffer %d: (%d %d) %s .\n",
+ __FILE__, __LINE__, bo_gem->gem_handle, (int)offset,
+ (int)size, strerror(errno));
}
- return 0;
+
+ return ret;
}
static int
int ret;
get_pipe_from_crtc_id.crtc_id = crtc_id;
- ret = ioctl(bufmgr_gem->fd, DRM_IOCTL_I915_GET_PIPE_FROM_CRTC_ID,
- &get_pipe_from_crtc_id);
+ ret = drmIoctl(bufmgr_gem->fd,
+ DRM_IOCTL_I915_GET_PIPE_FROM_CRTC_ID,
+ &get_pipe_from_crtc_id);
if (ret != 0) {
/* We return -1 here to signal that we don't
* know which pipe is associated with this crtc.
pread.offset = offset;
pread.size = size;
pread.data_ptr = (uint64_t) (uintptr_t) data;
- do {
- ret = ioctl(bufmgr_gem->fd,
- DRM_IOCTL_I915_GEM_PREAD,
- &pread);
- } while (ret == -1 && errno == EINTR);
+ ret = drmIoctl(bufmgr_gem->fd,
+ DRM_IOCTL_I915_GEM_PREAD,
+ &pread);
if (ret != 0) {
ret = -errno;
- fprintf(stderr,
- "%s:%d: Error reading data from buffer %d: (%d %d) %s .\n",
- __FILE__, __LINE__, bo_gem->gem_handle, (int)offset,
- (int)size, strerror(errno));
+ DBG("%s:%d: Error reading data from buffer %d: (%d %d) %s .\n",
+ __FILE__, __LINE__, bo_gem->gem_handle, (int)offset,
+ (int)size, strerror(errno));
}
+
return ret;
}
-/** Waits for all GPU rendering to the object to have completed. */
+/** Waits for all GPU rendering with the object to have completed. */
static void
drm_intel_gem_bo_wait_rendering(drm_intel_bo *bo)
{
- drm_intel_gem_bo_start_gtt_access(bo, 0);
+ drm_intel_gem_bo_start_gtt_access(bo, 1);
}
/**
set_domain.handle = bo_gem->gem_handle;
set_domain.read_domains = I915_GEM_DOMAIN_GTT;
set_domain.write_domain = write_enable ? I915_GEM_DOMAIN_GTT : 0;
- do {
- ret = ioctl(bufmgr_gem->fd,
- DRM_IOCTL_I915_GEM_SET_DOMAIN,
- &set_domain);
- } while (ret == -1 && errno == EINTR);
+ ret = drmIoctl(bufmgr_gem->fd,
+ DRM_IOCTL_I915_GEM_SET_DOMAIN,
+ &set_domain);
if (ret != 0) {
- fprintf(stderr,
- "%s:%d: Error setting memory domains %d (%08x %08x): %s .\n",
- __FILE__, __LINE__, bo_gem->gem_handle,
- set_domain.read_domains, set_domain.write_domain,
- strerror(errno));
+ DBG("%s:%d: Error setting memory domains %d (%08x %08x): %s .\n",
+ __FILE__, __LINE__, bo_gem->gem_handle,
+ set_domain.read_domains, set_domain.write_domain,
+ strerror(errno));
}
}
pthread_mutex_destroy(&bufmgr_gem->lock);
/* Free any cached buffer objects we were going to reuse */
- for (i = 0; i < DRM_INTEL_GEM_BO_BUCKETS; i++) {
+ for (i = 0; i < bufmgr_gem->num_buckets; i++) {
struct drm_intel_gem_bo_bucket *bucket =
&bufmgr_gem->cache_bucket[i];
drm_intel_bo_gem *bo_gem;
do_bo_emit_reloc(drm_intel_bo *bo, uint32_t offset,
drm_intel_bo *target_bo, uint32_t target_offset,
uint32_t read_domains, uint32_t write_domain,
- int need_fence)
+ bool need_fence)
{
drm_intel_bufmgr_gem *bufmgr_gem = (drm_intel_bufmgr_gem *) bo->bufmgr;
drm_intel_bo_gem *bo_gem = (drm_intel_bo_gem *) bo;
drm_intel_bo_gem *target_bo_gem = (drm_intel_bo_gem *) target_bo;
+ bool fenced_command;
if (bo_gem->has_error)
return -ENOMEM;
if (target_bo_gem->has_error) {
- bo_gem->has_error = 1;
+ bo_gem->has_error = true;
return -ENOMEM;
}
- if (target_bo_gem->tiling_mode == I915_TILING_NONE)
- need_fence = 0;
-
/* We never use HW fences for rendering on 965+ */
- if (IS_GEN4(bufmgr_gem))
- need_fence = 0;
+ if (bufmgr_gem->gen >= 4)
+ need_fence = false;
+
+ fenced_command = need_fence;
+ if (target_bo_gem->tiling_mode == I915_TILING_NONE)
+ need_fence = false;
/* Create a new relocation list if needed */
if (bo_gem->relocs == NULL && drm_intel_setup_reloc_list(bo))
* already been accounted for.
*/
assert(!bo_gem->used_as_reloc_target);
- bo_gem->reloc_tree_size += target_bo_gem->reloc_tree_size;
- /* An object needing a fence is a tiled buffer, and so it won't have
+ if (target_bo_gem != bo_gem) {
+ target_bo_gem->used_as_reloc_target = true;
+ bo_gem->reloc_tree_size += target_bo_gem->reloc_tree_size;
+ }
+ /* An object needing a fence is a tiled buffer, so it won't have
* relocs to other buffers.
*/
if (need_fence)
target_bo_gem->reloc_tree_fences = 1;
bo_gem->reloc_tree_fences += target_bo_gem->reloc_tree_fences;
- /* Flag the target to disallow further relocations in it. */
- target_bo_gem->used_as_reloc_target = 1;
-
bo_gem->relocs[bo_gem->reloc_count].offset = offset;
bo_gem->relocs[bo_gem->reloc_count].delta = target_offset;
bo_gem->relocs[bo_gem->reloc_count].target_handle =
bo_gem->relocs[bo_gem->reloc_count].presumed_offset = target_bo->offset;
bo_gem->reloc_target_info[bo_gem->reloc_count].bo = target_bo;
- drm_intel_gem_bo_reference(target_bo);
- if (need_fence)
+ if (target_bo != bo)
+ drm_intel_gem_bo_reference(target_bo);
+ if (fenced_command)
bo_gem->reloc_target_info[bo_gem->reloc_count].flags =
DRM_INTEL_RELOC_FENCE;
else
uint32_t read_domains, uint32_t write_domain)
{
return do_bo_emit_reloc(bo, offset, target_bo, target_offset,
- read_domains, write_domain, 1);
+ read_domains, write_domain, true);
+}
+
+int
+drm_intel_gem_bo_get_reloc_count(drm_intel_bo *bo)
+{
+ drm_intel_bo_gem *bo_gem = (drm_intel_bo_gem *) bo;
+
+ return bo_gem->reloc_count;
+}
+
+/**
+ * Removes existing relocation entries in the BO after "start".
+ *
+ * This allows a user to avoid a two-step process for state setup with
+ * counting up all the buffer objects and doing a
+ * drm_intel_bufmgr_check_aperture_space() before emitting any of the
+ * relocations for the state setup. Instead, save the state of the
+ * batchbuffer including drm_intel_gem_get_reloc_count(), emit all the
+ * state, and then check if it still fits in the aperture.
+ *
+ * Any further drm_intel_bufmgr_check_aperture_space() queries
+ * involving this buffer in the tree are undefined after this call.
+ */
+void
+drm_intel_gem_bo_clear_relocs(drm_intel_bo *bo, int start)
+{
+ drm_intel_bo_gem *bo_gem = (drm_intel_bo_gem *) bo;
+ int i;
+ struct timespec time;
+
+ clock_gettime(CLOCK_MONOTONIC, &time);
+
+ assert(bo_gem->reloc_count >= start);
+ /* Unreference the cleared target buffers */
+ for (i = start; i < bo_gem->reloc_count; i++) {
+ if (bo_gem->reloc_target_info[i].bo != bo) {
+ drm_intel_gem_bo_unreference_locked_timed(bo_gem->
+ reloc_target_info[i].bo,
+ time.tv_sec);
+ }
+ }
+ bo_gem->reloc_count = start;
}
/**
for (i = 0; i < bo_gem->reloc_count; i++) {
drm_intel_bo *target_bo = bo_gem->reloc_target_info[i].bo;
+ if (target_bo == bo)
+ continue;
+
/* Continue walking the tree depth-first. */
drm_intel_gem_bo_process_reloc(target_bo);
drm_intel_bo *target_bo = bo_gem->reloc_target_info[i].bo;
int need_fence;
+ if (target_bo == bo)
+ continue;
+
/* Continue walking the tree depth-first. */
drm_intel_gem_bo_process_reloc2(target_bo);
execbuf.DR1 = 0;
execbuf.DR4 = DR4;
- do {
- ret = ioctl(bufmgr_gem->fd,
- DRM_IOCTL_I915_GEM_EXECBUFFER,
- &execbuf);
- } while (ret != 0 && errno == EINTR);
-
+ ret = drmIoctl(bufmgr_gem->fd,
+ DRM_IOCTL_I915_GEM_EXECBUFFER,
+ &execbuf);
if (ret != 0) {
ret = -errno;
if (errno == ENOSPC) {
- fprintf(stderr,
- "Execbuffer fails to pin. "
- "Estimate: %u. Actual: %u. Available: %u\n",
- drm_intel_gem_estimate_batch_space(bufmgr_gem->exec_bos,
- bufmgr_gem->
- exec_count),
- drm_intel_gem_compute_batch_space(bufmgr_gem->exec_bos,
- bufmgr_gem->
- exec_count),
- (unsigned int)bufmgr_gem->gtt_size);
+ DBG("Execbuffer fails to pin. "
+ "Estimate: %u. Actual: %u. Available: %u\n",
+ drm_intel_gem_estimate_batch_space(bufmgr_gem->exec_bos,
+ bufmgr_gem->
+ exec_count),
+ drm_intel_gem_compute_batch_space(bufmgr_gem->exec_bos,
+ bufmgr_gem->
+ exec_count),
+ (unsigned int)bufmgr_gem->gtt_size);
}
}
drm_intel_update_buffer_offsets(bufmgr_gem);
}
static int
-drm_intel_gem_bo_exec2(drm_intel_bo *bo, int used,
- drm_clip_rect_t *cliprects, int num_cliprects,
- int DR4)
+drm_intel_gem_bo_mrb_exec2(drm_intel_bo *bo, int used,
+ drm_clip_rect_t *cliprects, int num_cliprects, int DR4,
+ unsigned int flags)
{
drm_intel_bufmgr_gem *bufmgr_gem = (drm_intel_bufmgr_gem *)bo->bufmgr;
struct drm_i915_gem_execbuffer2 execbuf;
int ret, i;
+ switch (flags & 0x7) {
+ default:
+ return -EINVAL;
+ case I915_EXEC_BLT:
+ if (!bufmgr_gem->has_blt)
+ return -EINVAL;
+ break;
+ case I915_EXEC_BSD:
+ if (!bufmgr_gem->has_bsd)
+ return -EINVAL;
+ break;
+ case I915_EXEC_RENDER:
+ case I915_EXEC_DEFAULT:
+ break;
+ }
+
pthread_mutex_lock(&bufmgr_gem->lock);
/* Update indices and set up the validate list. */
drm_intel_gem_bo_process_reloc2(bo);
execbuf.num_cliprects = num_cliprects;
execbuf.DR1 = 0;
execbuf.DR4 = DR4;
- execbuf.flags = 0;
+ execbuf.flags = flags;
execbuf.rsvd1 = 0;
execbuf.rsvd2 = 0;
- do {
- ret = ioctl(bufmgr_gem->fd, DRM_IOCTL_I915_GEM_EXECBUFFER2,
- &execbuf);
- } while (ret != 0 && errno == EAGAIN);
-
- if (ret != 0 && errno == ENOMEM) {
- fprintf(stderr,
- "Execbuffer fails to pin. "
- "Estimate: %u. Actual: %u. Available: %u\n",
- drm_intel_gem_estimate_batch_space(bufmgr_gem->exec_bos,
- bufmgr_gem->exec_count),
- drm_intel_gem_compute_batch_space(bufmgr_gem->exec_bos,
- bufmgr_gem->exec_count),
- (unsigned int) bufmgr_gem->gtt_size);
+ ret = drmIoctl(bufmgr_gem->fd,
+ DRM_IOCTL_I915_GEM_EXECBUFFER2,
+ &execbuf);
+ if (ret != 0) {
+ ret = -errno;
+ if (ret == -ENOSPC) {
+ DBG("Execbuffer fails to pin. "
+ "Estimate: %u. Actual: %u. Available: %u\n",
+ drm_intel_gem_estimate_batch_space(bufmgr_gem->exec_bos,
+ bufmgr_gem->exec_count),
+ drm_intel_gem_compute_batch_space(bufmgr_gem->exec_bos,
+ bufmgr_gem->exec_count),
+ (unsigned int) bufmgr_gem->gtt_size);
+ }
}
drm_intel_update_buffer_offsets2(bufmgr_gem);
bufmgr_gem->exec_count = 0;
pthread_mutex_unlock(&bufmgr_gem->lock);
- return 0;
+ return ret;
+}
+
+static int
+drm_intel_gem_bo_exec2(drm_intel_bo *bo, int used,
+ drm_clip_rect_t *cliprects, int num_cliprects,
+ int DR4)
+{
+ return drm_intel_gem_bo_mrb_exec2(bo, used,
+ cliprects, num_cliprects, DR4,
+ I915_EXEC_RENDER);
}
static int
pin.handle = bo_gem->gem_handle;
pin.alignment = alignment;
- do {
- ret = ioctl(bufmgr_gem->fd,
- DRM_IOCTL_I915_GEM_PIN,
- &pin);
- } while (ret == -1 && errno == EINTR);
-
+ ret = drmIoctl(bufmgr_gem->fd,
+ DRM_IOCTL_I915_GEM_PIN,
+ &pin);
if (ret != 0)
return -errno;
memset(&unpin, 0, sizeof(unpin));
unpin.handle = bo_gem->gem_handle;
- ret = ioctl(bufmgr_gem->fd, DRM_IOCTL_I915_GEM_UNPIN, &unpin);
+ ret = drmIoctl(bufmgr_gem->fd, DRM_IOCTL_I915_GEM_UNPIN, &unpin);
if (ret != 0)
return -errno;
}
static int
-drm_intel_gem_bo_set_tiling(drm_intel_bo *bo, uint32_t * tiling_mode,
- uint32_t stride)
+drm_intel_gem_bo_set_tiling_internal(drm_intel_bo *bo,
+ uint32_t tiling_mode,
+ uint32_t stride)
{
drm_intel_bufmgr_gem *bufmgr_gem = (drm_intel_bufmgr_gem *) bo->bufmgr;
drm_intel_bo_gem *bo_gem = (drm_intel_bo_gem *) bo;
struct drm_i915_gem_set_tiling set_tiling;
int ret;
- if (bo_gem->global_name == 0 && *tiling_mode == bo_gem->tiling_mode)
+ if (bo_gem->global_name == 0 &&
+ tiling_mode == bo_gem->tiling_mode &&
+ stride == bo_gem->stride)
return 0;
memset(&set_tiling, 0, sizeof(set_tiling));
- set_tiling.handle = bo_gem->gem_handle;
-
do {
- set_tiling.tiling_mode = *tiling_mode;
+ /* set_tiling is slightly broken and overwrites the
+ * input on the error path, so we have to open code
+ * rmIoctl.
+ */
+ set_tiling.handle = bo_gem->gem_handle;
+ set_tiling.tiling_mode = tiling_mode;
set_tiling.stride = stride;
ret = ioctl(bufmgr_gem->fd,
DRM_IOCTL_I915_GEM_SET_TILING,
&set_tiling);
- } while (ret == -1 && errno == EINTR);
+ } while (ret == -1 && (errno == EINTR || errno == EAGAIN));
+ if (ret == -1)
+ return -errno;
+
bo_gem->tiling_mode = set_tiling.tiling_mode;
bo_gem->swizzle_mode = set_tiling.swizzle_mode;
+ bo_gem->stride = set_tiling.stride;
+ return 0;
+}
- drm_intel_bo_gem_set_in_aperture_size(bufmgr_gem, bo_gem);
+static int
+drm_intel_gem_bo_set_tiling(drm_intel_bo *bo, uint32_t * tiling_mode,
+ uint32_t stride)
+{
+ drm_intel_bufmgr_gem *bufmgr_gem = (drm_intel_bufmgr_gem *) bo->bufmgr;
+ drm_intel_bo_gem *bo_gem = (drm_intel_bo_gem *) bo;
+ int ret;
+
+ /* Linear buffers have no stride. By ensuring that we only ever use
+ * stride 0 with linear buffers, we simplify our code.
+ */
+ if (*tiling_mode == I915_TILING_NONE)
+ stride = 0;
+
+ ret = drm_intel_gem_bo_set_tiling_internal(bo, *tiling_mode, stride);
+ if (ret == 0)
+ drm_intel_bo_gem_set_in_aperture_size(bufmgr_gem, bo_gem);
*tiling_mode = bo_gem->tiling_mode;
- return ret == 0 ? 0 : -errno;
+ return ret;
}
static int
memset(&flink, 0, sizeof(flink));
flink.handle = bo_gem->gem_handle;
- ret = ioctl(bufmgr_gem->fd, DRM_IOCTL_GEM_FLINK, &flink);
+ ret = drmIoctl(bufmgr_gem->fd, DRM_IOCTL_GEM_FLINK, &flink);
if (ret != 0)
return -errno;
bo_gem->global_name = flink.name;
- bo_gem->reusable = 0;
+ bo_gem->reusable = false;
+
+ DRMLISTADDTAIL(&bo_gem->name_list, &bufmgr_gem->named);
}
*name = bo_gem->global_name;
{
drm_intel_bufmgr_gem *bufmgr_gem = (drm_intel_bufmgr_gem *) bufmgr;
- bufmgr_gem->bo_reuse = 1;
+ bufmgr_gem->bo_reuse = true;
}
/**
void
drm_intel_bufmgr_gem_enable_fenced_relocs(drm_intel_bufmgr *bufmgr)
{
- drm_intel_bufmgr_gem *bufmgr_gem = (drm_intel_bufmgr_gem *)bufmgr;
+ drm_intel_bufmgr_gem *bufmgr_gem = (drm_intel_bufmgr_gem *)bufmgr;
- bufmgr_gem->fenced_relocs = 1;
+ if (bufmgr_gem->bufmgr.bo_exec == drm_intel_gem_bo_exec2)
+ bufmgr_gem->fenced_relocs = true;
}
/**
return 0;
total += bo->size;
- bo_gem->included_in_check_aperture = 1;
+ bo_gem->included_in_check_aperture = true;
for (i = 0; i < bo_gem->reloc_count; i++)
total +=
if (bo == NULL || !bo_gem->included_in_check_aperture)
return;
- bo_gem->included_in_check_aperture = 0;
+ bo_gem->included_in_check_aperture = false;
for (i = 0; i < bo_gem->reloc_count; i++)
drm_intel_gem_bo_clear_aperture_space_flag(bo_gem->
{
drm_intel_bo_gem *bo_gem = (drm_intel_bo_gem *) bo;
- bo_gem->reusable = 0;
+ bo_gem->reusable = false;
return 0;
}
+static int
+drm_intel_gem_bo_is_reusable(drm_intel_bo *bo)
+{
+ drm_intel_bo_gem *bo_gem = (drm_intel_bo_gem *) bo;
+
+ return bo_gem->reusable;
+}
+
static int
_drm_intel_gem_bo_references(drm_intel_bo *bo, drm_intel_bo *target_bo)
{
for (i = 0; i < bo_gem->reloc_count; i++) {
if (bo_gem->reloc_target_info[i].bo == target_bo)
return 1;
+ if (bo == bo_gem->reloc_target_info[i].bo)
+ continue;
if (_drm_intel_gem_bo_references(bo_gem->reloc_target_info[i].bo,
target_bo))
return 1;
return 0;
}
+static void
+add_bucket(drm_intel_bufmgr_gem *bufmgr_gem, int size)
+{
+ unsigned int i = bufmgr_gem->num_buckets;
+
+ assert(i < ARRAY_SIZE(bufmgr_gem->cache_bucket));
+
+ DRMINITLISTHEAD(&bufmgr_gem->cache_bucket[i].head);
+ bufmgr_gem->cache_bucket[i].size = size;
+ bufmgr_gem->num_buckets++;
+}
+
+static void
+init_cache_buckets(drm_intel_bufmgr_gem *bufmgr_gem)
+{
+ unsigned long size, cache_max_size = 64 * 1024 * 1024;
+
+ /* OK, so power of two buckets was too wasteful of memory.
+ * Give 3 other sizes between each power of two, to hopefully
+ * cover things accurately enough. (The alternative is
+ * probably to just go for exact matching of sizes, and assume
+ * that for things like composited window resize the tiled
+ * width/height alignment and rounding of sizes to pages will
+ * get us useful cache hit rates anyway)
+ */
+ add_bucket(bufmgr_gem, 4096);
+ add_bucket(bufmgr_gem, 4096 * 2);
+ add_bucket(bufmgr_gem, 4096 * 3);
+
+ /* Initialize the linked lists for BO reuse cache. */
+ for (size = 4 * 4096; size <= cache_max_size; size *= 2) {
+ add_bucket(bufmgr_gem, size);
+
+ add_bucket(bufmgr_gem, size + size * 1 / 4);
+ add_bucket(bufmgr_gem, size + size * 2 / 4);
+ add_bucket(bufmgr_gem, size + size * 3 / 4);
+ }
+}
+
+void
+drm_intel_bufmgr_gem_set_vma_cache_size(drm_intel_bufmgr *bufmgr, int limit)
+{
+ drm_intel_bufmgr_gem *bufmgr_gem = (drm_intel_bufmgr_gem *)bufmgr;
+
+ bufmgr_gem->vma_max = limit;
+
+ drm_intel_gem_bo_purge_vma_cache(bufmgr_gem);
+}
+
/**
* Initializes the GEM buffer manager, which uses the kernel to allocate, map,
* and manage map buffer objections.
drm_intel_bufmgr_gem *bufmgr_gem;
struct drm_i915_gem_get_aperture aperture;
drm_i915_getparam_t gp;
- int ret, i;
- unsigned long size;
- int exec2 = 0;
+ int ret, tmp;
+ bool exec2 = false;
bufmgr_gem = calloc(1, sizeof(*bufmgr_gem));
if (bufmgr_gem == NULL)
return NULL;
}
- ret = ioctl(bufmgr_gem->fd, DRM_IOCTL_I915_GEM_GET_APERTURE, &aperture);
+ ret = drmIoctl(bufmgr_gem->fd,
+ DRM_IOCTL_I915_GEM_GET_APERTURE,
+ &aperture);
if (ret == 0)
bufmgr_gem->gtt_size = aperture.aper_available_size;
gp.param = I915_PARAM_CHIPSET_ID;
gp.value = &bufmgr_gem->pci_device;
- ret = ioctl(bufmgr_gem->fd, DRM_IOCTL_I915_GETPARAM, &gp);
+ ret = drmIoctl(bufmgr_gem->fd, DRM_IOCTL_I915_GETPARAM, &gp);
if (ret) {
fprintf(stderr, "get chip id failed: %d [%d]\n", ret, errno);
fprintf(stderr, "param: %d, val: %d\n", gp.param, *gp.value);
}
+ if (IS_GEN2(bufmgr_gem->pci_device))
+ bufmgr_gem->gen = 2;
+ else if (IS_GEN3(bufmgr_gem->pci_device))
+ bufmgr_gem->gen = 3;
+ else if (IS_GEN4(bufmgr_gem->pci_device))
+ bufmgr_gem->gen = 4;
+ else if (IS_GEN5(bufmgr_gem->pci_device))
+ bufmgr_gem->gen = 5;
+ else if (IS_GEN6(bufmgr_gem->pci_device))
+ bufmgr_gem->gen = 6;
+ else if (IS_GEN7(bufmgr_gem->pci_device))
+ bufmgr_gem->gen = 7;
+ else
+ assert(0);
+
+ if (IS_GEN3(bufmgr_gem->pci_device) &&
+ bufmgr_gem->gtt_size > 256*1024*1024) {
+ /* The unmappable part of gtt on gen 3 (i.e. above 256MB) can't
+ * be used for tiled blits. To simplify the accounting, just
+ * substract the unmappable part (fixed to 256MB on all known
+ * gen3 devices) if the kernel advertises it. */
+ bufmgr_gem->gtt_size -= 256*1024*1024;
+ }
+
+ gp.value = &tmp;
+
gp.param = I915_PARAM_HAS_EXECBUF2;
- ret = ioctl(bufmgr_gem->fd, DRM_IOCTL_I915_GETPARAM, &gp);
+ ret = drmIoctl(bufmgr_gem->fd, DRM_IOCTL_I915_GETPARAM, &gp);
if (!ret)
- exec2 = 1;
+ exec2 = true;
+
+ gp.param = I915_PARAM_HAS_BSD;
+ ret = drmIoctl(bufmgr_gem->fd, DRM_IOCTL_I915_GETPARAM, &gp);
+ bufmgr_gem->has_bsd = ret == 0;
- if (IS_GEN2(bufmgr_gem) || IS_GEN3(bufmgr_gem)) {
+ gp.param = I915_PARAM_HAS_BLT;
+ ret = drmIoctl(bufmgr_gem->fd, DRM_IOCTL_I915_GETPARAM, &gp);
+ bufmgr_gem->has_blt = ret == 0;
+
+ gp.param = I915_PARAM_HAS_RELAXED_FENCING;
+ ret = drmIoctl(bufmgr_gem->fd, DRM_IOCTL_I915_GETPARAM, &gp);
+ bufmgr_gem->has_relaxed_fencing = ret == 0;
+
+ gp.param = I915_PARAM_HAS_LLC;
+ ret = drmIoctl(bufmgr_gem->fd, DRM_IOCTL_I915_GETPARAM, &gp);
+ if (ret == -EINVAL) {
+ /* Kernel does not supports HAS_LLC query, fallback to GPU
+ * generation detection and assume that we have LLC on GEN6/7
+ */
+ bufmgr_gem->has_llc = (IS_GEN6(bufmgr_gem->pci_device) |
+ IS_GEN7(bufmgr_gem->pci_device));
+ } else
+ bufmgr_gem->has_llc = ret == 0;
+
+ if (bufmgr_gem->gen < 4) {
gp.param = I915_PARAM_NUM_FENCES_AVAIL;
gp.value = &bufmgr_gem->available_fences;
- ret = ioctl(bufmgr_gem->fd, DRM_IOCTL_I915_GETPARAM, &gp);
+ ret = drmIoctl(bufmgr_gem->fd, DRM_IOCTL_I915_GETPARAM, &gp);
if (ret) {
fprintf(stderr, "get fences failed: %d [%d]\n", ret,
errno);
bufmgr_gem->bufmgr.bo_set_tiling = drm_intel_gem_bo_set_tiling;
bufmgr_gem->bufmgr.bo_flink = drm_intel_gem_bo_flink;
/* Use the new one if available */
- if (exec2)
+ if (exec2) {
bufmgr_gem->bufmgr.bo_exec = drm_intel_gem_bo_exec2;
- else
+ bufmgr_gem->bufmgr.bo_mrb_exec = drm_intel_gem_bo_mrb_exec2;
+ } else
bufmgr_gem->bufmgr.bo_exec = drm_intel_gem_bo_exec;
bufmgr_gem->bufmgr.bo_busy = drm_intel_gem_bo_busy;
bufmgr_gem->bufmgr.bo_madvise = drm_intel_gem_bo_madvise;
bufmgr_gem->bufmgr.check_aperture_space =
drm_intel_gem_check_aperture_space;
bufmgr_gem->bufmgr.bo_disable_reuse = drm_intel_gem_bo_disable_reuse;
+ bufmgr_gem->bufmgr.bo_is_reusable = drm_intel_gem_bo_is_reusable;
bufmgr_gem->bufmgr.get_pipe_from_crtc_id =
drm_intel_gem_get_pipe_from_crtc_id;
bufmgr_gem->bufmgr.bo_references = drm_intel_gem_bo_references;
- /* Initialize the linked lists for BO reuse cache. */
- for (i = 0, size = 4096; i < DRM_INTEL_GEM_BO_BUCKETS; i++, size *= 2) {
- DRMINITLISTHEAD(&bufmgr_gem->cache_bucket[i].head);
- bufmgr_gem->cache_bucket[i].size = size;
- }
+ DRMINITLISTHEAD(&bufmgr_gem->named);
+ init_cache_buckets(bufmgr_gem);
+
+ DRMINITLISTHEAD(&bufmgr_gem->vma_cache);
+ bufmgr_gem->vma_max = -1; /* unlimited by default */
return &bufmgr_gem->bufmgr;
}