index 0f33b71d7f2e9a865059859c059bba2b082e47f6..43c49a9cb582ec7076e098cd3b695af3750b4383 100644 (file)
--- a/intel/intel_bufmgr_gem.c
+++ b/intel/intel_bufmgr_gem.c
/**************************************************************************
*
* Copyright © 2007 Red Hat Inc.
- * Copyright © 2007 Intel Corporation
+ * Copyright © 2007-2012 Intel Corporation
* Copyright 2006 Tungsten Graphics, Inc., Bismarck, ND., USA
* All Rights Reserved.
*
#include "intel_bufmgr.h"
#include "intel_bufmgr_priv.h"
#include "intel_chipset.h"
+#include "intel_aub.h"
#include "string.h"
#include "i915_drm.h"
unsigned int has_blt : 1;
unsigned int has_relaxed_fencing : 1;
unsigned int has_llc : 1;
+ unsigned int has_wait_timeout : 1;
unsigned int bo_reuse : 1;
+ unsigned int no_exec : 1;
bool fenced_relocs;
+
+ FILE *aub_file;
+ uint32_t aub_offset;
} drm_intel_bufmgr_gem;
#define DRM_INTEL_RELOC_FENCE (1<<0)
/** Flags that we may need to do the SW_FINSIH ioctl on unmap. */
bool mapped_cpu_write;
+
+ uint32_t aub_offset;
+
+ drm_intel_aub_annotation *aub_annotations;
+ unsigned aub_annotation_count;
};
static unsigned int
bo_gem->used_as_reloc_target = false;
bo_gem->has_error = false;
bo_gem->reusable = true;
+ bo_gem->aub_annotations = NULL;
+ bo_gem->aub_annotation_count = 0;
drm_intel_bo_gem_set_in_aperture_size(bufmgr_gem, bo_gem);
DBG("DRM_IOCTL_GEM_CLOSE %d failed (%s): %s\n",
bo_gem->gem_handle, bo_gem->name, strerror(errno));
}
+ free(bo_gem->aub_annotations);
free(bo);
}
return 0;
}
-int drm_intel_gem_bo_map_gtt(drm_intel_bo *bo)
+static int
+map_gtt(drm_intel_bo *bo)
{
drm_intel_bufmgr_gem *bufmgr_gem = (drm_intel_bufmgr_gem *) bo->bufmgr;
drm_intel_bo_gem *bo_gem = (drm_intel_bo_gem *) bo;
- struct drm_i915_gem_set_domain set_domain;
int ret;
- pthread_mutex_lock(&bufmgr_gem->lock);
-
if (bo_gem->map_count++ == 0)
drm_intel_gem_bo_open_vma(bufmgr_gem, bo_gem);
strerror(errno));
if (--bo_gem->map_count == 0)
drm_intel_gem_bo_close_vma(bufmgr_gem, bo_gem);
- pthread_mutex_unlock(&bufmgr_gem->lock);
return ret;
}
strerror(errno));
if (--bo_gem->map_count == 0)
drm_intel_gem_bo_close_vma(bufmgr_gem, bo_gem);
- pthread_mutex_unlock(&bufmgr_gem->lock);
return ret;
}
}
DBG("bo_map_gtt: %d (%s) -> %p\n", bo_gem->gem_handle, bo_gem->name,
bo_gem->gtt_virtual);
- /* Now move it to the GTT domain so that the CPU caches are flushed */
+ return 0;
+}
+
+int drm_intel_gem_bo_map_gtt(drm_intel_bo *bo)
+{
+ drm_intel_bufmgr_gem *bufmgr_gem = (drm_intel_bufmgr_gem *) bo->bufmgr;
+ drm_intel_bo_gem *bo_gem = (drm_intel_bo_gem *) bo;
+ struct drm_i915_gem_set_domain set_domain;
+ int ret;
+
+ pthread_mutex_lock(&bufmgr_gem->lock);
+
+ ret = map_gtt(bo);
+ if (ret) {
+ pthread_mutex_unlock(&bufmgr_gem->lock);
+ return ret;
+ }
+
+ /* Now move it to the GTT domain so that the GPU and CPU
+ * caches are flushed and the GPU isn't actively using the
+ * buffer.
+ *
+ * The pagefault handler does this domain change for us when
+ * it has unbound the BO from the GTT, but it's up to us to
+ * tell it when we're about to use things if we had done
+ * rendering and it still happens to be bound to the GTT.
+ */
VG_CLEAR(set_domain);
set_domain.handle = bo_gem->gem_handle;
set_domain.read_domains = I915_GEM_DOMAIN_GTT;
return 0;
}
+/**
+ * Performs a mapping of the buffer object like the normal GTT
+ * mapping, but avoids waiting for the GPU to be done reading from or
+ * rendering to the buffer.
+ *
+ * This is used in the implementation of GL_ARB_map_buffer_range: The
+ * user asks to create a buffer, then does a mapping, fills some
+ * space, runs a drawing command, then asks to map it again without
+ * synchronizing because it guarantees that it won't write over the
+ * data that the GPU is busy using (or, more specifically, that if it
+ * does write over the data, it acknowledges that rendering is
+ * undefined).
+ */
+
+int drm_intel_gem_bo_map_unsynchronized(drm_intel_bo *bo)
+{
+ drm_intel_bufmgr_gem *bufmgr_gem = (drm_intel_bufmgr_gem *) bo->bufmgr;
+ int ret;
+
+ /* If the CPU cache isn't coherent with the GTT, then use a
+ * regular synchronized mapping. The problem is that we don't
+ * track where the buffer was last used on the CPU side in
+ * terms of drm_intel_bo_map vs drm_intel_gem_bo_map_gtt, so
+ * we would potentially corrupt the buffer even when the user
+ * does reasonable things.
+ */
+ if (!bufmgr_gem->has_llc)
+ return drm_intel_gem_bo_map_gtt(bo);
+
+ pthread_mutex_lock(&bufmgr_gem->lock);
+ ret = map_gtt(bo);
+ pthread_mutex_unlock(&bufmgr_gem->lock);
+
+ return ret;
+}
+
static int drm_intel_gem_bo_unmap(drm_intel_bo *bo)
{
drm_intel_bufmgr_gem *bufmgr_gem = (drm_intel_bufmgr_gem *) bo->bufmgr;
drm_intel_gem_bo_start_gtt_access(bo, 1);
}
+/**
+ * Waits on a BO for the given amount of time.
+ *
+ * @bo: buffer object to wait for
+ * @timeout_ns: amount of time to wait in nanoseconds.
+ * If value is less than 0, an infinite wait will occur.
+ *
+ * Returns 0 if the wait was successful ie. the last batch referencing the
+ * object has completed within the allotted time. Otherwise some negative return
+ * value describes the error. Of particular interest is -ETIME when the wait has
+ * failed to yield the desired result.
+ *
+ * Similar to drm_intel_gem_bo_wait_rendering except a timeout parameter allows
+ * the operation to give up after a certain amount of time. Another subtle
+ * difference is the internal locking semantics are different (this variant does
+ * not hold the lock for the duration of the wait). This makes the wait subject
+ * to a larger userspace race window.
+ *
+ * The implementation shall wait until the object is no longer actively
+ * referenced within a batch buffer at the time of the call. The wait will
+ * not guarantee that the buffer is re-issued via another thread, or an flinked
+ * handle. Userspace must make sure this race does not occur if such precision
+ * is important.
+ */
+int drm_intel_gem_bo_wait(drm_intel_bo *bo, int64_t timeout_ns)
+{
+ drm_intel_bufmgr_gem *bufmgr_gem = (drm_intel_bufmgr_gem *) bo->bufmgr;
+ drm_intel_bo_gem *bo_gem = (drm_intel_bo_gem *) bo;
+ struct drm_i915_gem_wait wait;
+ int ret;
+
+ if (!bufmgr_gem->has_wait_timeout) {
+ DBG("%s:%d: Timed wait is not supported. Falling back to "
+ "infinite wait\n", __FILE__, __LINE__);
+ if (timeout_ns) {
+ drm_intel_gem_bo_wait_rendering(bo);
+ return 0;
+ } else {
+ return drm_intel_gem_bo_busy(bo) ? -ETIME : 0;
+ }
+ }
+
+ wait.bo_handle = bo_gem->gem_handle;
+ wait.timeout_ns = timeout_ns;
+ wait.flags = 0;
+ ret = drmIoctl(bufmgr_gem->fd, DRM_IOCTL_I915_GEM_WAIT, &wait);
+ if (ret == -1)
+ return -errno;
+
+ return ret;
+}
+
/**
* Sets the object to the GTT read and possibly write domain, used by the X
* 2D driver in the absence of kernel support to do drm_intel_gem_bo_map_gtt().
}
}
+static void
+aub_out(drm_intel_bufmgr_gem *bufmgr_gem, uint32_t data)
+{
+ fwrite(&data, 1, 4, bufmgr_gem->aub_file);
+}
+
+static void
+aub_out_data(drm_intel_bufmgr_gem *bufmgr_gem, void *data, size_t size)
+{
+ fwrite(data, 1, size, bufmgr_gem->aub_file);
+}
+
+static void
+aub_write_bo_data(drm_intel_bo *bo, uint32_t offset, uint32_t size)
+{
+ drm_intel_bufmgr_gem *bufmgr_gem = (drm_intel_bufmgr_gem *) bo->bufmgr;
+ drm_intel_bo_gem *bo_gem = (drm_intel_bo_gem *) bo;
+ uint32_t *data;
+ unsigned int i;
+
+ data = malloc(bo->size);
+ drm_intel_bo_get_subdata(bo, offset, size, data);
+
+ /* Easy mode: write out bo with no relocations */
+ if (!bo_gem->reloc_count) {
+ aub_out_data(bufmgr_gem, data, size);
+ free(data);
+ return;
+ }
+
+ /* Otherwise, handle the relocations while writing. */
+ for (i = 0; i < size / 4; i++) {
+ int r;
+ for (r = 0; r < bo_gem->reloc_count; r++) {
+ struct drm_i915_gem_relocation_entry *reloc;
+ drm_intel_reloc_target *info;
+
+ reloc = &bo_gem->relocs[r];
+ info = &bo_gem->reloc_target_info[r];
+
+ if (reloc->offset == offset + i * 4) {
+ drm_intel_bo_gem *target_gem;
+ uint32_t val;
+
+ target_gem = (drm_intel_bo_gem *)info->bo;
+
+ val = reloc->delta;
+ val += target_gem->aub_offset;
+
+ aub_out(bufmgr_gem, val);
+ data[i] = val;
+ break;
+ }
+ }
+ if (r == bo_gem->reloc_count) {
+ /* no relocation, just the data */
+ aub_out(bufmgr_gem, data[i]);
+ }
+ }
+
+ free(data);
+}
+
+static void
+aub_bo_get_address(drm_intel_bo *bo)
+{
+ drm_intel_bufmgr_gem *bufmgr_gem = (drm_intel_bufmgr_gem *) bo->bufmgr;
+ drm_intel_bo_gem *bo_gem = (drm_intel_bo_gem *) bo;
+
+ /* Give the object a graphics address in the AUB file. We
+ * don't just use the GEM object address because we do AUB
+ * dumping before execution -- we want to successfully log
+ * when the hardware might hang, and we might even want to aub
+ * capture for a driver trying to execute on a different
+ * generation of hardware by disabling the actual kernel exec
+ * call.
+ */
+ bo_gem->aub_offset = bufmgr_gem->aub_offset;
+ bufmgr_gem->aub_offset += bo->size;
+ /* XXX: Handle aperture overflow. */
+ assert(bufmgr_gem->aub_offset < 256 * 1024 * 1024);
+}
+
+static void
+aub_write_trace_block(drm_intel_bo *bo, uint32_t type, uint32_t subtype,
+ uint32_t offset, uint32_t size)
+{
+ drm_intel_bufmgr_gem *bufmgr_gem = (drm_intel_bufmgr_gem *) bo->bufmgr;
+ drm_intel_bo_gem *bo_gem = (drm_intel_bo_gem *) bo;
+
+ aub_out(bufmgr_gem,
+ CMD_AUB_TRACE_HEADER_BLOCK |
+ (5 - 2));
+ aub_out(bufmgr_gem,
+ AUB_TRACE_MEMTYPE_GTT | type | AUB_TRACE_OP_DATA_WRITE);
+ aub_out(bufmgr_gem, subtype);
+ aub_out(bufmgr_gem, bo_gem->aub_offset + offset);
+ aub_out(bufmgr_gem, size);
+ aub_write_bo_data(bo, offset, size);
+}
+
+/**
+ * Break up large objects into multiple writes. Otherwise a 128kb VBO
+ * would overflow the 16 bits of size field in the packet header and
+ * everything goes badly after that.
+ */
+static void
+aub_write_large_trace_block(drm_intel_bo *bo, uint32_t type, uint32_t subtype,
+ uint32_t offset, uint32_t size)
+{
+ uint32_t block_size;
+ uint32_t sub_offset;
+
+ for (sub_offset = 0; sub_offset < size; sub_offset += block_size) {
+ block_size = size - sub_offset;
+
+ if (block_size > 8 * 4096)
+ block_size = 8 * 4096;
+
+ aub_write_trace_block(bo, type, subtype, offset + sub_offset,
+ block_size);
+ }
+}
+
+static void
+aub_write_bo(drm_intel_bo *bo)
+{
+ drm_intel_bo_gem *bo_gem = (drm_intel_bo_gem *) bo;
+ uint32_t offset = 0;
+ unsigned i;
+
+ aub_bo_get_address(bo);
+
+ /* Write out each annotated section separately. */
+ for (i = 0; i < bo_gem->aub_annotation_count; ++i) {
+ drm_intel_aub_annotation *annotation =
+ &bo_gem->aub_annotations[i];
+ uint32_t ending_offset = annotation->ending_offset;
+ if (ending_offset > bo->size)
+ ending_offset = bo->size;
+ if (ending_offset > offset) {
+ aub_write_large_trace_block(bo, annotation->type,
+ annotation->subtype,
+ offset,
+ ending_offset - offset);
+ offset = ending_offset;
+ }
+ }
+
+ /* Write out any remaining unannotated data */
+ if (offset < bo->size) {
+ aub_write_large_trace_block(bo, AUB_TRACE_TYPE_NOTYPE, 0,
+ offset, bo->size - offset);
+ }
+}
+
+/*
+ * Make a ringbuffer on fly and dump it
+ */
+static void
+aub_build_dump_ringbuffer(drm_intel_bufmgr_gem *bufmgr_gem,
+ uint32_t batch_buffer, int ring_flag)
+{
+ uint32_t ringbuffer[4096];
+ int ring = AUB_TRACE_TYPE_RING_PRB0; /* The default ring */
+ int ring_count = 0;
+
+ if (ring_flag == I915_EXEC_BSD)
+ ring = AUB_TRACE_TYPE_RING_PRB1;
+
+ /* Make a ring buffer to execute our batchbuffer. */
+ memset(ringbuffer, 0, sizeof(ringbuffer));
+ ringbuffer[ring_count++] = AUB_MI_BATCH_BUFFER_START;
+ ringbuffer[ring_count++] = batch_buffer;
+
+ /* Write out the ring. This appears to trigger execution of
+ * the ring in the simulator.
+ */
+ aub_out(bufmgr_gem,
+ CMD_AUB_TRACE_HEADER_BLOCK |
+ (5 - 2));
+ aub_out(bufmgr_gem,
+ AUB_TRACE_MEMTYPE_GTT | ring | AUB_TRACE_OP_COMMAND_WRITE);
+ aub_out(bufmgr_gem, 0); /* general/surface subtype */
+ aub_out(bufmgr_gem, bufmgr_gem->aub_offset);
+ aub_out(bufmgr_gem, ring_count * 4);
+
+ /* FIXME: Need some flush operations here? */
+ aub_out_data(bufmgr_gem, ringbuffer, ring_count * 4);
+
+ /* Update offset pointer */
+ bufmgr_gem->aub_offset += 4096;
+}
+
+void
+drm_intel_gem_bo_aub_dump_bmp(drm_intel_bo *bo,
+ int x1, int y1, int width, int height,
+ enum aub_dump_bmp_format format,
+ int pitch, int offset)
+{
+ drm_intel_bufmgr_gem *bufmgr_gem = (drm_intel_bufmgr_gem *) bo->bufmgr;
+ drm_intel_bo_gem *bo_gem = (drm_intel_bo_gem *)bo;
+ uint32_t cpp;
+
+ switch (format) {
+ case AUB_DUMP_BMP_FORMAT_8BIT:
+ cpp = 1;
+ break;
+ case AUB_DUMP_BMP_FORMAT_ARGB_4444:
+ cpp = 2;
+ break;
+ case AUB_DUMP_BMP_FORMAT_ARGB_0888:
+ case AUB_DUMP_BMP_FORMAT_ARGB_8888:
+ cpp = 4;
+ break;
+ default:
+ printf("Unknown AUB dump format %d\n", format);
+ return;
+ }
+
+ if (!bufmgr_gem->aub_file)
+ return;
+
+ aub_out(bufmgr_gem, CMD_AUB_DUMP_BMP | 4);
+ aub_out(bufmgr_gem, (y1 << 16) | x1);
+ aub_out(bufmgr_gem,
+ (format << 24) |
+ (cpp << 19) |
+ pitch / 4);
+ aub_out(bufmgr_gem, (height << 16) | width);
+ aub_out(bufmgr_gem, bo_gem->aub_offset + offset);
+ aub_out(bufmgr_gem,
+ ((bo_gem->tiling_mode != I915_TILING_NONE) ? (1 << 2) : 0) |
+ ((bo_gem->tiling_mode == I915_TILING_Y) ? (1 << 3) : 0));
+}
+
+static void
+aub_exec(drm_intel_bo *bo, int ring_flag, int used)
+{
+ drm_intel_bufmgr_gem *bufmgr_gem = (drm_intel_bufmgr_gem *) bo->bufmgr;
+ drm_intel_bo_gem *bo_gem = (drm_intel_bo_gem *) bo;
+ int i;
+ bool batch_buffer_needs_annotations;
+
+ if (!bufmgr_gem->aub_file)
+ return;
+
+ /* If batch buffer is not annotated, annotate it the best we
+ * can.
+ */
+ batch_buffer_needs_annotations = bo_gem->aub_annotation_count == 0;
+ if (batch_buffer_needs_annotations) {
+ drm_intel_aub_annotation annotations[2] = {
+ { AUB_TRACE_TYPE_BATCH, 0, used },
+ { AUB_TRACE_TYPE_NOTYPE, 0, bo->size }
+ };
+ drm_intel_bufmgr_gem_set_aub_annotations(bo, annotations, 2);
+ }
+
+ /* Write out all buffers to AUB memory */
+ for (i = 0; i < bufmgr_gem->exec_count; i++) {
+ aub_write_bo(bufmgr_gem->exec_bos[i]);
+ }
+
+ /* Remove any annotations we added */
+ if (batch_buffer_needs_annotations)
+ drm_intel_bufmgr_gem_set_aub_annotations(bo, NULL, 0);
+
+ /* Dump ring buffer */
+ aub_build_dump_ringbuffer(bufmgr_gem, bo_gem->aub_offset, ring_flag);
+
+ fflush(bufmgr_gem->aub_file);
+
+ /*
+ * One frame has been dumped. So reset the aub_offset for the next frame.
+ *
+ * FIXME: Can we do this?
+ */
+ bufmgr_gem->aub_offset = 0x10000;
+}
+
static int
drm_intel_gem_bo_exec(drm_intel_bo *bo, int used,
drm_clip_rect_t * cliprects, int num_cliprects, int DR4)
}
static int
-drm_intel_gem_bo_mrb_exec2(drm_intel_bo *bo, int used,
- drm_clip_rect_t *cliprects, int num_cliprects, int DR4,
- unsigned int flags)
+do_exec2(drm_intel_bo *bo, int used, drm_intel_context *ctx,
+ drm_clip_rect_t *cliprects, int num_cliprects, int DR4,
+ unsigned int flags)
{
drm_intel_bufmgr_gem *bufmgr_gem = (drm_intel_bufmgr_gem *)bo->bufmgr;
struct drm_i915_gem_execbuffer2 execbuf;
- int ret, i;
+ int ret = 0;
+ int i;
switch (flags & 0x7) {
default:
execbuf.DR1 = 0;
execbuf.DR4 = DR4;
execbuf.flags = flags;
- execbuf.rsvd1 = 0;
+ if (ctx == NULL)
+ i915_execbuffer2_set_context_id(execbuf, 0);
+ else
+ i915_execbuffer2_set_context_id(execbuf, ctx->ctx_id);
execbuf.rsvd2 = 0;
+ aub_exec(bo, flags, used);
+
+ if (bufmgr_gem->no_exec)
+ goto skip_execution;
+
ret = drmIoctl(bufmgr_gem->fd,
DRM_IOCTL_I915_GEM_EXECBUFFER2,
&execbuf);
}
drm_intel_update_buffer_offsets2(bufmgr_gem);
+skip_execution:
if (bufmgr_gem->bufmgr.debug)
drm_intel_gem_dump_validation_list(bufmgr_gem);
drm_clip_rect_t *cliprects, int num_cliprects,
int DR4)
{
- return drm_intel_gem_bo_mrb_exec2(bo, used,
- cliprects, num_cliprects, DR4,
- I915_EXEC_RENDER);
+ return do_exec2(bo, used, NULL, cliprects, num_cliprects, DR4,
+ I915_EXEC_RENDER);
+}
+
+static int
+drm_intel_gem_bo_mrb_exec2(drm_intel_bo *bo, int used,
+ drm_clip_rect_t *cliprects, int num_cliprects, int DR4,
+ unsigned int flags)
+{
+ return do_exec2(bo, used, NULL, cliprects, num_cliprects, DR4,
+ flags);
+}
+
+int
+drm_intel_gem_bo_context_exec(drm_intel_bo *bo, drm_intel_context *ctx,
+ int used, unsigned int flags)
+{
+ return do_exec2(bo, used, ctx, NULL, 0, 0, flags);
}
static int
return 0;
}
+drm_intel_bo *
+drm_intel_bo_gem_create_from_prime(drm_intel_bufmgr *bufmgr, int prime_fd, int size)
+{
+ drm_intel_bufmgr_gem *bufmgr_gem = (drm_intel_bufmgr_gem *) bufmgr;
+ int ret;
+ uint32_t handle;
+ drm_intel_bo_gem *bo_gem;
+ struct drm_i915_gem_get_tiling get_tiling;
+
+ ret = drmPrimeFDToHandle(bufmgr_gem->fd, prime_fd, &handle);
+ if (ret) {
+ fprintf(stderr,"ret is %d %d\n", ret, errno);
+ return NULL;
+ }
+
+ bo_gem = calloc(1, sizeof(*bo_gem));
+ if (!bo_gem)
+ return NULL;
+
+ bo_gem->bo.size = size;
+ bo_gem->bo.handle = handle;
+ bo_gem->bo.bufmgr = bufmgr;
+
+ bo_gem->gem_handle = handle;
+
+ atomic_set(&bo_gem->refcount, 1);
+
+ bo_gem->name = "prime";
+ bo_gem->validate_index = -1;
+ bo_gem->reloc_tree_fences = 0;
+ bo_gem->used_as_reloc_target = false;
+ bo_gem->has_error = false;
+ bo_gem->reusable = false;
+
+ DRMINITLISTHEAD(&bo_gem->name_list);
+ DRMINITLISTHEAD(&bo_gem->vma_list);
+
+ VG_CLEAR(get_tiling);
+ get_tiling.handle = bo_gem->gem_handle;
+ ret = drmIoctl(bufmgr_gem->fd,
+ DRM_IOCTL_I915_GEM_GET_TILING,
+ &get_tiling);
+ if (ret != 0) {
+ drm_intel_gem_bo_unreference(&bo_gem->bo);
+ return NULL;
+ }
+ bo_gem->tiling_mode = get_tiling.tiling_mode;
+ bo_gem->swizzle_mode = get_tiling.swizzle_mode;
+ /* XXX stride is unknown */
+ drm_intel_bo_gem_set_in_aperture_size(bufmgr_gem, bo_gem);
+
+ return &bo_gem->bo;
+}
+
+int
+drm_intel_bo_gem_export_to_prime(drm_intel_bo *bo, int *prime_fd)
+{
+ drm_intel_bufmgr_gem *bufmgr_gem = (drm_intel_bufmgr_gem *) bo->bufmgr;
+ drm_intel_bo_gem *bo_gem = (drm_intel_bo_gem *) bo;
+
+ return drmPrimeHandleToFD(bufmgr_gem->fd, bo_gem->gem_handle, DRM_CLOEXEC, prime_fd);
+}
+
static int
drm_intel_gem_bo_flink(drm_intel_bo *bo, uint32_t * name)
{
@@ -2314,6 +2807,187 @@ drm_intel_bufmgr_gem_set_vma_cache_size(drm_intel_bufmgr *bufmgr, int limit)
drm_intel_gem_bo_purge_vma_cache(bufmgr_gem);
}
+/**
+ * Get the PCI ID for the device. This can be overridden by setting the
+ * INTEL_DEVID_OVERRIDE environment variable to the desired ID.
+ */
+static int
+get_pci_device_id(drm_intel_bufmgr_gem *bufmgr_gem)
+{
+ char *devid_override;
+ int devid;
+ int ret;
+ drm_i915_getparam_t gp;
+
+ if (geteuid() == getuid()) {
+ devid_override = getenv("INTEL_DEVID_OVERRIDE");
+ if (devid_override) {
+ bufmgr_gem->no_exec = true;
+ return strtod(devid_override, NULL);
+ }
+ }
+
+ VG_CLEAR(devid);
+ VG_CLEAR(gp);
+ gp.param = I915_PARAM_CHIPSET_ID;
+ gp.value = &devid;
+ ret = drmIoctl(bufmgr_gem->fd, DRM_IOCTL_I915_GETPARAM, &gp);
+ if (ret) {
+ fprintf(stderr, "get chip id failed: %d [%d]\n", ret, errno);
+ fprintf(stderr, "param: %d, val: %d\n", gp.param, *gp.value);
+ }
+ return devid;
+}
+
+int
+drm_intel_bufmgr_gem_get_devid(drm_intel_bufmgr *bufmgr)
+{
+ drm_intel_bufmgr_gem *bufmgr_gem = (drm_intel_bufmgr_gem *)bufmgr;
+
+ return bufmgr_gem->pci_device;
+}
+
+/**
+ * Sets up AUB dumping.
+ *
+ * This is a trace file format that can be used with the simulator.
+ * Packets are emitted in a format somewhat like GPU command packets.
+ * You can set up a GTT and upload your objects into the referenced
+ * space, then send off batchbuffers and get BMPs out the other end.
+ */
+void
+drm_intel_bufmgr_gem_set_aub_dump(drm_intel_bufmgr *bufmgr, int enable)
+{
+ drm_intel_bufmgr_gem *bufmgr_gem = (drm_intel_bufmgr_gem *)bufmgr;
+ int entry = 0x200003;
+ int i;
+ int gtt_size = 0x10000;
+
+ if (!enable) {
+ if (bufmgr_gem->aub_file) {
+ fclose(bufmgr_gem->aub_file);
+ bufmgr_gem->aub_file = NULL;
+ }
+ }
+
+ if (geteuid() != getuid())
+ return;
+
+ bufmgr_gem->aub_file = fopen("intel.aub", "w+");
+ if (!bufmgr_gem->aub_file)
+ return;
+
+ /* Start allocating objects from just after the GTT. */
+ bufmgr_gem->aub_offset = gtt_size;
+
+ /* Start with a (required) version packet. */
+ aub_out(bufmgr_gem, CMD_AUB_HEADER | (13 - 2));
+ aub_out(bufmgr_gem,
+ (4 << AUB_HEADER_MAJOR_SHIFT) |
+ (0 << AUB_HEADER_MINOR_SHIFT));
+ for (i = 0; i < 8; i++) {
+ aub_out(bufmgr_gem, 0); /* app name */
+ }
+ aub_out(bufmgr_gem, 0); /* timestamp */
+ aub_out(bufmgr_gem, 0); /* timestamp */
+ aub_out(bufmgr_gem, 0); /* comment len */
+
+ /* Set up the GTT. The max we can handle is 256M */
+ aub_out(bufmgr_gem, CMD_AUB_TRACE_HEADER_BLOCK | (5 - 2));
+ aub_out(bufmgr_gem, AUB_TRACE_MEMTYPE_NONLOCAL | 0 | AUB_TRACE_OP_DATA_WRITE);
+ aub_out(bufmgr_gem, 0); /* subtype */
+ aub_out(bufmgr_gem, 0); /* offset */
+ aub_out(bufmgr_gem, gtt_size); /* size */
+ for (i = 0x000; i < gtt_size; i += 4, entry += 0x1000) {
+ aub_out(bufmgr_gem, entry);
+ }
+}
+
+drm_intel_context *
+drm_intel_gem_context_create(drm_intel_bufmgr *bufmgr)
+{
+ drm_intel_bufmgr_gem *bufmgr_gem = (drm_intel_bufmgr_gem *)bufmgr;
+ struct drm_i915_gem_context_create create;
+ drm_intel_context *context = NULL;
+ int ret;
+
+ ret = drmIoctl(bufmgr_gem->fd, DRM_IOCTL_I915_GEM_CONTEXT_CREATE, &create);
+ if (ret != 0) {
+ DBG("DRM_IOCTL_I915_GEM_CONTEXT_CREATE failed: %s\n",
+ strerror(errno));
+ return NULL;
+ }
+
+ context = calloc(1, sizeof(*context));
+ context->ctx_id = create.ctx_id;
+ context->bufmgr = bufmgr;
+
+ return context;
+}
+
+void
+drm_intel_gem_context_destroy(drm_intel_context *ctx)
+{
+ drm_intel_bufmgr_gem *bufmgr_gem;
+ struct drm_i915_gem_context_destroy destroy;
+ int ret;
+
+ if (ctx == NULL)
+ return;
+
+ bufmgr_gem = (drm_intel_bufmgr_gem *)ctx->bufmgr;
+ destroy.ctx_id = ctx->ctx_id;
+ ret = drmIoctl(bufmgr_gem->fd, DRM_IOCTL_I915_GEM_CONTEXT_DESTROY,
+ &destroy);
+ if (ret != 0)
+ fprintf(stderr, "DRM_IOCTL_I915_GEM_CONTEXT_DESTROY failed: %s\n",
+ strerror(errno));
+
+ free(ctx);
+}
+
+
+/**
+ * Annotate the given bo for use in aub dumping.
+ *
+ * \param annotations is an array of drm_intel_aub_annotation objects
+ * describing the type of data in various sections of the bo. Each
+ * element of the array specifies the type and subtype of a section of
+ * the bo, and the past-the-end offset of that section. The elements
+ * of \c annotations must be sorted so that ending_offset is
+ * increasing.
+ *
+ * \param count is the number of elements in the \c annotations array.
+ * If \c count is zero, then \c annotations will not be dereferenced.
+ *
+ * Annotations are copied into a private data structure, so caller may
+ * re-use the memory pointed to by \c annotations after the call
+ * returns.
+ *
+ * Annotations are stored for the lifetime of the bo; to reset to the
+ * default state (no annotations), call this function with a \c count
+ * of zero.
+ */
+void
+drm_intel_bufmgr_gem_set_aub_annotations(drm_intel_bo *bo,
+ drm_intel_aub_annotation *annotations,
+ unsigned count)
+{
+ drm_intel_bo_gem *bo_gem = (drm_intel_bo_gem *) bo;
+ unsigned size = sizeof(*annotations) * count;
+ drm_intel_aub_annotation *new_annotations =
+ count > 0 ? realloc(bo_gem->aub_annotations, size) : NULL;
+ if (new_annotations == NULL) {
+ free(bo_gem->aub_annotations);
+ bo_gem->aub_annotations = NULL;
+ bo_gem->aub_annotation_count = 0;
+ return;
+ }
+ memcpy(new_annotations, annotations, size);
+ bo_gem->aub_annotations = new_annotations;
+ bo_gem->aub_annotation_count = count;
+}
+
/**
* Initializes the GEM buffer manager, which uses the kernel to allocate, map,
* and manage map buffer objections.
(int)bufmgr_gem->gtt_size / 1024);
}
- VG_CLEAR(gp);
- gp.param = I915_PARAM_CHIPSET_ID;
- gp.value = &bufmgr_gem->pci_device;
- ret = drmIoctl(bufmgr_gem->fd, DRM_IOCTL_I915_GETPARAM, &gp);
- if (ret) {
- fprintf(stderr, "get chip id failed: %d [%d]\n", ret, errno);
- fprintf(stderr, "param: %d, val: %d\n", gp.param, *gp.value);
- }
+ bufmgr_gem->pci_device = get_pci_device_id(bufmgr_gem);
if (IS_GEN2(bufmgr_gem->pci_device))
bufmgr_gem->gen = 2;
bufmgr_gem->gtt_size -= 256*1024*1024;
}
+ VG_CLEAR(gp);
gp.value = &tmp;
gp.param = I915_PARAM_HAS_EXECBUF2;
ret = drmIoctl(bufmgr_gem->fd, DRM_IOCTL_I915_GETPARAM, &gp);
bufmgr_gem->has_relaxed_fencing = ret == 0;
+ gp.param = I915_PARAM_HAS_WAIT_TIMEOUT;
+ ret = drmIoctl(bufmgr_gem->fd, DRM_IOCTL_I915_GETPARAM, &gp);
+ bufmgr_gem->has_wait_timeout = ret == 0;
+
gp.param = I915_PARAM_HAS_LLC;
ret = drmIoctl(bufmgr_gem->fd, DRM_IOCTL_I915_GETPARAM, &gp);
- if (ret == -EINVAL) {
+ if (ret != 0) {
/* Kernel does not supports HAS_LLC query, fallback to GPU
* generation detection and assume that we have LLC on GEN6/7
*/