index 3931ec869c64195d3a67de61d4210905e0b051af..a957c2855dabd2bbbf906f78b030b6c5549a963b 100644 (file)
--- a/intel/intel_bufmgr_gem.c
+++ b/intel/intel_bufmgr_gem.c
/**************************************************************************
*
* Copyright © 2007 Red Hat Inc.
- * Copyright © 2007 Intel Corporation
+ * Copyright © 2007-2012 Intel Corporation
* Copyright 2006 Tungsten Graphics, Inc., Bismarck, ND., USA
* All Rights Reserved.
*
#include <sys/mman.h>
#include <sys/stat.h>
#include <sys/types.h>
+#include <stdbool.h>
#include "errno.h"
#include "libdrm_lists.h"
#include "intel_bufmgr.h"
#include "intel_bufmgr_priv.h"
#include "intel_chipset.h"
+#include "intel_aub.h"
#include "string.h"
#include "i915_drm.h"
+#ifdef HAVE_VALGRIND
+#include <valgrind.h>
+#include <memcheck.h>
+#define VG(x) x
+#else
+#define VG(x)
+#endif
+
+#define VG_CLEAR(s) VG(memset(&s, 0, sizeof(s)))
+
#define DBG(...) do { \
if (bufmgr_gem->bufmgr.debug) \
fprintf(stderr, __VA_ARGS__); \
int num_buckets;
time_t time;
+ drmMMListHead named;
+ drmMMListHead vma_cache;
+ int vma_count, vma_open, vma_max;
+
uint64_t gtt_size;
int available_fences;
int pci_device;
int gen;
- char bo_reuse;
- char fenced_relocs;
+ unsigned int has_bsd : 1;
+ unsigned int has_blt : 1;
+ unsigned int has_relaxed_fencing : 1;
+ unsigned int has_llc : 1;
+ unsigned int has_wait_timeout : 1;
+ unsigned int bo_reuse : 1;
+ unsigned int no_exec : 1;
+ bool fenced_relocs;
+
+ FILE *aub_file;
+ uint32_t aub_offset;
} drm_intel_bufmgr_gem;
#define DRM_INTEL_RELOC_FENCE (1<<0)
* Kenel-assigned global name for this object
*/
unsigned int global_name;
+ drmMMListHead name_list;
/**
* Index of the buffer within the validation list while preparing a
void *mem_virtual;
/** GTT virtual address for the buffer, saved across map/unmap cycles */
void *gtt_virtual;
+ int map_count;
+ drmMMListHead vma_list;
/** BO cache list */
drmMMListHead head;
* Boolean of whether this BO and its children have been included in
* the current drm_intel_bufmgr_check_aperture_space() total.
*/
- char included_in_check_aperture;
+ bool included_in_check_aperture;
/**
* Boolean of whether this buffer has been used as a relocation
* target and had its size accounted for, and thus can't have any
* further relocations added to it.
*/
- char used_as_reloc_target;
+ bool used_as_reloc_target;
/**
* Boolean of whether we have encountered an error whilst building the relocation tree.
*/
- char has_error;
+ bool has_error;
/**
* Boolean of whether this buffer can be re-used
*/
- char reusable;
+ bool reusable;
/**
* Size in bytes of this buffer and its relocation descendents.
* relocations.
*/
int reloc_tree_fences;
+
+ /** Flags that we may need to do the SW_FINSIH ioctl on unmap. */
+ bool mapped_cpu_write;
+
+ uint32_t aub_offset;
+
+ drm_intel_aub_annotation *aub_annotations;
+ unsigned aub_annotation_count;
};
static unsigned int
@@ -241,6 +277,10 @@ drm_intel_gem_bo_tile_size(drm_intel_bufmgr_gem *bufmgr_gem, unsigned long size,
return size;
}
+ /* Do we need to allocate every page for the fence? */
+ if (bufmgr_gem->has_relaxed_fencing)
+ return ROUND_UP_TO(size, 4096);
+
for (i = min_size; i < size; i <<= 1)
;
@@ -254,7 +294,7 @@ drm_intel_gem_bo_tile_size(drm_intel_bufmgr_gem *bufmgr_gem, unsigned long size,
*/
static unsigned long
drm_intel_gem_bo_tile_pitch(drm_intel_bufmgr_gem *bufmgr_gem,
- unsigned long pitch, uint32_t tiling_mode)
+ unsigned long pitch, uint32_t *tiling_mode)
{
unsigned long tile_width;
unsigned long i;
/* If untiled, then just align it so that we can do rendering
* to it with the 3D engine.
*/
- if (tiling_mode == I915_TILING_NONE)
+ if (*tiling_mode == I915_TILING_NONE)
return ALIGN(pitch, 64);
- if (tiling_mode == I915_TILING_X)
+ if (*tiling_mode == I915_TILING_X
+ || (IS_915(bufmgr_gem->pci_device)
+ && *tiling_mode == I915_TILING_Y))
tile_width = 512;
else
tile_width = 128;
if (bufmgr_gem->gen >= 4)
return ROUND_UP_TO(pitch, tile_width);
+ /* The older hardware has a maximum pitch of 8192 with tiled
+ * surfaces, so fallback to untiled if it's too large.
+ */
+ if (pitch > 8192) {
+ *tiling_mode = I915_TILING_NONE;
+ return ALIGN(pitch, 64);
+ }
+
/* Pre-965 needs power of two tile width */
for (i = tile_width; i < pitch; i <<= 1)
;
{
drm_intel_bo_gem *bo_gem = (drm_intel_bo_gem *) bo;
- assert(atomic_read(&bo_gem->refcount) > 0);
atomic_inc(&bo_gem->refcount);
}
* aperture. Optimal packing is for wimps.
*/
size = bo_gem->bo.size;
- if (bufmgr_gem->gen < 4 && bo_gem->tiling_mode != I915_TILING_NONE)
- size *= 2;
+ if (bufmgr_gem->gen < 4 && bo_gem->tiling_mode != I915_TILING_NONE) {
+ int min_size;
+
+ if (bufmgr_gem->has_relaxed_fencing) {
+ if (bufmgr_gem->gen == 3)
+ min_size = 1024*1024;
+ else
+ min_size = 512*1024;
+
+ while (min_size < size)
+ min_size *= 2;
+ } else
+ min_size = size;
+
+ /* Account for worst-case alignment. */
+ size = 2 * min_size;
+ }
bo_gem->reloc_tree_size = size;
}
bo_gem->reloc_target_info = malloc(max_relocs *
sizeof(drm_intel_reloc_target));
if (bo_gem->relocs == NULL || bo_gem->reloc_target_info == NULL) {
- bo_gem->has_error = 1;
+ bo_gem->has_error = true;
free (bo_gem->relocs);
bo_gem->relocs = NULL;
struct drm_i915_gem_busy busy;
int ret;
- memset(&busy, 0, sizeof(busy));
+ VG_CLEAR(busy);
busy.handle = bo_gem->gem_handle;
- do {
- ret = ioctl(bufmgr_gem->fd, DRM_IOCTL_I915_GEM_BUSY, &busy);
- } while (ret == -1 && errno == EINTR);
+ ret = drmIoctl(bufmgr_gem->fd, DRM_IOCTL_I915_GEM_BUSY, &busy);
return (ret == 0 && busy.busy);
}
{
struct drm_i915_gem_madvise madv;
+ VG_CLEAR(madv);
madv.handle = bo_gem->gem_handle;
madv.madv = state;
madv.retained = 1;
- ioctl(bufmgr_gem->fd, DRM_IOCTL_I915_GEM_MADVISE, &madv);
+ drmIoctl(bufmgr_gem->fd, DRM_IOCTL_I915_GEM_MADVISE, &madv);
return madv.retained;
}
unsigned int page_size = getpagesize();
int ret;
struct drm_intel_gem_bo_bucket *bucket;
- int alloc_from_cache;
+ bool alloc_from_cache;
unsigned long bo_size;
- int for_render = 0;
+ bool for_render = false;
if (flags & BO_ALLOC_FOR_RENDER)
- for_render = 1;
+ for_render = true;
/* Round the allocated size up to a power of two number of pages. */
bucket = drm_intel_gem_bo_bucket_for_size(bufmgr_gem, size);
pthread_mutex_lock(&bufmgr_gem->lock);
/* Get a buffer out of the cache if available */
retry:
- alloc_from_cache = 0;
+ alloc_from_cache = false;
if (bucket != NULL && !DRMLISTEMPTY(&bucket->head)) {
if (for_render) {
/* Allocate new render-target BOs from the tail (MRU)
bo_gem = DRMLISTENTRY(drm_intel_bo_gem,
bucket->head.prev, head);
DRMLISTDEL(&bo_gem->head);
- alloc_from_cache = 1;
+ alloc_from_cache = true;
} else {
/* For non-render-target BOs (where we're probably
* going to map it first thing in order to fill it
bo_gem = DRMLISTENTRY(drm_intel_bo_gem,
bucket->head.next, head);
if (!drm_intel_gem_bo_busy(&bo_gem->bo)) {
- alloc_from_cache = 1;
+ alloc_from_cache = true;
DRMLISTDEL(&bo_gem->head);
}
}
return NULL;
bo_gem->bo.size = bo_size;
- memset(&create, 0, sizeof(create));
+
+ VG_CLEAR(create);
create.size = bo_size;
- do {
- ret = ioctl(bufmgr_gem->fd,
- DRM_IOCTL_I915_GEM_CREATE,
- &create);
- } while (ret == -1 && errno == EINTR);
+ ret = drmIoctl(bufmgr_gem->fd,
+ DRM_IOCTL_I915_GEM_CREATE,
+ &create);
bo_gem->gem_handle = create.handle;
bo_gem->bo.handle = bo_gem->gem_handle;
if (ret != 0) {
drm_intel_gem_bo_free(&bo_gem->bo);
return NULL;
}
+
+ DRMINITLISTHEAD(&bo_gem->name_list);
+ DRMINITLISTHEAD(&bo_gem->vma_list);
}
bo_gem->name = name;
atomic_set(&bo_gem->refcount, 1);
bo_gem->validate_index = -1;
bo_gem->reloc_tree_fences = 0;
- bo_gem->used_as_reloc_target = 0;
- bo_gem->has_error = 0;
- bo_gem->reusable = 1;
+ bo_gem->used_as_reloc_target = false;
+ bo_gem->has_error = false;
+ bo_gem->reusable = true;
+ bo_gem->aub_annotations = NULL;
+ bo_gem->aub_annotation_count = 0;
drm_intel_bo_gem_set_in_aperture_size(bufmgr_gem, bo_gem);
unsigned long *pitch, unsigned long flags)
{
drm_intel_bufmgr_gem *bufmgr_gem = (drm_intel_bufmgr_gem *)bufmgr;
- drm_intel_bo *bo;
unsigned long size, stride;
uint32_t tiling;
do {
- unsigned long aligned_y;
+ unsigned long aligned_y, height_alignment;
tiling = *tiling_mode;
* too so we try to be careful.
*/
aligned_y = y;
- if (tiling == I915_TILING_NONE)
- aligned_y = ALIGN(y, 2);
- else if (tiling == I915_TILING_X)
- aligned_y = ALIGN(y, 8);
+ height_alignment = 2;
+
+ if ((bufmgr_gem->gen == 2) && tiling != I915_TILING_NONE)
+ height_alignment = 16;
+ else if (tiling == I915_TILING_X
+ || (IS_915(bufmgr_gem->pci_device)
+ && tiling == I915_TILING_Y))
+ height_alignment = 8;
else if (tiling == I915_TILING_Y)
- aligned_y = ALIGN(y, 32);
+ height_alignment = 32;
+ aligned_y = ALIGN(y, height_alignment);
stride = x * cpp;
- stride = drm_intel_gem_bo_tile_pitch(bufmgr_gem, stride, tiling);
+ stride = drm_intel_gem_bo_tile_pitch(bufmgr_gem, stride, tiling_mode);
size = stride * aligned_y;
size = drm_intel_gem_bo_tile_size(bufmgr_gem, size, tiling_mode);
} while (*tiling_mode != tiling);
+ *pitch = stride;
- if (*tiling_mode == I915_TILING_NONE)
+ if (tiling == I915_TILING_NONE)
stride = 0;
- bo = drm_intel_gem_bo_alloc_internal(bufmgr, name, size, flags,
- *tiling_mode, stride);
- if (!bo)
- return NULL;
-
- *pitch = stride;
- return bo;
+ return drm_intel_gem_bo_alloc_internal(bufmgr, name, size, flags,
+ tiling, stride);
}
/**
int ret;
struct drm_gem_open open_arg;
struct drm_i915_gem_get_tiling get_tiling;
+ drmMMListHead *list;
+
+ /* At the moment most applications only have a few named bo.
+ * For instance, in a DRI client only the render buffers passed
+ * between X and the client are named. And since X returns the
+ * alternating names for the front/back buffer a linear search
+ * provides a sufficiently fast match.
+ */
+ for (list = bufmgr_gem->named.next;
+ list != &bufmgr_gem->named;
+ list = list->next) {
+ bo_gem = DRMLISTENTRY(drm_intel_bo_gem, list, name_list);
+ if (bo_gem->global_name == handle) {
+ drm_intel_gem_bo_reference(&bo_gem->bo);
+ return &bo_gem->bo;
+ }
+ }
bo_gem = calloc(1, sizeof(*bo_gem));
if (!bo_gem)
return NULL;
- memset(&open_arg, 0, sizeof(open_arg));
+ VG_CLEAR(open_arg);
open_arg.name = handle;
- do {
- ret = ioctl(bufmgr_gem->fd,
- DRM_IOCTL_GEM_OPEN,
- &open_arg);
- } while (ret == -1 && errno == EINTR);
+ ret = drmIoctl(bufmgr_gem->fd,
+ DRM_IOCTL_GEM_OPEN,
+ &open_arg);
if (ret != 0) {
- fprintf(stderr, "Couldn't reference %s handle 0x%08x: %s\n",
- name, handle, strerror(errno));
+ DBG("Couldn't reference %s handle 0x%08x: %s\n",
+ name, handle, strerror(errno));
free(bo_gem);
return NULL;
}
atomic_set(&bo_gem->refcount, 1);
bo_gem->validate_index = -1;
bo_gem->gem_handle = open_arg.handle;
+ bo_gem->bo.handle = open_arg.handle;
bo_gem->global_name = handle;
- bo_gem->reusable = 0;
+ bo_gem->reusable = false;
- memset(&get_tiling, 0, sizeof(get_tiling));
+ VG_CLEAR(get_tiling);
get_tiling.handle = bo_gem->gem_handle;
- ret = ioctl(bufmgr_gem->fd, DRM_IOCTL_I915_GEM_GET_TILING, &get_tiling);
+ ret = drmIoctl(bufmgr_gem->fd,
+ DRM_IOCTL_I915_GEM_GET_TILING,
+ &get_tiling);
if (ret != 0) {
drm_intel_gem_bo_unreference(&bo_gem->bo);
return NULL;
/* XXX stride is unknown */
drm_intel_bo_gem_set_in_aperture_size(bufmgr_gem, bo_gem);
+ DRMINITLISTHEAD(&bo_gem->vma_list);
+ DRMLISTADDTAIL(&bo_gem->name_list, &bufmgr_gem->named);
DBG("bo_create_from_handle: %d (%s)\n", handle, bo_gem->name);
return &bo_gem->bo;
struct drm_gem_close close;
int ret;
- if (bo_gem->mem_virtual)
+ DRMLISTDEL(&bo_gem->vma_list);
+ if (bo_gem->mem_virtual) {
+ VG(VALGRIND_FREELIKE_BLOCK(bo_gem->mem_virtual, 0));
munmap(bo_gem->mem_virtual, bo_gem->bo.size);
- if (bo_gem->gtt_virtual)
+ bufmgr_gem->vma_count--;
+ }
+ if (bo_gem->gtt_virtual) {
munmap(bo_gem->gtt_virtual, bo_gem->bo.size);
+ bufmgr_gem->vma_count--;
+ }
/* Close this object */
- memset(&close, 0, sizeof(close));
+ VG_CLEAR(close);
close.handle = bo_gem->gem_handle;
- ret = ioctl(bufmgr_gem->fd, DRM_IOCTL_GEM_CLOSE, &close);
+ ret = drmIoctl(bufmgr_gem->fd, DRM_IOCTL_GEM_CLOSE, &close);
if (ret != 0) {
- fprintf(stderr,
- "DRM_IOCTL_GEM_CLOSE %d failed (%s): %s\n",
- bo_gem->gem_handle, bo_gem->name, strerror(errno));
+ DBG("DRM_IOCTL_GEM_CLOSE %d failed (%s): %s\n",
+ bo_gem->gem_handle, bo_gem->name, strerror(errno));
}
+ free(bo_gem->aub_annotations);
free(bo);
}
+static void
+drm_intel_gem_bo_mark_mmaps_incoherent(drm_intel_bo *bo)
+{
+#if HAVE_VALGRIND
+ drm_intel_bo_gem *bo_gem = (drm_intel_bo_gem *) bo;
+
+ if (bo_gem->mem_virtual)
+ VALGRIND_MAKE_MEM_NOACCESS(bo_gem->mem_virtual, bo->size);
+
+ if (bo_gem->gtt_virtual)
+ VALGRIND_MAKE_MEM_NOACCESS(bo_gem->gtt_virtual, bo->size);
+#endif
+}
+
/** Frees all cached buffers significantly older than @time. */
static void
drm_intel_gem_cleanup_bo_cache(drm_intel_bufmgr_gem *bufmgr_gem, time_t time)
bufmgr_gem->time = time;
}
+static void drm_intel_gem_bo_purge_vma_cache(drm_intel_bufmgr_gem *bufmgr_gem)
+{
+ int limit;
+
+ DBG("%s: cached=%d, open=%d, limit=%d\n", __FUNCTION__,
+ bufmgr_gem->vma_count, bufmgr_gem->vma_open, bufmgr_gem->vma_max);
+
+ if (bufmgr_gem->vma_max < 0)
+ return;
+
+ /* We may need to evict a few entries in order to create new mmaps */
+ limit = bufmgr_gem->vma_max - 2*bufmgr_gem->vma_open;
+ if (limit < 0)
+ limit = 0;
+
+ while (bufmgr_gem->vma_count > limit) {
+ drm_intel_bo_gem *bo_gem;
+
+ bo_gem = DRMLISTENTRY(drm_intel_bo_gem,
+ bufmgr_gem->vma_cache.next,
+ vma_list);
+ assert(bo_gem->map_count == 0);
+ DRMLISTDELINIT(&bo_gem->vma_list);
+
+ if (bo_gem->mem_virtual) {
+ munmap(bo_gem->mem_virtual, bo_gem->bo.size);
+ bo_gem->mem_virtual = NULL;
+ bufmgr_gem->vma_count--;
+ }
+ if (bo_gem->gtt_virtual) {
+ munmap(bo_gem->gtt_virtual, bo_gem->bo.size);
+ bo_gem->gtt_virtual = NULL;
+ bufmgr_gem->vma_count--;
+ }
+ }
+}
+
+static void drm_intel_gem_bo_close_vma(drm_intel_bufmgr_gem *bufmgr_gem,
+ drm_intel_bo_gem *bo_gem)
+{
+ bufmgr_gem->vma_open--;
+ DRMLISTADDTAIL(&bo_gem->vma_list, &bufmgr_gem->vma_cache);
+ if (bo_gem->mem_virtual)
+ bufmgr_gem->vma_count++;
+ if (bo_gem->gtt_virtual)
+ bufmgr_gem->vma_count++;
+ drm_intel_gem_bo_purge_vma_cache(bufmgr_gem);
+}
+
+static void drm_intel_gem_bo_open_vma(drm_intel_bufmgr_gem *bufmgr_gem,
+ drm_intel_bo_gem *bo_gem)
+{
+ bufmgr_gem->vma_open++;
+ DRMLISTDEL(&bo_gem->vma_list);
+ if (bo_gem->mem_virtual)
+ bufmgr_gem->vma_count--;
+ if (bo_gem->gtt_virtual)
+ bufmgr_gem->vma_count--;
+ drm_intel_gem_bo_purge_vma_cache(bufmgr_gem);
+}
+
static void
drm_intel_gem_bo_unreference_final(drm_intel_bo *bo, time_t time)
{
}
}
bo_gem->reloc_count = 0;
- bo_gem->used_as_reloc_target = 0;
+ bo_gem->used_as_reloc_target = false;
DBG("bo_unreference final: %d (%s)\n",
bo_gem->gem_handle, bo_gem->name);
bo_gem->relocs = NULL;
}
+ /* Clear any left-over mappings */
+ if (bo_gem->map_count) {
+ DBG("bo freed with non-zero map-count %d\n", bo_gem->map_count);
+ bo_gem->map_count = 0;
+ drm_intel_gem_bo_close_vma(bufmgr_gem, bo_gem);
+ drm_intel_gem_bo_mark_mmaps_incoherent(bo);
+ }
+
+ DRMLISTDEL(&bo_gem->name_list);
+
bucket = drm_intel_gem_bo_bucket_for_size(bufmgr_gem, bo->size);
/* Put the buffer into our internal cache for reuse if we can. */
if (bufmgr_gem->bo_reuse && bo_gem->reusable && bucket != NULL &&
pthread_mutex_lock(&bufmgr_gem->lock);
- /* Allow recursive mapping. Mesa may recursively map buffers with
- * nested display loops.
- */
+ if (bo_gem->map_count++ == 0)
+ drm_intel_gem_bo_open_vma(bufmgr_gem, bo_gem);
+
if (!bo_gem->mem_virtual) {
struct drm_i915_gem_mmap mmap_arg;
- DBG("bo_map: %d (%s)\n", bo_gem->gem_handle, bo_gem->name);
+ DBG("bo_map: %d (%s), map_count=%d\n",
+ bo_gem->gem_handle, bo_gem->name, bo_gem->map_count);
- memset(&mmap_arg, 0, sizeof(mmap_arg));
+ VG_CLEAR(mmap_arg);
mmap_arg.handle = bo_gem->gem_handle;
mmap_arg.offset = 0;
mmap_arg.size = bo->size;
- do {
- ret = ioctl(bufmgr_gem->fd,
- DRM_IOCTL_I915_GEM_MMAP,
- &mmap_arg);
- } while (ret == -1 && errno == EINTR);
+ ret = drmIoctl(bufmgr_gem->fd,
+ DRM_IOCTL_I915_GEM_MMAP,
+ &mmap_arg);
if (ret != 0) {
ret = -errno;
- fprintf(stderr,
- "%s:%d: Error mapping buffer %d (%s): %s .\n",
- __FILE__, __LINE__, bo_gem->gem_handle,
- bo_gem->name, strerror(errno));
+ DBG("%s:%d: Error mapping buffer %d (%s): %s .\n",
+ __FILE__, __LINE__, bo_gem->gem_handle,
+ bo_gem->name, strerror(errno));
+ if (--bo_gem->map_count == 0)
+ drm_intel_gem_bo_close_vma(bufmgr_gem, bo_gem);
pthread_mutex_unlock(&bufmgr_gem->lock);
return ret;
}
+ VG(VALGRIND_MALLOCLIKE_BLOCK(mmap_arg.addr_ptr, mmap_arg.size, 0, 1));
bo_gem->mem_virtual = (void *)(uintptr_t) mmap_arg.addr_ptr;
}
DBG("bo_map: %d (%s) -> %p\n", bo_gem->gem_handle, bo_gem->name,
bo_gem->mem_virtual);
bo->virtual = bo_gem->mem_virtual;
+ VG_CLEAR(set_domain);
set_domain.handle = bo_gem->gem_handle;
set_domain.read_domains = I915_GEM_DOMAIN_CPU;
if (write_enable)
set_domain.write_domain = I915_GEM_DOMAIN_CPU;
else
set_domain.write_domain = 0;
- do {
- ret = ioctl(bufmgr_gem->fd,
- DRM_IOCTL_I915_GEM_SET_DOMAIN,
- &set_domain);
- } while (ret == -1 && errno == EINTR);
+ ret = drmIoctl(bufmgr_gem->fd,
+ DRM_IOCTL_I915_GEM_SET_DOMAIN,
+ &set_domain);
if (ret != 0) {
- ret = -errno;
- fprintf(stderr, "%s:%d: Error setting to CPU domain %d: %s\n",
- __FILE__, __LINE__, bo_gem->gem_handle,
- strerror(errno));
- pthread_mutex_unlock(&bufmgr_gem->lock);
- return ret;
+ DBG("%s:%d: Error setting to CPU domain %d: %s\n",
+ __FILE__, __LINE__, bo_gem->gem_handle,
+ strerror(errno));
}
+ if (write_enable)
+ bo_gem->mapped_cpu_write = true;
+
+ drm_intel_gem_bo_mark_mmaps_incoherent(bo);
+ VG(VALGRIND_MAKE_MEM_DEFINED(bo_gem->mem_virtual, bo->size));
pthread_mutex_unlock(&bufmgr_gem->lock);
return 0;
}
-int drm_intel_gem_bo_map_gtt(drm_intel_bo *bo)
+static int
+map_gtt(drm_intel_bo *bo)
{
drm_intel_bufmgr_gem *bufmgr_gem = (drm_intel_bufmgr_gem *) bo->bufmgr;
drm_intel_bo_gem *bo_gem = (drm_intel_bo_gem *) bo;
- struct drm_i915_gem_set_domain set_domain;
int ret;
- pthread_mutex_lock(&bufmgr_gem->lock);
+ if (bo_gem->map_count++ == 0)
+ drm_intel_gem_bo_open_vma(bufmgr_gem, bo_gem);
/* Get a mapping of the buffer if we haven't before. */
if (bo_gem->gtt_virtual == NULL) {
struct drm_i915_gem_mmap_gtt mmap_arg;
- DBG("bo_map_gtt: mmap %d (%s)\n", bo_gem->gem_handle,
- bo_gem->name);
+ DBG("bo_map_gtt: mmap %d (%s), map_count=%d\n",
+ bo_gem->gem_handle, bo_gem->name, bo_gem->map_count);
- memset(&mmap_arg, 0, sizeof(mmap_arg));
+ VG_CLEAR(mmap_arg);
mmap_arg.handle = bo_gem->gem_handle;
/* Get the fake offset back... */
- do {
- ret = ioctl(bufmgr_gem->fd,
- DRM_IOCTL_I915_GEM_MMAP_GTT,
- &mmap_arg);
- } while (ret == -1 && errno == EINTR);
+ ret = drmIoctl(bufmgr_gem->fd,
+ DRM_IOCTL_I915_GEM_MMAP_GTT,
+ &mmap_arg);
if (ret != 0) {
ret = -errno;
- fprintf(stderr,
- "%s:%d: Error preparing buffer map %d (%s): %s .\n",
- __FILE__, __LINE__,
- bo_gem->gem_handle, bo_gem->name,
- strerror(errno));
- pthread_mutex_unlock(&bufmgr_gem->lock);
+ DBG("%s:%d: Error preparing buffer map %d (%s): %s .\n",
+ __FILE__, __LINE__,
+ bo_gem->gem_handle, bo_gem->name,
+ strerror(errno));
+ if (--bo_gem->map_count == 0)
+ drm_intel_gem_bo_close_vma(bufmgr_gem, bo_gem);
return ret;
}
if (bo_gem->gtt_virtual == MAP_FAILED) {
bo_gem->gtt_virtual = NULL;
ret = -errno;
- fprintf(stderr,
- "%s:%d: Error mapping buffer %d (%s): %s .\n",
- __FILE__, __LINE__,
- bo_gem->gem_handle, bo_gem->name,
- strerror(errno));
- pthread_mutex_unlock(&bufmgr_gem->lock);
+ DBG("%s:%d: Error mapping buffer %d (%s): %s .\n",
+ __FILE__, __LINE__,
+ bo_gem->gem_handle, bo_gem->name,
+ strerror(errno));
+ if (--bo_gem->map_count == 0)
+ drm_intel_gem_bo_close_vma(bufmgr_gem, bo_gem);
return ret;
}
}
DBG("bo_map_gtt: %d (%s) -> %p\n", bo_gem->gem_handle, bo_gem->name,
bo_gem->gtt_virtual);
- /* Now move it to the GTT domain so that the CPU caches are flushed */
+ return 0;
+}
+
+int drm_intel_gem_bo_map_gtt(drm_intel_bo *bo)
+{
+ drm_intel_bufmgr_gem *bufmgr_gem = (drm_intel_bufmgr_gem *) bo->bufmgr;
+ drm_intel_bo_gem *bo_gem = (drm_intel_bo_gem *) bo;
+ struct drm_i915_gem_set_domain set_domain;
+ int ret;
+
+ pthread_mutex_lock(&bufmgr_gem->lock);
+
+ ret = map_gtt(bo);
+ if (ret) {
+ pthread_mutex_unlock(&bufmgr_gem->lock);
+ return ret;
+ }
+
+ /* Now move it to the GTT domain so that the GPU and CPU
+ * caches are flushed and the GPU isn't actively using the
+ * buffer.
+ *
+ * The pagefault handler does this domain change for us when
+ * it has unbound the BO from the GTT, but it's up to us to
+ * tell it when we're about to use things if we had done
+ * rendering and it still happens to be bound to the GTT.
+ */
+ VG_CLEAR(set_domain);
set_domain.handle = bo_gem->gem_handle;
set_domain.read_domains = I915_GEM_DOMAIN_GTT;
set_domain.write_domain = I915_GEM_DOMAIN_GTT;
- do {
- ret = ioctl(bufmgr_gem->fd,
- DRM_IOCTL_I915_GEM_SET_DOMAIN,
- &set_domain);
- } while (ret == -1 && errno == EINTR);
-
+ ret = drmIoctl(bufmgr_gem->fd,
+ DRM_IOCTL_I915_GEM_SET_DOMAIN,
+ &set_domain);
if (ret != 0) {
- ret = -errno;
- fprintf(stderr, "%s:%d: Error setting domain %d: %s\n",
- __FILE__, __LINE__, bo_gem->gem_handle,
- strerror(errno));
+ DBG("%s:%d: Error setting domain %d: %s\n",
+ __FILE__, __LINE__, bo_gem->gem_handle,
+ strerror(errno));
}
+ drm_intel_gem_bo_mark_mmaps_incoherent(bo);
+ VG(VALGRIND_MAKE_MEM_DEFINED(bo_gem->gtt_virtual, bo->size));
pthread_mutex_unlock(&bufmgr_gem->lock);
- return ret;
+ return 0;
}
-int drm_intel_gem_bo_unmap_gtt(drm_intel_bo *bo)
+/**
+ * Performs a mapping of the buffer object like the normal GTT
+ * mapping, but avoids waiting for the GPU to be done reading from or
+ * rendering to the buffer.
+ *
+ * This is used in the implementation of GL_ARB_map_buffer_range: The
+ * user asks to create a buffer, then does a mapping, fills some
+ * space, runs a drawing command, then asks to map it again without
+ * synchronizing because it guarantees that it won't write over the
+ * data that the GPU is busy using (or, more specifically, that if it
+ * does write over the data, it acknowledges that rendering is
+ * undefined).
+ */
+
+int drm_intel_gem_bo_map_unsynchronized(drm_intel_bo *bo)
{
drm_intel_bufmgr_gem *bufmgr_gem = (drm_intel_bufmgr_gem *) bo->bufmgr;
- drm_intel_bo_gem *bo_gem = (drm_intel_bo_gem *) bo;
- int ret = 0;
-
- if (bo == NULL)
- return 0;
+ int ret;
- assert(bo_gem->gtt_virtual != NULL);
+ /* If the CPU cache isn't coherent with the GTT, then use a
+ * regular synchronized mapping. The problem is that we don't
+ * track where the buffer was last used on the CPU side in
+ * terms of drm_intel_bo_map vs drm_intel_gem_bo_map_gtt, so
+ * we would potentially corrupt the buffer even when the user
+ * does reasonable things.
+ */
+ if (!bufmgr_gem->has_llc)
+ return drm_intel_gem_bo_map_gtt(bo);
pthread_mutex_lock(&bufmgr_gem->lock);
- bo->virtual = NULL;
+ ret = map_gtt(bo);
pthread_mutex_unlock(&bufmgr_gem->lock);
return ret;
{
drm_intel_bufmgr_gem *bufmgr_gem = (drm_intel_bufmgr_gem *) bo->bufmgr;
drm_intel_bo_gem *bo_gem = (drm_intel_bo_gem *) bo;
- struct drm_i915_gem_sw_finish sw_finish;
- int ret;
+ int ret = 0;
if (bo == NULL)
return 0;
- assert(bo_gem->mem_virtual != NULL);
-
pthread_mutex_lock(&bufmgr_gem->lock);
- /* Cause a flush to happen if the buffer's pinned for scanout, so the
- * results show up in a timely manner.
- */
- sw_finish.handle = bo_gem->gem_handle;
- do {
- ret = ioctl(bufmgr_gem->fd,
- DRM_IOCTL_I915_GEM_SW_FINISH,
- &sw_finish);
- } while (ret == -1 && errno == EINTR);
- ret = ret == -1 ? -errno : 0;
+ if (bo_gem->map_count <= 0) {
+ DBG("attempted to unmap an unmapped bo\n");
+ pthread_mutex_unlock(&bufmgr_gem->lock);
+ /* Preserve the old behaviour of just treating this as a
+ * no-op rather than reporting the error.
+ */
+ return 0;
+ }
+
+ if (bo_gem->mapped_cpu_write) {
+ struct drm_i915_gem_sw_finish sw_finish;
- bo->virtual = NULL;
+ /* Cause a flush to happen if the buffer's pinned for
+ * scanout, so the results show up in a timely manner.
+ * Unlike GTT set domains, this only does work if the
+ * buffer should be scanout-related.
+ */
+ VG_CLEAR(sw_finish);
+ sw_finish.handle = bo_gem->gem_handle;
+ ret = drmIoctl(bufmgr_gem->fd,
+ DRM_IOCTL_I915_GEM_SW_FINISH,
+ &sw_finish);
+ ret = ret == -1 ? -errno : 0;
+
+ bo_gem->mapped_cpu_write = false;
+ }
+
+ /* We need to unmap after every innovation as we cannot track
+ * an open vma for every bo as that will exhaasut the system
+ * limits and cause later failures.
+ */
+ if (--bo_gem->map_count == 0) {
+ drm_intel_gem_bo_close_vma(bufmgr_gem, bo_gem);
+ drm_intel_gem_bo_mark_mmaps_incoherent(bo);
+ bo->virtual = NULL;
+ }
pthread_mutex_unlock(&bufmgr_gem->lock);
return ret;
}
+int drm_intel_gem_bo_unmap_gtt(drm_intel_bo *bo)
+{
+ return drm_intel_gem_bo_unmap(bo);
+}
+
static int
drm_intel_gem_bo_subdata(drm_intel_bo *bo, unsigned long offset,
unsigned long size, const void *data)
struct drm_i915_gem_pwrite pwrite;
int ret;
- memset(&pwrite, 0, sizeof(pwrite));
+ VG_CLEAR(pwrite);
pwrite.handle = bo_gem->gem_handle;
pwrite.offset = offset;
pwrite.size = size;
pwrite.data_ptr = (uint64_t) (uintptr_t) data;
- do {
- ret = ioctl(bufmgr_gem->fd,
- DRM_IOCTL_I915_GEM_PWRITE,
- &pwrite);
- } while (ret == -1 && errno == EINTR);
+ ret = drmIoctl(bufmgr_gem->fd,
+ DRM_IOCTL_I915_GEM_PWRITE,
+ &pwrite);
if (ret != 0) {
ret = -errno;
- fprintf(stderr,
- "%s:%d: Error writing data to buffer %d: (%d %d) %s .\n",
- __FILE__, __LINE__, bo_gem->gem_handle, (int)offset,
- (int)size, strerror(errno));
+ DBG("%s:%d: Error writing data to buffer %d: (%d %d) %s .\n",
+ __FILE__, __LINE__, bo_gem->gem_handle, (int)offset,
+ (int)size, strerror(errno));
}
return ret;
struct drm_i915_get_pipe_from_crtc_id get_pipe_from_crtc_id;
int ret;
+ VG_CLEAR(get_pipe_from_crtc_id);
get_pipe_from_crtc_id.crtc_id = crtc_id;
- ret = ioctl(bufmgr_gem->fd, DRM_IOCTL_I915_GET_PIPE_FROM_CRTC_ID,
- &get_pipe_from_crtc_id);
+ ret = drmIoctl(bufmgr_gem->fd,
+ DRM_IOCTL_I915_GET_PIPE_FROM_CRTC_ID,
+ &get_pipe_from_crtc_id);
if (ret != 0) {
/* We return -1 here to signal that we don't
* know which pipe is associated with this crtc.
struct drm_i915_gem_pread pread;
int ret;
- memset(&pread, 0, sizeof(pread));
+ VG_CLEAR(pread);
pread.handle = bo_gem->gem_handle;
pread.offset = offset;
pread.size = size;
pread.data_ptr = (uint64_t) (uintptr_t) data;
- do {
- ret = ioctl(bufmgr_gem->fd,
- DRM_IOCTL_I915_GEM_PREAD,
- &pread);
- } while (ret == -1 && errno == EINTR);
+ ret = drmIoctl(bufmgr_gem->fd,
+ DRM_IOCTL_I915_GEM_PREAD,
+ &pread);
if (ret != 0) {
ret = -errno;
- fprintf(stderr,
- "%s:%d: Error reading data from buffer %d: (%d %d) %s .\n",
- __FILE__, __LINE__, bo_gem->gem_handle, (int)offset,
- (int)size, strerror(errno));
+ DBG("%s:%d: Error reading data from buffer %d: (%d %d) %s .\n",
+ __FILE__, __LINE__, bo_gem->gem_handle, (int)offset,
+ (int)size, strerror(errno));
}
return ret;
}
-/** Waits for all GPU rendering to the object to have completed. */
+/** Waits for all GPU rendering with the object to have completed. */
static void
drm_intel_gem_bo_wait_rendering(drm_intel_bo *bo)
{
- drm_intel_gem_bo_start_gtt_access(bo, 0);
+ drm_intel_gem_bo_start_gtt_access(bo, 1);
+}
+
+/**
+ * Waits on a BO for the given amount of time.
+ *
+ * @bo: buffer object to wait for
+ * @timeout_ns: amount of time to wait in nanoseconds.
+ * If value is less than 0, an infinite wait will occur.
+ *
+ * Returns 0 if the wait was successful ie. the last batch referencing the
+ * object has completed within the allotted time. Otherwise some negative return
+ * value describes the error. Of particular interest is -ETIME when the wait has
+ * failed to yield the desired result.
+ *
+ * Similar to drm_intel_gem_bo_wait_rendering except a timeout parameter allows
+ * the operation to give up after a certain amount of time. Another subtle
+ * difference is the internal locking semantics are different (this variant does
+ * not hold the lock for the duration of the wait). This makes the wait subject
+ * to a larger userspace race window.
+ *
+ * The implementation shall wait until the object is no longer actively
+ * referenced within a batch buffer at the time of the call. The wait will
+ * not guarantee that the buffer is re-issued via another thread, or an flinked
+ * handle. Userspace must make sure this race does not occur if such precision
+ * is important.
+ */
+int drm_intel_gem_bo_wait(drm_intel_bo *bo, int64_t timeout_ns)
+{
+ drm_intel_bufmgr_gem *bufmgr_gem = (drm_intel_bufmgr_gem *) bo->bufmgr;
+ drm_intel_bo_gem *bo_gem = (drm_intel_bo_gem *) bo;
+ struct drm_i915_gem_wait wait;
+ int ret;
+
+ if (!bufmgr_gem->has_wait_timeout) {
+ DBG("%s:%d: Timed wait is not supported. Falling back to "
+ "infinite wait\n", __FILE__, __LINE__);
+ if (timeout_ns) {
+ drm_intel_gem_bo_wait_rendering(bo);
+ return 0;
+ } else {
+ return drm_intel_gem_bo_busy(bo) ? -ETIME : 0;
+ }
+ }
+
+ wait.bo_handle = bo_gem->gem_handle;
+ wait.timeout_ns = timeout_ns;
+ wait.flags = 0;
+ ret = drmIoctl(bufmgr_gem->fd, DRM_IOCTL_I915_GEM_WAIT, &wait);
+ if (ret == -1)
+ return -errno;
+
+ return ret;
}
/**
struct drm_i915_gem_set_domain set_domain;
int ret;
+ VG_CLEAR(set_domain);
set_domain.handle = bo_gem->gem_handle;
set_domain.read_domains = I915_GEM_DOMAIN_GTT;
set_domain.write_domain = write_enable ? I915_GEM_DOMAIN_GTT : 0;
- do {
- ret = ioctl(bufmgr_gem->fd,
- DRM_IOCTL_I915_GEM_SET_DOMAIN,
- &set_domain);
- } while (ret == -1 && errno == EINTR);
+ ret = drmIoctl(bufmgr_gem->fd,
+ DRM_IOCTL_I915_GEM_SET_DOMAIN,
+ &set_domain);
if (ret != 0) {
- fprintf(stderr,
- "%s:%d: Error setting memory domains %d (%08x %08x): %s .\n",
- __FILE__, __LINE__, bo_gem->gem_handle,
- set_domain.read_domains, set_domain.write_domain,
- strerror(errno));
+ DBG("%s:%d: Error setting memory domains %d (%08x %08x): %s .\n",
+ __FILE__, __LINE__, bo_gem->gem_handle,
+ set_domain.read_domains, set_domain.write_domain,
+ strerror(errno));
}
}
do_bo_emit_reloc(drm_intel_bo *bo, uint32_t offset,
drm_intel_bo *target_bo, uint32_t target_offset,
uint32_t read_domains, uint32_t write_domain,
- int need_fence)
+ bool need_fence)
{
drm_intel_bufmgr_gem *bufmgr_gem = (drm_intel_bufmgr_gem *) bo->bufmgr;
drm_intel_bo_gem *bo_gem = (drm_intel_bo_gem *) bo;
drm_intel_bo_gem *target_bo_gem = (drm_intel_bo_gem *) target_bo;
+ bool fenced_command;
if (bo_gem->has_error)
return -ENOMEM;
if (target_bo_gem->has_error) {
- bo_gem->has_error = 1;
+ bo_gem->has_error = true;
return -ENOMEM;
}
- if (target_bo_gem->tiling_mode == I915_TILING_NONE)
- need_fence = 0;
-
/* We never use HW fences for rendering on 965+ */
if (bufmgr_gem->gen >= 4)
- need_fence = 0;
+ need_fence = false;
+
+ fenced_command = need_fence;
+ if (target_bo_gem->tiling_mode == I915_TILING_NONE)
+ need_fence = false;
/* Create a new relocation list if needed */
if (bo_gem->relocs == NULL && drm_intel_setup_reloc_list(bo))
*/
assert(!bo_gem->used_as_reloc_target);
if (target_bo_gem != bo_gem) {
- target_bo_gem->used_as_reloc_target = 1;
+ target_bo_gem->used_as_reloc_target = true;
bo_gem->reloc_tree_size += target_bo_gem->reloc_tree_size;
}
/* An object needing a fence is a tiled buffer, so it won't have
target_bo_gem->reloc_tree_fences = 1;
bo_gem->reloc_tree_fences += target_bo_gem->reloc_tree_fences;
- /* Flag the target to disallow further relocations in it. */
-
bo_gem->relocs[bo_gem->reloc_count].offset = offset;
bo_gem->relocs[bo_gem->reloc_count].delta = target_offset;
bo_gem->relocs[bo_gem->reloc_count].target_handle =
bo_gem->reloc_target_info[bo_gem->reloc_count].bo = target_bo;
if (target_bo != bo)
drm_intel_gem_bo_reference(target_bo);
- if (need_fence)
+ if (fenced_command)
bo_gem->reloc_target_info[bo_gem->reloc_count].flags =
DRM_INTEL_RELOC_FENCE;
else
uint32_t read_domains, uint32_t write_domain)
{
return do_bo_emit_reloc(bo, offset, target_bo, target_offset,
- read_domains, write_domain, 1);
+ read_domains, write_domain, true);
+}
+
+int
+drm_intel_gem_bo_get_reloc_count(drm_intel_bo *bo)
+{
+ drm_intel_bo_gem *bo_gem = (drm_intel_bo_gem *) bo;
+
+ return bo_gem->reloc_count;
+}
+
+/**
+ * Removes existing relocation entries in the BO after "start".
+ *
+ * This allows a user to avoid a two-step process for state setup with
+ * counting up all the buffer objects and doing a
+ * drm_intel_bufmgr_check_aperture_space() before emitting any of the
+ * relocations for the state setup. Instead, save the state of the
+ * batchbuffer including drm_intel_gem_get_reloc_count(), emit all the
+ * state, and then check if it still fits in the aperture.
+ *
+ * Any further drm_intel_bufmgr_check_aperture_space() queries
+ * involving this buffer in the tree are undefined after this call.
+ */
+void
+drm_intel_gem_bo_clear_relocs(drm_intel_bo *bo, int start)
+{
+ drm_intel_bo_gem *bo_gem = (drm_intel_bo_gem *) bo;
+ int i;
+ struct timespec time;
+
+ clock_gettime(CLOCK_MONOTONIC, &time);
+
+ assert(bo_gem->reloc_count >= start);
+ /* Unreference the cleared target buffers */
+ for (i = start; i < bo_gem->reloc_count; i++) {
+ if (bo_gem->reloc_target_info[i].bo != bo) {
+ drm_intel_gem_bo_unreference_locked_timed(bo_gem->
+ reloc_target_info[i].bo,
+ time.tv_sec);
+ }
+ }
+ bo_gem->reloc_count = start;
}
/**
if (target_bo == bo)
continue;
+ drm_intel_gem_bo_mark_mmaps_incoherent(bo);
+
/* Continue walking the tree depth-first. */
drm_intel_gem_bo_process_reloc(target_bo);
if (target_bo == bo)
continue;
+ drm_intel_gem_bo_mark_mmaps_incoherent(bo);
+
/* Continue walking the tree depth-first. */
drm_intel_gem_bo_process_reloc2(target_bo);
}
}
+static void
+aub_out(drm_intel_bufmgr_gem *bufmgr_gem, uint32_t data)
+{
+ fwrite(&data, 1, 4, bufmgr_gem->aub_file);
+}
+
+static void
+aub_out_data(drm_intel_bufmgr_gem *bufmgr_gem, void *data, size_t size)
+{
+ fwrite(data, 1, size, bufmgr_gem->aub_file);
+}
+
+static void
+aub_write_bo_data(drm_intel_bo *bo, uint32_t offset, uint32_t size)
+{
+ drm_intel_bufmgr_gem *bufmgr_gem = (drm_intel_bufmgr_gem *) bo->bufmgr;
+ drm_intel_bo_gem *bo_gem = (drm_intel_bo_gem *) bo;
+ uint32_t *data;
+ unsigned int i;
+
+ data = malloc(bo->size);
+ drm_intel_bo_get_subdata(bo, offset, size, data);
+
+ /* Easy mode: write out bo with no relocations */
+ if (!bo_gem->reloc_count) {
+ aub_out_data(bufmgr_gem, data, size);
+ free(data);
+ return;
+ }
+
+ /* Otherwise, handle the relocations while writing. */
+ for (i = 0; i < size / 4; i++) {
+ int r;
+ for (r = 0; r < bo_gem->reloc_count; r++) {
+ struct drm_i915_gem_relocation_entry *reloc;
+ drm_intel_reloc_target *info;
+
+ reloc = &bo_gem->relocs[r];
+ info = &bo_gem->reloc_target_info[r];
+
+ if (reloc->offset == offset + i * 4) {
+ drm_intel_bo_gem *target_gem;
+ uint32_t val;
+
+ target_gem = (drm_intel_bo_gem *)info->bo;
+
+ val = reloc->delta;
+ val += target_gem->aub_offset;
+
+ aub_out(bufmgr_gem, val);
+ data[i] = val;
+ break;
+ }
+ }
+ if (r == bo_gem->reloc_count) {
+ /* no relocation, just the data */
+ aub_out(bufmgr_gem, data[i]);
+ }
+ }
+
+ free(data);
+}
+
+static void
+aub_bo_get_address(drm_intel_bo *bo)
+{
+ drm_intel_bufmgr_gem *bufmgr_gem = (drm_intel_bufmgr_gem *) bo->bufmgr;
+ drm_intel_bo_gem *bo_gem = (drm_intel_bo_gem *) bo;
+
+ /* Give the object a graphics address in the AUB file. We
+ * don't just use the GEM object address because we do AUB
+ * dumping before execution -- we want to successfully log
+ * when the hardware might hang, and we might even want to aub
+ * capture for a driver trying to execute on a different
+ * generation of hardware by disabling the actual kernel exec
+ * call.
+ */
+ bo_gem->aub_offset = bufmgr_gem->aub_offset;
+ bufmgr_gem->aub_offset += bo->size;
+ /* XXX: Handle aperture overflow. */
+ assert(bufmgr_gem->aub_offset < 256 * 1024 * 1024);
+}
+
+static void
+aub_write_trace_block(drm_intel_bo *bo, uint32_t type, uint32_t subtype,
+ uint32_t offset, uint32_t size)
+{
+ drm_intel_bufmgr_gem *bufmgr_gem = (drm_intel_bufmgr_gem *) bo->bufmgr;
+ drm_intel_bo_gem *bo_gem = (drm_intel_bo_gem *) bo;
+
+ aub_out(bufmgr_gem,
+ CMD_AUB_TRACE_HEADER_BLOCK |
+ (5 - 2));
+ aub_out(bufmgr_gem,
+ AUB_TRACE_MEMTYPE_GTT | type | AUB_TRACE_OP_DATA_WRITE);
+ aub_out(bufmgr_gem, subtype);
+ aub_out(bufmgr_gem, bo_gem->aub_offset + offset);
+ aub_out(bufmgr_gem, size);
+ aub_write_bo_data(bo, offset, size);
+}
+
+/**
+ * Break up large objects into multiple writes. Otherwise a 128kb VBO
+ * would overflow the 16 bits of size field in the packet header and
+ * everything goes badly after that.
+ */
+static void
+aub_write_large_trace_block(drm_intel_bo *bo, uint32_t type, uint32_t subtype,
+ uint32_t offset, uint32_t size)
+{
+ uint32_t block_size;
+ uint32_t sub_offset;
+
+ for (sub_offset = 0; sub_offset < size; sub_offset += block_size) {
+ block_size = size - sub_offset;
+
+ if (block_size > 8 * 4096)
+ block_size = 8 * 4096;
+
+ aub_write_trace_block(bo, type, subtype, offset + sub_offset,
+ block_size);
+ }
+}
+
+static void
+aub_write_bo(drm_intel_bo *bo)
+{
+ drm_intel_bo_gem *bo_gem = (drm_intel_bo_gem *) bo;
+ uint32_t offset = 0;
+ unsigned i;
+
+ aub_bo_get_address(bo);
+
+ /* Write out each annotated section separately. */
+ for (i = 0; i < bo_gem->aub_annotation_count; ++i) {
+ drm_intel_aub_annotation *annotation =
+ &bo_gem->aub_annotations[i];
+ uint32_t ending_offset = annotation->ending_offset;
+ if (ending_offset > bo->size)
+ ending_offset = bo->size;
+ if (ending_offset > offset) {
+ aub_write_large_trace_block(bo, annotation->type,
+ annotation->subtype,
+ offset,
+ ending_offset - offset);
+ offset = ending_offset;
+ }
+ }
+
+ /* Write out any remaining unannotated data */
+ if (offset < bo->size) {
+ aub_write_large_trace_block(bo, AUB_TRACE_TYPE_NOTYPE, 0,
+ offset, bo->size - offset);
+ }
+}
+
+/*
+ * Make a ringbuffer on fly and dump it
+ */
+static void
+aub_build_dump_ringbuffer(drm_intel_bufmgr_gem *bufmgr_gem,
+ uint32_t batch_buffer, int ring_flag)
+{
+ uint32_t ringbuffer[4096];
+ int ring = AUB_TRACE_TYPE_RING_PRB0; /* The default ring */
+ int ring_count = 0;
+
+ if (ring_flag == I915_EXEC_BSD)
+ ring = AUB_TRACE_TYPE_RING_PRB1;
+
+ /* Make a ring buffer to execute our batchbuffer. */
+ memset(ringbuffer, 0, sizeof(ringbuffer));
+ ringbuffer[ring_count++] = AUB_MI_BATCH_BUFFER_START;
+ ringbuffer[ring_count++] = batch_buffer;
+
+ /* Write out the ring. This appears to trigger execution of
+ * the ring in the simulator.
+ */
+ aub_out(bufmgr_gem,
+ CMD_AUB_TRACE_HEADER_BLOCK |
+ (5 - 2));
+ aub_out(bufmgr_gem,
+ AUB_TRACE_MEMTYPE_GTT | ring | AUB_TRACE_OP_COMMAND_WRITE);
+ aub_out(bufmgr_gem, 0); /* general/surface subtype */
+ aub_out(bufmgr_gem, bufmgr_gem->aub_offset);
+ aub_out(bufmgr_gem, ring_count * 4);
+
+ /* FIXME: Need some flush operations here? */
+ aub_out_data(bufmgr_gem, ringbuffer, ring_count * 4);
+
+ /* Update offset pointer */
+ bufmgr_gem->aub_offset += 4096;
+}
+
+void
+drm_intel_gem_bo_aub_dump_bmp(drm_intel_bo *bo,
+ int x1, int y1, int width, int height,
+ enum aub_dump_bmp_format format,
+ int pitch, int offset)
+{
+ drm_intel_bufmgr_gem *bufmgr_gem = (drm_intel_bufmgr_gem *) bo->bufmgr;
+ drm_intel_bo_gem *bo_gem = (drm_intel_bo_gem *)bo;
+ uint32_t cpp;
+
+ switch (format) {
+ case AUB_DUMP_BMP_FORMAT_8BIT:
+ cpp = 1;
+ break;
+ case AUB_DUMP_BMP_FORMAT_ARGB_4444:
+ cpp = 2;
+ break;
+ case AUB_DUMP_BMP_FORMAT_ARGB_0888:
+ case AUB_DUMP_BMP_FORMAT_ARGB_8888:
+ cpp = 4;
+ break;
+ default:
+ printf("Unknown AUB dump format %d\n", format);
+ return;
+ }
+
+ if (!bufmgr_gem->aub_file)
+ return;
+
+ aub_out(bufmgr_gem, CMD_AUB_DUMP_BMP | 4);
+ aub_out(bufmgr_gem, (y1 << 16) | x1);
+ aub_out(bufmgr_gem,
+ (format << 24) |
+ (cpp << 19) |
+ pitch / 4);
+ aub_out(bufmgr_gem, (height << 16) | width);
+ aub_out(bufmgr_gem, bo_gem->aub_offset + offset);
+ aub_out(bufmgr_gem,
+ ((bo_gem->tiling_mode != I915_TILING_NONE) ? (1 << 2) : 0) |
+ ((bo_gem->tiling_mode == I915_TILING_Y) ? (1 << 3) : 0));
+}
+
+static void
+aub_exec(drm_intel_bo *bo, int ring_flag, int used)
+{
+ drm_intel_bufmgr_gem *bufmgr_gem = (drm_intel_bufmgr_gem *) bo->bufmgr;
+ drm_intel_bo_gem *bo_gem = (drm_intel_bo_gem *) bo;
+ int i;
+ bool batch_buffer_needs_annotations;
+
+ if (!bufmgr_gem->aub_file)
+ return;
+
+ /* If batch buffer is not annotated, annotate it the best we
+ * can.
+ */
+ batch_buffer_needs_annotations = bo_gem->aub_annotation_count == 0;
+ if (batch_buffer_needs_annotations) {
+ drm_intel_aub_annotation annotations[2] = {
+ { AUB_TRACE_TYPE_BATCH, 0, used },
+ { AUB_TRACE_TYPE_NOTYPE, 0, bo->size }
+ };
+ drm_intel_bufmgr_gem_set_aub_annotations(bo, annotations, 2);
+ }
+
+ /* Write out all buffers to AUB memory */
+ for (i = 0; i < bufmgr_gem->exec_count; i++) {
+ aub_write_bo(bufmgr_gem->exec_bos[i]);
+ }
+
+ /* Remove any annotations we added */
+ if (batch_buffer_needs_annotations)
+ drm_intel_bufmgr_gem_set_aub_annotations(bo, NULL, 0);
+
+ /* Dump ring buffer */
+ aub_build_dump_ringbuffer(bufmgr_gem, bo_gem->aub_offset, ring_flag);
+
+ fflush(bufmgr_gem->aub_file);
+
+ /*
+ * One frame has been dumped. So reset the aub_offset for the next frame.
+ *
+ * FIXME: Can we do this?
+ */
+ bufmgr_gem->aub_offset = 0x10000;
+}
+
static int
drm_intel_gem_bo_exec(drm_intel_bo *bo, int used,
drm_clip_rect_t * cliprects, int num_cliprects, int DR4)
*/
drm_intel_add_validate_buffer(bo);
+ VG_CLEAR(execbuf);
execbuf.buffers_ptr = (uintptr_t) bufmgr_gem->exec_objects;
execbuf.buffer_count = bufmgr_gem->exec_count;
execbuf.batch_start_offset = 0;
execbuf.DR1 = 0;
execbuf.DR4 = DR4;
- do {
- ret = ioctl(bufmgr_gem->fd,
- DRM_IOCTL_I915_GEM_EXECBUFFER,
- &execbuf);
- } while (ret != 0 && errno == EINTR);
-
+ ret = drmIoctl(bufmgr_gem->fd,
+ DRM_IOCTL_I915_GEM_EXECBUFFER,
+ &execbuf);
if (ret != 0) {
ret = -errno;
if (errno == ENOSPC) {
- fprintf(stderr,
- "Execbuffer fails to pin. "
- "Estimate: %u. Actual: %u. Available: %u\n",
- drm_intel_gem_estimate_batch_space(bufmgr_gem->exec_bos,
- bufmgr_gem->
- exec_count),
- drm_intel_gem_compute_batch_space(bufmgr_gem->exec_bos,
- bufmgr_gem->
- exec_count),
- (unsigned int)bufmgr_gem->gtt_size);
+ DBG("Execbuffer fails to pin. "
+ "Estimate: %u. Actual: %u. Available: %u\n",
+ drm_intel_gem_estimate_batch_space(bufmgr_gem->exec_bos,
+ bufmgr_gem->
+ exec_count),
+ drm_intel_gem_compute_batch_space(bufmgr_gem->exec_bos,
+ bufmgr_gem->
+ exec_count),
+ (unsigned int)bufmgr_gem->gtt_size);
}
}
drm_intel_update_buffer_offsets(bufmgr_gem);
}
static int
-drm_intel_gem_bo_mrb_exec2(drm_intel_bo *bo, int used,
- drm_clip_rect_t *cliprects, int num_cliprects, int DR4,
- int ring_flag)
+do_exec2(drm_intel_bo *bo, int used, drm_intel_context *ctx,
+ drm_clip_rect_t *cliprects, int num_cliprects, int DR4,
+ unsigned int flags)
{
drm_intel_bufmgr_gem *bufmgr_gem = (drm_intel_bufmgr_gem *)bo->bufmgr;
struct drm_i915_gem_execbuffer2 execbuf;
- int ret, i;
+ int ret = 0;
+ int i;
- if ((ring_flag != I915_EXEC_RENDER) && (ring_flag != I915_EXEC_BSD))
+ switch (flags & 0x7) {
+ default:
return -EINVAL;
+ case I915_EXEC_BLT:
+ if (!bufmgr_gem->has_blt)
+ return -EINVAL;
+ break;
+ case I915_EXEC_BSD:
+ if (!bufmgr_gem->has_bsd)
+ return -EINVAL;
+ break;
+ case I915_EXEC_RENDER:
+ case I915_EXEC_DEFAULT:
+ break;
+ }
pthread_mutex_lock(&bufmgr_gem->lock);
/* Update indices and set up the validate list. */
*/
drm_intel_add_validate_buffer2(bo, 0);
+ VG_CLEAR(execbuf);
execbuf.buffers_ptr = (uintptr_t)bufmgr_gem->exec2_objects;
execbuf.buffer_count = bufmgr_gem->exec_count;
execbuf.batch_start_offset = 0;
execbuf.num_cliprects = num_cliprects;
execbuf.DR1 = 0;
execbuf.DR4 = DR4;
- execbuf.flags = ring_flag;
- execbuf.rsvd1 = 0;
+ execbuf.flags = flags;
+ if (ctx == NULL)
+ i915_execbuffer2_set_context_id(execbuf, 0);
+ else
+ i915_execbuffer2_set_context_id(execbuf, ctx->ctx_id);
execbuf.rsvd2 = 0;
- do {
- ret = ioctl(bufmgr_gem->fd, DRM_IOCTL_I915_GEM_EXECBUFFER2,
- &execbuf);
- } while (ret != 0 && errno == EINTR);
+ aub_exec(bo, flags, used);
+ if (bufmgr_gem->no_exec)
+ goto skip_execution;
+
+ ret = drmIoctl(bufmgr_gem->fd,
+ DRM_IOCTL_I915_GEM_EXECBUFFER2,
+ &execbuf);
if (ret != 0) {
ret = -errno;
if (ret == -ENOSPC) {
- fprintf(stderr,
- "Execbuffer fails to pin. "
- "Estimate: %u. Actual: %u. Available: %u\n",
- drm_intel_gem_estimate_batch_space(bufmgr_gem->exec_bos,
- bufmgr_gem->exec_count),
- drm_intel_gem_compute_batch_space(bufmgr_gem->exec_bos,
- bufmgr_gem->exec_count),
- (unsigned int) bufmgr_gem->gtt_size);
+ DBG("Execbuffer fails to pin. "
+ "Estimate: %u. Actual: %u. Available: %u\n",
+ drm_intel_gem_estimate_batch_space(bufmgr_gem->exec_bos,
+ bufmgr_gem->exec_count),
+ drm_intel_gem_compute_batch_space(bufmgr_gem->exec_bos,
+ bufmgr_gem->exec_count),
+ (unsigned int) bufmgr_gem->gtt_size);
}
}
drm_intel_update_buffer_offsets2(bufmgr_gem);
+skip_execution:
if (bufmgr_gem->bufmgr.debug)
drm_intel_gem_dump_validation_list(bufmgr_gem);
drm_clip_rect_t *cliprects, int num_cliprects,
int DR4)
{
- return drm_intel_gem_bo_mrb_exec2(bo, used,
- cliprects, num_cliprects, DR4,
- I915_EXEC_RENDER);
+ return do_exec2(bo, used, NULL, cliprects, num_cliprects, DR4,
+ I915_EXEC_RENDER);
+}
+
+static int
+drm_intel_gem_bo_mrb_exec2(drm_intel_bo *bo, int used,
+ drm_clip_rect_t *cliprects, int num_cliprects, int DR4,
+ unsigned int flags)
+{
+ return do_exec2(bo, used, NULL, cliprects, num_cliprects, DR4,
+ flags);
+}
+
+int
+drm_intel_gem_bo_context_exec(drm_intel_bo *bo, drm_intel_context *ctx,
+ int used, unsigned int flags)
+{
+ return do_exec2(bo, used, ctx, NULL, 0, 0, flags);
}
static int
struct drm_i915_gem_pin pin;
int ret;
- memset(&pin, 0, sizeof(pin));
+ VG_CLEAR(pin);
pin.handle = bo_gem->gem_handle;
pin.alignment = alignment;
- do {
- ret = ioctl(bufmgr_gem->fd,
- DRM_IOCTL_I915_GEM_PIN,
- &pin);
- } while (ret == -1 && errno == EINTR);
-
+ ret = drmIoctl(bufmgr_gem->fd,
+ DRM_IOCTL_I915_GEM_PIN,
+ &pin);
if (ret != 0)
return -errno;
struct drm_i915_gem_unpin unpin;
int ret;
- memset(&unpin, 0, sizeof(unpin));
+ VG_CLEAR(unpin);
unpin.handle = bo_gem->gem_handle;
- ret = ioctl(bufmgr_gem->fd, DRM_IOCTL_I915_GEM_UNPIN, &unpin);
+ ret = drmIoctl(bufmgr_gem->fd, DRM_IOCTL_I915_GEM_UNPIN, &unpin);
if (ret != 0)
return -errno;
struct drm_i915_gem_set_tiling set_tiling;
int ret;
- if (tiling_mode == bo_gem->tiling_mode &&
+ if (bo_gem->global_name == 0 &&
+ tiling_mode == bo_gem->tiling_mode &&
stride == bo_gem->stride)
return 0;
memset(&set_tiling, 0, sizeof(set_tiling));
do {
+ /* set_tiling is slightly broken and overwrites the
+ * input on the error path, so we have to open code
+ * rmIoctl.
+ */
set_tiling.handle = bo_gem->gem_handle;
set_tiling.tiling_mode = tiling_mode;
set_tiling.stride = stride;
ret = ioctl(bufmgr_gem->fd,
DRM_IOCTL_I915_GEM_SET_TILING,
&set_tiling);
- } while (ret == -1 && errno == EINTR);
+ } while (ret == -1 && (errno == EINTR || errno == EAGAIN));
if (ret == -1)
return -errno;
bo_gem->tiling_mode = set_tiling.tiling_mode;
bo_gem->swizzle_mode = set_tiling.swizzle_mode;
- bo_gem->stride = stride;
+ bo_gem->stride = set_tiling.stride;
return 0;
}
drm_intel_bo_gem *bo_gem = (drm_intel_bo_gem *) bo;
int ret;
- if (bo_gem->global_name == 0)
- return 0;
-
/* Linear buffers have no stride. By ensuring that we only ever use
* stride 0 with linear buffers, we simplify our code.
*/
{
drm_intel_bufmgr_gem *bufmgr_gem = (drm_intel_bufmgr_gem *) bo->bufmgr;
drm_intel_bo_gem *bo_gem = (drm_intel_bo_gem *) bo;
- struct drm_gem_flink flink;
int ret;
if (!bo_gem->global_name) {
- memset(&flink, 0, sizeof(flink));
+ struct drm_gem_flink flink;
+
+ VG_CLEAR(flink);
flink.handle = bo_gem->gem_handle;
- ret = ioctl(bufmgr_gem->fd, DRM_IOCTL_GEM_FLINK, &flink);
+ ret = drmIoctl(bufmgr_gem->fd, DRM_IOCTL_GEM_FLINK, &flink);
if (ret != 0)
return -errno;
+
bo_gem->global_name = flink.name;
- bo_gem->reusable = 0;
+ bo_gem->reusable = false;
+
+ DRMLISTADDTAIL(&bo_gem->name_list, &bufmgr_gem->named);
}
*name = bo_gem->global_name;
{
drm_intel_bufmgr_gem *bufmgr_gem = (drm_intel_bufmgr_gem *) bufmgr;
- bufmgr_gem->bo_reuse = 1;
+ bufmgr_gem->bo_reuse = true;
}
/**
drm_intel_bufmgr_gem *bufmgr_gem = (drm_intel_bufmgr_gem *)bufmgr;
if (bufmgr_gem->bufmgr.bo_exec == drm_intel_gem_bo_exec2)
- bufmgr_gem->fenced_relocs = 1;
+ bufmgr_gem->fenced_relocs = true;
}
/**
return 0;
total += bo->size;
- bo_gem->included_in_check_aperture = 1;
+ bo_gem->included_in_check_aperture = true;
for (i = 0; i < bo_gem->reloc_count; i++)
total +=
if (bo == NULL || !bo_gem->included_in_check_aperture)
return;
- bo_gem->included_in_check_aperture = 0;
+ bo_gem->included_in_check_aperture = false;
for (i = 0; i < bo_gem->reloc_count; i++)
drm_intel_gem_bo_clear_aperture_space_flag(bo_gem->
{
drm_intel_bo_gem *bo_gem = (drm_intel_bo_gem *) bo;
- bo_gem->reusable = 0;
+ bo_gem->reusable = false;
return 0;
}
}
}
+void
+drm_intel_bufmgr_gem_set_vma_cache_size(drm_intel_bufmgr *bufmgr, int limit)
+{
+ drm_intel_bufmgr_gem *bufmgr_gem = (drm_intel_bufmgr_gem *)bufmgr;
+
+ bufmgr_gem->vma_max = limit;
+
+ drm_intel_gem_bo_purge_vma_cache(bufmgr_gem);
+}
+
+/**
+ * Get the PCI ID for the device. This can be overridden by setting the
+ * INTEL_DEVID_OVERRIDE environment variable to the desired ID.
+ */
+static int
+get_pci_device_id(drm_intel_bufmgr_gem *bufmgr_gem)
+{
+ char *devid_override;
+ int devid;
+ int ret;
+ drm_i915_getparam_t gp;
+
+ if (geteuid() == getuid()) {
+ devid_override = getenv("INTEL_DEVID_OVERRIDE");
+ if (devid_override) {
+ bufmgr_gem->no_exec = true;
+ return strtod(devid_override, NULL);
+ }
+ }
+
+ VG_CLEAR(devid);
+ VG_CLEAR(gp);
+ gp.param = I915_PARAM_CHIPSET_ID;
+ gp.value = &devid;
+ ret = drmIoctl(bufmgr_gem->fd, DRM_IOCTL_I915_GETPARAM, &gp);
+ if (ret) {
+ fprintf(stderr, "get chip id failed: %d [%d]\n", ret, errno);
+ fprintf(stderr, "param: %d, val: %d\n", gp.param, *gp.value);
+ }
+ return devid;
+}
+
+int
+drm_intel_bufmgr_gem_get_devid(drm_intel_bufmgr *bufmgr)
+{
+ drm_intel_bufmgr_gem *bufmgr_gem = (drm_intel_bufmgr_gem *)bufmgr;
+
+ return bufmgr_gem->pci_device;
+}
+
+/**
+ * Sets up AUB dumping.
+ *
+ * This is a trace file format that can be used with the simulator.
+ * Packets are emitted in a format somewhat like GPU command packets.
+ * You can set up a GTT and upload your objects into the referenced
+ * space, then send off batchbuffers and get BMPs out the other end.
+ */
+void
+drm_intel_bufmgr_gem_set_aub_dump(drm_intel_bufmgr *bufmgr, int enable)
+{
+ drm_intel_bufmgr_gem *bufmgr_gem = (drm_intel_bufmgr_gem *)bufmgr;
+ int entry = 0x200003;
+ int i;
+ int gtt_size = 0x10000;
+
+ if (!enable) {
+ if (bufmgr_gem->aub_file) {
+ fclose(bufmgr_gem->aub_file);
+ bufmgr_gem->aub_file = NULL;
+ }
+ }
+
+ if (geteuid() != getuid())
+ return;
+
+ bufmgr_gem->aub_file = fopen("intel.aub", "w+");
+ if (!bufmgr_gem->aub_file)
+ return;
+
+ /* Start allocating objects from just after the GTT. */
+ bufmgr_gem->aub_offset = gtt_size;
+
+ /* Start with a (required) version packet. */
+ aub_out(bufmgr_gem, CMD_AUB_HEADER | (13 - 2));
+ aub_out(bufmgr_gem,
+ (4 << AUB_HEADER_MAJOR_SHIFT) |
+ (0 << AUB_HEADER_MINOR_SHIFT));
+ for (i = 0; i < 8; i++) {
+ aub_out(bufmgr_gem, 0); /* app name */
+ }
+ aub_out(bufmgr_gem, 0); /* timestamp */
+ aub_out(bufmgr_gem, 0); /* timestamp */
+ aub_out(bufmgr_gem, 0); /* comment len */
+
+ /* Set up the GTT. The max we can handle is 256M */
+ aub_out(bufmgr_gem, CMD_AUB_TRACE_HEADER_BLOCK | (5 - 2));
+ aub_out(bufmgr_gem, AUB_TRACE_MEMTYPE_NONLOCAL | 0 | AUB_TRACE_OP_DATA_WRITE);
+ aub_out(bufmgr_gem, 0); /* subtype */
+ aub_out(bufmgr_gem, 0); /* offset */
+ aub_out(bufmgr_gem, gtt_size); /* size */
+ for (i = 0x000; i < gtt_size; i += 4, entry += 0x1000) {
+ aub_out(bufmgr_gem, entry);
+ }
+}
+
+drm_intel_context *
+drm_intel_gem_context_create(drm_intel_bufmgr *bufmgr)
+{
+ drm_intel_bufmgr_gem *bufmgr_gem = (drm_intel_bufmgr_gem *)bufmgr;
+ struct drm_i915_gem_context_create create;
+ drm_i915_getparam_t gp;
+ drm_intel_context *context = NULL;
+ int tmp = 0, ret;
+
+ ret = drmIoctl(bufmgr_gem->fd, DRM_IOCTL_I915_GEM_CONTEXT_CREATE, &create);
+ if (ret != 0) {
+ fprintf(stderr, "DRM_IOCTL_I915_GEM_CONTEXT_CREATE failed: %s\n",
+ strerror(errno));
+ return NULL;
+ }
+
+ context = calloc(1, sizeof(*context));
+ context->ctx_id = create.ctx_id;
+ context->bufmgr = bufmgr;
+
+ return context;
+}
+
+void
+drm_intel_gem_context_destroy(drm_intel_context *ctx)
+{
+ drm_intel_bufmgr_gem *bufmgr_gem;
+ struct drm_i915_gem_context_destroy destroy;
+ int ret;
+
+ if (ctx == NULL)
+ return;
+
+ bufmgr_gem = (drm_intel_bufmgr_gem *)ctx->bufmgr;
+ destroy.ctx_id = ctx->ctx_id;
+ ret = drmIoctl(bufmgr_gem->fd, DRM_IOCTL_I915_GEM_CONTEXT_DESTROY,
+ &destroy);
+ if (ret != 0)
+ fprintf(stderr, "DRM_IOCTL_I915_GEM_CONTEXT_DESTROY failed: %s\n",
+ strerror(errno));
+
+ free(ctx);
+}
+
+
+/**
+ * Annotate the given bo for use in aub dumping.
+ *
+ * \param annotations is an array of drm_intel_aub_annotation objects
+ * describing the type of data in various sections of the bo. Each
+ * element of the array specifies the type and subtype of a section of
+ * the bo, and the past-the-end offset of that section. The elements
+ * of \c annotations must be sorted so that ending_offset is
+ * increasing.
+ *
+ * \param count is the number of elements in the \c annotations array.
+ * If \c count is zero, then \c annotations will not be dereferenced.
+ *
+ * Annotations are copied into a private data structure, so caller may
+ * re-use the memory pointed to by \c annotations after the call
+ * returns.
+ *
+ * Annotations are stored for the lifetime of the bo; to reset to the
+ * default state (no annotations), call this function with a \c count
+ * of zero.
+ */
+void
+drm_intel_bufmgr_gem_set_aub_annotations(drm_intel_bo *bo,
+ drm_intel_aub_annotation *annotations,
+ unsigned count)
+{
+ drm_intel_bo_gem *bo_gem = (drm_intel_bo_gem *) bo;
+ unsigned size = sizeof(*annotations) * count;
+ drm_intel_aub_annotation *new_annotations =
+ count > 0 ? realloc(bo_gem->aub_annotations, size) : NULL;
+ if (new_annotations == NULL) {
+ free(bo_gem->aub_annotations);
+ bo_gem->aub_annotations = NULL;
+ bo_gem->aub_annotation_count = 0;
+ return;
+ }
+ memcpy(new_annotations, annotations, size);
+ bo_gem->aub_annotations = new_annotations;
+ bo_gem->aub_annotation_count = count;
+}
+
/**
* Initializes the GEM buffer manager, which uses the kernel to allocate, map,
* and manage map buffer objections.
drm_intel_bufmgr_gem *bufmgr_gem;
struct drm_i915_gem_get_aperture aperture;
drm_i915_getparam_t gp;
- int ret;
- int exec2 = 0, has_bsd = 0;
+ int ret, tmp;
+ bool exec2 = false;
bufmgr_gem = calloc(1, sizeof(*bufmgr_gem));
if (bufmgr_gem == NULL)
return NULL;
}
- ret = ioctl(bufmgr_gem->fd, DRM_IOCTL_I915_GEM_GET_APERTURE, &aperture);
+ ret = drmIoctl(bufmgr_gem->fd,
+ DRM_IOCTL_I915_GEM_GET_APERTURE,
+ &aperture);
if (ret == 0)
bufmgr_gem->gtt_size = aperture.aper_available_size;
(int)bufmgr_gem->gtt_size / 1024);
}
- gp.param = I915_PARAM_CHIPSET_ID;
- gp.value = &bufmgr_gem->pci_device;
- ret = ioctl(bufmgr_gem->fd, DRM_IOCTL_I915_GETPARAM, &gp);
- if (ret) {
- fprintf(stderr, "get chip id failed: %d [%d]\n", ret, errno);
- fprintf(stderr, "param: %d, val: %d\n", gp.param, *gp.value);
- }
+ bufmgr_gem->pci_device = get_pci_device_id(bufmgr_gem);
- if (IS_GEN2(bufmgr_gem))
+ if (IS_GEN2(bufmgr_gem->pci_device))
bufmgr_gem->gen = 2;
- else if (IS_GEN3(bufmgr_gem))
+ else if (IS_GEN3(bufmgr_gem->pci_device))
bufmgr_gem->gen = 3;
- else if (IS_GEN4(bufmgr_gem))
+ else if (IS_GEN4(bufmgr_gem->pci_device))
bufmgr_gem->gen = 4;
- else
+ else if (IS_GEN5(bufmgr_gem->pci_device))
+ bufmgr_gem->gen = 5;
+ else if (IS_GEN6(bufmgr_gem->pci_device))
bufmgr_gem->gen = 6;
+ else if (IS_GEN7(bufmgr_gem->pci_device))
+ bufmgr_gem->gen = 7;
+ else
+ assert(0);
+
+ if (IS_GEN3(bufmgr_gem->pci_device) &&
+ bufmgr_gem->gtt_size > 256*1024*1024) {
+ /* The unmappable part of gtt on gen 3 (i.e. above 256MB) can't
+ * be used for tiled blits. To simplify the accounting, just
+ * substract the unmappable part (fixed to 256MB on all known
+ * gen3 devices) if the kernel advertises it. */
+ bufmgr_gem->gtt_size -= 256*1024*1024;
+ }
+
+ VG_CLEAR(gp);
+ gp.value = &tmp;
gp.param = I915_PARAM_HAS_EXECBUF2;
- ret = ioctl(bufmgr_gem->fd, DRM_IOCTL_I915_GETPARAM, &gp);
+ ret = drmIoctl(bufmgr_gem->fd, DRM_IOCTL_I915_GETPARAM, &gp);
if (!ret)
- exec2 = 1;
+ exec2 = true;
gp.param = I915_PARAM_HAS_BSD;
- ret = ioctl(bufmgr_gem->fd, DRM_IOCTL_I915_GETPARAM, &gp);
- if (!ret)
- has_bsd = 1;
+ ret = drmIoctl(bufmgr_gem->fd, DRM_IOCTL_I915_GETPARAM, &gp);
+ bufmgr_gem->has_bsd = ret == 0;
+
+ gp.param = I915_PARAM_HAS_BLT;
+ ret = drmIoctl(bufmgr_gem->fd, DRM_IOCTL_I915_GETPARAM, &gp);
+ bufmgr_gem->has_blt = ret == 0;
+
+ gp.param = I915_PARAM_HAS_RELAXED_FENCING;
+ ret = drmIoctl(bufmgr_gem->fd, DRM_IOCTL_I915_GETPARAM, &gp);
+ bufmgr_gem->has_relaxed_fencing = ret == 0;
+
+ gp.param = I915_PARAM_HAS_WAIT_TIMEOUT;
+ ret = drmIoctl(bufmgr_gem->fd, DRM_IOCTL_I915_GETPARAM, &gp);
+ bufmgr_gem->has_wait_timeout = ret == 0;
+
+ gp.param = I915_PARAM_HAS_LLC;
+ ret = drmIoctl(bufmgr_gem->fd, DRM_IOCTL_I915_GETPARAM, &gp);
+ if (ret != 0) {
+ /* Kernel does not supports HAS_LLC query, fallback to GPU
+ * generation detection and assume that we have LLC on GEN6/7
+ */
+ bufmgr_gem->has_llc = (IS_GEN6(bufmgr_gem->pci_device) |
+ IS_GEN7(bufmgr_gem->pci_device));
+ } else
+ bufmgr_gem->has_llc = ret == 0;
if (bufmgr_gem->gen < 4) {
gp.param = I915_PARAM_NUM_FENCES_AVAIL;
gp.value = &bufmgr_gem->available_fences;
- ret = ioctl(bufmgr_gem->fd, DRM_IOCTL_I915_GETPARAM, &gp);
+ ret = drmIoctl(bufmgr_gem->fd, DRM_IOCTL_I915_GETPARAM, &gp);
if (ret) {
fprintf(stderr, "get fences failed: %d [%d]\n", ret,
errno);
/* Use the new one if available */
if (exec2) {
bufmgr_gem->bufmgr.bo_exec = drm_intel_gem_bo_exec2;
- if (has_bsd)
- bufmgr_gem->bufmgr.bo_mrb_exec = drm_intel_gem_bo_mrb_exec2;
+ bufmgr_gem->bufmgr.bo_mrb_exec = drm_intel_gem_bo_mrb_exec2;
} else
bufmgr_gem->bufmgr.bo_exec = drm_intel_gem_bo_exec;
bufmgr_gem->bufmgr.bo_busy = drm_intel_gem_bo_busy;
drm_intel_gem_get_pipe_from_crtc_id;
bufmgr_gem->bufmgr.bo_references = drm_intel_gem_bo_references;
+ DRMINITLISTHEAD(&bufmgr_gem->named);
init_cache_buckets(bufmgr_gem);
+ DRMINITLISTHEAD(&bufmgr_gem->vma_cache);
+ bufmgr_gem->vma_max = -1; /* unlimited by default */
+
return &bufmgr_gem->bufmgr;
}