diff --git a/xf86drmMode.h b/xf86drmMode.h
index 705369fe326d46ecad4eecf08178af2b53805f87..8e40034052792c2b7e8a5cce815214d7205b2a03 100644 (file)
--- a/xf86drmMode.h
+++ b/xf86drmMode.h
*
*/
+#ifndef _XF86DRMMODE_H_
+#define _XF86DRMMODE_H_
+
+#if defined(__cplusplus) || defined(c_plusplus)
+extern "C" {
+#endif
+
#include <drm.h>
/*
#define DRM_MODE_CONNECTOR_DisplayPort 10
#define DRM_MODE_CONNECTOR_HDMIA 11
#define DRM_MODE_CONNECTOR_HDMIB 12
+#define DRM_MODE_CONNECTOR_TV 13
+#define DRM_MODE_CONNECTOR_eDP 14
#define DRM_MODE_PROP_PENDING (1<<0)
#define DRM_MODE_PROP_RANGE (1<<1)
#endif /* _DRM_MODE_H */
+
+/*
+ * Feature defines
+ *
+ * Just because these are defined doesn't mean that the kernel
+ * can do that feature, its just for new code vs old libdrm.
+ */
+#define DRM_MODE_FEATURE_KMS 1
+#define DRM_MODE_FEATURE_DIRTYFB 1
+
+
typedef struct _drmModeRes {
int count_fbs;
uint16_t hdisplay, hsync_start, hsync_end, htotal, hskew;
uint16_t vdisplay, vsync_start, vsync_end, vtotal, vscan;
- uint32_t vrefresh; /* vertical refresh * 1000 */
+ uint32_t vrefresh;
uint32_t flags;
uint32_t type;
uint32_t handle;
} drmModeFB, *drmModeFBPtr;
+typedef struct drm_clip_rect drmModeClip, *drmModeClipPtr;
+
typedef struct _drmModePropertyBlob {
uint32_t id;
uint32_t length;
uint32_t *encoders; /**< List of encoder ids */
} drmModeConnector, *drmModeConnectorPtr;
+typedef struct _drmModeObjectProperties {
+ uint32_t count_props;
+ uint32_t *props;
+ uint64_t *prop_values;
+} drmModeObjectProperties, *drmModeObjectPropertiesPtr;
+
+typedef struct _drmModePlane {
+ uint32_t count_formats;
+ uint32_t *formats;
+ uint32_t plane_id;
+
+ uint32_t crtc_id;
+ uint32_t fb_id;
+
+ uint32_t crtc_x, crtc_y;
+ uint32_t x, y;
+
+ uint32_t possible_crtcs;
+ uint32_t gamma_size;
+} drmModePlane, *drmModePlanePtr;
+typedef struct _drmModePlaneRes {
+ uint32_t count_planes;
+ uint32_t *planes;
+} drmModePlaneRes, *drmModePlaneResPtr;
extern void drmModeFreeModeInfo( drmModeModeInfoPtr ptr );
extern void drmModeFreeResources( drmModeResPtr ptr );
extern void drmModeFreeCrtc( drmModeCrtcPtr ptr );
extern void drmModeFreeConnector( drmModeConnectorPtr ptr );
extern void drmModeFreeEncoder( drmModeEncoderPtr ptr );
+extern void drmModeFreePlane( drmModePlanePtr ptr );
+extern void drmModeFreePlaneResources(drmModePlaneResPtr ptr);
/**
* Retrives all of the resources associated with a card.
extern int drmModeAddFB(int fd, uint32_t width, uint32_t height, uint8_t depth,
uint8_t bpp, uint32_t pitch, uint32_t bo_handle,
uint32_t *buf_id);
+/* ...with a specific pixel format */
+extern int drmModeAddFB2(int fd, uint32_t width, uint32_t height,
+ uint32_t pixel_format, uint32_t bo_handles[4],
+ uint32_t pitches[4], uint32_t offsets[4],
+ uint32_t *buf_id, uint32_t flags);
/**
* Destroies the given framebuffer.
*/
extern int drmModeRmFB(int fd, uint32_t bufferId);
+/**
+ * Mark a region of a framebuffer as dirty.
+ */
+extern int drmModeDirtyFB(int fd, uint32_t bufferId,
+ drmModeClipPtr clips, uint32_t num_clips);
+
+
/*
* Crtc functions
*/
uint16_t *red, uint16_t *green, uint16_t *blue);
extern int drmModePageFlip(int fd, uint32_t crtc_id, uint32_t fb_id,
uint32_t flags, void *user_data);
+
+extern drmModePlaneResPtr drmModeGetPlaneResources(int fd);
+extern drmModePlanePtr drmModeGetPlane(int fd, uint32_t plane_id);
+extern int drmModeSetPlane(int fd, uint32_t plane_id, uint32_t crtc_id,
+ uint32_t fb_id, uint32_t flags,
+ uint32_t crtc_x, uint32_t crtc_y,
+ uint32_t crtc_w, uint32_t crtc_h,
+ uint32_t src_x, uint32_t src_y,
+ uint32_t src_w, uint32_t src_h);
+
+extern drmModeObjectPropertiesPtr drmModeObjectGetProperties(int fd,
+ uint32_t object_id,
+ uint32_t object_type);
+extern void drmModeFreeObjectProperties(drmModeObjectPropertiesPtr ptr);
+extern int drmModeObjectSetProperty(int fd, uint32_t object_id,
+ uint32_t object_type, uint32_t property_id,
+ uint64_t value);
+
+#if defined(__cplusplus) || defined(c_plusplus)
+}
+#endif
+
+#endif